BSEC internal peripheral
Stable: 12.06.2023 - 07:49 / Revision: 08.06.2023 - 14:29
Template:ArticleMainWriter
Template:ArticleApprovedVersion
Contents
1 Article purpose
The purpose of this article is to
- briefly introduce the BSEC peripheral and its main features
- indicate the level of security supported by this hardware block
- explain how each instance can be allocated to the three runtime contexts and linked to the corresponding software components
- explain, when necessary, how to configure the BSEC peripheral.
2 Peripheral overview
The BSEC peripheral is used to control an OTP (one time programmable) fuse box, used for on-chip non-volatile storage for device configuration and security parameters.
2.1 Features
Refer to STM32MP15 reference manuals for the complete list of features, and to the software components, introduced below, to see which features are implemented.
2.2 Security support
The BSEC is a secure peripheral.
3 Peripheral usage and associated software
3.1 Boot time
The BSEC is configured at boot time to set up platform security.
3.2 Runtime
3.2.1 Overview
The BSEC instance is a system peripheral and is controlled by the Arm®Cortex®-A7 secure.
3.2.2 Software frameworks
Domain | Peripheral | Software frameworks | Comment | ||
Cortex-A7 S (OP-TEE) |
Cortex-A7 NS (Linux) |
Cortex-M4 (STM32Cube) |
|||
Security | BSEC | OP-TEE BSEC driver | Linux NVMEM framework |
3.2.3 Peripheral configuration
The configuration is applied by the firmware running in a secure context.
This configuration is done in TF-A or in OP-TEE.
3.2.4 Peripheral assignment
Check boxes illustrate the possible peripheral allocations supported by STM32 MPU Embedded Software:
- ☐ means that the peripheral can be assigned (☑) to the given runtime context.
- ✓ is used for system peripherals that cannot be unchecked because they are statically connected in the device.
Refer to How to assign an internal peripheral to a runtime context for more information on how to assign peripherals manually or via STM32CubeMX.
The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possiblities might be described in STM32MP15 reference manuals.
Domain | Peripheral | Runtime allocation | Comment | |||
Instance |
Cortex-A7 S (OP-TEE) |
Cortex-A7 NS (Linux) |
Cortex-M4 (STM32Cube) |
|||
Security | BSEC | BSEC | ✓ | ✓ |