Difference between revisions of "Signing tool release note"

[quality revision] [quality revision]
m
m
 

The STM32MPU Signing tool generates signed binary files from:

  • a binary image file,
  • a public Key file,
  • a private Key file,

More information can be found in the detailed release note referenced later in this article.


Signing tool - Version 1.0.0[edit]

Signing tool for Linux® and Windows® host PC
Download

Version 1.0.0

Installing the Signing tool
  • To use STM32MP Signing Tool, the installation of STM32CubeProgrammer is needed.
  • The installation is then complete. To use this tool, follow the instruction given in Signing tool.
Detailed release note
  • Full details about the content of this tool release are available here.


The STM32MPU Signing tool generates signed binary files from:
*a binary image file,
*a public Key file,
*a private Key file,
More information can be found in the detailed release note referenced later in this article.

{{ReviewsComments|NSA W816 : in the release note it is not explained how to use it, may be it could be useful to create and article explaining the usage of keyGen and signing tools}}

==Signing tool - Version 1.0.0 ==
{| class="st-tablewikitable"
|-
!colspan="3" | Signing tool for Linux<sup>&reg;</sup> and Windows<sup>&reg;</sup> host PC
|-
| '''Download''' 
|colspan="2" |
'''Version 1.0.0'''
* Signing tool is integrated in [[STM32CubeProgrammer]] package available [https://www.st.com/en/development-tools/stm32cubeprog.html here]
|-
| '''Installing the Signing tool''' 
|colspan="2" |
* To use STM32MP Signing Tool, the installation of [[STM32CubeProgrammer]] is needed.
* '''The installation is then complete'''. To use this tool, follow the instruction given in [[Signing tool]].
|-
| '''Detailed release note''' 
| colspan="2" | 
* Full details about the content of this tool release are available [https://www.st.com/en/development-tools/stm32cubeprog.html here].
{{ReviewsComments | DHU W906.4: I can't see this file in the Windows installation of the STM32Cubeprogrammer, which is supposed to host the complete Signing tool resources}}
|}
<noinclude>

[[Category:Release notes]]
[[Category:Signing tool]]
{{PublicationRequestId | 7991 | 2018-06-28 | AnneJ}}
{{UpdateNeededForNewRelease|
* Copy the current release (first chapter) in the "Archives" chapter
* Change the version of the tool
* Change the name of the archive file
* Change the download URLs
}}</noinclude>
Line 8: Line 8:
   
 
==Signing tool - Version 1.0.0 ==
 
==Signing tool - Version 1.0.0 ==
 
+
{| class="st-table"
{| class="wikitable"
 
 
|-
 
|-
 
!colspan="3" | Signing tool for Linux<sup>&reg;</sup> and Windows<sup>&reg;</sup> host PC
 
!colspan="3" | Signing tool for Linux<sup>&reg;</sup> and Windows<sup>&reg;</sup> host PC