Difference between revisions of "SYSRAM internal memory"

[quality revision] [quality revision]
m
 

1 Article purpose[edit]

The purpose of this article is to briefly introduce the SYSRAM internal memory and indicate the level of security supported by this memory.

2 Peripheral overview[edit]

The STM32MP15 SYSRAM is a 256-Kbyte internal memory peripheral. It is physically located near the Arm® Cortex-A to optimize the core performance.

2.1 Features[edit]

Refer to the STM32MP15 reference manuals for the complete list of features, and to the software components, introduced below, to see which features are really implemented.

2.2 Security support[edit]

The SYSRAM is a secure peripheral (under ETZPC TrustZone memory adapter (TZMA)): it can be split into a secure and a non-secure regions with a 4-Kbyte granularity.

3 Peripheral usage and associated software[edit]

3.1 Boot time[edit]

The STM32MP15 ROM code mainly configures the SYSRAM as a secure peripheral during its execution. The ROM code uses 9 Kbytes located at the beginning of the SYSRAM to store its read and write data. The ROM code stores the boot context in the first 512 bytes of SYSRAM: this boot context contains several information (such as the selected boot device) and pointers to the ROM code services (used for secure boot authentication). The ROM code loads the FSBL just after the boot context, into the remaining 247 Kbytes of SYSRAM, and eventually branches the Cortex®-A7 core 0 execution to this FSBL.


The FSBL code can use the whole SYSRAM, but it must take care not to overwrite the boot context before taking it into account.

3.2 Runtime[edit]

3.2.1 Overview[edit]

In STMicroelectronics distribution, the SYSRAM runtime mapping is the one reached at the end of the boot. It is consequently fully secure and contains a minimal secure monitor (from TF-A or U-Boot) or a secure OS (like OP-TEE).


You may decide to split the SYSRAM at runtime. In this case:

  • set the SYSRAM bottom secure, for a Cortex®-A7 secure monitor (from TF-A or U-Boot) or a secure OS (such as OP-TEE)

and

  • set the SYSRAM top non-secure, for instance for using in Linux® as reserved memory

3.2.2 Software frameworks[edit]

Domain Peripheral Software frameworks Comment
Cortex-A7
secure
(OP-TEE)
Cortex-A7
non-secure
(Linux)
Cortex-M4

(STM32Cube)
Core/RAM SYSRAM TF-A overview Linux reserved memory

3.2.3 Peripheral configuration[edit]

The configuration is applied by the firmware running in the context to which the peripheral is assigned. The configuration can be done alone via the STM32CubeMX tool for all internal peripherals, and then manually completed (particularly for external peripherals), according to the information given in the corresponding software framework article.

3.2.4 Peripheral assignment[edit]

Internal peripherals

Check boxes illustrate the possible peripheral allocations supported by STM32 MPU Embedded Software:

  • means that the peripheral can be assigned () to the given runtime context.
  • is used for system peripherals that cannot be unchecked because they are statically connected in the device.

Refer to How to assign an internal peripheral to a runtime context for more information on how to assign peripherals manually or via STM32CubeMX.
The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possiblities might be described in STM32MP15 reference manuals.

Domain Peripheral Runtime allocation Comment
Instance Cortex-A7
secure
(OP-TEE)
Cortex-A7
non-secure
(Linux)
Cortex-M4

(STM32Cube)
Core/RAM SYSRAM SYSRAM Shareable (multiple choices supported)

4 References[edit]



==Article purpose==
The purpose of this article is to briefly introduce the SYSRAM internal memory and indicate the level of security supported by this memory.

==Peripheral overview==
The STM32MP15 '''SYSRAM''' is a 256-Kbyte internal memory peripheral. It is physically located near the Arm<sup>&reg;</sup> Cortex-A to optimize the core performance.

===Features===
Refer to the [[STM32MP15 resources#Reference manuals|STM32MP15 reference manuals]] for the complete list of features, and to the software components, introduced below, to see which features are really implemented.

===Security support===
The SYSRAM is a '''secure''' peripheral (under [[ETZPC_internal_peripheral|ETZPC TrustZone memory adapter (TZMA)]]): it can be split into a secure and a non-secure regions with a 4-Kbyte granularity.

==Peripheral usage and associated software==
===Boot time===
The [[STM32MP15 ROM code overview|STM32MP15 ROM code]] mainly configures the SYSRAM as a secure peripheral during its execution. The [[STM32MP15 ROM code overview|ROM code]] uses 9 Kbytes located at the beginning of the SYSRAM to store its read and write data. The [[STM32MP15 ROM code overview|ROM code]] stores the boot context in the first 512 bytes of SYSRAM: this boot context contains several information (such as the selected boot device) and pointers to the [[STM32MP15 ROM code overview|ROM code]] services (used for secure boot authentication). The [[STM32MP15 ROM code overview|ROM code]] loads the [[Boot chainschain overview|FSBL]] just after the boot context, into the remaining 247 Kbytes of SYSRAM, and eventually branches the Cortex<sup>&reg;</sup>-A7 core 0 execution to this [[Boot chainschain overview|FSBL]].

The [[Boot chainschain overview|FSBL]] code can use the whole SYSRAM, but it must take care not to overwrite the boot context before taking it into account.

===Runtime===
====Overview====
In STMicroelectronics distribution, the SYSRAM runtime mapping is the one reached at the end of the boot. It is consequently fully secure and contains a minimal secure monitor (from [[TF-A overview|TF-A]] or [[U-Boot overview|U-Boot]]) or a secure OS (like [[OP-TEE overview|OP-TEE]]).

You may decide to split the SYSRAM at runtime. In this case:
* set the SYSRAM bottom secure, for a Cortex<sup>&reg;</sup>-A7 secure monitor (from [[TF-A overview|TF-A]] or [[U-Boot overview|U-Boot]]) or a secure OS (such as [[OP-TEE overview|OP-TEE]])
and
* set the SYSRAM top non-secure, for instance for using in Linux<sup>&reg;</sup> as [[Reserved memory|reserved memory]]

====Software frameworks====
{{:Internal_peripherals_software_table_template}}
 | Core/RAM
 | [[SYSRAM internal memory|SYSRAM]]
 | [[TF-A overview#BL32|TF-A overview]]
 | [[Reserved memory|Linux reserved memory]]
 | 
 |
 |-
 |}

====Peripheral configuration====
The configuration is applied by the firmware running in the context to which the peripheral is assigned. The configuration can be done alone via the [[STM32CubeMX]] tool for all internal peripherals, and then manually completed (particularly for external peripherals), according to the information given in the corresponding software framework article.

====Peripheral assignment====
{{:Internal_peripherals_assignment_table_template}}<onlyinclude>

 | rowspan="1" | Core/RAM
 | rowspan="1" | [[SYSRAM internal memory|SYSRAM]]
 | SYSRAM
 | <span title="assignable peripheral" style="font-size:21px"></span>

 | <span title="assignable peripheral" style="font-size:21px"></span>

 |
 | Shareable (multiple choices supported)
 |-</onlyinclude>

 |}

==References==<references/>

<noinclude>

[[Category:RAM interfaces]]
{{PublicationRequestId | 9290 | 2018-10-22 | AnneJ}}
{{ArticleBasedOnModel | Internal peripheral article model}}</noinclude>
Line 13: Line 13:
 
==Peripheral usage and associated software==
 
==Peripheral usage and associated software==
 
===Boot time===
 
===Boot time===
The [[STM32MP15 ROM code overview|STM32MP15 ROM code]] mainly configures the SYSRAM as a secure peripheral during its execution. The [[STM32MP15 ROM code overview|ROM code]] uses 9 Kbytes located at the beginning of the SYSRAM to store its read and write data. The [[STM32MP15 ROM code overview|ROM code]] stores the boot context in the first 512 bytes of SYSRAM: this boot context contains several information (such as the selected boot device) and pointers to the [[STM32MP15 ROM code overview|ROM code]] services (used for secure boot authentication). The [[STM32MP15 ROM code overview|ROM code]] loads the [[Boot chains overview|FSBL]] just after the boot context, into the remaining 247 Kbytes of SYSRAM, and eventually branches the Cortex<sup>&reg;</sup>-A7 core 0 execution to this [[Boot chains overview|FSBL]].
+
The [[STM32MP15 ROM code overview|STM32MP15 ROM code]] mainly configures the SYSRAM as a secure peripheral during its execution. The [[STM32MP15 ROM code overview|ROM code]] uses 9 Kbytes located at the beginning of the SYSRAM to store its read and write data. The [[STM32MP15 ROM code overview|ROM code]] stores the boot context in the first 512 bytes of SYSRAM: this boot context contains several information (such as the selected boot device) and pointers to the [[STM32MP15 ROM code overview|ROM code]] services (used for secure boot authentication). The [[STM32MP15 ROM code overview|ROM code]] loads the [[Boot chain overview|FSBL]] just after the boot context, into the remaining 247 Kbytes of SYSRAM, and eventually branches the Cortex<sup>&reg;</sup>-A7 core 0 execution to this [[Boot chain overview|FSBL]].
   
   
The [[Boot chains overview|FSBL]] code can use the whole SYSRAM, but it must take care not to overwrite the boot context before taking it into account.
+
The [[Boot chain overview|FSBL]] code can use the whole SYSRAM, but it must take care not to overwrite the boot context before taking it into account.
   
 
===Runtime===
 
===Runtime===