1. Article purpose[edit source]
The article aims to help rebase an STM32 MPU project on a new ecosystem release by focusing on the impacts of the main changes.
2. Scope of this article[edit source]
This article provides some details for the main changes between STM32 MPU ecosystem release v4.1.0 and new STM32 MPU ecosystem release v5.0.0 . The aim is to help migrate your project.
All Information about the features delivered in the new release is also available in the OpenSTLinux release note.
3. Impacted domains[edit source]
3.1. Yocto build environment for Distribution Package[edit source]
- For the process to enable secure boot from Distribution package updated, refer to dedicated wiki page.
3.2. Hardware configuration[edit source]
Check the device tree files for the STMP32 MPU board for more details:
Linux® kernel: between Linux kernel v6.1-stm32mp-r1 (v6.1.28) and previous Linux kernel v5.15-stm32mp-r2 (v5.15.67)
- arm_wdt node enabled for watchdog
- New etzpc node section
U-Boot: between U-Boot v2022.10-stm32mp-r1 and previous U-Boot v2021.10-stm32mp-r2
- Alignment with Linux® kernel device tree
OP-TEE: between OP-TEE 3.19.0-stm32mp-r1 and previous OP-TEE 3.16.0-stm32mp-r2
- Alignment with Linux® kernel device tree
TF-A: between TF-A v2.8-stm32mp-r1 and previous TF-A v2.6-stm32mp-r2
- Alignment with Linux® kernel device tree
- BL2 always runs at 650MHz (PLL1 configuration removed from DT)
- Move compatible field to secure RCC from SoC DT to board DT
- Shared memory with OP-TEE removed
- For STM32MP15x lines
- RCC configuration updated to follow new bindings
Information |
This is possible with git diff command to get delta between two branches in the same repository. Example with STLINUX GitHub repository and for all STM32MP1 device tree files: git diff v5.15-stm32mp-r2 v6.1-stm32mp-r1 -- arch/arm/boot/dts/stm32mp1* |
3.3. System configuration[edit source]
- None
3.4. Boot stages[edit source]
- This ecosystem release v5.0.0 does not support anymore the TF-A SP-MIN as secure monitor.
OP-TEE is only the supported BL32 and you must migrate the STM32MP15x lines projects to be able to use it. - The MTD partitions are defined in U-Boot device tree and are no more defined in U-Boot defconfig.
3.5. Security[edit source]
- New implementation of a secure watchdog
- New device-tree RNG configuration
- Use of a watchdog framework
- IWDG early-interrupt fixing
3.6. User space and applications[edit source]
- None
4. References[edit source]