Approved version. Approved on: 11:08, 31 May 2022
You are viewing an old version of this page. Return to the latest version.
Difference between revisions of "STM32MP1 Platform trace and debug environment overview"
[unchecked revision] | [quality revision] |
m
|
m
|
Applicable for | STM32MP13x lines, STM32MP15x lines |
The block diagram below shows the STM32MP1 Platform trace and debug environment components and their possible interfaces:
- The STM32MPU Embedded Software package (see STM32MPU Embedded Software architecture overview) that includes:
- The STM32MPU peripherals shared between Cortex®-A (on STM32MP1 Series) and Cortex®-M (on STM32MP15x lines
only) cores (such as GPIO, I2C and SPI)
- The user interfaces or tools, which allow to interact with different trace and debug Tools, such as:
- The remote shell using terminal console
- The debugger tools (such as GDB)
- The graphical IDE (such as GDBGUI or SystemWorkbench)
- The trace and debug interfaces or hardware paths that provide access to trace and debug components through:
- The network interface (e.g. Ethernet)
- The communication port (e.g UART)
- The hardware connector interfaces:
- JTag port
- Trace port to access ETM, STM, ITM and SWD
- I/O probes to access HDP
- The hardware probes such as ST-Link.
This block diagram also illustrates the Arm® debugging modes:
- Invasive debug: debug process that allows the control and monitoring of the processor. Most debug features are considered invasive because they enable you to halt the processor and modify its state.
- Non-invasive debug: debug process that allows the monitoring of the processor but not the control. The embedded trace macrocell (ETM) interface and the performance monitor registers are non-invasive debug features.
Click the figure below to directly jump to the component you want to trace, monitor or debug:
- By selecting a hardware component, you will be redirected to the corresponding hardware board article in order to check if the hardware connector is supported on your board.
- By selecting a target software component, you will be be redirected to an article that explains in details how to trace, monitor or debug this component.
- By selecting a host software component, you will be redirected to an article that explains how to use this remote tool.
<noinclude>{{ApplicableFor |MPUs list=STM32MP13x, STM32MP15x |MPUs checklist=STM32MP13x, STM32MP15x }}</noinclude> The block diagram below shows the {{highlight|'''STM32MP1 Platform trace and debug environment'''}} components and their possible interfaces: * The '''STM32MPU Embedded Software''' package (see [[STM32MPU Embedded Software architecture overview]]) that includes: ** The '''OpenSTLinux BSP''' and '''application frameworks''' components, running on the Arm<sup>®</sup> Cortex<sup>®</sup>-A core ** The '''STM32Cube MPU Package''', on {{MicroprocessorDevice | device=15}} only, running on the Arm<sup>®</sup> Cortex<sup>®</sup>-M core * The '''STM32MPU peripherals''' shared between Cortex<sup>®</sup>-A (on {{MicroprocessorDevice | device=1}}) and Cortex<sup>®</sup>-M (on {{MicroprocessorDevice | device=15}} only) cores (such as GPIO, I2C and SPI) * The '''user interfaces or tools''', which allow to interact with different trace and debug Tools, such as: ** The '''remote shell''' using terminal console ** The '''debugger tools''' (such as GDB) ** The '''graphical IDE''' (such as GDBGUI or SystemWorkbench) * The '''trace and debug interfaces or hardware paths''' that provide access to trace and debug components through: ** The '''network''' interface (e.g. Ethernet) ** The '''communication port''' (e.g UART) ** The hardware connector interfaces: *** '''JTag''' port *** '''Trace''' port to access ETM, STM, ITM and SWD *** '''I/O probes''' to access HDP * The '''hardware probes''' such as ST-Link. This block diagram also illustrates the Arm<sup>®</sup> debugging modes: * '''Invasive debug''': debug process that allows the control and monitoring of the processor. Most debug features are considered invasive because they enable you to halt the processor and modify its state. * '''Non-invasive debug''': debug process that allows the monitoring of the processor but not the control. The embedded trace macrocell (ETM) interface and the performance monitor registers are non-invasive debug features. {{highlight|Click the figure below}} to directly jump to the component you want to trace, monitor or debug: * By selecting a '''hardware component''', you will be redirected to the corresponding hardware board article in order to check if the hardware connector is supported on your board. <br> * By selecting a '''target software component''', you will be be redirected to an article that explains in details how to trace, monitor or debug this component.<br> * By selecting a '''host software component''', you will be redirected to an article that explains how to use this remote tool. {{ImageMap|Image: STM32MP1 Platform trace and debug environment overview.png{{!}} thumb{{!}} 800px {{!}} center {{!}} STM32MP1 Platform trace and debug environment overview. rect 128 0 360 63 [[How to get Terminal | Remote shell]] rect 402 0 635 63 [[GDB]] rect 563 390 676 455 [[Linux tracing, monitoring and debugging | Linux kernel]] rect 563 263 676 330 [[Linux tracing, monitoring and debugging | Linux applications]] rect 217 389 330 454 [[How to debug OP-TEE | OP-TEE]] rect 341 390 439 454 [[How to debug TF-A BL2 | TF-A]] rect 458 390 555 454 [[U-Boot - How to debug | U-Boot]] rect 808 228 926 476 [[STM32CubeMP1 Package | STM32CubeMP1 Package]] rect 78 320 197 380 [[:Category:STM32 MPU boards | ComPort connector]] rect 504 152 625 212 [[:Category:STM32 MPU boards | Network link]] rect 936 328 1054 392 [[:Category:STM32 MPU boards | JTag connector]] rect 1005 411 1122 472 [[:Category:STM32 MPU boards | Trace connector]] rect 1071 497 1188 559 [[:Category:STM32 MPU boards | IOProbe connector]] rect 672 73 906 137 [[:Category:HW probes | HW probes]] rect 450 600 565 625 [[STM32MP13_microprocessor]] rect 515 640 625 665 [[STM32MP15_microprocessor]]<!-- rect 217 389 330 454 [[OpteeOS]] rect 217 264 330 329 [[OpteeApp]] rect 671 0 909 61 [[DedicatedTools]] rect 946 1 1183 65 [(Scope]] --> }} [[File:STM32MP1 Platform trace and debug environment overview legend.png|center|link=]] <noinclude> {{PublicationRequestId | 9565 | 2018-11-12 | AnneJ}} [[Category:Trace and debug tools|0]]</noinclude>
Line 52: | Line 52: | ||
rect 1005 411 1122 472 [[:Category:STM32 MPU boards | Trace connector]] |
rect 1005 411 1122 472 [[:Category:STM32 MPU boards | Trace connector]] |
||
rect 1071 497 1188 559 [[:Category:STM32 MPU boards | IOProbe connector]] |
rect 1071 497 1188 559 [[:Category:STM32 MPU boards | IOProbe connector]] |
||
− | rect 672 73 906 137 [[:Category:HW probes]] |
+ | rect 672 73 906 137 [[:Category:HW probes | HW probes]] |
rect 450 600 565 625 [[STM32MP13_microprocessor]] |
rect 450 600 565 625 [[STM32MP13_microprocessor]] |
||
rect 515 640 625 665 [[STM32MP15_microprocessor]] |
rect 515 640 625 665 [[STM32MP15_microprocessor]] |