Difference between revisions of "STM32MP15 peripherals overview"

[quality revision] [quality revision]
m (Internal peripherals overview)
m
 

This article lists all internal peripherals embedded in STM32MP15 device and shows the assignment possibilities to the runtime contexts for each one of them.
Via this article, you can also access to individual peripheral articles in which information related to the overview and configuration can be found.

1 Internal peripherals overview[edit]

The figure below shows all peripherals embedded in STM32MP15 device, grouped per functional domains that are reused in many places of this wiki to structure the articles.

Several runtime contexts exist on STM32MP15 device[1], corresponding to the different Arm cores and associated security modes:

  •  Arm dual core Cortex-A7 secure  (Trustzone), running a Secure Monitor or Secure OS like OP-TEE
  •  Arm dual core Cortex-A7 non secure , running Linux
  •  Arm Cortex-M4  (non-secure), running STM32Cube


Some peripherals can be strictly assigned to one runtime context: this is the case for most of the peripherals, like USART or I2C.
Other ones can be shared between several runtime contexts: this is the case for system peripherals, like PWR or RCC.
The legend below shows how assigned and shared peripherals are identified in the assignment diagram that follows:

STM32MP1IPsOverview legend.png

Both the diagram below and the following summary table (in Internal peripherals assignment chapter below) are clickable in order to jump to each peripheral overview articles and get more detailed information (like software frameworks used to control them). They list STMicroelectronics recommendations. The STM32MP15 reference manual [2] may expose more possibilities than what is shown here.


STGEN SYSCFG RTC EXTI GIC NVIC IWDG IWDG WWDG DMA DMA DMAMUX MDMA SYSRAM DDR via DDR CTRL BKPSRAM MCU SRAM MCU SRAM RETRAM TIM TIM LPTIM GPIO GPIO IPCC HSEM RCC PWR DTS DDRPERFM DBGMCU HDP STM BSEC QUADSPI FMC SDMMC FDCAN ETH SDMMC USBH OTG USBPHYC USART USART USART I2C I2C I2C SPI SPI RNG HASH ETZPC CRYP CRC TZC RNG HASH TAMP CRYP CRC GPU DSI LTDC DCMI CEC VREFBUF DAC DFSDM ADC SPI I2S SPDIFRX SAI
STM32MP1 internal peripherals overview

2 Internal peripherals assignment[edit]

Internal peripherals

Check boxes illustrate the possible peripheral allocations supported by STM32 MPU Embedded Software:

  • means that the peripheral can be assigned () to the given runtime context.
  • is used for system peripherals that cannot be unchecked because they are statically connected in the device.

Refer to How to assign an internal peripheral to a runtime context for more information on how to assign peripherals manually or via STM32CubeMX.
The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possiblities might be described in STM32MP15 reference manuals.

Domain Peripheral Runtime allocation Comment
Instance Cortex-A7
secure
(OP-TEE)
Cortex-A7
non-secure
(Linux)
Cortex-M4

(STM32Cube)
Analog ADC ADC Assignment (single choice)
Analog DAC DAC Assignment (single choice)
Analog DFSDM DFSDM Assignment (single choice)
Analog VREFBUF VREFBUF Assignment (single choice)
Audio SAI SAI1 Assignment (single choice)
SAI2 Assignment (single choice)
SAI3 Assignment (single choice)
SAI4 Assignment (single choice)
Audio SPDIFRX SPDIFRX Assignment (single choice)
Coprocessor IPCC IPCC Shared (none or both)
Coprocessor HSEM HSEM
Core RTC RTC RTC is mandatory to resynchronize STGEN after exiting low-power modes.
Core STGEN STGEN
Core SYSCFG SYSCFG
Core/DMA DMA DMA1 Assignment (single choice)
DMA2 Assignment (single choice)
Core/DMA DMAMUX DMAMUX Shareable (multiple choices supported)
Core/DMA MDMA MDMA Shareable (multiple choices supported)
Core/Interrupts EXTI EXTI Shareable (multiple choices supported)
Core/Interrupts GIC GIC
Core/Interrupts NVIC NVIC
Core/IOs GPIO GPIOA (16 pins) Shareable (with pin granularity)
GPIOB (16 pins) Shareable (with pin granularity)
GPIOC (16 pins) Shareable (with pin granularity)
GPIOD (16 pins) Shareable (with pin granularity)
GPIOE (16 pins) Shareable (with pin granularity)
GPIOF (16 pins) Shareable (with pin granularity)
GPIOG (16 pins) Shareable (with pin granularity)
GPIOH (16 pins) Shareable (with pin granularity)
GPIOI (16 pins) Shareable (with pin granularity)
GPIOJ (16 pins) Shareable (with pin granularity)
GPIOK (8 pins) Shareable (with pin granularity)
GPIOZ (8 pins) Shareable (with pin granularity)
Core/RAM BKPSRAM BKPSRAM Assignment (single choice)
Core/RAM DDR via DDRCTRL DDR
Core/RAM MCU SRAM SRAM1 Assignment (between A7 S and A7 NS / M4)
Shareable (between A7 NS and M4)
SRAM2 Assignment (between A7 S and A7 NS / M4)
Shareable (between A7 NS and M4)
SRAM3 Assignment (between A7 S and A7 NS / M4)
Shareable (between A7 NS and M4)
SRAM4 Assignment (between A7 S and A7 NS / M4)
Shareable (between A7 NS and M4)
Core/RAM RETRAM RETRAM Assignment (single choice)
Core/RAM SYSRAM SYSRAM Shareable (multiple choices supported)
Core/Timers LPTIM LPTIM1 Assignment (single choice)
LPTIM2 Assignment (single choice)
LPTIM3 Assignment (single choice)
LPTIM4 Assignment (single choice)
LPTIM5 Assignment (single choice)
Core/Timers TIM TIM1 (APB2 group) Assignment (single choice)
TIM2 (APB1 group) Assignment (single choice)
TIM3 (APB1 group) Assignment (single choice)
TIM4 (APB1 group) Assignment (single choice)
TIM5 (APB1 group) Assignment (single choice)
TIM6 (APB1 group) Assignment (single choice)
TIM7 (APB1 group) Assignment (single choice)
TIM8 (APB2 group) Assignment (single choice)
TIM12 (APB1 group) Assignment (single choice)
TIM13 (APB1 group) Assignment (single choice)
TIM14 (APB1 group) Assignment (single choice)
TIM15 (APB2 group) Assignment (single choice)
TIM16 (APB2 group) Assignment (single choice)
TIM17 (APB2 group) Assignment (single choice)
Core/Watchdog IWDG IWDG1
IWDG2 Shared (none or both):
  • Cortex-A7 non secure for reload
  • Cortex-A7 secure for early interrupt handling
Core/Watchdog WWDG WWDG
High speed interface OTG (USB OTG) OTG (USB OTG)
High speed interface USBH (USB Host) USBH (USB Host)
High speed interface USBPHYC (USB HS PHY controller) USBPHYC (USB HS PHY controller)
Low speed interface I2C I2C1 Assignment (single choice)
I2C2 Assignment (single choice)
I2C3 Assignment (single choice)
I2C4 Assignment (single choice).
Used for PMIC control on ST boards.
I2C5 Assignment (single choice)
I2C6 Assignment (single choice)
Low speed interface
or
audio
SPI SPI2S1 Assignment (single choice)
SPI2S2 Assignment (single choice)
SPI2S3 Assignment (single choice)
SPI4 Assignment (single choice)
SPI5 Assignment (single choice)
SPI6 Assignment (single choice)
Low speed interface USART USART1 Assignment (single choice)
USART2 Assignment (single choice)
USART3 Assignment (single choice)
UART4 Assignment (single choice).
Used for Linux® serial console on ST boards.
UART5 Assignment (single choice)
USART6 Assignment (single choice)
UART7 Assignment (single choice)
UART8 Assignment (single choice)
Mass storage FMC FMC Assignment (single choice)
Mass storage QUADSPI QUADSPI Assignment (single choice)
Mass storage SDMMC SDMMC1
SDMMC2
SDMMC3 Assignment (single choice)
Networking ETH ETH Assignment (single choice)
Networking FDCAN FDCAN1 Assignment (single choice)
FDCAN2 Assignment (single choice)
Power & Thermal DTS DTS
Power & Thermal PWR PWR
Power & Thermal RCC RCC
Security BSEC BSEC
Security CRC CRC1
CRC2
Security CRYP CRYP1 Assignment (single choice)
CRYP2
Security ETZPC ETZPC
Security HASH HASH1 Assignment (single choice)
HASH2
Security RNG RNG1 Assignment (single choice)
RNG2
Security TZC TZC
Security TAMP TAMP
Trace & Debug DDRPERFM DDRPERFM
Trace & Debug DBGMCU DBGMCU No assignment
Trace & Debug HDP HDP
Trace & Debug STM STM
Visual CEC CEC Assignment (single choice)
Visual DCMI DCMI Assignment (single choice)
Visual DSI DSI
Visual GPU GPU
Visual LTDC LTDC

3 References[edit]



This article lists all internal peripherals embedded in STM32MP15 device and shows the assignment possibilities to the runtime contexts for each one of them.<br>

Via this article, you can also access to individual peripheral articles in which information related to the overview and configuration can be found.

==Internal peripherals overview==
The figure below shows all '''peripherals''' embedded in STM32MP15 device, grouped per '''functional domains''' that are reused in many places of this wiki to structure the articles. <br />


Several '''runtime contexts''' exist on STM32MP15 device<ref name="STM32MPU multiple cores">[[Getting started with STM32 MPU devices#Multiple-core architecture concepts]]</ref>, corresponding to the different '''Arm cores and associated security modes''':
* <span style="color:#FFFFFF; background:{{STPink}};">&nbsp;Arm dual core Cortex-A7 secure&nbsp;</span> (Trustzone), running a Secure Monitor or Secure OS like [[OP-TEE overview|OP-TEE]]
* <span style="color:#FFFFFF; background:{{STDarkBlue}};">&nbsp;Arm dual core Cortex-A7 non secure&nbsp;</span>, running [[STM32MP15 Linux kernel overview|Linux]]
* <span style="color:#FFFFFF; background:{{STLightBlue}};">&nbsp;Arm Cortex-M4&nbsp;</span> (non-secure), running [[STM32CubeMP1 architecture|STM32Cube]]<br />

Some peripherals can be strictly '''assigned''' to one runtime context: this is the case for most of the peripherals, like [[USART internal peripheral|USART]] or [[I2C internal peripheral|I2C]].<br />

Other ones can be '''shared''' between several runtime contexts: this is the case for system peripherals, like [[PWR internal peripheral|PWR]] or [[RCC internal peripheral|RCC]].<br />

The legend below shows how assigned and shared peripherals are identified in the assignment diagram that follows:<br /><br />


[[File: STM32MP1IPsOverview legend.png]]<br /><br />


Both the diagram below and the following summary table (in [[#Internal peripherals assignment|Internal peripherals assignment]] chapter below) are clickable in order to jump to each peripheral overview articles and get more detailed information (like software frameworks used to control them). 
They list STMicroelectronics recommendations. The STM32MP15 reference manual <ref>[[STM32MP15 resources#Reference manuals|STM32MP15 reference manuals]]</ref>  may expose more possibilities than what is shown here.

{{
ImageMap|
Image:STM32MP1IPsOverview.png {{!}} frame {{!}} center{{!}} STM32MP1 internal peripherals overview
rect 18 113 103 141[[STGEN internal peripheral | STGEN]]
rect 18 146 103 175[[SYSCFG internal peripheral | SYSCFG]]
rect 18 181 103 208[[RTC internal peripheral | RTC]]
rect 123 113 206 141[[EXTI internal peripheral | EXTI]]
rect 123 146 206 175[[GIC internal peripheral | GIC]]
rect 123 181 206 208[[NVIC internal peripheral | NVIC]]
rect 229 110 314 139[[IWDG internal peripheral | IWDG]]
rect 229 146 314 173[[IWDG internal peripheral | IWDG]]
rect 229 181 314 206[[WWDG internal peripheral | WWDG]]
rect 333 144 417 172[[DMA internal peripheral | DMA]]
rect 466 144 549 172[[DMA internal peripheral | DMA]]
rect 400 111 484 138[[DMAMUX internal peripheral | DMAMUX]]
rect 400 181 484 206[[MDMA internal peripheral | MDMA]]
rect 29 241 113 268[[SYSRAM internal memory | SYSRAM]]
rect 122 241 206 268[[DDRCTRL and DDRPHYC internal peripherals| DDR via DDR CTRL]]
rect 214 241 298 268[[BKPSRAM internal memory| BKPSRAM]]
rect 307 241 392 268[[MCU SRAM internal memory | MCU SRAM]]
rect 400 241 484 268[[MCU SRAM internal memory | MCU SRAM]]
rect 492 241 577 268[[RETRAM internal memory| RETRAM]]
rect 28 304 113 331[[TIM internal peripheral | TIM]]
rect 122 304 207 331[[TIM internal peripheral | TIM]]
rect 214 304 298 331[[LPTIM internal peripheral | LPTIM]]
rect 400 304 484 331[[GPIO internal peripheral | GPIO]]
rect 492 304 577 331[[GPIO internal peripheral | GPIO]]
rect 352 37 438 65 [[IPCC internal peripheral | IPCC]]
rect 445 37 531 65 [[HSEM internal peripheral | HSEM]]
rect 13 415 97 442 [[RCC internal peripheral | RCC]]
rect 13 448 97 474 [[PWR internal peripheral | PWR]]
rect 13 480 97 508 [[DTS internal peripheral | DTS]]
rect  111 379 195 409 [[DDRPERFM internal peripheral | DDRPERFM]]
rect  111 415 195 442 [[DBGMCU internal peripheral | DBGMCU]]
rect 111 448 195 474 [[HDP internal peripheral | HDP]]
rect 111 480 195 508 [[STM internal peripheral | STM]]
rect 215 381 298 408 [[BSEC internal peripheral | BSEC]]
rect 215 415 298 442 [[QUADSPI internal peripheral | QUADSPI]]
rect 215 448 298 474 [[FMC internal peripheral | FMC]]
rect 215 480 298 508 [[SDMMC internal peripheral | SDMMC]]
rect 413 480 496 508 [[FDCAN internal peripheral | FDCAN]]
rect 501 480 584 508 [[ETH internal peripheral | ETH]]
rect 316 381 401 408 [[SDMMC internal peripheral | SDMMC]]
rect 316 415 401 442 [[USBH internal peripheral | USBH]]
rect 316 448 401 474 [[OTG internal peripheral | OTG]]
rect 316 480 401 508 [[USBPHYC internal peripheral | USBPHYC]]
rect 413 365 496 393 [[USART internal peripheral | USART]]
rect 413 400 496 426[[USART internal peripheral | USART]]
rect 501 365 585 393 [[USART internal peripheral | USART]]
rect 413 434 496 460 [[I2C internal peripheral | I2C]]
rect 501 400 585 426 [[I2C internal peripheral | I2C]]
rect 501 434 585 460 [[I2C internal peripheral | I2C]]
rect 591 365 674 393 [[SPI internal peripheral | SPI]]
rect 591 400 674 426 [[SPI internal peripheral | SPI]]
rect 708 111 792 138 [[RNG internal peripheral | RNG]]
rect 800 111 883 138 [[HASH internal peripheral | HASH]]
rect 616 144 700 172 [[ETZPC internal peripheral | ETZPC]]
rect 708 144 792 172 [[CRYP internal peripheral | CRYP]]
rect 800 144 883 172 [[CRC internal peripheral | CRC]]
rect 617 179 701 206 [[TZC internal peripheral | TZC]]
rect 708 179 792 206 [[RNG internal peripheral | RNG]]
rect 800 179 883 206 [[HASH internal peripheral | HASH]]
rect 617 213 701 240 [[TAMP internal peripheral | TAMP]]
rect 709 213 792 240 [[CRYP internal peripheral | CRYP]]
rect 800 213 883 240 [[CRC internal peripheral | CRC]]
rect 617 278 700 306 [[GPU internal peripheral | GPU]]
rect 709 278 792 306 [[DSI internal peripheral | DSI]]
rect 800 278 883 306 [[LTDC internal peripheral | LTDC]]
rect 617 312 700 338 [[DCMI internal peripheral | DCMI]]
rect 709 312 792 338 [[CEC internal peripheral | CEC]]
rect 709 400 792 426 [[VREFBUF internal peripheral | VREFBUF]]
rect 800 400 883 426 [[DAC internal peripheral | DAC]]
rect 709 436 792 462 [[DFSDM internal peripheral | DFSDM]]
rect 800 436 883 462 [[ADC internal peripheral | ADC]]
rect 617 481 700 508 [[SPI internal peripheral | SPI I2S]]
rect 709 481 792 508 [[SPDIFRX internal peripheral | SPDIFRX]]
rect 800 481 883 508 [[SAI internal peripheral | SAI]]
}}

==Internal peripherals assignment==
{{:Internal_peripherals_assignment_table_template}}
{{:ADC_internal_peripheral}}
{{:DAC_internal_peripheral}}
{{:DFSDM_internal_peripheral}}
{{:VREFBUF_internal_peripheral}}
{{:SAI_internal_peripheral}}
{{:SPDIFRX_internal_peripheral}}
{{:IPCC_internal_peripheral}}
{{:HSEM_internal_peripheral}}
{{:RTC_internal_peripheral}}
{{:STGEN_internal_peripheral}}
{{:SYSCFG_internal_peripheral}}
{{:DMA_internal_peripheral}}
{{:DMAMUX_internal_peripheral}}
{{:MDMA_internal_peripheral}}
{{:EXTI_internal_peripheral}}
{{:GIC_internal_peripheral}}
{{:NVIC_internal_peripheral}}
{{:GPIO internal peripheral}}
{{:BKPSRAM internal memory}}
{{:DDRCTRL and DDRPHYC internal peripherals}}
{{:MCU_SRAM_internal_memory}}
{{:RETRAM internal memory}}
{{:SYSRAM_internal_memory}}
{{:LPTIM_internal_peripheral}}
{{:TIM_internal_peripheral}}
{{:IWDG_internal_peripheral}}
{{:WWDG_internal_peripheral}}
{{:OTG_internal_peripheral}}
{{:USBH_internal_peripheral}}
{{:USBPHYC internal peripheral}}
{{:I2C_internal_peripheral}}
{{:SPI_internal_peripheral}}
{{:USART_internal_peripheral}}
{{:FMC internal peripheral}}
{{:QUADSPI internal peripheral}}
{{:SDMMC internal peripheral}}
{{:ETH internal peripheral}}
{{:FDCAN internal peripheral}}
{{:DTS_internal_peripheral}}
{{:PWR_internal_peripheral}}
{{:RCC_internal_peripheral}}
{{:BSEC_internal_peripheral}}
{{:CRC_internal_peripheral}}
{{:CRYP_internal_peripheral}}
{{:ETZPC_internal_peripheral}}
{{:HASH_internal_peripheral}}
{{:RNG_internal_peripheral}}
{{:TZC_internal_peripheral}}
{{:TAMP_internal_peripheral}}
{{:DDRPERFM_internal_peripheral}}
{{:DBGMCU_internal_peripheral}}
{{:HDP_internal_peripheral}}
{{:STM_internal_peripheral}}
{{:CEC_internal_peripheral}}
{{:DCMI_internal_peripheral}}
{{:DSI_internal_peripheral}}
{{:GPU_internal_peripheral}}
{{:LTDC_internal_peripheral}}
 |}

==References==<references/>

<noinclude>

{{PublicationRequestId | 9171 | 2018-10-17 | AlainF}}
[[Category:Peripherals overview]]
[[Category:STM32MP15]]</noinclude>
(One intermediate revision by the same user not shown)
Line 55: Line 55:
 
rect 13 448 97 474 [[PWR internal peripheral | PWR]]
 
rect 13 448 97 474 [[PWR internal peripheral | PWR]]
 
rect 13 480 97 508 [[DTS internal peripheral | DTS]]
 
rect 13 480 97 508 [[DTS internal peripheral | DTS]]
  +
rect  111 379 195 409 [[DDRPERFM internal peripheral | DDRPERFM]]
 
rect  111 415 195 442 [[DBGMCU internal peripheral | DBGMCU]]
 
rect  111 415 195 442 [[DBGMCU internal peripheral | DBGMCU]]
 
rect 111 448 195 474 [[HDP internal peripheral | HDP]]
 
rect 111 448 195 474 [[HDP internal peripheral | HDP]]
Line 152: Line 153:
 
{{:TZC_internal_peripheral}}
 
{{:TZC_internal_peripheral}}
 
{{:TAMP_internal_peripheral}}
 
{{:TAMP_internal_peripheral}}
  +
{{:DDRPERFM_internal_peripheral}}
 
{{:DBGMCU_internal_peripheral}}
 
{{:DBGMCU_internal_peripheral}}
 
{{:HDP_internal_peripheral}}
 
{{:HDP_internal_peripheral}}