Difference between revisions of "STM32MP15 peripherals overview"

[quality revision] [quality revision]
m
m
 

This article lists all internal peripherals embedded in STM32MP15 device and shows the assignment possibilities to the runtime contexts for each one of them.
Via this article, you can also access to individual peripheral articles in which information related to the overview and configuration can be found.

1 Internal peripherals overview[edit]

The figure below shows all peripherals embedded in STM32MP15 device, grouped per functional domains that are reused in many places of this wiki to structure the articles.

Several runtime contexts exist on STM32MP15 device[1], corresponding to the different Arm cores and associated security modes:

  •  Arm dual core Cortex-A7 secure  (Trustzone), running a Secure Monitor or Secure OS like OP-TEE
  •  Arm dual core Cortex-A7 non secure , running Linux
  •  Arm Cortex-M4  (non-secure), running STM32Cube


Some peripherals can be strictly assigned to one runtime context: this is the case for most of the peripherals, like USART or I2C.
Other ones can be shared between several runtime contexts: this is the case for system peripherals, like PWR or RCC.
The legend below shows how assigned and shared peripherals are identified in the assignment diagram that follows:

STM32MP1IPsOverview legend.png

Both the diagram below and the following summary table (in Internal peripherals assignment chapter below) are clickable in order to jump to each peripheral overview articles and get more detailed information (like software frameworks used to control them). They list STMicroelectronics recommendations. The STM32MP15 reference manual [2] may expose more possibilities than what is shown here.


STGEN SYSCFG RTC EXTI GIC NVIC IWDG IWDG WWDG DMA DMA DMAMUX MDMA SYSRAM DDR via DDR CTRL BKPSRAM MCU SRAM MCU SRAM RETRAM TIM TIM LPTIM GPIO GPIO IPCC HSEM RCC PWR DTS DDRPERFM DBGMCU HDP STM BSEC QUADSPI FMC SDMMC FDCAN ETH SDMMC USBH OTG USBPHYC USART USART USART I2C I2C I2C SPI SPI RNG HASH ETZPC CRYP CRC TZC RNG HASH TAMP CRYP CRC GPU DSI LTDC DCMI CEC VREFBUF DAC DFSDM ADC SPI I2S SPDIFRX SAI
STM32MP1 internal peripherals overview

2 Internal peripherals assignment[edit]

Internal peripherals

Check boxes illustrate the possible peripheral allocations supported by STM32 MPU Embedded Software:

  • means that the peripheral can be assigned () to the given runtime context.
  • is used for system peripherals that cannot be unchecked because they are statically connected in the device.

Refer to How to assign an internal peripheral to a runtime context for more information on how to assign peripherals manually or via STM32CubeMX.
The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possiblities might be described in STM32MP15 reference manuals.

Domain Peripheral Runtime allocation Comment
Instance Cortex-A7
secure
(OP-TEE)
Cortex-A7
non-secure
(Linux)
Cortex-M4

(STM32Cube)
Analog ADC ADC Assignment (single choice)
Analog DAC DAC Assignment (single choice)
Analog DFSDM DFSDM Assignment (single choice)
Analog VREFBUF VREFBUF Assignment (single choice)
Audio SAI SAI1 Assignment (single choice)
SAI2 Assignment (single choice)
SAI3 Assignment (single choice)
SAI4 Assignment (single choice)
Audio SPDIFRX SPDIFRX Assignment (single choice)
Coprocessor IPCC IPCC Shared (none or both)
Coprocessor HSEM HSEM
Core RTC RTC RTC is mandatory to resynchronize STGEN after exiting low-power modes.
Core STGEN STGEN
Core SYSCFG SYSCFG
Core/DMA DMA DMA1 Assignment (single choice)
DMA2 Assignment (single choice)
Core/DMA DMAMUX DMAMUX Shareable (multiple choices supported)
Core/DMA MDMA MDMA Shareable (multiple choices supported)
Core/Interrupts EXTI EXTI Shareable (multiple choices supported)
Core/Interrupts GIC GIC
Core/Interrupts NVIC NVIC
Core/IOs GPIO GPIOA (16 pins) Shareable (with pin granularity)
GPIOB (16 pins) Shareable (with pin granularity)
GPIOC (16 pins) Shareable (with pin granularity)
GPIOD (16 pins) Shareable (with pin granularity)
GPIOE (16 pins) Shareable (with pin granularity)
GPIOF (16 pins) Shareable (with pin granularity)
GPIOG (16 pins) Shareable (with pin granularity)
GPIOH (16 pins) Shareable (with pin granularity)
GPIOI (16 pins) Shareable (with pin granularity)
GPIOJ (16 pins) Shareable (with pin granularity)
GPIOK (8 pins) Shareable (with pin granularity)
GPIOZ (8 pins) Shareable (with pin granularity)
Core/RAM BKPSRAM BKPSRAM Assignment (single choice)
Core/RAM DDR via DDRCTRL DDR
Core/RAM MCU SRAM SRAM1 Assignment (between A7 S and A7 NS / M4)
Shareable (between A7 NS and M4)
SRAM2 Assignment (between A7 S and A7 NS / M4)
Shareable (between A7 NS and M4)
SRAM3 Assignment (between A7 S and A7 NS / M4)
Shareable (between A7 NS and M4)
SRAM4 Assignment (between A7 S and A7 NS / M4)
Shareable (between A7 NS and M4)
Core/RAM RETRAM RETRAM Assignment (single choice)
Core/RAM SYSRAM SYSRAM Shareable (multiple choices supported)
Core/Timers LPTIM LPTIM1 Assignment (single choice)
LPTIM2 Assignment (single choice)
LPTIM3 Assignment (single choice)
LPTIM4 Assignment (single choice)
LPTIM5 Assignment (single choice)
Core/Timers TIM TIM1 (APB2 group) Assignment (single choice)
TIM2 (APB1 group) Assignment (single choice)
TIM3 (APB1 group) Assignment (single choice)
TIM4 (APB1 group) Assignment (single choice)
TIM5 (APB1 group) Assignment (single choice)
TIM6 (APB1 group) Assignment (single choice)
TIM7 (APB1 group) Assignment (single choice)
TIM8 (APB2 group) Assignment (single choice)
TIM12 (APB1 group) Assignment (single choice)
TIM13 (APB1 group) Assignment (single choice)
TIM14 (APB1 group) Assignment (single choice)
TIM15 (APB2 group) Assignment (single choice)
TIM16 (APB2 group) Assignment (single choice)
TIM17 (APB2 group) Assignment (single choice)
Core/Watchdog IWDG IWDG1
IWDG2 Shared (none or both):
  • Cortex-A7 non secure for reload
  • Cortex-A7 secure for early interrupt handling
Core/Watchdog WWDG WWDG
High speed interface OTG (USB OTG) OTG (USB OTG)
High speed interface USBH (USB Host) USBH (USB Host)
High speed interface USBPHYC (USB HS PHY controller) USBPHYC (USB HS PHY controller)
Low speed interface I2C I2C1 Assignment (single choice)
I2C2 Assignment (single choice)
I2C3 Assignment (single choice)
I2C4 Assignment (single choice).
Used for PMIC control on ST boards.
I2C5 Assignment (single choice)
I2C6 Assignment (single choice)
Low speed interface
or
audio
SPI SPI2S1 Assignment (single choice)
SPI2S2 Assignment (single choice)
SPI2S3 Assignment (single choice)
SPI4 Assignment (single choice)
SPI5 Assignment (single choice)
SPI6 Assignment (single choice)
Low speed interface USART USART1 Assignment (single choice)
USART2 Assignment (single choice)
USART3 Assignment (single choice)
UART4 Assignment (single choice).
Used for Linux® serial console on ST boards.
UART5 Assignment (single choice)
USART6 Assignment (single choice)
UART7 Assignment (single choice)
UART8 Assignment (single choice)
Mass storage FMC FMC Assignment (single choice)
Mass storage QUADSPI QUADSPI Assignment (single choice)
Mass storage SDMMC SDMMC1
SDMMC2
SDMMC3 Assignment (single choice)
Networking ETH ETH Assignment (single choice)
Networking FDCAN FDCAN1 Assignment (single choice)
FDCAN2 Assignment (single choice)
Power & Thermal DTS DTS
Power & Thermal PWR PWR
Power & Thermal RCC RCC
Security BSEC BSEC
Security CRC CRC1
CRC2
Security CRYP CRYP1 Assignment (single choice)
CRYP2
Security ETZPC ETZPC
Security HASH HASH1 Assignment (single choice)
HASH2
Security RNG RNG1 Assignment (single choice)
RNG2
Security TZC TZC
Security TAMP TAMP
Trace & Debug DDRPERFM DDRPERFM
Trace & Debug DBGMCU DBGMCU No assignment
Trace & Debug HDP HDP
Trace & Debug STM STM
Visual CEC CEC Assignment (single choice)
Visual DCMI DCMI Assignment (single choice)
Visual DSI DSI
Visual GPU GPU
Visual LTDC LTDC

3 References[edit]



This article lists all internal peripherals embedded in STM32MP15 device and shows the assignment possibilities to the runtime contexts for each one of them.<br>

Via this article, you can also access to individual peripheral articles in which information related to the overview and configuration can be found.

==Internal peripherals overview==
The figure below shows all '''peripherals''' embedded in STM32MP15 device, grouped per '''functional domains''' that are reused in many places of this wiki to structure the articles. <br />


Several '''runtime contexts''' exist on STM32MP15 device<ref name="STM32MPU multiple cores">[[Getting started with STM32 MPU devices#Multiple-core architecture concepts]]</ref>, corresponding to the different '''Arm cores and associated security modes''':
* <span style="color:#FFFFFF; background:#D4007A{{STPink}};">&nbsp;Arm dual core Cortex-A7 secure&nbsp;</span> (Trustzone), running a Secure Monitor or Secure OS like [[OP-TEE overview|OP-TEE]]
* <span style="color:#FFFFFF; background:#002052{{STDarkBlue}};">&nbsp;Arm dual core Cortex-A7 non secure&nbsp;</span>, running [[STM32MP15 Linux kernel overview|Linux]]
* <span style="color:#FFFFFF; background:#39A9DC{{STLightBlue}};">&nbsp;Arm Cortex-M4&nbsp;</span> (non-secure), running [[STM32CubeMP1 architecture|STM32Cube]]<br />

Some peripherals can be strictly '''assigned''' to one runtime context: this is the case for most of the peripherals, like [[USART internal peripheral|USART]] or [[I2C internal peripheral|I2C]].<br />

Other ones can be '''shared''' between several runtime contexts: this is the case for system peripherals, like [[PWR internal peripheral|PWR]] or [[RCC internal peripheral|RCC]].<br />

The legend below shows how assigned and shared peripherals are identified in the assignment diagram that follows:<br /><br />


[[File: STM32MP1IPsOverview legend.png]]<br /><br />


Both the diagram below and the following summary table (in [[#Internal peripherals assignment|Internal peripherals assignment]] chapter below) are clickable in order to jump to each peripheral overview articles and get more detailed information (like software frameworks used to control them). 
They list STMicroelectronics recommendations. The STM32MP15 reference manual <ref>[[STM32MP15 resources#Reference manuals|STM32MP15 reference manuals]]</ref>  may expose more possibilities than what is shown here.

{{
ImageMap|
Image:STM32MP1IPsOverview.png {{!}} frame {{!}} center{{!}} STM32MP1 internal peripherals overview
rect 18 113 103 141[[STGEN internal peripheral | STGEN]]
rect 18 146 103 175[[SYSCFG internal peripheral | SYSCFG]]
rect 18 181 103 208[[RTC internal peripheral | RTC]]
rect 123 113 206 141[[EXTI internal peripheral | EXTI]]
rect 123 146 206 175[[GIC internal peripheral | GIC]]
rect 123 181 206 208[[NVIC internal peripheral | NVIC]]
rect 228 113 312 141229 110 314 139[[IWDG internal peripheral | IWDG]]
rect 228229 146 312 175314 173[[IWDG internal peripheral | IWDG]]
rect 228229 181 312 208314 206[[WWDG internal peripheral | WWDG]]
rect 333 146 416 175144 417 172[[DMA internal peripheral | DMA]]
rect 465 146 550 175466 144 549 172[[DMA internal peripheral | DMA]]
rect 400 113111 484 141138[[DMAMUX internal peripheral | DMAMUX]]
rect 400 181 484 208206[[MDMA internal peripheral | MDMA]]
rect 29 244 114 271241 113 268[[SYSRAM internal memory | SYSRAM]]
rect 121 244122 241 206 271268[[DDRCTRL and DDRPHYC internal peripherals| DDR via DDR CTRL]]
rect 215 244214 241 298 271268[[BKPSRAM internal memory| BKPSRAM]]
rect 307 244 390 271241 392 268[[MCU SRAM internal memory | MCU SRAM]]
rect 400 244241 484 271268[[MCU SRAM internal memory | MCU SRAM]]
rect 493 244 576 271492 241 577 268[[RETRAM internal memory| RETRAM]]
rect 28 306 112 333304 113 331[[TIM internal peripheral | TIM]]
rect 122 306 205 333304 207 331[[TIM internal peripheral | TIM]]
rect 214 306304 298 333331[[LPTIM internal peripheral | LPTIM]]
rect 400 306304 484 333331[[GPIO internal peripheral | GPIO]]
rect 492 306304 577 333331[[GPIO internal peripheral | GPIO]]
rect 354 41352 37 438 6865 [[IPCC internal peripheral | IPCC]]
rect 447 41445 37 531 6865 [[HSEM internal peripheral | HSEM]]
rect 13 418415 97 444442 [[RCC internal peripheral | RCC]]
rect 13 450448 97 478474 [[PWR internal peripheral | PWR]]
rect 13 484480 97 512508 [[DTS internal peripheral | DTS]]
rect  112 418111 379 195 444 [[409 [[DDRPERFM internal peripheral | DDRPERFM]]
rect  111 415 195 442 [[DBGMCU internal peripheral | DBGMCU]]
rect 112 450111 448 195 478474 [[HDP internal peripheral | HDP]]
rect 112 484111 480 195 512508 [[STM internal peripheral | STM]]
rect 215 384 299 411381 298 408 [[BSEC internal peripheral | BSEC]]
rect 215 418 299 444415 298 442 [[QUADSPI internal peripheral | QUADSPI]]
rect 215 450 299 478448 298 474 [[FMC internal peripheral | FMC]]
rect 214 484 299 512215 480 298 508 [[SDMMC internal peripheral | SDMMC]]
rect 412 485 497 512413 480 496 508 [[FDCAN internal peripheral | FDCAN]]
rect 501 485 585 512480 584 508 [[ETH internal peripheral | ETH]]
rect 316 384381 401 412408 [[SDMMC internal peripheral | SDMMC]]
rect 316 418415 401 445442 [[USBH internal peripheral | USBH]]
rect 316 451448 401 479474 [[OTG internal peripheral | OTG]]
rect 316 484480 401 511508 [[USBPHYC internal peripheral | USBPHYC]]
rect 413 369 497 396365 496 393 [[USART internal peripheral | USART]]
rect 413 402 497 430400 496 426[[USART internal peripheral | USART]]
rect 502 369 586 396501 365 585 393 [[USART internal peripheral | USART]]
rect 413 437 497 463434 496 460 [[I2C internal peripheral | I2C]]
rect 502 402 586 430501 400 585 426 [[I2C internal peripheral | I2C]]
rect 502 437 586 463501 434 585 460 [[I2C internal peripheral | I2C]]
rect 591 369365 674 396393 [[SPI internal peripheral | SPI]]
rect 591 402400 674 430426 [[SPI internal peripheral | SPI]]
rect 709 113708 111 792 140138 [[RNG internal peripheral | RNG]]
rect 800 113111 883 140138 [[HASH internal peripheral | HASH]]
rect 617 148616 144 700 174172 [[ETZPC internal peripheral | ETZPC]]
rect 709 148708 144 792 174172 [[CRYP internal peripheral | CRYP]]
rect 800 148144 883 174172 [[CRC internal peripheral | CRC]]
rect 617 182179 701 209206 [[TZC internal peripheral | TZC]]
rect 709 182708 179 792 209206 [[RNG internal peripheral | RNG]]
rect 800 182179 883 209206 [[HASH internal peripheral | HASH]]
rect 617 216213 701 242240 [[TAMP internal peripheral | TAMP]]
rect 709 216213 792 242240 [[CRYP internal peripheral | CRYP]]
rect 800 216 884 242213 883 240 [[CRC internal peripheral | CRC]]
rect 617 281 701 307278 700 306 [[GPU internal peripheral | GPU]]
rect 709 281 791 307278 792 306 [[DSI internal peripheral | DSI]]
rect 800 281278 883 307306 [[LTDC internal peripheral | LTDC]]
rect 617 314 701 341312 700 338 [[DCMI internal peripheral | DCMI]]
rect 709 314312 792 340338 [[CEC internal peripheral | CEC]]
rect 709 402400 792 430426 [[VREFBUF internal peripheral | VREFBUF]]
rect 800 402400 883 430426 [[DAC internal peripheral | DAC]]
rect 709 438436 792 464462 [[DFSDM internal peripheral | DFSDM]]
rect 800 438436 883 464462 [[ADC internal peripheral | ADC]]
rect 618 485 701 512617 481 700 508 [[SPI internal peripheral | SPI I2S]]
rect 709 485481 792 512508 [[SPDIFRX internal peripheral | SPDIFRX]]
rect 800 485481 883 512508 [[SAI internal peripheral | SAI]]
}}

==Internal peripherals assignment==
{{:Internal_peripherals_assignment_table_template}}
{{:ADC_internal_peripheral}}
{{:DAC_internal_peripheral}}
{{:DFSDM_internal_peripheral}}
{{:VREFBUF_internal_peripheral}}
{{:SAI_internal_peripheral}}
{{:SPDIFRX_internal_peripheral}}
{{:IPCC_internal_peripheral}}
{{:HSEM_internal_peripheral}}
{{:RTC_internal_peripheral}}
{{:STGEN_internal_peripheral}}
{{:SYSCFG_internal_peripheral}}
{{:DMA_internal_peripheral}}
{{:DMAMUX_internal_peripheral}}
{{:MDMA_internal_peripheral}}
{{:EXTI_internal_peripheral}}
{{:GIC_internal_peripheral}}
{{:NVIC_internal_peripheral}}
{{:GPIO internal peripheral}}
{{:BKPSRAM internal memory}}
{{:DDRCTRL and DDRPHYC internal peripherals}}
{{:MCU_SRAM_internal_memory}}
{{:RETRAM internal memory}}
{{:SYSRAM_internal_memory}}
{{:LPTIM_internal_peripheral}}
{{:TIM_internal_peripheral}}
{{:IWDG_internal_peripheral}}
{{:WWDG_internal_peripheral}}
{{:OTG_internal_peripheral}}
{{:USBH_internal_peripheral}}
{{:USBPHYC internal peripheral}}
{{:I2C_internal_peripheral}}
{{:SPI_internal_peripheral}}
{{:USART_internal_peripheral}}
{{:FMC internal peripheral}}
{{:QUADSPI internal peripheral}}
{{:SDMMC internal peripheral}}
{{:ETH internal peripheral}}
{{:FDCAN internal peripheral}}
{{:DTS_internal_peripheral}}
{{:PWR_internal_peripheral}}
{{:RCC_internal_peripheral}}
{{:BSEC_internal_peripheral}}
{{:CRC_internal_peripheral}}
{{:CRYP_internal_peripheral}}
{{:ETZPC_internal_peripheral}}
{{:HASH_internal_peripheral}}
{{:RNG_internal_peripheral}}
{{:TZC_internal_peripheral}}
{{:TAMP_internal_peripheral}}
{{:DDRPERFM_internal_peripheral}}
{{:DBGMCU_internal_peripheral}}
{{:HDP_internal_peripheral}}
{{:STM_internal_peripheral}}
{{:CEC_internal_peripheral}}
{{:DCMI_internal_peripheral}}
{{:DSI_internal_peripheral}}
{{:GPU_internal_peripheral}}
{{:LTDC_internal_peripheral}}
 |}

==References==<references/>

<noinclude>

{{PublicationRequestId | 9171 | 2018-10-17 | AlainF}}
[[Category:Peripherals overview]]
[[Category:STM32MP15]]</noinclude>
(15 intermediate revisions by 2 users not shown)
Line 7: Line 7:
   
 
Several '''runtime contexts''' exist on STM32MP15 device<ref name="STM32MPU multiple cores">[[Getting started with STM32 MPU devices#Multiple-core architecture concepts]]</ref>, corresponding to the different '''Arm cores and associated security modes''':
 
Several '''runtime contexts''' exist on STM32MP15 device<ref name="STM32MPU multiple cores">[[Getting started with STM32 MPU devices#Multiple-core architecture concepts]]</ref>, corresponding to the different '''Arm cores and associated security modes''':
* <span style="color:#FFFFFF; background:#D4007A">&nbsp;Arm dual core Cortex-A7 secure&nbsp;</span> (Trustzone), running a Secure Monitor or Secure OS like [[OP-TEE overview|OP-TEE]]
+
* <span style="color:#FFFFFF; background:{{STPink}};">&nbsp;Arm dual core Cortex-A7 secure&nbsp;</span> (Trustzone), running a Secure Monitor or Secure OS like [[OP-TEE overview|OP-TEE]]
* <span style="color:#FFFFFF; background:#002052">&nbsp;Arm dual core Cortex-A7 non secure&nbsp;</span>, running [[STM32MP15 Linux kernel overview|Linux]]
+
* <span style="color:#FFFFFF; background:{{STDarkBlue}};">&nbsp;Arm dual core Cortex-A7 non secure&nbsp;</span>, running [[STM32MP15 Linux kernel overview|Linux]]
* <span style="color:#FFFFFF; background:#39A9DC">&nbsp;Arm Cortex-M4&nbsp;</span> (non-secure), running [[STM32CubeMP1 architecture|STM32Cube]]
+
* <span style="color:#FFFFFF; background:{{STLightBlue}};">&nbsp;Arm Cortex-M4&nbsp;</span> (non-secure), running [[STM32CubeMP1 architecture|STM32Cube]]
 
<br />
 
<br />
 
Some peripherals can be strictly '''assigned''' to one runtime context: this is the case for most of the peripherals, like [[USART internal peripheral|USART]] or [[I2C internal peripheral|I2C]].<br />
 
Some peripherals can be strictly '''assigned''' to one runtime context: this is the case for most of the peripherals, like [[USART internal peripheral|USART]] or [[I2C internal peripheral|I2C]].<br />
Line 32: Line 32:
 
rect 123 146 206 175[[GIC internal peripheral | GIC]]
 
rect 123 146 206 175[[GIC internal peripheral | GIC]]
 
rect 123 181 206 208[[NVIC internal peripheral | NVIC]]
 
rect 123 181 206 208[[NVIC internal peripheral | NVIC]]
rect 228 113 312 141[[IWDG internal peripheral | IWDG]]
+
rect 229 110 314 139[[IWDG internal peripheral | IWDG]]
rect 228 146 312 175[[IWDG internal peripheral | IWDG]]
+
rect 229 146 314 173[[IWDG internal peripheral | IWDG]]
rect 228 181 312 208[[WWDG internal peripheral | WWDG]]
+
rect 229 181 314 206[[WWDG internal peripheral | WWDG]]
rect 333 146 416 175[[DMA internal peripheral | DMA]]
+
rect 333 144 417 172[[DMA internal peripheral | DMA]]
rect 465 146 550 175[[DMA internal peripheral | DMA]]
+
rect 466 144 549 172[[DMA internal peripheral | DMA]]
rect 400 113 484 141[[DMAMUX internal peripheral | DMAMUX]]
+
rect 400 111 484 138[[DMAMUX internal peripheral | DMAMUX]]
rect 400 181 484 208[[MDMA internal peripheral | MDMA]]
+
rect 400 181 484 206[[MDMA internal peripheral | MDMA]]
rect 29 244 114 271[[SYSRAM internal memory | SYSRAM]]
+
rect 29 241 113 268[[SYSRAM internal memory | SYSRAM]]
rect 121 244 206 271[[DDRCTRL and DDRPHYC internal peripherals| DDR via DDR CTRL]]
+
rect 122 241 206 268[[DDRCTRL and DDRPHYC internal peripherals| DDR via DDR CTRL]]
rect 215 244 298 271[[BKPSRAM internal memory| BKPSRAM]]
+
rect 214 241 298 268[[BKPSRAM internal memory| BKPSRAM]]
rect 307 244 390 271[[MCU SRAM internal memory | MCU SRAM]]
+
rect 307 241 392 268[[MCU SRAM internal memory | MCU SRAM]]
rect 400 244 484 271[[MCU SRAM internal memory | MCU SRAM]]
+
rect 400 241 484 268[[MCU SRAM internal memory | MCU SRAM]]
rect 493 244 576 271[[RETRAM internal memory| RETRAM]]
+
rect 492 241 577 268[[RETRAM internal memory| RETRAM]]
rect 28 306 112 333[[TIM internal peripheral | TIM]]
+
rect 28 304 113 331[[TIM internal peripheral | TIM]]
rect 122 306 205 333[[TIM internal peripheral | TIM]]
+
rect 122 304 207 331[[TIM internal peripheral | TIM]]
rect 214 306 298 333[[LPTIM internal peripheral | LPTIM]]
+
rect 214 304 298 331[[LPTIM internal peripheral | LPTIM]]
rect 400 306 484 333[[GPIO internal peripheral | GPIO]]
+
rect 400 304 484 331[[GPIO internal peripheral | GPIO]]
rect 492 306 577 333[[GPIO internal peripheral | GPIO]]
+
rect 492 304 577 331[[GPIO internal peripheral | GPIO]]
rect 354 41 438 68 [[IPCC internal peripheral | IPCC]]
+
rect 352 37 438 65 [[IPCC internal peripheral | IPCC]]
rect 447 41 531 68 [[HSEM internal peripheral | HSEM]]
+
rect 445 37 531 65 [[HSEM internal peripheral | HSEM]]
rect 13 418 97 444 [[RCC internal peripheral | RCC]]
+
rect 13 415 97 442 [[RCC internal peripheral | RCC]]
rect 13 450 97 478 [[PWR internal peripheral | PWR]]
+
rect 13 448 97 474 [[PWR internal peripheral | PWR]]
rect 13 484 97 512 [[DTS internal peripheral | DTS]]
+
rect 13 480 97 508 [[DTS internal peripheral | DTS]]
rect  112 418 195 444 [[DBGMCU internal peripheral | DBGMCU]]
+
rect  111 379 195 409 [[DDRPERFM internal peripheral | DDRPERFM]]
rect 112 450 195 478 [[HDP internal peripheral | HDP]]
+
rect  111 415 195 442 [[DBGMCU internal peripheral | DBGMCU]]
rect 112 484 195 512 [[STM internal peripheral | STM]]
+
rect 111 448 195 474 [[HDP internal peripheral | HDP]]
rect 215 384 299 411 [[BSEC internal peripheral | BSEC]]
+
rect 111 480 195 508 [[STM internal peripheral | STM]]
rect 215 418 299 444 [[QUADSPI internal peripheral | QUADSPI]]
+
rect 215 381 298 408 [[BSEC internal peripheral | BSEC]]
rect 215 450 299 478 [[FMC internal peripheral | FMC]]
+
rect 215 415 298 442 [[QUADSPI internal peripheral | QUADSPI]]
rect 214 484 299 512 [[SDMMC internal peripheral | SDMMC]]
+
rect 215 448 298 474 [[FMC internal peripheral | FMC]]
rect 412 485 497 512 [[FDCAN internal peripheral | FDCAN]]
+
rect 215 480 298 508 [[SDMMC internal peripheral | SDMMC]]
rect 501 485 585 512 [[ETH internal peripheral | ETH]]
+
rect 413 480 496 508 [[FDCAN internal peripheral | FDCAN]]
rect 316 384 401 412 [[SDMMC internal peripheral | SDMMC]]
+
rect 501 480 584 508 [[ETH internal peripheral | ETH]]
rect 316 418 401 445 [[USBH internal peripheral | USBH]]
+
rect 316 381 401 408 [[SDMMC internal peripheral | SDMMC]]
rect 316 451 401 479 [[OTG internal peripheral | OTG]]
+
rect 316 415 401 442 [[USBH internal peripheral | USBH]]
rect 316 484 401 511 [[USBPHYC internal peripheral | USBPHYC]]
+
rect 316 448 401 474 [[OTG internal peripheral | OTG]]
rect 413 369 497 396 [[USART internal peripheral | USART]]
+
rect 316 480 401 508 [[USBPHYC internal peripheral | USBPHYC]]
rect 413 402 497 430[[USART internal peripheral | USART]]
+
rect 413 365 496 393 [[USART internal peripheral | USART]]
rect 502 369 586 396 [[USART internal peripheral | USART]]
+
rect 413 400 496 426[[USART internal peripheral | USART]]
rect 413 437 497 463 [[I2C internal peripheral | I2C]]
+
rect 501 365 585 393 [[USART internal peripheral | USART]]
rect 502 402 586 430 [[I2C internal peripheral | I2C]]
+
rect 413 434 496 460 [[I2C internal peripheral | I2C]]
rect 502 437 586 463 [[I2C internal peripheral | I2C]]
+
rect 501 400 585 426 [[I2C internal peripheral | I2C]]
rect 591 369 674 396 [[SPI internal peripheral | SPI]]
+
rect 501 434 585 460 [[I2C internal peripheral | I2C]]
rect 591 402 674 430 [[SPI internal peripheral | SPI]]
+
rect 591 365 674 393 [[SPI internal peripheral | SPI]]
rect 709 113 792 140 [[RNG internal peripheral | RNG]]
+
rect 591 400 674 426 [[SPI internal peripheral | SPI]]
rect 800 113 883 140 [[HASH internal peripheral | HASH]]
+
rect 708 111 792 138 [[RNG internal peripheral | RNG]]
rect 617 148 700 174 [[ETZPC internal peripheral | ETZPC]]
+
rect 800 111 883 138 [[HASH internal peripheral | HASH]]
rect 709 148 792 174 [[CRYP internal peripheral | CRYP]]
+
rect 616 144 700 172 [[ETZPC internal peripheral | ETZPC]]
rect 800 148 883 174 [[CRC internal peripheral | CRC]]
+
rect 708 144 792 172 [[CRYP internal peripheral | CRYP]]
rect 617 182 701 209 [[TZC internal peripheral | TZC]]
+
rect 800 144 883 172 [[CRC internal peripheral | CRC]]
rect 709 182 792 209 [[RNG internal peripheral | RNG]]
+
rect 617 179 701 206 [[TZC internal peripheral | TZC]]
rect 800 182 883 209 [[HASH internal peripheral | HASH]]
+
rect 708 179 792 206 [[RNG internal peripheral | RNG]]
rect 617 216 701 242 [[TAMP internal peripheral | TAMP]]
+
rect 800 179 883 206 [[HASH internal peripheral | HASH]]
rect 709 216 792 242 [[CRYP internal peripheral | CRYP]]
+
rect 617 213 701 240 [[TAMP internal peripheral | TAMP]]
rect 800 216 884 242 [[CRC internal peripheral | CRC]]
+
rect 709 213 792 240 [[CRYP internal peripheral | CRYP]]
rect 617 281 701 307 [[GPU internal peripheral | GPU]]
+
rect 800 213 883 240 [[CRC internal peripheral | CRC]]
rect 709 281 791 307 [[DSI internal peripheral | DSI]]
+
rect 617 278 700 306 [[GPU internal peripheral | GPU]]
rect 800 281 883 307 [[LTDC internal peripheral | LTDC]]
+
rect 709 278 792 306 [[DSI internal peripheral | DSI]]
rect 617 314 701 341 [[DCMI internal peripheral | DCMI]]
+
rect 800 278 883 306 [[LTDC internal peripheral | LTDC]]
rect 709 314 792 340 [[CEC internal peripheral | CEC]]
+
rect 617 312 700 338 [[DCMI internal peripheral | DCMI]]
rect 709 402 792 430 [[VREFBUF internal peripheral | VREFBUF]]
+
rect 709 312 792 338 [[CEC internal peripheral | CEC]]
rect 800 402 883 430 [[DAC internal peripheral | DAC]]
+
rect 709 400 792 426 [[VREFBUF internal peripheral | VREFBUF]]
rect 709 438 792 464 [[DFSDM internal peripheral | DFSDM]]
+
rect 800 400 883 426 [[DAC internal peripheral | DAC]]
rect 800 438 883 464 [[ADC internal peripheral | ADC]]
+
rect 709 436 792 462 [[DFSDM internal peripheral | DFSDM]]
rect 618 485 701 512 [[SPI internal peripheral | SPI I2S]]
+
rect 800 436 883 462 [[ADC internal peripheral | ADC]]
rect 709 485 792 512 [[SPDIFRX internal peripheral | SPDIFRX]]
+
rect 617 481 700 508 [[SPI internal peripheral | SPI I2S]]
rect 800 485 883 512 [[SAI internal peripheral | SAI]]
+
rect 709 481 792 508 [[SPDIFRX internal peripheral | SPDIFRX]]
  +
rect 800 481 883 508 [[SAI internal peripheral | SAI]]
 
}}
 
}}
   
Line 152: Line 153:
 
{{:TZC_internal_peripheral}}
 
{{:TZC_internal_peripheral}}
 
{{:TAMP_internal_peripheral}}
 
{{:TAMP_internal_peripheral}}
  +
{{:DDRPERFM_internal_peripheral}}
 
{{:DBGMCU_internal_peripheral}}
 
{{:DBGMCU_internal_peripheral}}
 
{{:HDP_internal_peripheral}}
 
{{:HDP_internal_peripheral}}