Difference between revisions of "STM32MP15 ecosystem release note - v1.2.0"

[quality revision] [pending revision]
m
 

This article aims The objective of this article is to describe the content of the release STM32MP15-Ecosystem-v1.2.0 for release of STM32MPU Embedded Software distributions and its associated ecosystem.

1 Delivery purpose and scope[edit]

The new STM32MP15-Ecosystem-v1.2.0 release , is dedicated to STM32MP15 microprocessors, . It is an evolutive maintenance release , including that includes minor evolutions and corrections.

The release, as the previous one, aims:

to provide

Like previous release, STM32MP15-Ecosystem-v1.2.0 aims at

  • providing a full ecosystem for STM32MP15x devices.
  • to work working efficiently with STM32MP15 boards, using one of the packages (Starter Package, Developer Package , or Distribution Package) developed by STMicroelectronics for STM32MPUsSTM32 MPUs.

See Refer to Which Package better suits your needs for more information on these packages.


This ecosystem release is constituted byconsists of:

  • Two two STM32MPU distributions
  • The the STM32MPU Embedded Software distribution
  • The the STM32MPU Embedded Software distribution for Android
  • The STM32 referenced tools
  • STM32CubeIDE - New new STM32 IDE targeted to replace SW4STM32 (STM32-CoPro-MPU Eclipse plugin)
  • STM32CubeMX
  • STM32CubeProgrammer
  • Keygen tool
  • Signing tool
(For more details in refer to Referenced tools release notes chapter below).
  • Documentation
  • This The present user guide (in wiki format)
  • Documentation package (for more details in refer to Reference documents chapter below)
  • Supported STM32MP15 boards
  • STM32MP15 Evaluation board ( for "STM32MPU Embedded Software distribution" and "STM32MPU Embedded Software distribution for Android")
  • STM32MP15 Discovery kit (for STM32MPU Embedded Software distribution)
(more More details ca nbe found in Board chapter below).

2 Intended audience[edit]

The targeted audience consists in is STMicroelectronics customers.

3 Licensing[edit]

This software package is licensed under a SOFTWARE LICENSE AGREEMENT , the "SLA". Customer FOR ST MATERIALS (SLA). The customers may not use this package except in compliance with the software license agreement (SLA).

4 Main features / main highlights[edit]

4.1 Boards[edit]

Boards supported with this This STM32MP15-Ecosystem-v1.2.0 release are supports the same than those supported with the boards as STM32MP15-Ecosystem-v1.0.0.

Boards PCBs list Content Availability
STM32MP157C-EV1 board (board with Crypto)
  • MB1263C (Daughter)
  • MB1262C (Mother)
  • MB1230C (Display)
  • MB1379A (Camera)
  • STM32MP1 STM32MP157CAA3 Rev.B
  • PMIC STPMIC1APQR cut1.2
  • External oscillator
Jan'19
STM32MP157A-EV1 board (board without Crypto)
  • MB1263C (Daughter)
  • MB1262C (Mother)
  • MB1230C (Display)
  • MB1379A (Camera)
  • STM32MP1 STM32MP157AAA3 Rev.B
  • PMIC STPMIC1APQR cut1.2
  • External oscillator
Jan'19
STM32MP157C-DK2 board (board with Crypto)
  • MB1272C (Mother)
  • MB1407B (Display)
  • STM32MP1 STM32MP157CAC3 Rev.B
  • PMIC STPMIC1APQR cut1.2
  • External oscillator
Jan'19
STM32MP157A-DK1 board (board without Crypto)
  • MB1272C (Mother)
  • STM32MP1 STM32MP157AAC3 Rev.B
  • PMIC STPMIC1APQR cut1.2
  • External oscillator
Jan'19


Info.png STLINK in EVAL and DISCO Rev.C boards integrates the latest firmware STLINK (V2J32M22) which requires upgraded USB PC drivers - Windows USB driver

4.2 Embedded software[edit]

4.2.1 OpenSTLinux (Cortex®-A7)[edit]

Openstlinux-20-02-19 is the new version delivered with STM32MP15-Ecosystem-v1.2.0 release. This software set is constituted with following components consists of the following components:

  • Build process
    • OpenEmbedded Thud (v2.6.4)
    • GCC version v8.2
  • Software components
    • Kernel version LTS v4.19.94 - NEW version versus STM32MP15-Ecosystem-v1.1.0 release
    • TF-A version v2.0
    • U-Boot version v2018.11
    • OP-TEE version v3.3.0
    • OpenOCD version v0.10.0
  • Applicative components
    • Weston version v5.0.0
    • GStreamer version v1.14.4
    • GCnano version v6.2.4
  • Main NEW features coming with STM32MP15-Ecosystem-v1.2.0 release
    • Add Added support of for STM32MP15x Rev.Z
    • New SoC Part numbers D, F with 800 MHz support Added support for new 800 MHz part numbers (D and F) - STM32MP15_microprocessor
    • Added support for DMA FIFO bypass (Direct mode) support.
    • Added PINCTRL RSVD (Reserved) pin configuration to reserve pins for the co-processorcoprocessor.
    • Added support for I2C SMBus Alert
    • Added support for UART DMA TX/RX support
    • Added STMIPI02 DCMI/CSI convertor + Omnivision 5MP
    • Added STMFX (GPIO expander) driver backport from kernel mainline (STM32MP157x-EV1)
    • Added STPMIC driver backport from kernel mainline
    • Add Added SPI driver in U-boot
    • Add Added RTC driver for UEFI in U-boot
    • Migrate qspi Migrated QUADSPI driver to spi-mem framework in U-boot
    • Activate Activated U-Boot ENV support in boot device (NOR/NAND/eMMC or SD card)
  • Internal peripherals peripheral assignment at boot time
At boot time, you can select two kernel configurations:
  • Configuration 1: All all internal peripherals are assigned to Cortex-A7 for Linux drivers, . Cortex-M4 coprocessing firmware TTY is executed by default.
  • Configuration 2: Some some internal peripherals are assigned to Cortex-M4 to execute Cortex-M4 delivered examples on the board (EVAL or DISCO) see (How to run Cortex-M4 examples).
Configuration 1 is activated by default if you do not specify "2" in the U-Boot console.
More information can be found in How to assign an internal peripheral to a runtime context article.
  • Userland part
    • NEW This release introduces the package repository service that enables the live installation of packages.

4.2.2 STM32CubeMP1 (Cortex®-M4)[edit]

  • Main NEW features coming with STM32CubeMP1-v1.2.0 version, delivered with within STM32MP15-Ecosystem-v1.2.0 release release:
    • Add Added support of for STM32MP15x Rev.Z
    • New SoC Part numbers Added support for new 800 MHz part numbers (D, F with 800 MHz supportKEIL )
    • Added Keil® Project examples on STM32MP157C-DK2
    • Added IAR Project examples on STM32MP157C-DK2
    • Added CubeIDE Project examples on STM32MP157C-DK2
    • New Added new PSRAM HAL driver
    • Added RTC HAL + LL driver
    • Added new FreeRTOS + OpenAMP new example
  • Features already available in previous version
    • The STM32Cube HAL, STM32 abstraction layer embedded software ensuring maximized portability across the STM32 portfolio. HAL APIs are available for all peripherals.
    • Low-layer APIs (LL) offering a fast lightweight light-weight expert-oriented layer that is closer to the hardware than the HAL. LL APIs are available only for a set of peripherals.
    • A consistent set of middleware components such as FreeRTOS, OpenAMP.
    • All embedded software utilities, delivered with a full set of examples.

4.2.3 STM32MP15 distribution for Android (Cortex®-A7) - NEW[edit]

STM32MP15 distribution for Android™ v1.1.0 (st-android-10.0.0-2020-02-21 tag) is the version delivered with within STM32MP15-Ecosystem-v1.2.0 release.

Aim The objectives of this release are the following:

  • Android™ 10.0.0 porting on OpenSTLinux BSP v1.2.0 (TF-A, U-Boot, OP-TEE, Linux kernel), provided as demonstrator
  • Android™ certifications are not ensured

See STM32MP15 distribution for Android release note for more details.

4.3 STM32CubeProgrammer, Signing tool, Keygen[edit]

STM32CubeProgrammer v2.4.0 is the version delivered with within STM32MP15-Ecosystem-v1.2.0 release. This is an evolutive maintenance release for STM32CubeProgrammer.

  • Main NEW features coming with STM32CubeProgrammer-v2.4.0 version, delivered with within STM32MP15-Ecosystem-v1.2.0 release:
  • Flashload speed improvement over USB on Windows PC
  • Parallel programming on several targets
  • Features already available in previous version
  • STM32CubeProg installer includes STM32CubeProgrammer, Keygen and Signing tools
  • Flashload SDCard, eMMC, NAND, NOR images through USB and UART for STM32MP157C-EV1, STM32MP157A-DK1, STM32MP157C-DK2 boards
  • Private and public keys generation
  • Images signature
  • Flashlayout file format change
  • STM32MP1 fuses management (with console interface only)
  • PMIC NVM management (with console interface only)

4.4 STM32CubeMX[edit]

STM32CubeMX-v5.6 is the version delivered with within STM32MP15-Ecosystem-v1.2.0 release

  • Main NEW features coming with STM32CubeMX-v5.6 version, delivered with within STM32MP15-Ecosystem-v1.2.0 release
  • New SoC Added support for new D and F part numbers D, F support
  • Device tree (A7)
    • Device tree compliance with Openstlinux-20-02-19
  • DDR
    • Added support for LPDDR support on 18x18, 16x16 packages
    • DDR Parameters savingtuning parameters saving: see the restriction below in this article
  • STM32CubeMP1 (M4)
    • Compliant Compliance with STM32CubeMP1 V1.2.0
  • Added support for Engineering mode
  • Added support for SMBus alert bit support.
  • PCC : Power data update
  • Tutorial Added tutorial Videos
    • DDR tuning [1]
    • How to customize a DT from a an ST board [2]
Info.png CubeMX STM32CubeMX V5.6 indicates the manifest refers to Openstlinux-4.19-thud-mp1-20-02-19 and this manifest, which corresponds to Openstlinux-20-02-19 tag
  • Features already available in previous version
  • IO I/O muxing , and clock trees tree configuration
  • STM32MP1 contexts management (A7 non-secure, A7 secure, M4)
  • Device tree code generation
    • dtsi and header files file inclusions
    • pinctrl and clocks clock generation
    • System-Onon-Chip chip device nodes node positioning
    • multi-core related configurations (ETZPC binding, resources manager binding, peripherals peripheral assignment).
Info.png Note: the The other device tree parameters must be filled in manually through user sections tag section tags (from /* USER CODE BEGIN <node> */ to /* USER CODE END <node> */)
  • ST32MP1Cube code generation
  • Tuning of DDR settings tuning

4.5 STM32CubeIDE[edit]

STM32CubeIDE V1.3.0 is the version delivered with within STM32MP15-Ecosystem-v1.2.0 release.

  • Main NEW features coming with STM32CubeIDE V1.3.0 version, delivered with within STM32MP15-Ecosystem-v1.2.0 release
    • New SoC Added support for new D and F part numbers D, F support
  • Features already available in previous version
  • Cortex-M4 STM32CubeMP1 in "Production mode" and "Engineering mode"
  • Cortex-M4 Firmware compilation, load, debugloading and debugging
  • PC Linux with Ethernet (recommended) or serial link
  • PC Windows with Ethernet or Ethernet over USB link
  • Cortex-M4 Firmware installation directory configurable
Info.png Customers can continue to use go on using SW4STM32 IDE but the ST . However STMicroelectronics Eclipse reference is STM32CubeIDE. In case of support, ST will focus and recommend STM32CubeIDE toolSTMicroelectronics recommends the use of STM32CubeIDE tool and focuses on STM32CubeIDE support. SW4STM32 projects can be imported in STM32CubeIDE V1.3.0 - Migration process explained in . Refer to Reference documents for explanations on the migration process.

4.6 Miscellaneous[edit]

5 Main restriction listrestrictions[edit]

5.1 Embedded software[edit]

5.1.1 OpenSTLinux (Cortex®-A7)[edit]

  • On STM32MP157C-DK2 boards, BT stack doesn't does not work any more after suspend / resume in Standby mode (function with Stop mode). The This issue is linked to the Murata WifiWi-Fi/BT module that expects the 3V3 3.3 V supply to be kept : in STM32MP1 Standby mode, kept, while this supply is switched off and so the Murata firmware is lostin STM32MP1 Standby mode. A similar workaround as for Wi-Fi can be put in place like for wifi GitHub patch with unbind/bind driver BT respectively before used (GitHub patch). it consists in calling BT unbind and bind drivers before and after resume (modprobe -r hci_uart && modprobe hci_uart).
  • For DDR initialization in TF-A, it is recommended to setup set up and to enable all "boot-on" and "always-on" regulators at bootloader stage, after DDR power initialization. Not This is not yet implemented on in V1.2.0 delivery and an . A patch is under preparation being prepared and will be pushed available on GithubGitHub.

5.1.2 STM32CubeMP1 (Cortex®-M4)[edit]

  • To avoid errors in OpenAMP when compiling in MDK-ARM IDE, you have to disable the « Use MicroLIB » in « Target » tab.
  • The HAL RTC is delivered in within this release but it should be used with caution because the RTC is . However use it with caution since this driver is also used by Linux, by default. To remove any risk of contention between Linux and the HAL, proceed as follows:
    • The write protect (wpr) should must be disabled by default and its should it must never be enabled in any driver (Linux nor HAL).
    • The HAL should must use only use Alarm B, since Linux is only using uses Alarm A.
    • The RTC interrupt should must be shared between Linux and the HAL , to be able to receive alarm notification on each sidenotifications on both sides.

5.2 STM32CubeProgrammer, Signing tool , and Keygen[edit]

  • Flashload through UART fails
  • Key generation is not functional with STM32MP_KeyGen_CLI on Linux with under Ubuntu 16.04 (functional with Ubuntu 18.04)

5.3 STM32CubeMX[edit]

  • MR0 register for LPDDR settings is not set by CubeMX STM32CubeMX in the generated device tree - Need to . This register must be set manually this register at 0Warning : when you open a previous project (built with CubeMX versions .
  • DDR tuning parameters saving does not work when DDR Test Suite tool is used. Use U-Boot tag v2018.11-stm32mp-r4.1 on top of the ecosystem release v1.2.0 More info.png. This tag contains only one patch required by STM32CubeMX v5.6 ("ram: stm32mp1: display result for software read DQS gating").
  • Warning: when opening a previous project built with STM32CubeMX version older than V5.6), the migration will does not take into account the user sections section part. This part needs to be updated manually according the Openstlinux-20-02-19 manifest.

5.4 STM32CubeIDE[edit]

  • Using OpenOCD with ST-LINK does not check and force ST-LINK firmware update at debug launch. It is therefore recommended to manually update to the latest ST-LINK firmware for the best debug experience. Use the menu: Help > ST-LINK Upgrade menu"

5.5 Miscelleanous[edit]

Restrictions Restriction lists are available in each sub-component subcomponent release note, accessible from . They are available in the following chapters in this same the present article:

Moreover, the software workarounds implemented in the ecosystem to answer provide solutions to the STM32MPU device errata are listed in STM32MP15 ecosystem errata sheet.

6 Minor release updates[edit]

STMicroelectronics regularly delivers updates through the following github® components which are : tf-a, u-boot, optee-os, Linux kernel.
You can decide to incorporate them into your Developer Package (please refer to STM32MP1 Developer Package) or Distribution Package (see below).

To update the Distribution package please , proceed as followfollows:

  1. Switch your Distribution package reference source code to github mode.
  2. Use the command devtool modify <recipe name> command to have direct access to the source code git repository used by the build process.
  3. In the freshly cloned source code, checkout check out the revision you want to start from via git checkout -b WORK <github® TAG>.

More rarely and independently, STMicroelectronics also delivers dedicated fixes on layers through github®. These changes can be integrated (via git commands) into your local STM32MP1 Distribution Package environment. Please find below Below the github® links of the quoted layers corresponding to each layers:

6.1 v1.2.1[edit]

OpenSTLinux updates v1.2.1

7 Reference documents[edit]

All the resources for the STM32MP1 Series are located in the Resources area of the STM32MP1 Series web page.

The resources below are referenced in some of the articles of this user guide.

Info.png The different STM32MP15 microprocessor part numbers available (with their corresponding internal peripherals, security options and packages) are described in the STM32MP15 microprocessor part numbers.

New.png means that the document (or its version) is new compared to what was delivered within the previous ecosystem release.


Reference Name Link Version
Application notes
AN4803 High-speed SI simulations using IBIS and board-level simulations using HyperLynx® SI on STM32 MCUs and MPUs AN4803.pdf v2.0
AN5027 Interfacing PDM digital microphones using STM32 MCUs and MPUs AN5027.pdf v2.0
AN5031 Getting started with STM32MP15 Series hardware development AN5031.pdf v1.0
AN5036 Thermal management guidelines for STM32 applications AN5036.pdf v3.0
AN5109 STM32MP1 Series using low-power modes AN5109.pdf v3.0
AN5122 STM32MP1 Series DDR memory routing guidelines AN5122.pdf v3.0
AN5168 STM32MP1 series DDR configuration AN5168.pdf v1.0
AN5225 USB Type-C™ Power Delivery using STM32xx Series MCUs and STM32xxx Series MPUs AN5225.pdf v2.0
AN5253 Migration of microcontroller applications from STM32F4x9 lines to STM32MP151, STM32MP153 and STM32MP157 lines microprocessor AN5253.pdf v1.0
AN5256 STM32MP151, STM32MP153 and STM32MP157 discrete power supply hardware integration AN5256.pdf v1.0
New.png AN5260 STM32MP151/153/157 MPU lines and STPMIC1B integration on a battery powered application AN5260.pdf v1.0
AN5275 USB DFU/USART protocols used in STM32MP1 Series bootloaders AN5275.pdf v1.0
AN5284 STM32MP1 series system power consumption AN5284.pdf v1.0
AN5348 FDCAN peripheral on STM32 devices AN5348.pdf v1.0
New.png AN5438 STM32MP1 Series lifetime estimates AN5438.pdf v1.0
Datasheets[1]
DS12505 STM32MP157C/F datasheet
(secure)
DS12505.pdf New.png v3.0
DS12504 STM32MP157A/D datasheet
(basic)
DS12504.pdf New.png v3.0
DS12503 STM32MP153C/F datasheet
(secure)
DS12503.pdf New.png v3.0
DS12502 STM32MP153A/D datasheet
(basic)
DS12502.pdf New.png v3.0
DS12501 STM32MP151C/F datasheet
(secure)
DS12501.pdf New.png v3.0
DS12500 STM32MP151A/D datasheet
(basic)
DS12500.pdf New.png v3.0
DS12792 STPMIC1 datasheet
stpmic1.pdf New.png v3.0
Errata sheets
ES0438 STM32MP15xx device errata ES0438.pdf New.png v4.0
Reference manuals[1]
RM0436 STM32MP157 reference manual
(STM32MP157xxx advanced Arm®-based 32-bit MPUs)
RM0436.pdf New.png v4.0
RM0442 STM32MP153 reference manual
(STM32MP153xxx advanced Arm®-based 32-bit MPUs)
RM0442.pdf New.png v4.0
RM0441 STM32MP151 reference manual
(STM32MP151xxx advanced Arm®-based 32-bit MPUs)
RM0441.pdf New.png v4.0
Boards schematics
MB1262 schematics STM32MP157C-EV1 motherboard schematics
MB1262-C01 board schematic (Evaluation board)
MB1262-C01.pdf v1.0
MB1263 schematics STM32MP157C-EV1 daughterboard schematics
MB1263-C01 board schematic (Evaluation board)
MB1263-C01.pdf v1.0
MB1230 schematics DSI 720p LCD display daughterboard schematics
MB1230-C board schematic (Evaluation board)
MB1230-C.pdf v1.1
MB1379 schematics Camera daughterboard schematics
MB1379-A01 board schematic (Evaluation board)
MB1379-A01.pdf v1.0
MB1272 schematics STM32MP157x-DKx motherboard schematics
MB1272-DK2-C01 board schematic (Discovery kit)
MB1272-C01.pdf v1.0
MB1407 schematics STM32MP157x-DKx daughterboard schematics
MB1407-LCD-C01 board schematic (Discovery kit)
MB1407-C01.pdf v1.0
Boards user manuals
UM2535 STM32MP157x-EV1 evaluation board user manual UM2535.pdf v2.0
UM2534 STM32MP157x-DKx discovery board user manual UM2534.pdf v1.0
Tools user manuals
New.png UM2563 STM32CubeIDE installation guide UM2563.pdf v1.0
New.png UM2579 Migration guide from System Workbench to STM32CubeIDE UM2579.pdf v1.0
New.png UM1718 STM32CubeMX user manual UM1718.pdf v31.0
New.png UM2237 STM32CubeProgrammer tool user manual UM2237.pdf v10.0
New.png UM2238 STM32 Trusted Package Creator tool user manual UM2238.pdf v5.0
New.png UM2542 STM32 Series Key Generator tool user manual UM2542.pdf v1.0
New.png UM2543 STM32 Series Signing tool user manual UM2543.pdf v1.0


8 How to get download the software and start with this release?[edit]

The list of embedded software packages available for download depends on the selected package.

The table below provides the available board part numbers and the source of as well as information in order to:

  • Get get started with one of the three available Packages (Starter, Developer or Distribution PackagesPackage)
  • Get get started with the board
  • Find find the associated embedded software distributions
  • Download download source code
  • Build build an embedded software
Board part number Jump to
STM32MP157C-EV1
Evaluation board
STM32MP15 Evaluation boards - getting started, including software download
STM32MP157X-DKX
Discovery kit
STM32MP15 Discovery kits - getting started, including software download

9 STM32MPU Embedded Software distribution detailed release notes[edit]

The table below lists the software packages available in the STM32MPU Embedded Software distributions, and provides the corresponding release notes.
The release notes provide give more information and details about the features and content of each packagethe packages.
The release notes does They do not explain how to get download the software. For that, refer chapter Refer to How to get the software and start with this release .

Firmware Release note Version
OpenSTLinux Distribution STM32MP15 OpenSTLinux release note - v1.2.0 openstlinux-20-02-19
STM32Cube MPU Package STM32CubeMP1 Package release note - v1.2.0 STM32CubeMP1-v1.2.0
STM32 MPU Distribution for Android STM32MP15 distribution for Android release note - v1.1.0 st-android-10.0.0-2020-02-21

10 Referenced tools release notes[edit]

The table below lists the available tools, and provides links to the respective corresponding release notes.

Each release note provides gives information on how to install and use the corresponding tool.

The set of tools to that can be downloaded depends on the Package to be that is used (double check Which Package better suits your needs article to find for more information on each Package).

Tools Release notes Host PC Which Package may need the tool ?
Linux version Windows version Starter Package Developer Package Distribution Package
STM32CubeIDE STM32CubeIDE_release_note 1.3.0 1.3.0
STM32CubeMX STM32CubeMX release note from 5.6 from 5.6
STM32CubeProg STM32CubeProgrammer release note 2.4.0 2.4.0
Keygen KeyGen release note 1.0.0 1.0.0
Signing tool Signing tool release note 1.0.0 1.0.0

11 References[edit]

  1. 1.01.1 The part numbers are specified in STM32MP15 microprocessor part numbers


This article aimsThe objective of this article is to describe the content of the release '''''STM32MP15-Ecosystem-v1.2.0''''' for release of ''STM32MPU Embedded Software distributions'' and its associated ecosystem.

==Delivery purpose and scope==
The new STM32MP15-Ecosystem-v1.2.0 release,  is dedicated to STM32MP15 microprocessors, . It is an evolutive maintenance release, including  that includes minor evolutions and corrections. 
The Like previous release, as the previous one, aims:
* to provide STM32MP15-Ecosystem-v1.2.0 aims at 
* providing a full ecosystem for STM32MP15x devices.
* to work 

* working efficiently with STM32MP15 boards, using one of the packages (Starter Package, Developer Package,  or Distribution Package) developed by STMicroelectronics for STM32MPUsSTM32 MPUs. <br>
See Refer to [[Which Package better suits your needs]] for more information on these packages.

This ecosystem release is constituted by:
* '''Two STM32MPU distributions '''
:* Theconsists of:
* '''two STM32MPU distributions '''
:* the ''STM32MPU Embedded Software distribution''
:* Thethe ''STM32MPU Embedded Software distribution for Android''

* '''The STM32 referenced tools'''
:*STM32CubeIDE - Newnew STM32 IDE targeted to replace SW4STM32 (STM32-CoPro-MPU Eclipse plugin) 
:*STM32CubeMX
:*STM32CubeProgrammer
:*Keygen tool
:*Signing tool
:(For more details in refer to [[#Referenced tools release notes |chapter]] below)

* '''Documentation '''
:* This user guide (wiki format) 
:* Documentation package (more details in [[#Reference_documents|chapter]] Referenced tools release notes ]] chapter below.

* '''Documentation '''
:* The present user guide in wiki format 
:* Documentation package (for more details refer to [[#Reference_documents|Reference documents]] chapter below)

* ''' Supported STM32MP15 boards'''
:*STM32MP15 Evaluation board ( for "STM32MPU Embedded Software distribution" and "STM32MPU Embedded Software distribution for Android")
:*STM32MP15 Discovery kit (for ''STM32MPU Embedded Software distribution'')
:(moreMore details in [[#Boards|chapter]] below)ca nbe found in [[#Boards|Board]] chapter below.


==Intended audience==
The targeted audience consists in is STMicroelectronics customers.

==Licensing==
This software package is licensed under a SOFTWARE LICENSE AGREEMENT, the "SLA". Customer  FOR ST MATERIALS (SLA). The customers may not use this package except in compliance with the [[LegalInformation:OpenSTLinux licenses - v1.2.0#Top Software license agreement (SLA) and third-party licences|software license agreement (SLA)]].

==Main features / main highlights==
=== Boards ===Boards supported with this This STM32MP15-Ecosystem-v1.2.0 release aresupports the same than those supported with the boards as STM32MP15-Ecosystem-v1.0.0.

{|class="st_table"
!Boards !! PCBs list !! Content !! Availability
|-
| STM32MP157C-EV1 board (board with Crypto) || 
*MB1263C (Daughter)
*MB1262C (Mother)
*MB1230C (Display)
*MB1379A (Camera)
|| 
*STM32MP1 STM32MP157CAA3 Rev.B
*PMIC STPMIC1APQR cut1.2
* External oscillator
||Jan'19  
|-
| STM32MP157A-EV1 board (board without Crypto) || 
*MB1263C (Daughter)
*MB1262C (Mother)
*MB1230C (Display)
*MB1379A (Camera)
|| 
*STM32MP1 STM32MP157AAA3 Rev.B
*PMIC STPMIC1APQR cut1.2
* External oscillator
||Jan'19  
|-
| STM32MP157C-DK2 board (board with Crypto) || 
*MB1272C (Mother)
*MB1407B (Display)
||
*STM32MP1 STM32MP157CAC3 Rev.B
*PMIC STPMIC1APQR cut1.2
*External oscillator
 ||Jan'19 
|-
| STM32MP157A-DK1 board (board without Crypto) || 
*MB1272C (Mother)
||
*STM32MP1 STM32MP157AAC3 Rev.B
*PMIC STPMIC1APQR cut1.2
*External oscillator
 ||Jan'19 
|}

{{Info|STLINK in EVAL and DISCO Rev.C boards integrates the latest firmware STLINK (V2J32M22) which requires upgraded USB PC drivers - [https://www.st.com/content/st_com/en/products/development-tools/software-development-tools/stm32-software-development-tools/stm32-utilities/stsw-link009.html Windows USB driver]}}

=== Embedded software ===
==== OpenSTLinux (Cortex<sup>&reg;</sup>-A7)  ====
'''Openstlinux-20-02-19''' is the new version delivered with STM32MP15-Ecosystem-v1.2.0 release. This software set is constituted withconsists of the following components :
*Build process
**OpenEmbedded Thud (v2.6.4) 
**GCC version v8.2 
*Software components
** Kernel version LTS v4.19.94  {{STDarkBlue|''''' - NEW''''' version versus STM32MP15-Ecosystem-v1.1.0 release}}
**TF-A version v2.0
**U-Boot version v2018.11
**OP-TEE version v3.3.0 
**OpenOCD version v0.10.0
* Applicative components
** Weston version v5.0.0  
** GStreamer version v1.14.4
** GCnano version v6.2.4

*'''Main {{STDarkBlue|NEW}} features coming with STM32MP15-Ecosystem-v1.2.0 release
** AddAdded support offor STM32MP15x Rev.Z
** New SoC Part numbers D, F with 800 MHz support Added support for new 800 MHz part numbers (D and F) - [[STM32MP15_microprocessor]]
*** Operating points DT management wiki article - [[How_to_change_the_CPU_frequency]]
** Added support for DMA FIFO bypass (Direct mode)support.
** ** Added PINCTRL RSVD (Reserved) pin configuration to reserve pins for the co-processor.
** I2C SMBus Alert support
** coprocessor.
** Added support for I2C SMBus Alert 
** Added support for UART DMA TX/RX support
** 

** Added STMIPI02 DCMI/CSI convertor + Omnivision 5MP
** Added STMFX (GPIO expander) driver backport from kernel mainline (STM32MP157x-EV1)
** Added STPMIC driver backport from kernel mainline
** AddAdded SPI driver in U-boot
** AddAdded RTC driver for UEFI in U-boot
** Migrate qspiMigrated QUADSPI driver to spi-mem framework in U-boot
** ActivateActivated U-Boot ENV support in boot device (NOR/NAND/eMMC or SD card)

*'''Internal peripheralsperipheral assignment at boot time'''
:At boot time, you can select two kernel configurations:
::* Configuration 1: Allall internal peripherals are assigned to Cortex-A7 for Linux drivers,. Cortex-M4 coprocessing firmware TTY is executed by default.
::* Configuration 2: Somesome internal peripherals are assigned to Cortex-M4 to execute Cortex-M4 delivered examples on the board (EVAL or DISCO) see ([[STM32CubeMP1 Package#How to run the Examples|How to run Cortex-M4 examples]]).

:Configuration 1 is activated by default if you do not specify "2" in the U-Boot console.
:More information can be found in [[How to assign an internal peripheral to a runtime context]] article.
*'''Userland part''' 
**'''{{STDarkBlue|NEW}}''' This release introduces the [[Package_repository_for_OpenSTLinux_distribution|package repository]] service that enables the live installation of packages.
==== STM32CubeMP1 (Cortex<sup>&reg;</sup>-M4) ====
*''' Main {{STDarkBlue|NEW}} features coming with STM32CubeMP1-v1.2.0 version,  delivered withwithin STM32MP15-Ecosystem-v1.2.0 release :
** Add support of STM32MP15x Rev.Z
** New SoC Part numbers D, F with 800 MHz support 
** KEIL :
** Added support for STM32MP15x Rev.Z
** Added support for new 800 MHz part numbers (D, F) 
** Added Keil<sup>&reg;</sup> Project examples on STM32MP157C-DK2
** Added IAR<sup>&trade;</sup> Project examples on STM32MP157C-DK2
** Added CubeIDE Project examples on STM32MP157C-DK2
** New Added new PSRAM HAL driver
** Added RTC HAL + LL driver
** Added new FreeRTOS + OpenAMP new example

*'''Features already available in previous version'''
** The ''STM32Cube HAL'', ''STM32 abstraction layer embedded software'' ensuring maximized portability across the STM32 portfolio. HAL APIs are available for all peripherals.
** Low-layer APIs (LL) offering a fast lightweightlight-weight expert-oriented layer that is closer to the hardware than the HAL. LL APIs are available only for a set of peripherals.
** A consistent set of middleware components such as FreeRTOS, OpenAMP.
** All embedded software utilities, delivered with a full set of examples.

==== STM32MP15 distribution for Android (Cortex<sup>&reg;</sup>-A7) {{STDarkBlue|'''''- NEW'''''}} ====
''STM32MP15 distribution for Android&trade;'' v1.1.0 ('''st-android-10.0.0-2020-02-21''' tag) is the version delivered withwithin STM32MP15-Ecosystem-v1.2.0 release


Aim .

The objectives of this release are the following:
* '''Android&trade; 10.0.0''' porting on OpenSTLinux BSP v1.2.0 (TF-A, U-Boot, OP-TEE, Linux kernel), provided as '''demonstrator'''
* Android&trade; certifications are not ensured

See [[STM32MP15 distribution for Android release note - v1.1.0|STM32MP15 distribution for Android release note]] for more details.

=== STM32CubeProgrammer, Signing tool, Keygen ===
STM32CubeProgrammer v2.4.0 is the version delivered withwithin STM32MP15-Ecosystem-v1.2.0 release. This is an evolutive maintenance release for STM32CubeProgrammer.

*'''Main {{STDarkBlue|NEW}} features coming with STM32CubeProgrammer-v2.4.0 version, delivered withwithin STM32MP15-Ecosystem-v1.2.0 release: 

:* Flashload speed improvement over USB on Windows PC
:* Parallel programming on several targets

*'''Features already available in previous version'''
:* STM32CubeProg installer includes STM32CubeProgrammer, Keygen and Signing tools
:* Flashload SDCard, eMMC, NAND, NOR images through USB and UART for STM32MP157C-EV1, STM32MP157A-DK1, STM32MP157C-DK2 boards
:* Private and public keys generation
:* Images signature
:* Flashlayout file format change
:* STM32MP1 fuses management (with console interface only)
:* PMIC NVM management (with console interface only)

=== STM32CubeMX===
STM32CubeMX-v5.6 is the version delivered withwithin STM32MP15-Ecosystem-v1.2.0 release 

*'''Main {{STDarkBlue|NEW}} features coming with STM32CubeMX-v5.6 version, delivered withwithin STM32MP15-Ecosystem-v1.2.0 release 
:* New SoC part numbers D, F supportAdded support for new D and F part numbers:* Device tree (A7)
:** Device tree compliance with Openstlinux-20-02-19
:* DDR
:** LPDDRAdded support for LPDDR on 18x18, 16x16 packages
:** DDR Parameters tuning parameters saving

:*  STM32CubeMP1 (M4)
:** Compliant: see the [[#STM32CubeMX_2|restriction]] below in this article
:*  STM32CubeMP1 (M4)
:** Compliance with STM32CubeMP1 V1.2.0
:* Engineering mode support
:* SMBus alert bit support.Added support for Engineering mode 
:* Added support for SMBus alert bit:* PCC : Power data update
:* Tutorial Added tutorial Videos
:** DDR tuning [https://www.youtube.com/watch?v=FMGhBCKZ0Dk&feature=youtu.be]
:** How to customize a DT from aan ST board [https://www.youtube.com/watch?v=xZ5zqOqLWhI&feature=youtu.be]
{{Info|CubeMXSTM32CubeMX V5.6 indicates the manifest refers to '''Openstlinux-4.19-thud-mp1-20-02-19''' and this manifest manifest, which corresponds to '''Openstlinux-20-02-19''' tag}}

*'''Features already available in previous version'''
:* IOI/O muxing,  and clock treestree configuration
:* STM32MP1 contexts management (A7 non-secure, A7 secure, M4)
:* Device tree code generation 
:** dtsi and header filesfile inclusions
:** pinctrl and clocksclock generation
:** System-On-Chipon-chip device nodesnode positioning
:** multi-core related configurations (ETZPC binding, resources manager binding, peripheralsperipheral assignment).
{{Info|Note: theThe other device tree parameters must be filled in manually through user sections tagsection tags (from /* USER CODE BEGIN <node> */ to /* USER CODE END <node> */)}}
:* ST32MP1Cube code generation
:* Tuning of DDR settingstuning

=== STM32CubeIDE ===
'''STM32CubeIDE V1.3.0''' is the version delivered withwithin STM32MP15-Ecosystem-v1.2.0 release.

*'''Main {{STDarkBlue|NEW}} features coming with STM32CubeIDE V1.3.0 version, delivered withwithin STM32MP15-Ecosystem-v1.2.0 release 
** New SoC part numbers D, F support
Added support for new D and F part numbers
*'''Features already available in previous version'''
:* Cortex-M4 STM32CubeMP1 in "Production mode" and "Engineering mode"
:* Cortex-M4 Firmware compilation, load, debugloading and debugging:* PC Linux with Ethernet (recommended) or serial link
:* PC Windows with Ethernet or Ethernet over USB link
:* Cortex-M4 Firmware installation directory configurable

{{Info|Customers can continue to usego on using SW4STM32 IDE but the ST . However STMicroelectronics Eclipse reference is STM32CubeIDE. In case of support, ST will focus and recommend STM32CubeIDE toolSTMicroelectronics recommends the use of STM32CubeIDE tool and focuses on STM32CubeIDE support. SW4STM32 projects can be imported in STM32CubeIDE V1.3.0 - Migration process explained in  . Refer to  [[#Reference documents|Reference documents]] for explanations on the migration process.}}

=== Miscellaneous ===
* Detailed features are available in the release notes of the different items constitutingcomponents of this delivery.<br>

* See sections  [[#STM32MPU Embedded Software distribution detailed release notes|STM32MPU Embedded Software distribution detailed release notes]], [[#Referenced tools release notes | Referenced tools release notes ]] and [[#Reference documents|Reference documents]]

==Main restriction listrestrictions==
=== Embedded software ===
==== OpenSTLinux (Cortex<sup>&reg;</sup>-A7)  ====
* On STM32MP157C-DK2 boards, BT stack doesn't does not work any more after suspend / resume in Standby mode (function with Stop mode). TheThis issue is linked to the Murata WifiWi-Fi/BT module that expects the 3V3 3.3 V supply to be kept : in STM32MP1 Standby mode, , while this supply is switched off and so the Murata firmware is lost. A workaround can be put in place like for wifi in STM32MP1 Standby mode. A similar workaround as for Wi-Fi can be used ([https://github.com/STMicroelectronics/meta-st-stm32mp/blob/thud/recipes-connectivity/wifi/wifi-suspend.bb GitHub patch] with unbind/bind driver BT respectively before ). it consists in calling BT unbind and bind drivers before and after resume (modprobe -r hci_uart && modprobe hci_uart).


* For DDR initialization in TF-A, it is recommended to setup set up and to enable all "boot-on" and "always-on" regulators at bootloader stage, after DDR power initialization. Not yet implemented onThis is not yet implemented in V1.2.0 delivery and an . A patch is under preparationbeing prepared and will be pushedavailable on GithubGitHub.


==== STM32CubeMP1 (Cortex<sup>&reg;</sup>-M4) ====
* To avoid errors in OpenAMP when compiling in MDK-ARM IDE, you have to disable the « Use MicroLIB » in « Target » tab.

* The HAL RTC is delivered inwithin this release but it should be used with caution because the RTC is used by Linux, by default. However use it with caution since this driver is also used by Linux. To remove any risk of contention between Linux and the HAL, proceed as follows:
** The write protect (wpr) shouldmust be disabled by default and its shouldit must never be enabled in any driver (Linux nor HAL) 
.** The HAL should must use only use Alarm B, since Linux is only using Alarm Auses Alarm A.

** The RTC interrupt shouldmust be shared between Linux and the HAL, to be able to receive alarm notificationnotifications on each sideboth sides.


=== STM32CubeProgrammer, Signing tool,  and Keygen ===
* Flashload through UART fails
* Key generation is not functional with STM32MP_KeyGen_CLI on Linux withunder Ubuntu 16.04 (functional with Ubuntu 18.04)

=== STM32CubeMX===
* MR0 register for LPDDR settings is not set by CubeMXSTM32CubeMX in the generated device tree - Need to set manually this register at 0
* Warning : when you open a previous project (built with CubeMX versions. This register must be set manually at 0.
* DDR tuning parameters saving does not work when DDR Test Suite tool is used. Use U-Boot tag [https://github.com/STMicroelectronics/u-boot/releases/tag/v2018.11-stm32mp-r4.1 v2018.11-stm32mp-r4.1] on top of the {{EcosystemRelease | revision=1.2.0}}. This tag contains only one patch required by STM32CubeMX v5.6 ("ram: stm32mp1: display result for software read DQS gating").
* Warning: when opening a previous project built with STM32CubeMX version older than V5.6), the migration willdoes not take into account the user sectionssection part. This part needs to be updated manually according the Openstlinux-20-02-19 manifest.


=== STM32CubeIDE ===
* Using OpenOCD with ST-LINK does not check and force ST-LINK firmware update at debug launch. It is therefore recommended to manually update to the latest ST-LINK firmware for the best debug experience. Use the menu: Help > ST-LINK Upgrade menu"

=== Miscelleanous ===RestrictionsRestriction lists are available in each sub-componentsubcomponent release note, accessible from . They are available in the following chapters in this samethe present article:
* [[#STM32MPU Embedded Software distribution detailed release notes|STM32MPU Embedded Software distribution detailed release notes]]
* [[#Referenced tools release notes |Referenced tools release notes]]

Moreover, the software workarounds implemented in the ecosystem to answer provide solutions to the STM32MPU device errata are listed in [[STM32MP15 ecosystem errata sheet]].

==Minor release updates ==
STMicroelectronics regularly delivers updates through the following github<sup>&reg;</sup> components which are :  [https://github.com/STMicroelectronics/arm-trusted-firmware tf-a], [https://github.com/STMicroelectronics/u-boot/ u-boot], [https://github.com/STMicroelectronics/optee_os optee-os],  [https://github.com/STMicroelectronics/linux Linux kernel]. <br>

You can decide to incorporate them into your Developer Package (please refer to [[STM32MP1 Developer Package]]) or Distribution Package (see below).<br/>


To update the Distribution package please , proceed as followfollows:
:# Switch your Distribution package [[OpenSTLinux_distribution#Reference_source_code|reference source code]] to github mode 
.:# Use the command ''' [[OpenEmbedded_-_devtool#devtool_modify|devtool modify]] <recipe name>''' command to have direct access to the source code git repository used by the build process.

:# In the freshly cloned source code, checkout check out the revision you want to start from via '''git checkout  -b WORK <github<sup>&reg;</sup> TAG>'''


More rarely and independently, STMicroelectronics also delivers .

STMicroelectronics also delivers dedicated fixes on layers through github<sup>&reg;</sup>. These changes can be integrated (via [[git]] commands) into your local [[STM32MP1 Distribution Package]] environment. Please find below Below the github<sup>&reg;</sup> links of the quotedcorresponding to each layers :
* [https://github.com/STMicroelectronics/meta-st-stm32mp/ meta-st-stm32mp]
* [https://github.com/STMicroelectronics/meta-st-openstlinux/ meta-st-openstlinux ]
* [https://github.com/STMicroelectronics/meta-st-stm32mp-addons/ meta-st-stm32mp-addons]

===v1.2.1===
[[STM32MP15_OpenSTLinux_release_note_-_v1.2.0#v1.2.1 |OpenSTLinux updates v1.2.1]]<br>


==Reference documents==
{{:STM32MP15 resources - v1.2.0}}

== How to get{{ReviewsComments|-- [[User:Emmanuel Combette|Emmanuel Combette]] ([[User talk:Emmanuel Combette|talk]]) 10:55, 5 May 2020 (CEST)<br />Add : AN5431 The-stpmic1-pcb-layout-guidlines-stmicroelectronics.pdf}}
== How to download the software and start with this release? ==
'''The list of embedded software packages available for download depends on the selected package'''.

The table below provides the available board part numbers and the source of as well as information in order to:
*Getget started with one of the three available Packages (Starter, Developer or Distribution Packages)
*GetPackage)
*get started with the board
*Findfind the associated embedded software distributions 
*'''Downloaddownload''' source code 
*'''Buildbuild''' an embedded software 
{| class="st-table"
|-
! style="width: 50%;" | Board part number
! style=" width:50%" | Jump to
|-style="text-align: center;"   
| '''STM32MP157C-EV1'''<br>Evaluation board
|| [[STM32MP15 Evaluation boards - getting started|STM32MP15 Evaluation boards - getting started, including software download]]
|-style="text-align: center;"   
| '''STM32MP157X-DKX'''<br>Discovery kit
|| [[STM32MP15 Discovery kits - getting started|STM32MP15 Discovery kits - getting started, including software download]]
|}

==STM32MPU Embedded Software distribution detailed release notes==
The table below lists the software packages available in the STM32MPU Embedded Software distributions, and provides the corresponding release notes.<br>

The release notes providegive more information and details about the features and content of each packagethe packages. <br>
The release notes does They do not explain how to get download the software. For that, refer chapter Refer to [[#How to get the software and start with this release?|How to get the software and start with this release ]].


{|class="st-table" style="width: 98%;" 
|-
| | ''' Firmware ''' </font>

| ''' Release note''' </font>

|''' Version ''' </font>

|-
| | OpenSTLinux Distribution
| | [[STM32MP15 OpenSTLinux release note - v1.2.0]]
| | openstlinux-20-02-19
|-
| | STM32Cube MPU Package
| | [[STM32CubeMP1 Package release note - v1.2.0]]
| | STM32CubeMP1-v1.2.0
|-
| | STM32 MPU Distribution for Android
| | [[STM32MP15 distribution for Android release note - v1.1.0]]
| | st-android-10.0.0-2020-02-21
|}

==Referenced tools release notes ==
The table below lists the available tools, and provides links to the respectivecorresponding release notes.

Each release note providesgives information on how to install and use the corresponding tool.

The set of tools to that can be downloaded depends on the Package to bethat is used (double check [[Which Package better suits your needs]] article to find for more information on each Package).

{|class="st-table" style="text-align:center; width:95%; cellspacing=0"
|-
|| ''' Tools''' 
|| ''' Release notes'''
| colspan='2' | ''' Host PC''' 
| colspan='3' |'''Which Package may need the tool ?'''
|-
||
|| 
|| ''' Linux version '''
|| ''' Windows version ''' 
|| ''' Starter Package''' 
|| ''' Developer Package''' 
|| ''' Distribution Package''' 
|-
|| STM32CubeIDE
|| [[STM32CubeIDE_release_note]]
|| 1.3.0
|| 1.3.0
|| <span style="font-size:21px"></span>

|| <span style="font-size:21px"></span>

|| <span style="font-size:21px"></span>

|-
|| STM32CubeMX
|| [https://www.st.com/en/development-tools/stm32cubemx.html STM32CubeMX release note] 
|| from 5.6
|| from 5.6
||<span style="font-size:21px"></span>

|| <span style="font-size:21px"></span>

|| <span style="font-size:21px"></span>

|-
||STM32CubeProg  
|| [[STM32CubeProgrammer release note]] 
|| 2.4.0
|| 2.4.0
|| <span style="font-size:21px"></span>

|| <span style="font-size:21px"></span>

||<span style="font-size:21px"></span>

|-
||Keygen
||[[KeyGen release note]]
|| 1.0.0
|| 1.0.0
|| <span style="font-size:21px"></span>

|| <span style="font-size:21px"></span>

|| <span style="font-size:21px"></span> 

|-
|| Signing tool
||[[Signing tool release note]]
|| 1.0.0
|| 1.0.0
|| <span style="font-size:21px"></span>

|| <span style="font-size:21px"></span>

|| <span style="font-size:21px"></span>

|}

==References==<references/>

<noinclude>

[[Category:Release notes archives]]
{{PublicationRequestId| 15059 | 2020-20-21 | AnneJ}}</noinclude>
(47 intermediate revisions by 5 users not shown)
Line 1: Line 1:
This article aims to describe the content of the release '''''STM32MP15-Ecosystem-v1.2.0''''' for ''STM32MPU Embedded Software distributions'' and its associated ecosystem.
+
The objective of this article is to describe the content of '''''STM32MP15-Ecosystem-v1.2.0''''' release of ''STM32MPU Embedded Software distributions'' and its associated ecosystem.
   
 
==Delivery purpose and scope==
 
==Delivery purpose and scope==
The new STM32MP15-Ecosystem-v1.2.0 release, dedicated to STM32MP15 microprocessors, is an evolutive maintenance release, including minor evolutions and corrections.  
+
The new STM32MP15-Ecosystem-v1.2.0 release is dedicated to STM32MP15 microprocessors. It is an evolutive maintenance release that includes minor evolutions and corrections.  
   
The release, as the previous one, aims:
+
Like previous release, STM32MP15-Ecosystem-v1.2.0 aims at
* to provide a full ecosystem for STM32MP15x devices.
+
* providing a full ecosystem for STM32MP15x devices
* to work efficiently with STM32MP15 boards, using one of the packages (Starter Package, Developer Package, Distribution Package) developed by STMicroelectronics for STM32MPUs. <br>
+
* working efficiently with STM32MP15 boards, using one of the packages (Starter Package, Developer Package or Distribution Package) developed by STMicroelectronics for STM32 MPUs. <br>
See [[Which Package better suits your needs]] for more information on these packages.
+
Refer to [[Which Package better suits your needs]] for more information on these packages.
   
   
This ecosystem release is constituted by:
+
This ecosystem release consists of:
* '''Two STM32MPU distributions '''
+
* '''two STM32MPU distributions '''
:* The ''STM32MPU Embedded Software distribution''
+
:* the ''STM32MPU Embedded Software distribution''
:* The ''STM32MPU Embedded Software distribution for Android''
+
:* the ''STM32MPU Embedded Software distribution for Android''
   
* '''The STM32 referenced tools'''
+
* STM32 referenced tools'''
:*STM32CubeIDE - New STM32 IDE targeted to replace SW4STM32 (STM32-CoPro-MPU Eclipse plugin)  
+
:*STM32CubeIDE - new STM32 IDE targeted to replace SW4STM32 (STM32-CoPro-MPU Eclipse plugin)  
 
:*STM32CubeMX
 
:*STM32CubeMX
 
:*STM32CubeProgrammer
 
:*STM32CubeProgrammer
 
:*Keygen tool
 
:*Keygen tool
 
:*Signing tool
 
:*Signing tool
:(more details in [[#Referenced tools release notes |chapter]] below)
+
:For more details refer to [[#Referenced tools release notes |Referenced tools release notes ]] chapter below.
   
 
* '''Documentation '''
 
* '''Documentation '''
:* This user guide (wiki format)
+
:* The present user guide in wiki format  
:* Documentation package (more details in [[#Reference_documents|chapter]] below)
+
:* Documentation package (for more details refer to [[#Reference_documents|Reference documents]] chapter below)
   
 
* ''' Supported STM32MP15 boards'''
 
* ''' Supported STM32MP15 boards'''
 
:*STM32MP15 Evaluation board ( for "STM32MPU Embedded Software distribution" and "STM32MPU Embedded Software distribution for Android")
 
:*STM32MP15 Evaluation board ( for "STM32MPU Embedded Software distribution" and "STM32MPU Embedded Software distribution for Android")
 
:*STM32MP15 Discovery kit (for ''STM32MPU Embedded Software distribution'')
 
:*STM32MP15 Discovery kit (for ''STM32MPU Embedded Software distribution'')
:(more details in [[#Boards|chapter]] below)
+
:More details ca nbe found in [[#Boards|Board]] chapter below.
   
 
==Intended audience==
 
==Intended audience==
The targeted audience consists in STMicroelectronics customers.
+
The targeted audience is STMicroelectronics customers.
   
 
==Licensing==
 
==Licensing==
This software package is licensed under SOFTWARE LICENSE AGREEMENT, the "SLA". Customer may not use this package except in compliance with the [[OpenSTLinux licenses - v1.2.0#Top Software license agreement (SLA) and third-party licences|software license agreement (SLA)]].
+
This software package is licensed under a SOFTWARE LICENSE AGREEMENT FOR ST MATERIALS (SLA). The customers may not use this package except in compliance with the [[LegalInformation:OpenSTLinux licenses - v1.2.0#Top Software license agreement (SLA) and third-party licences|software license agreement (SLA)]].
   
 
==Main features / main highlights==
 
==Main features / main highlights==
 
=== Boards ===
 
=== Boards ===
Boards supported with this STM32MP15-Ecosystem-v1.2.0 release are the same than those supported with the STM32MP15-Ecosystem-v1.0.0.
+
This STM32MP15-Ecosystem-v1.2.0 release supports the same boards as STM32MP15-Ecosystem-v1.0.0.
   
 
{|class="st_table"
 
{|class="st_table"
Line 90: Line 90:
 
=== Embedded software ===
 
=== Embedded software ===
 
==== OpenSTLinux (Cortex<sup>&reg;</sup>-A7)  ====
 
==== OpenSTLinux (Cortex<sup>&reg;</sup>-A7)  ====
'''Openstlinux-20-02-19''' is the new version delivered with STM32MP15-Ecosystem-v1.2.0 release. This software set is constituted with following components :
+
'''Openstlinux-20-02-19''' is the new version delivered with STM32MP15-Ecosystem-v1.2.0 release. This software set consists of the following components:
 
*Build process
 
*Build process
 
**OpenEmbedded Thud (v2.6.4)  
 
**OpenEmbedded Thud (v2.6.4)  
Line 106: Line 106:
   
 
*'''Main {{STDarkBlue|NEW}} features coming with STM32MP15-Ecosystem-v1.2.0 release
 
*'''Main {{STDarkBlue|NEW}} features coming with STM32MP15-Ecosystem-v1.2.0 release
** Add support of STM32MP15x Rev.Z
+
** Added support for STM32MP15x Rev.Z
** New SoC Part numbers D, F with 800 MHz support - [[STM32MP15_microprocessor]]
+
** Added support for new 800 MHz part numbers (D and F) - [[STM32MP15_microprocessor]]
 
*** Operating points DT management wiki article - [[How_to_change_the_CPU_frequency]]
 
*** Operating points DT management wiki article - [[How_to_change_the_CPU_frequency]]
** DMA FIFO bypass (Direct mode) support.
+
** Added support for DMA FIFO bypass (Direct mode)
** PINCTRL RSVD (Reserved) pin configuration to reserve pins for the co-processor.
+
** Added PINCTRL RSVD (Reserved) pin configuration to reserve pins for the coprocessor.
** I2C SMBus Alert support
+
** Added support for I2C SMBus Alert  
** UART DMA TX/RX support
+
** Added support for UART DMA TX/RX  
** STMIPI02 DCMI/CSI convertor + Omnivision 5MP
+
** Added STMIPI02 DCMI/CSI convertor + Omnivision 5MP
** STMFX (GPIO expander) driver backport from kernel mainline (STM32MP157x-EV1)
+
** Added STMFX (GPIO expander) driver backport from kernel mainline (STM32MP157x-EV1)
** STPMIC driver backport from kernel mainline
+
** Added STPMIC driver backport from kernel mainline
** Add SPI driver in U-boot
+
** Added SPI driver in U-boot
** Add RTC driver for UEFI in U-boot
+
** Added RTC driver for UEFI in U-boot
** Migrate qspi driver to spi-mem framework in U-boot
+
** Migrated QUADSPI driver to spi-mem framework in U-boot
** Activate U-Boot ENV support in boot device (NOR/NAND/eMMC or SD card)
+
** Activated U-Boot ENV support in boot device (NOR/NAND/eMMC or SD card)
   
*'''Internal peripherals assignment at boot time'''
+
*'''Internal peripheral assignment at boot time'''
:At boot, you can select two kernel configurations:
+
:At boot time, you can select two kernel configurations:
::* Configuration 1: All internal peripherals assigned to Cortex-A7 for Linux drivers, Cortex-M4 coprocessing firmware TTY executed by default.
+
::* Configuration 1: all internal peripherals are assigned to Cortex-A7 for Linux drivers. Cortex-M4 coprocessing firmware TTY is executed by default.
::* Configuration 2: Some internal peripherals assigned to Cortex-M4 to execute Cortex-M4 delivered examples on the board (EVAL or DISCO) see ([[STM32CubeMP1 Package#How to run the Examples|How to run Cortex-M4 examples]]).
+
::* Configuration 2: some internal peripherals are assigned to Cortex-M4 to execute Cortex-M4 delivered examples on the board (EVAL or DISCO) see ([[STM32CubeMP1 Package#How to run the Examples|How to run Cortex-M4 examples]]).
   
 
:Configuration 1 is activated by default if you do not specify "2" in the U-Boot console.
 
:Configuration 1 is activated by default if you do not specify "2" in the U-Boot console.
 
:More information can be found in [[How to assign an internal peripheral to a runtime context]] article.
 
:More information can be found in [[How to assign an internal peripheral to a runtime context]] article.
  +
  +
*'''Userland part'''
  +
**'''{{STDarkBlue|NEW}}''' This release introduces the [[Package_repository_for_OpenSTLinux_distribution|package repository]] service that enables the live installation of packages.
   
 
==== STM32CubeMP1 (Cortex<sup>&reg;</sup>-M4) ====
 
==== STM32CubeMP1 (Cortex<sup>&reg;</sup>-M4) ====
*''' Main {{STDarkBlue|NEW}} features coming with STM32CubeMP1-v1.2.0 version,  delivered with STM32MP15-Ecosystem-v1.2.0 release :
+
*''' Main {{STDarkBlue|NEW}} features coming with STM32CubeMP1-v1.2.0 version,  delivered within STM32MP15-Ecosystem-v1.2.0 release:
** Add support of STM32MP15x Rev.Z
+
** Added support for STM32MP15x Rev.Z
** New SoC Part numbers D, F with 800 MHz support
+
** Added support for new 800 MHz part numbers (D, F)
** KEIL Project examples on STM32MP157C-DK2
+
** Added Keil<sup>&reg;</sup> Project examples on STM32MP157C-DK2
** IAR Project examples on STM32MP157C-DK2
+
** Added IAR<sup>&trade;</sup> Project examples on STM32MP157C-DK2
** CubeIDE Project examples on STM32MP157C-DK2
+
** Added CubeIDE Project examples on STM32MP157C-DK2
** New PSRAM HAL driver
+
** Added new PSRAM HAL driver
** RTC HAL + LL driver
+
** Added RTC HAL + LL driver
** FreeRTOS + OpenAMP new example
+
** Added new FreeRTOS + OpenAMP example
   
 
*'''Features already available in previous version'''
 
*'''Features already available in previous version'''
 
** The ''STM32Cube HAL'', ''STM32 abstraction layer embedded software'' ensuring maximized portability across the STM32 portfolio. HAL APIs are available for all peripherals.
 
** The ''STM32Cube HAL'', ''STM32 abstraction layer embedded software'' ensuring maximized portability across the STM32 portfolio. HAL APIs are available for all peripherals.
** Low-layer APIs (LL) offering a fast lightweight expert-oriented layer that is closer to the hardware than the HAL. LL APIs are available only for a set of peripherals.
+
** Low-layer APIs (LL) offering a fast light-weight expert-oriented layer that is closer to the hardware than the HAL. LL APIs are available only for a set of peripherals.
 
** A consistent set of middleware components such as FreeRTOS, OpenAMP.
 
** A consistent set of middleware components such as FreeRTOS, OpenAMP.
 
** All embedded software utilities, delivered with a full set of examples.
 
** All embedded software utilities, delivered with a full set of examples.
   
 
==== STM32MP15 distribution for Android (Cortex<sup>&reg;</sup>-A7) {{STDarkBlue|'''''- NEW'''''}} ====
 
==== STM32MP15 distribution for Android (Cortex<sup>&reg;</sup>-A7) {{STDarkBlue|'''''- NEW'''''}} ====
''STM32MP15 distribution for Android&trade;'' v1.1.0 ('''st-android-10.0.0-2020-02-21''' tag) is the version delivered with STM32MP15-Ecosystem-v1.2.0 release
+
''STM32MP15 distribution for Android&trade;'' v1.1.0 ('''st-android-10.0.0-2020-02-21''' tag) is the version delivered within STM32MP15-Ecosystem-v1.2.0 release.
   
Aim of this release:
+
The objectives of this release are the following:
 
* '''Android&trade; 10.0.0''' porting on OpenSTLinux BSP v1.2.0 (TF-A, U-Boot, OP-TEE, Linux kernel), provided as '''demonstrator'''
 
* '''Android&trade; 10.0.0''' porting on OpenSTLinux BSP v1.2.0 (TF-A, U-Boot, OP-TEE, Linux kernel), provided as '''demonstrator'''
 
* Android&trade; certifications are not ensured
 
* Android&trade; certifications are not ensured
Line 156: Line 159:
   
 
=== STM32CubeProgrammer, Signing tool, Keygen ===
 
=== STM32CubeProgrammer, Signing tool, Keygen ===
STM32CubeProgrammer v2.4.0 is the version delivered with STM32MP15-Ecosystem-v1.2.0 release. This is an evolutive maintenance release for STM32CubeProgrammer.
+
STM32CubeProgrammer v2.4.0 is the version delivered within STM32MP15-Ecosystem-v1.2.0 release. This is an evolutive maintenance release for STM32CubeProgrammer.
   
*'''Main {{STDarkBlue|NEW}} features coming with STM32CubeProgrammer-v2.4.0 version, delivered with STM32MP15-Ecosystem-v1.2.0 release  
+
*'''Main {{STDarkBlue|NEW}} features coming with STM32CubeProgrammer-v2.4.0 version, delivered within STM32MP15-Ecosystem-v1.2.0 release:
 
:* Flashload speed improvement over USB on Windows PC
 
:* Flashload speed improvement over USB on Windows PC
 
:* Parallel programming on several targets
 
:* Parallel programming on several targets
Line 172: Line 175:
   
 
=== STM32CubeMX===
 
=== STM32CubeMX===
STM32CubeMX-v5.6 is the version delivered with STM32MP15-Ecosystem-v1.2.0 release  
+
STM32CubeMX-v5.6 is the version delivered within STM32MP15-Ecosystem-v1.2.0 release  
   
*'''Main {{STDarkBlue|NEW}} features coming with STM32CubeMX-v5.6 version, delivered with STM32MP15-Ecosystem-v1.2.0 release  
+
*'''Main {{STDarkBlue|NEW}} features coming with STM32CubeMX-v5.6 version, delivered within STM32MP15-Ecosystem-v1.2.0 release  
:* New SoC part numbers D, F support
+
:* Added support for new D and F part numbers
 
:* Device tree (A7)
 
:* Device tree (A7)
 
:** Device tree compliance with Openstlinux-20-02-19
 
:** Device tree compliance with Openstlinux-20-02-19
 
:* DDR
 
:* DDR
:** LPDDR support on 18x18, 16x16 packages
+
:** Added support for LPDDR on 18x18, 16x16 packages
:** DDR Parameters saving
+
:** DDR tuning parameters saving: see the [[#STM32CubeMX_2|restriction]] below in this article
 
:*  STM32CubeMP1 (M4)
 
:*  STM32CubeMP1 (M4)
:** Compliant with STM32CubeMP1 V1.2.0
+
:** Compliance with STM32CubeMP1 V1.2.0
:* Engineering mode support
+
:* Added support for Engineering mode  
:* SMBus alert bit support.
+
:* Added support for SMBus alert bit
 
:* PCC : Power data update
 
:* PCC : Power data update
:* Tutorial Videos
+
:* Added tutorial Videos
 
:** DDR tuning [https://www.youtube.com/watch?v=FMGhBCKZ0Dk&feature=youtu.be]
 
:** DDR tuning [https://www.youtube.com/watch?v=FMGhBCKZ0Dk&feature=youtu.be]
:** How to customize a DT from a ST board [https://www.youtube.com/watch?v=xZ5zqOqLWhI&feature=youtu.be]
+
:** How to customize a DT from an ST board [https://www.youtube.com/watch?v=xZ5zqOqLWhI&feature=youtu.be]
{{Info|CubeMX V5.6 indicates the manifest '''Openstlinux-4.19-thud-mp1-20-02-19''' and this manifest corresponds to '''Openstlinux-20-02-19''' tag}}
+
{{Info|STM32CubeMX V5.6 refers to '''Openstlinux-4.19-thud-mp1-20-02-19''' manifest, which corresponds to '''Openstlinux-20-02-19''' tag}}
   
 
*'''Features already available in previous version'''
 
*'''Features already available in previous version'''
:* IO muxing, clock trees configuration
+
:* I/O muxing and clock tree configuration
 
:* STM32MP1 contexts management (A7 non-secure, A7 secure, M4)
 
:* STM32MP1 contexts management (A7 non-secure, A7 secure, M4)
 
:* Device tree code generation  
 
:* Device tree code generation  
:** dtsi and header files inclusions
+
:** dtsi and header file inclusions
:** pinctrl and clocks generation
+
:** pinctrl and clock generation
:** System-On-Chip device nodes positioning
+
:** System-on-chip device node positioning
:** multi-core related configurations (ETZPC binding, resources manager binding, peripherals assignment).
+
:** multi-core related configurations (ETZPC binding, resources manager binding, peripheral assignment).
{{Info|Note: the other device tree parameters must be filled in manually through user sections tag (from /* USER CODE BEGIN <node> */ to /* USER CODE END <node> */)}}
+
{{Info|Note: The other device tree parameters must be filled in manually through user section tags (from /* USER CODE BEGIN <node> */ to /* USER CODE END <node> */)}}
 
:* ST32MP1Cube code generation
 
:* ST32MP1Cube code generation
:* DDR settings tuning
+
:* Tuning of DDR settings
   
 
=== STM32CubeIDE ===
 
=== STM32CubeIDE ===
'''STM32CubeIDE V1.3.0''' is the version delivered with STM32MP15-Ecosystem-v1.2.0 release.
+
'''STM32CubeIDE V1.3.0''' is the version delivered within STM32MP15-Ecosystem-v1.2.0 release.
   
*'''Main {{STDarkBlue|NEW}} features coming with STM32CubeIDE V1.3.0 version, delivered with STM32MP15-Ecosystem-v1.2.0 release  
+
*'''Main {{STDarkBlue|NEW}} features coming with STM32CubeIDE V1.3.0 version, delivered within STM32MP15-Ecosystem-v1.2.0 release  
** New SoC part numbers D, F support
+
** Added support for new D and F part numbers
   
 
*'''Features already available in previous version'''
 
*'''Features already available in previous version'''
 
:* Cortex-M4 STM32CubeMP1 in "Production mode" and "Engineering mode"
 
:* Cortex-M4 STM32CubeMP1 in "Production mode" and "Engineering mode"
:* Cortex-M4 Firmware compilation, load, debug
+
:* Cortex-M4 Firmware compilation, loading and debugging
 
:* PC Linux with Ethernet (recommended) or serial link
 
:* PC Linux with Ethernet (recommended) or serial link
 
:* PC Windows with Ethernet or Ethernet over USB link
 
:* PC Windows with Ethernet or Ethernet over USB link
 
:* Cortex-M4 Firmware installation directory configurable
 
:* Cortex-M4 Firmware installation directory configurable
   
{{Info|Customers can continue to use SW4STM32 IDE but the ST Eclipse reference is STM32CubeIDE. In case of support, ST will focus and recommend STM32CubeIDE tool. SW4STM32 projects can be imported in STM32CubeIDE V1.3.0 - Migration process explained in [[#Reference documents|Reference documents]]}}
+
{{Info|Customers can go on using SW4STM32 IDE. However STMicroelectronics Eclipse reference is STM32CubeIDE. STMicroelectronics recommends the use of STM32CubeIDE tool and focuses on STM32CubeIDE support. SW4STM32 projects can be imported in STM32CubeIDE V1.3.0. Refer to [[#Reference documents|Reference documents]] for explanations on the migration process.}}
   
 
=== Miscellaneous ===
 
=== Miscellaneous ===
* Detailed features are available in the release notes of the different items constituting this delivery.<br>
+
* Detailed features are available in the release notes of the different components of this delivery.<br>
 
* See sections  [[#STM32MPU Embedded Software distribution detailed release notes|STM32MPU Embedded Software distribution detailed release notes]], [[#Referenced tools release notes | Referenced tools release notes ]] and [[#Reference documents|Reference documents]]
 
* See sections  [[#STM32MPU Embedded Software distribution detailed release notes|STM32MPU Embedded Software distribution detailed release notes]], [[#Referenced tools release notes | Referenced tools release notes ]] and [[#Reference documents|Reference documents]]
   
==Main restriction list==
+
==Main restrictions==
 
=== Embedded software ===
 
=== Embedded software ===
 
==== OpenSTLinux (Cortex<sup>&reg;</sup>-A7)  ====
 
==== OpenSTLinux (Cortex<sup>&reg;</sup>-A7)  ====
* On STM32MP157C-DK2 boards, BT stack doesn't work any more after suspend / resume in Standby mode (function with Stop mode). The issue linked to the Murata Wifi/BT module that expects the 3V3 supply to be kept : in STM32MP1 Standby mode, this supply is switched off and so the Murata firmware is lost. A workaround can be put in place like for wifi [https://github.com/STMicroelectronics/meta-st-stm32mp/blob/thud/recipes-connectivity/wifi/wifi-suspend.bb GitHub patch] with unbind/bind driver BT respectively before after resume (modprobe -r hci_uart && modprobe hci_uart)
+
* On STM32MP157C-DK2 boards, BT stack does not work any more after suspend / resume in Standby mode (function with Stop mode). This issue is linked to the Murata Wi-Fi/BT module that expects the 3.3 V supply to be kept, while this supply is switched off in STM32MP1 Standby mode. A similar workaround as for Wi-Fi can be used ([https://github.com/STMicroelectronics/meta-st-stm32mp/blob/thud/recipes-connectivity/wifi/wifi-suspend.bb GitHub patch]). it consists in calling BT unbind and bind drivers before and after resume (modprobe -r hci_uart && modprobe hci_uart).
   
* For DDR initialization in TF-A, it is recommended to setup and to enable all "boot-on" and "always-on" regulators at bootloader stage, after DDR power initialization. Not yet implemented on V1.2.0 delivery and an patch is under preparation and will be pushed on Github
+
* For DDR initialization in TF-A, it is recommended to set up and enable all "boot-on" and "always-on" regulators at bootloader stage, after DDR power initialization. This is not yet implemented in V1.2.0 delivery. A patch is being prepared and will be available on GitHub.
   
 
==== STM32CubeMP1 (Cortex<sup>&reg;</sup>-M4) ====
 
==== STM32CubeMP1 (Cortex<sup>&reg;</sup>-M4) ====
* To avoid errors in OpenAMP when compiling in MDK-ARM IDE, you have to disable the « Use MicroLIB » in « Target » tab
+
* To avoid errors in OpenAMP when compiling in MDK-ARM IDE, disable the « Use MicroLIB » in « Target » tab.
* The HAL RTC is delivered in this release but it should be used with caution because the RTC is used by Linux, by default. To remove any risk of contention between Linux and the HAL:
+
* The HAL RTC is delivered within this release. However use it with caution since this driver is also used by Linux. To remove any risk of contention between Linux and the HAL, proceed as follows:
** The write protect (wpr) should be disabled by default and its should never be enabled in any driver (Linux nor HAL)  
+
** The write protect (wpr) must be disabled by default and it must never be enabled in any driver (Linux nor HAL).
** The HAL should only use Alarm B, since Linux is only using Alarm A
+
** The HAL must use only Alarm B, since Linux uses Alarm A.
** The RTC interrupt should be shared between Linux and the HAL, to be able to receive alarm notification on each side
+
** The RTC interrupt must be shared between Linux and the HAL to be able to receive alarm notifications on both sides.
   
=== STM32CubeProgrammer, Signing tool, Keygen ===
+
=== STM32CubeProgrammer, Signing tool and Keygen ===
 
* Flashload through UART fails
 
* Flashload through UART fails
* Key generation not functional with STM32MP_KeyGen_CLI on Linux with Ubuntu 16.04 (functional with Ubuntu 18.04)
+
* Key generation is not functional with STM32MP_KeyGen_CLI on Linux under Ubuntu 16.04 (functional with Ubuntu 18.04)
   
 
=== STM32CubeMX===
 
=== STM32CubeMX===
* MR0 register for LPDDR settings not set by CubeMX in the generated device tree - Need to set manually this register at 0
+
* MR0 register for LPDDR settings is not set by STM32CubeMX in the generated device tree. This register must be set manually at 0.
* Warning : when you open a previous project (built with CubeMX versions older than V5.6), the migration will not take into account the user sections part. This part needs to be updated manually according the Openstlinux-20-02-19 manifest
+
* DDR tuning parameters saving does not work when DDR Test Suite tool is used. Use U-Boot tag [https://github.com/STMicroelectronics/u-boot/releases/tag/v2018.11-stm32mp-r4.1 v2018.11-stm32mp-r4.1] on top of the {{EcosystemRelease | revision=1.2.0}}. This tag contains only one patch required by STM32CubeMX v5.6 ("ram: stm32mp1: display result for software read DQS gating").
  +
* Warning: when opening a previous project built with STM32CubeMX version older than V5.6, the migration does not take into account the user section part. This part needs to be updated manually according the Openstlinux-20-02-19 manifest.
   
 
=== STM32CubeIDE ===
 
=== STM32CubeIDE ===
* Using OpenOCD with ST-LINK does not check and force ST-LINK firmware update at debug launch. It is therefore recommended to manually update to the latest ST-LINK firmware for the best debug experience. Use the menu: Help > ST-LINK Upgrade"
+
* Using OpenOCD with ST-LINK does not check and force ST-LINK firmware update at debug launch. It is therefore recommended to manually update to the latest ST-LINK firmware for the best debug experience. Use the Help > ST-LINK Upgrade menu"
   
 
=== Miscelleanous ===
 
=== Miscelleanous ===
Restrictions lists are available in each sub-component release note, accessible from the following chapters in this same article:
+
Restriction lists are available in each subcomponent release note. They are available in the following chapters in the present article:
 
* [[#STM32MPU Embedded Software distribution detailed release notes|STM32MPU Embedded Software distribution detailed release notes]]
 
* [[#STM32MPU Embedded Software distribution detailed release notes|STM32MPU Embedded Software distribution detailed release notes]]
 
* [[#Referenced tools release notes |Referenced tools release notes]]
 
* [[#Referenced tools release notes |Referenced tools release notes]]
   
Moreover, the software workarounds implemented in the ecosystem to answer to the STM32MPU device errata are listed in [[STM32MP15 ecosystem errata sheet]].
+
Moreover, the software workarounds implemented in the ecosystem to provide solutions to the STM32MPU device errata are listed in [[STM32MP15 ecosystem errata sheet]].
   
 
==Minor release updates ==
 
==Minor release updates ==
STMicroelectronics regularly delivers updates through github<sup>&reg;</sup> components which are [https://github.com/STMicroelectronics/arm-trusted-firmware tf-a], [https://github.com/STMicroelectronics/u-boot/ u-boot], [https://github.com/STMicroelectronics/optee_os optee-os],  [https://github.com/STMicroelectronics/linux Linux kernel]. <br>
+
STMicroelectronics regularly delivers updates through the following github<sup>&reg;</sup> components[https://github.com/STMicroelectronics/arm-trusted-firmware tf-a], [https://github.com/STMicroelectronics/u-boot/ u-boot], [https://github.com/STMicroelectronics/optee_os optee-os],  [https://github.com/STMicroelectronics/linux Linux kernel]. <br>
You can decide to incorporate them into your Developer Package (please refer to [[STM32MP1 Developer Package]]) or Distribution Package (see below).<br/>
+
You can decide to incorporate them into your Developer Package (refer to [[STM32MP1 Developer Package]] or Distribution Package below).<br/>
   
To update the Distribution package please proceed as follow:
+
To update the Distribution package, proceed as follows:
:# Switch your Distribution package [[OpenSTLinux_distribution#Reference_source_code|reference source code]] to github mode  
+
:# Switch your Distribution package [[OpenSTLinux_distribution#Reference_source_code|reference source code]] to github mode.
:# Use the command ''' [[OpenEmbedded_-_devtool#devtool_modify|devtool modify]] <recipe name>''' to have direct access to the source code git repository used by the build process
+
:# Use the ''' [[OpenEmbedded_-_devtool#devtool_modify|devtool modify]] <recipe name>''' command to have direct access to the source code git repository used by the build process.
:# In the freshly cloned source code, checkout the revision you want to start from via '''git checkout  -b WORK <github<sup>&reg;</sup> TAG>'''
+
:# In the freshly cloned source code, check out the revision you want to start from via '''git checkout  -b WORK <github<sup>&reg;</sup> TAG>'''.
   
More rarely and independently, STMicroelectronics also delivers fixes on layers through github<sup>&reg;</sup>. These changes can be integrated (via [[git]] commands) into your local [[STM32MP1 Distribution Package]] environment. Please find below the github<sup>&reg;</sup> links of the quoted layers :
+
STMicroelectronics also delivers dedicated fixes on layers through github<sup>&reg;</sup>. These changes can be integrated (via [[git]] commands) into your local [[STM32MP1 Distribution Package]] environment. Below the github<sup>&reg;</sup> links corresponding to each layers:
 
* [https://github.com/STMicroelectronics/meta-st-stm32mp/ meta-st-stm32mp]
 
* [https://github.com/STMicroelectronics/meta-st-stm32mp/ meta-st-stm32mp]
 
* [https://github.com/STMicroelectronics/meta-st-openstlinux/ meta-st-openstlinux ]
 
* [https://github.com/STMicroelectronics/meta-st-openstlinux/ meta-st-openstlinux ]
 
* [https://github.com/STMicroelectronics/meta-st-stm32mp-addons/ meta-st-stm32mp-addons]
 
* [https://github.com/STMicroelectronics/meta-st-stm32mp-addons/ meta-st-stm32mp-addons]
  +
  +
===v1.2.1===
  +
[[STM32MP15_OpenSTLinux_release_note_-_v1.2.0#v1.2.1 |OpenSTLinux updates v1.2.1]]<br>
   
 
==Reference documents==
 
==Reference documents==
 
{{:STM32MP15 resources - v1.2.0}}
 
{{:STM32MP15 resources - v1.2.0}}
 
+
{{ReviewsComments|-- [[User:Emmanuel Combette|Emmanuel Combette]] ([[User talk:Emmanuel Combette|talk]]) 10:55, 5 May 2020 (CEST)<br />Add : AN5431 The-stpmic1-pcb-layout-guidlines-stmicroelectronics.pdf}}
== How to get the software and start with this release? ==
+
== How to download the software and start with this release? ==
 
'''The list of embedded software packages available for download depends on the selected package'''.
 
'''The list of embedded software packages available for download depends on the selected package'''.
   
The table below provides the available board part numbers and the source of information in order to:
+
The table below provides the available board part numbers as well as information in order to:
*Get started with one of the three available Packages (Starter, Developer or Distribution Packages)
+
*get started with one of the three available Packages (Starter, Developer or Distribution Package)
*Get started with the board
+
*get started with the board
*Find the associated embedded software distributions  
+
*find the associated embedded software distributions  
*'''Download''' source code  
+
*'''download''' source code  
*'''Build''' an embedded software  
+
*'''build''' an embedded software  
 
{| class="st-table"
 
{| class="st-table"
 
|-
 
|-
Line 294: Line 301:
 
==STM32MPU Embedded Software distribution detailed release notes==
 
==STM32MPU Embedded Software distribution detailed release notes==
 
The table below lists the software packages available in the STM32MPU Embedded Software distributions, and provides the corresponding release notes.<br>
 
The table below lists the software packages available in the STM32MPU Embedded Software distributions, and provides the corresponding release notes.<br>
The release notes provide more information and details about the features and content of each package. <br>
+
The release notes give more information and details about the features and content of the packages. <br>
The release notes does not explain how to get software. For that, refer chapter [[#How to get the software and start with this release?|How to get the software and start with this release ]]
+
They do not explain how to download the software. Refer to [[#How to get the software and start with this release?|How to get the software and start with this release ]].
   
 
{|class="st-table" style="width: 98%;"  
 
{|class="st-table" style="width: 98%;"  
Line 317: Line 324:
   
 
==Referenced tools release notes ==
 
==Referenced tools release notes ==
The table below lists the available tools, and provides links to the respective release notes.
+
The table below lists the available tools, and provides links to the corresponding release notes.
   
Each release note provides information on how to install and use the corresponding tool.
+
Each release note gives information on how to install and use the corresponding tool.
   
The set of tools to be downloaded depends on the Package to be used (double check [[Which Package better suits your needs]] article to find more information on each Package).
+
The set of tools that can be downloaded depends on the Package that is used (double check [[Which Package better suits your needs]] article for more information on each Package).
   
 
{|class="st-table" style="text-align:center; width:95%; cellspacing=0"
 
{|class="st-table" style="text-align:center; width:95%; cellspacing=0"

Attachments

Discussions