Difference between revisions of "STM32MP15 VREFBUF internal peripheral"
[quality revision] | [quality revision] |
m
|
m
|
Applicable for | STM32MP15x lines |
Contents
1 Article purpose[edit]
The purpose of this article is to
- briefly introduce the VREFBUF peripheral and its main features
- indicate the level of security supported by this hardware block
- explain how each instance can be allocated to the runtime contexts and linked to the corresponding software components
- explain, when needed, how to configure the VREFBUF peripheral.
2 Peripheral overview[edit]
The VREFBUF peripheral is an internal voltage regulator.
2.1 Features[edit]
The VREFBUF is supplied via the VDDA pin. When enabled, it can provide a reference voltage in the range of: 1,5V, 1,8V, 2,048V or 2,5V.
The VREFBUF can be used to provide an analog voltage reference for:
- ADC internal peripheral[1]
- DAC internal peripheral[2]
- External components through the dedicated VREF+ pin.
The VREFBUF can be left unused. In this case, an external voltage regulator can provide reference voltage to VREF+ pin.
Refer to the STM32MP15 reference manuals for the complete list of features, and to the software components, introduced below, to know which features are really implemented.
2.2 Security support[edit]
The VREFBUF is a non-secure peripheral.
3 Peripheral usage and associated software[edit]
3.1 Boot time[edit]
The VREFBUF is usually not used at boot time. But it may be needed by the SSBL (see Boot chain overview), to supply the internal ADC[1] for example.
3.2 Runtime[edit]
3.2.1 Overview[edit]
The VREFBUF can be allocated to the Arm® Cortex®-A7 non-secure to be used under Linux® with regulator framework[3].
![]() |
The VREFBUF is a system resource[4] which needs to be also controlled by the resource manager[4] in case its consumers (e.g. ADC[1], DAC[2] or an external device connected to VREF+ pin) are spread across:
For this reason, the direct control of VREFBUF from the Arm® Cortex®-M4 is not recommended in STM32Cube[5] by default. |
The Peripheral assignment chapter describes which peripheral instance can be assigned to which context.
3.2.2 Software frameworks[edit]
Domain | Peripheral | Software components | Comment | ||
---|---|---|---|---|---|
OP-TEE | Linux | STM32Cube | |||
Analog | VREFBUF | Linux regulator framework |
3.2.3 Peripheral configuration[edit]
The configuration is applied by the firmware running in the context to which the peripheral is assigned. The configuration by itself can be performed via the STM32CubeMX tool for all internal peripherals. It can then be manually completed (especially for external peripherals) according to the information given in the corresponding software framework article.
- For the Linux kernel configuration, please refer to device internal regulator. An example can be found also in ADC DT configuration exampleexamples
- In case the control of VREFBUF consumers are spread across the various cores, see also Resource manager for coprocessing
3.2.4 Peripheral assignment[edit]
Click on the right to expand the legend...
Check boxes illustrate the possible peripheral allocations supported by STM32 MPU Embedded Software:
- ☐ means that the peripheral can be assigned (☑) to the given runtime context.
- ⬚ means that the peripheral can be assigned to the given runtime context, but this configuration is not supported in STM32 MPU Embedded Software distribution.
- ✓ is used for system peripherals that cannot be unchecked because they are statically connected in the device.
Refer to How to assign an internal peripheral to a runtime context for more information on how to assign peripherals manually or via STM32CubeMX.
The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possiblities might be described in STM32MP15 reference manuals.
Domain | Peripheral | Runtime allocation | Comment | |||
---|---|---|---|---|---|---|
Instance |
Cortex-A7 secure (OP-TEE) |
Cortex-A7 non-secure (Linux) |
Cortex-M4 (STM32Cube) |
|||
Analog | VREFBUF | VREFBUF | ☐ | Assignment (single choice) |
4 References[edit]
- ↑ 1.01.11.2 ADC internal peripheral
- ↑ 2.02.1 DAC internal peripheral
- ↑ Regulator overview, Linux® regulator framework overview
- ↑ 4.04.1 Resource manager for coprocessing, focus on system resources
- ↑ STM32CubeMP1 architecture
<noinclude>{{ApplicableFor |MPUs list=STM32MP15x |MPUs checklist=STM32MP13x, STM32MP15x }}</noinclude> ==Article purpose== The purpose of this article is to * briefly introduce the VREFBUF peripheral and its main features * indicate the level of security supported by this hardware block * explain how each instance can be allocated to the runtime contexts and linked to the corresponding software components * explain, when needed, how to configure the VREFBUF peripheral. ==Peripheral overview== The '''VREFBUF''' peripheral is an internal voltage regulator. ===Features=== The VREFBUF is supplied via the VDDA pin. When enabled, it can provide a reference voltage in the range of: 1,5V, 1,8V, 2,048V or 2,5V. The VREFBUF can be used to provide an analog voltage reference for: * ADC internal peripheral<ref name="adc_internal">[[ADC internal peripheral]]</ref> * DAC internal peripheral<ref name="dac_internal">[[DAC internal peripheral]]</ref> * External components through the dedicated VREF+ pin. The VREFBUF can be left unused. In this case, an external voltage regulator can provide reference voltage to VREF+ pin. Refer to the [[STM32MP15 resources#Reference manuals|STM32MP15 reference manuals]] for the complete list of features, and to the software components, introduced below, to know which features are really implemented. ===Security support=== The VREFBUF is a '''non-secure''' peripheral. ==Peripheral usage and associated software== ===Boot time=== The VREFBUF is usually not used at boot time. But it may be needed by the SSBL (see [[Boot chain overview]]), to supply the internal ADC<ref name="adc_internal"/> for example. ===Runtime=== ====Overview==== The VREFBUF can be allocated to the Arm<sup>®</sup> Cortex<sup>®</sup>-A7 non-secure to be used under Linux<sup>®</sup> with regulator framework<ref name="regulator">[[Regulator overview]], Linux<sup>®</sup> regulator framework overview</ref>. {{Info|The VREFBUF is a system resource<ref name="resource manager">[[Resource_manager_for_coprocessing#The_system_resources|Resource manager for coprocessing]], focus on system resources</ref> which needs to be also controlled by the resource manager<ref name="resource manager"/> in case its consumers (e.g. ADC<ref name="adc_internal"/>, DAC<ref name="dac_internal"/> or an external device connected to VREF+ pin) are spread across: * the Arm<sup>®</sup> Cortex<sup>®</sup>-A7 non-secure context * the Arm<sup>®</sup> Cortex<sup>®</sup>-M4 context For this reason, the direct control of VREFBUF from the Arm<sup>®</sup> Cortex<sup>®</sup>-M4 is not recommended in STM32Cube<ref name="STM32Cube">[[STM32CubeMP1 architecture]]</ref> by default.<br/> It's recommended to implement it in STM32Cube '''only if''' all consumers and the VDDA supply pin are controlled in the Arm<sup>®</sup> Cortex<sup>®</sup>-M4 context. }} The [[#Peripheral assignment|Peripheral assignment]] chapter describes which peripheral instance can be assigned to which context. ====Software frameworks==== {{:STM32MP15_internal_peripherals_software_table_template}} | Analog | [[STM32MP15 VREFBUF internal peripheral|VREFBUF]] | | Linux [[Regulator overview|regulator]] framework | | |- |} ====Peripheral configuration==== The configuration is applied by the firmware running in the context to which the peripheral is assigned. The configuration by itself can be performed via the [[STM32CubeMX]] tool for all internal peripherals. It can then be manually completed (especially for external peripherals) according to the information given in the corresponding software framework article. * For the Linux kernel configuration, please refer to [[Regulator_overview#Microcontroller_device_internal_regulator|device internal regulator]]. An example can be found also in [[ADC_device_tree_configuration#DT_configuration_exampleexamples|ADC DT configuration exampleexamples]] * In case the control of VREFBUF consumers are spread across the various cores, see also [[Resource manager for coprocessing]] ====Peripheral assignment==== {{:STM32MP15_internal_peripherals_assignment_table_template}}<onlyinclude> | rowspan="1" | Analog | rowspan="1" | [[STM32MP15 VREFBUF internal peripheral|VREFBUF]] | VREFBUF | | <span title="assignable peripheral" style="font-size:21px">☐</span> | | Assignment (single choice) |-</onlyinclude> |} ==References==<references/> <noinclude> [[Category:Analog peripherals|VREFBUF internal peripheral STM32MP15]] {{PublicationRequestId | 8312 | 2018-08-07 | AlainF}} {{ArticleBasedOnModel| Internal peripheral article model}} {{ReviewsComments|JCT 1840: alignment needed with the last version of the model<br> [[Category:ToBeAlignedWithModel]] }}</noinclude>
Line 59: | Line 59: | ||
The configuration is applied by the firmware running in the context to which the peripheral is assigned. The configuration by itself can be performed via the [[STM32CubeMX]] tool for all internal peripherals. It can then be manually completed (especially for external peripherals) according to the information given in the corresponding software framework article. |
The configuration is applied by the firmware running in the context to which the peripheral is assigned. The configuration by itself can be performed via the [[STM32CubeMX]] tool for all internal peripherals. It can then be manually completed (especially for external peripherals) according to the information given in the corresponding software framework article. |
||
− | * For the Linux kernel configuration, please refer to [[Regulator_overview#Microcontroller_device_internal_regulator|device internal regulator]]. An example can be found also in [[ADC_device_tree_configuration# |
+ | * For the Linux kernel configuration, please refer to [[Regulator_overview#Microcontroller_device_internal_regulator|device internal regulator]]. An example can be found also in [[ADC_device_tree_configuration#DT_configuration_examples|ADC DT configuration examples]] |
* In case the control of VREFBUF consumers are spread across the various cores, see also [[Resource manager for coprocessing]] |
* In case the control of VREFBUF consumers are spread across the various cores, see also [[Resource manager for coprocessing]] |
||