Difference between revisions of "STM32MP15 VREFBUF internal peripheral"

[quality revision] [quality revision]
m
 
m
Template:ArticleMainWriter Template:ArticleApprovedVersion
Applicable for STM32MP15x lines

1 Article purpose[edit]

The purpose of this article is to

  • briefly introduce the VREFBUF peripheral and its main features
  • indicate the level of security supported by this hardware block
  • explain how each instance can be allocated to the three runtime contexts and linked to the corresponding software components
  • explain, when needed, how to configure the VREFBUF peripheral.

2 Peripheral overview[edit]

The VREFBUF peripheral is an internal voltage regulator.

2.1 Features[edit]

The VREFBUF is supplied via the VDDA pin. When enabled, it can provide a reference voltage in the range of: 1,5V, 1,8V, 2,048V or 2,5V.

The VREFBUF can be used to provide an analog voltage reference for:

  • ADC internal peripheral[1]
  • DAC internal peripheral[2]
  • External components through the dedicated VREF+ pin.

The VREFBUF can be left unused. In this case, an external voltage regulator can provide reference voltage to VREF+ pin.

Refer to the STM32MP15 reference manuals for the complete list of features, and to the software components, introduced below, to know which features are really implemented.

2.2 Security support[edit]

The VREFBUF is a non-secure peripheral.

3 Peripheral usage and associated software[edit]

3.1 Boot time[edit]

The VREFBUF is usually not used at boot time. But it may be needed by the SSBL (see Boot chains chain overview), to supply the internal ADC[1] for example.

3.2 Runtime[edit]

3.2.1 Overview[edit]

The VREFBUF can be allocated to the Arm® Cortex®-A7 non-secure to be used under Linux® with regulator framework[3].

Info white.png Information
The VREFBUF is a system resource[4] which needs to be also controlled by the resource manager[4] in case its consumers (e.g. ADC[1], DAC[2] or an external device connected to VREF+ pin) are spread across:
  • the Arm® Cortex®-A7 non-secure context
  • the Arm® Cortex®-M4 context

For this reason, the direct control of VREFBUF from the Arm® Cortex®-M4 is not recommended in STM32Cube[5] by default.
It's recommended to implement it in STM32Cube only if all consumers and the VDDA supply pin are controlled in the Arm® Cortex®-M4 context.

The Peripheral assignment chapter describes which peripheral instance can be assigned to which context.

3.2.2 Software frameworks[edit]

Internal peripherals software table template

| Analog | VREFBUF | | Linux regulator framework | | |- |}
Domain Peripheral Software components Comment
OP-TEE Linux STM32Cube
Analog VREFBUF Linux regulator framework

3.2.3 Peripheral configuration[edit]

The configuration is applied by the firmware running in the context to which the peripheral is assigned. The configuration by itself can be performed via the STM32CubeMX tool for all internal peripherals. It can then be manually completed (especially for external peripherals) according to the information given in the corresponding software framework article.

3.2.4 Peripheral assignment[edit]

Internal peripherals assignment table template

| rowspan="1" | Analog
| rowspan="1" | VREFBUF
| VREFBUF
| 
| 
|
| Assignment (single choice)
|-

|}

Click on the right to expand the legend...

STM32MP15 internal peripherals

Check boxes illustrate the possible peripheral allocations supported by STM32 MPU Embedded Software:

  • means that the peripheral can be assigned () to the given runtime context.
  • means that the peripheral can be assigned to the given runtime context, but this configuration is not supported in STM32 MPU Embedded Software distribution.
  • is used for system peripherals that cannot be unchecked because they are statically connected in the device.

Refer to How to assign an internal peripheral to a runtime context for more information on how to assign peripherals manually or via STM32CubeMX.
The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possiblities might be described in STM32MP15 reference manuals.

Domain Peripheral Runtime allocation Comment
Instance Cortex-A7
secure
(OP-TEE)
Cortex-A7
non-secure
(Linux)
Cortex-M4

(STM32Cube)
Analog VREFBUF VREFBUF Assignment (single choice)

4 References[edit]



<noinclude>

{{ArticleBasedOnModel| [[Internal peripheral article model]]}}
{{ArticleMainWriter|FabriceG}}
{{ ArticleApprovedVersion|FabriceG| NathalieS, GeraldB, PascalP, AnthonyN | FabriceG - 27Aug'18 | AlainF - 07Aug'18 - 8312 | 13Sep'18 }} 

[[Category:Analog peripherals]]

{{ReviewsComments|JCT 1840: alignment needed with the last version of the model [[Internal peripheral article model]]<br>

[[Category:ToBeAlignedWithModel]]
}}</noinclude>

{{ApplicableFor
|MPUs list=STM32MP15x
|MPUs checklist=STM32MP13x, STM32MP15x
}}</noinclude>
==Article purpose==
The purpose of this article is to
* briefly introduce the VREFBUF  peripheral and its main features
* indicate the level of security supported by this hardware block
* explain how each instance can be allocated to the three runtime contexts and linked to the corresponding software components
* explain, when needed, how to configure the VREFBUF peripheral.

==Peripheral overview==
The '''VREFBUF''' peripheral is an internal voltage regulator.

===Features===
The VREFBUF is supplied via the VDDA pin. When enabled, it can provide a reference voltage in the range of: 1,5V, 1,8V, 2,048V or 2,5V.

The VREFBUF can be used to provide an analog voltage reference for:
* ADC internal peripheral<ref name="adc_internal">[[ADC internal peripheral]]</ref>

* DAC internal peripheral<ref name="dac_internal">[[DAC internal peripheral]]</ref>

* External components through the dedicated VREF+ pin.

The VREFBUF can be left unused. In this case, an external voltage regulator can provide reference voltage to VREF+ pin.

Refer to the [[STM32MP15 resources#Reference manuals|STM32MP15 reference manuals]] for the complete list of features, and to the software components, introduced below, to know which features are really implemented.

===Security support===
The VREFBUF is a '''non-secure''' peripheral.

==Peripheral usage and associated software==
===Boot time===
The VREFBUF is usually not used at boot time. But it may be needed by the SSBL (see [[Boot chainschain overview]]), to supply the internal ADC<ref name="adc_internal"/> for example.

===Runtime===
====Overview====
The VREFBUF can be allocated to the Arm<sup>&reg;</sup> Cortex<sup>&reg;</sup>-A7 non-secure to be used under Linux<sup>&reg;</sup> with regulator framework<ref name="regulator">[[Regulator overview]], Linux<sup>&reg;</sup> regulator framework overview</ref>.
{{Info|The VREFBUF is a system resource<ref name="resource manager">[[Resource_manager_for_coprocessing#The_system_resources|Resource manager for co-processingcoprocessing]], focus on system resources</ref> which needs to be also controlled by the resource manager<ref name="resource manager"/> in case its consumers (e.g. ADC<ref name="adc_internal"/>, DAC<ref name="dac_internal"/> or an external device connected to VREF+ pin) are spread across:
* the Arm<sup>&reg;</sup> Cortex<sup>&reg;</sup>-A7 non-secure context
* the Arm<sup>&reg;</sup> Cortex<sup>&reg;</sup>-M4 context

For this reason, the direct control of VREFBUF from the Arm<sup>&reg;</sup> Cortex<sup>&reg;</sup>-M4 is not recommended in STM32Cube<ref name="STM32Cube">[[STM32CubeMP1 architecture]]</ref> by default.<br/>

It's recommended to implement it in STM32Cube '''only if''' all consumers and the VDDA supply pin are controlled in the Arm<sup>&reg;</sup> Cortex<sup>&reg;</sup>-M4 context.
}}

The [[#Peripheral assignment|Peripheral assignment]] chapter describes which peripheral instance can be assigned to which context.

====Software frameworks====
{{:Internal_STM32MP15_internal_peripherals_software_table_template}}
 | Analog
 | [[STM32MP15 VREFBUF internal peripheral|VREFBUF]]
 | 
 | Linux [[Regulator overview|regulator]] framework
 |
 |
 |-
 |}

====Peripheral configuration====
The configuration is applied by the firmware running in the context to which the peripheral is assigned. The configuration by itself can be performed via the [[STM32CubeMX]] tool for all internal peripherals. It can then be manually completed (especially for external peripherals) according to the information given in the corresponding software framework article.

* For the Linux kernel configuration, please refer to [[Regulator_overview#Microcontroller_device_internal_regulator|device internal regulator]]. An example can be found also in [[ADC_device_tree_configuration#DT_configuration_example|ADC DT configuration example]]
* In case the control of VREFBUF consumers are spread across the various cores, see also [[Resource manager for coprocessing]]

====Peripheral assignment====
{{:Internal_STM32MP15_internal_peripherals_assignment_table_template}}<onlyinclude>

 | rowspan="1" | Analog
 | rowspan="1" | [[STM32MP15 VREFBUF internal peripheral|VREFBUF]]
 | VREFBUF
 | 
 | <span title="assignable peripheral" style="font-size:21px"></span>

 |
 | Assignment (single choice)
 |-</onlyinclude>

 |}

==References==<references/>
<noinclude>

[[Category:Analog peripherals|VREFBUF internal peripheral STM32MP15]]
{{PublicationRequestId | 8312 | 2018-08-07 | AlainF}}
{{ArticleBasedOnModel| Internal peripheral article model}}
{{ReviewsComments|JCT 1840: alignment needed with the last version of the model<br>

[[Category:ToBeAlignedWithModel]]
}}</noinclude>
(16 intermediate revisions by 4 users not shown)
Line 1: Line 1:
<noinclude>
+
<noinclude>{{ApplicableFor
{{ArticleBasedOnModel| [[Internal peripheral article model]]}}
+
|MPUs list=STM32MP15x
{{ArticleMainWriter|FabriceG}}
+
|MPUs checklist=STM32MP13x, STM32MP15x
{{ ArticleApprovedVersion|FabriceG| NathalieS, GeraldB, PascalP, AnthonyN | FabriceG - 27Aug'18 | AlainF - 07Aug'18 - 8312 | 13Sep'18 }}
+
}}</noinclude>
 
 
[[Category:Analog peripherals]]
 
 
 
{{ReviewsComments|JCT 1840: alignment needed with the last version of the model [[Internal peripheral article model]]<br>
 
[[Category:ToBeAlignedWithModel]]
 
}}
 
</noinclude>
 
 
 
 
==Article purpose==
 
==Article purpose==
 
The purpose of this article is to
 
The purpose of this article is to
 
* briefly introduce the VREFBUF  peripheral and its main features
 
* briefly introduce the VREFBUF  peripheral and its main features
 
* indicate the level of security supported by this hardware block
 
* indicate the level of security supported by this hardware block
* explain how each instance can be allocated to the three runtime contexts and linked to the corresponding software components
+
* explain how each instance can be allocated to the runtime contexts and linked to the corresponding software components
 
* explain, when needed, how to configure the VREFBUF peripheral.
 
* explain, when needed, how to configure the VREFBUF peripheral.
   
Line 38: Line 30:
 
==Peripheral usage and associated software==
 
==Peripheral usage and associated software==
 
===Boot time===
 
===Boot time===
The VREFBUF is usually not used at boot time. But it may be needed by the SSBL (see [[Boot chains overview]]), to supply the internal ADC<ref name="adc_internal"/> for example.
+
The VREFBUF is usually not used at boot time. But it may be needed by the SSBL (see [[Boot chain overview]]), to supply the internal ADC<ref name="adc_internal"/> for example.
   
 
===Runtime===
 
===Runtime===
 
====Overview====
 
====Overview====
 
The VREFBUF can be allocated to the Arm<sup>&reg;</sup> Cortex<sup>&reg;</sup>-A7 non-secure to be used under Linux<sup>&reg;</sup> with regulator framework<ref name="regulator">[[Regulator overview]], Linux<sup>&reg;</sup> regulator framework overview</ref>.
 
The VREFBUF can be allocated to the Arm<sup>&reg;</sup> Cortex<sup>&reg;</sup>-A7 non-secure to be used under Linux<sup>&reg;</sup> with regulator framework<ref name="regulator">[[Regulator overview]], Linux<sup>&reg;</sup> regulator framework overview</ref>.
{{Info|The VREFBUF is a system resource<ref name="resource manager">[[Resource_manager_for_coprocessing#The_system_resources|Resource manager for co-processing]], focus on system resources</ref> which needs to be also controlled by the resource manager<ref name="resource manager"/> in case its consumers (e.g. ADC<ref name="adc_internal"/>, DAC<ref name="dac_internal"/> or an external device connected to VREF+ pin) are spread across:
+
{{Info|The VREFBUF is a system resource<ref name="resource manager">[[Resource_manager_for_coprocessing#The_system_resources|Resource manager for coprocessing]], focus on system resources</ref> which needs to be also controlled by the resource manager<ref name="resource manager"/> in case its consumers (e.g. ADC<ref name="adc_internal"/>, DAC<ref name="dac_internal"/> or an external device connected to VREF+ pin) are spread across:
 
* the Arm<sup>&reg;</sup> Cortex<sup>&reg;</sup>-A7 non-secure context
 
* the Arm<sup>&reg;</sup> Cortex<sup>&reg;</sup>-A7 non-secure context
 
* the Arm<sup>&reg;</sup> Cortex<sup>&reg;</sup>-M4 context
 
* the Arm<sup>&reg;</sup> Cortex<sup>&reg;</sup>-M4 context
Line 54: Line 46:
   
 
====Software frameworks====
 
====Software frameworks====
{{:Internal_peripherals_software_table_template}}
+
{{:STM32MP15_internal_peripherals_software_table_template}}
 
  | Analog
 
  | Analog
  | [[VREFBUF internal peripheral|VREFBUF]]
+
  | [[STM32MP15 VREFBUF internal peripheral|VREFBUF]]
 
  |  
 
  |  
 
  | Linux [[Regulator overview|regulator]] framework
 
  | Linux [[Regulator overview|regulator]] framework
Line 71: Line 63:
   
 
====Peripheral assignment====
 
====Peripheral assignment====
{{:Internal_peripherals_assignment_table_template}}
+
{{:STM32MP15_internal_peripherals_assignment_table_template}}
 
<onlyinclude>
 
<onlyinclude>
 
  | rowspan="1" | Analog
 
  | rowspan="1" | Analog
  | rowspan="1" | [[VREFBUF internal peripheral|VREFBUF]]
+
  | rowspan="1" | [[STM32MP15 VREFBUF internal peripheral|VREFBUF]]
 
  | VREFBUF
 
  | VREFBUF
 
  |  
 
  |  
Line 86: Line 78:
 
==References==
 
==References==
 
<references/>
 
<references/>
  +
<noinclude>
  +
[[Category:Analog peripherals|VREFBUF internal peripheral STM32MP15]]
  +
{{PublicationRequestId | 8312 | 2018-08-07 | AlainF}}
  +
{{ArticleBasedOnModel| Internal peripheral article model}}
  +
{{ReviewsComments|JCT 1840: alignment needed with the last version of the model<br>
  +
[[Category:ToBeAlignedWithModel]]
  +
}}
  +
</noinclude>