Difference between revisions of "STM32MP15 RTC internal peripheral"

[quality revision] [quality revision]
m (Article purpose)
m
 
Applicable for STM32MP15x lines

1 Article purpose[edit]

The purpose of this article is to

  • briefly introduce the RTC peripheral and its main features
  • indicate the level of security supported by this hardware block
  • explain how it can be allocated to the runtime contexts and linked to the corresponding software components
  • explain, when needed, how to configure the RTC peripheral.

2 Peripheral overview[edit]

The RTC peripheral is used to provide the date and clock to the application. It supports programmable alarms and wake up capabilities.

2.1 Features[edit]

Refer to STM32MP15 reference manuals for the complete list of features, and to the software components, introduced below, to know which features are really implemented.

2.2 Security support[edit]

The RTC peripheral is a secure peripheral.

3 Peripheral usage and associated software[edit]

3.1 Boot time[edit]

By default after a backup domain power-on reset (performed at boot time), all RTC registers can be read or written in both secure and non-secure modes.
In OpenSTLinux distribution, the first stage bootloader (FSBL, running in secure mode) keeps this default configuration, leaving full control to Linux® at runtime.

The RTC peripheral is able to generate two interrupts:

  • A secure interrupt, connected to the Arm® Cortex®-A7 GIC, not used in OpenSTLinux distribution.
  • A non-secure interrupt, connected both to Arm® Cortex®-A7 GIC and Cortex-M4 NVIC: this interrupt is used on Linux® and by default in OpenSTLinux distribution.

The RTC peripheral is part of the backup domain which reset and clock are controlled via the RCC by the first stage bootloader (FSBL, running in secure mode) at boot time.
The RTC reset occurs when the backup domain is reset. To avoid clearing the TAMP register contents, this is only done on cold boot, not on wake up.

3.2 Runtime[edit]

3.2.1 Overview[edit]

The RTC peripheral can be allocated to the Arm® Cortex®-A7 non-secure core to be used under Linux® with RTC framework.

3.2.2 Software frameworks[edit]

Internal peripherals software table template

| Core | RTC | | Linux RTC framework | | |- |}
Domain Peripheral Software components Comment
OP-TEE Linux STM32Cube
Core RTC Linux RTC framework

3.2.3 Peripheral configuration[edit]

The configuration is applied by the firmware running in the context to which the peripheral is assigned. The configuration can be done alone via STM32CubeMX tool for all internal peripherals, and then manually completed (especially for external peripherals) according to the information given in the corresponding software framework article.

For Linux kernel configuration, please refer to RTC device tree configuration.

3.2.4 Peripheral assignment[edit]

Internal peripherals assignment table template

| rowspan="1" | Core
| rowspan="1" | RTC
| RTC
| 
| 
|
| RTC is mandatory to resynchronize  STGEN after exiting  low-power modes.
|-

|}

Click on the right to expand the legend...

STM32MP15 internal peripherals

Check boxes illustrate the possible peripheral allocations supported by STM32 MPU Embedded Software:

  • means that the peripheral can be assigned () to the given runtime context.
  • means that the peripheral can be assigned to the given runtime context, but this configuration is not supported in STM32 MPU Embedded Software distribution.
  • is used for system peripherals that cannot be unchecked because they are statically connected in the device.

Refer to How to assign an internal peripheral to a runtime context for more information on how to assign peripherals manually or via STM32CubeMX.
The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possiblities might be described in STM32MP15 reference manuals.

Domain Peripheral Runtime allocation Comment
Instance Cortex-A7
secure
(OP-TEE)
Cortex-A7
non-secure
(Linux)
Cortex-M4

(STM32Cube)
Core RTC RTC RTC is mandatory to resynchronize STGEN after exiting low-power modes.


<noinclude>{{ApplicableFor
|MPUs list=STM32MP15x
|MPUs checklist=STM32MP13x, STM32MP15x
}}</noinclude>

==Article purpose==
The purpose of this article is to
* briefly introduce the RTC peripheral and its main features
* indicate the level of security supported by this hardware block
* explain how it can be allocated to the runtime contexts and linked to the corresponding software components
* explain, when needed, how to configure the RTC peripheral.

==Peripheral overview==
The '''RTC''' peripheral is used to provide the date and clock to the application. It supports programmable alarms and wake up capabilities.<br />


===Features===
Refer to [[STM32MP15 resources#Reference manuals|STM32MP15 reference manuals]] for the complete list of features, and to the software components, introduced below, to know which features are really implemented.<br>


===Security support===
The '''RTC''' peripheral is a '''secure''' peripheral.

==Peripheral usage and associated software==
===Boot time===
By default after a backup domain power-on reset (performed at boot time), all RTC registers can be read or written in both secure and non-secure modes.<br />

In OpenSTLinux distribution, the first stage bootloader (FSBL, running in secure mode) keeps this default configuration, leaving full control to Linux<sup>&reg;</sup> at runtime.
{{InternalInfo|This configuration could be changed in RTC_SMCR register, per sub function (initialization, calibration, alarm A, alarm B, wake up timer and time-stamp). The customer may adapt this configuration to his needs, sharing some functions with the coprocessor or the secure world. This would require some code adaptation because, in case some functions are put in secure world, then secure services are needed to access to some control registers (like the write protection) from Linux.}}
The '''RTC''' peripheral is able to generate two interrupts:
* A secure interrupt, connected to the Arm<sup>&reg;</sup> Cortex<sup>&reg;</sup>-A7 [[GIC internal peripheral|GIC]], not used in OpenSTLinux distribution.
* A non-secure interrupt, connected both to Arm<sup>&reg;</sup> Cortex<sup>&reg;</sup>-A7 [[GIC internal peripheral|GIC]] and Cortex-M4 [[NVIC internal peripheral|NVIC]]: this interrupt is used on Linux<sup>&reg;</sup> and by default in OpenSTLinux distribution.<br />

The '''RTC''' peripheral is part of the backup domain which reset and clock are controlled via the [[RCC internal peripheral|RCC]] by the first stage bootloader (FSBL, running in secure mode) at boot time.<br />

The RTC reset occurs when the backup domain is reset. To avoid clearing the [[TAMP internal peripheral|TAMP]] register contents, this is only done on cold boot, not on wake up.

===Runtime===
====Overview====
The '''RTC''' peripheral can be allocated to the Arm<sup>&reg;</sup> Cortex<sup>&reg;</sup>-A7 non-secure core to be used under Linux<sup>&reg;</sup> with [[RTC overview|RTC framework]].

====Software frameworks====

{{:Internal_STM32MP15_internal_peripherals_software_table_template}}
 | Core
 | [[STM32MP15 RTC internal peripheral|RTC]]
 |
 | [[RTC overview|Linux RTC framework]]
 |
 |
 |-
 |}

====Peripheral configuration====
The configuration is applied by the firmware running in the context to which the peripheral is assigned. The configuration can be done alone via [[STM32CubeMX]] tool for all internal peripherals, and then manually completed (especially for external peripherals) according to the information given in the corresponding software framework article.

For Linux kernel configuration, please refer to [[RTC device tree configuration|RTC device tree configuration]].

====Peripheral assignment====

{{:Internal_STM32MP15_internal_peripherals_assignment_table_template}}<onlyinclude>

 | rowspan="1" | Core
 | rowspan="1" | [[STM32MP15 RTC internal peripheral|RTC]]
 | RTC
 | <span title="assignable peripheral" style="font-size:21px"></span>

 | <span title="assignable peripheral" style="font-size:21px"></span>

 |
 | RTC is mandatory to resynchronize [[STGEN_internal_peripheral | STGEN]] after exiting [[Power_overview | low-power modes]].
 |-</onlyinclude>

 |}
<noinclude>

[[Category:Core peripherals|RTC internal peripheral STM32MP15]]
{{PublicationRequestId | 10398 | 2019-01-21 | AnneJ}}
{{ArticleBasedOnModel| Internal peripheral article model}}</noinclude>
Line 36: Line 36:
 
====Software frameworks====
 
====Software frameworks====
   
{{:Internal_peripherals_software_table_template}}
+
{{:STM32MP15_internal_peripherals_software_table_template}}
 
  | Core
 
  | Core
 
  | [[STM32MP15 RTC internal peripheral|RTC]]
 
  | [[STM32MP15 RTC internal peripheral|RTC]]
Line 53: Line 53:
 
====Peripheral assignment====
 
====Peripheral assignment====
   
{{:Internal_peripherals_assignment_table_template}}
+
{{:STM32MP15_internal_peripherals_assignment_table_template}}
 
<onlyinclude>
 
<onlyinclude>
 
  | rowspan="1" | Core
 
  | rowspan="1" | Core