Difference between revisions of "STM32MP15 ROM code secure boot"

[unchecked revision] [quality revision]
m (ROM code authentication)
m (Closing the device)
 

1 Purpose[edit]

Secure boot is a key feature to guarantee a secure platform.

STM32MP1 boot sequence supports a trusted boot chain that ensures that the loaded images are authenticated and checked in integrity before being used.

Warning white.png Warning
The secure boot feature availability is indicated in the security field of the chip part number.

2 Authentication processing[edit]

STM32 MPU provides authentication processing with ECDSA [1] verification algorithm, based on ECC [2]. ECDSA offers better result than RSA with a smaller key. STM32 MPU relies on a 256 bits ECDSA key.

Two algorithms are supported for ECDSA calculation:

  • P-256 NIST
  • Brainpool 256

The algorithm selection is done via the signed binary header, as shown in STM32 header (subchapter in this same article).

The EDCSA verification follows the process below:

Bootrom Authentication.png

The BSEC OTP used by secure boot are:

3 U-Boot command stm32key[edit]

OpenSTLinux embeds a stm32key tool that can be called from U-Boot command line interface to manage these OTP.

 
STM32MP> help stm32key
 stm32key read [<addr>] : Read the hash stored at addr in memory or in OTP
 stm32key fuse [-y] <addr> : Fuse hash stored at addr in OTP
 stm32key close [-y] : Close the device, the hash stored in OTP

The optional option -y is used to skip the confirmation message.

Nota: the support of close is available in ecosystem release ≥ v3.1.0 More info.png

In this article, this stm32key tool is used to illustrate and experiment the steps needed to activate the secure boot, but these OTP can also be updated directly by customer application or with Secure Secret Provisioning (SSP).

4 Authentication steps[edit]

The expected sequence to test the secure boot on the device is

4.1 Key generation[edit]

First step is to generate the ECC pair of keys with STM32 KeyGen tool. This is the key pair that will be used to sign the images.
The tool also generates a third file containing the public key hash (PKH) that will be used to authenticate the public key on the target.

4.2 Key registration[edit]

Warning white.png Warning
Make sure that a device with Secure boot enabled is used: this is mentioned in the part number, otherwise the device will become permanently unusable.

4.2.1 Load hash public key[edit]

PKH file (publicKeyhash.bin) must be available in DDR before proceeding.

For example loaded from a filesystem partition on a storage device, like bootfs (partition 4) on SD card (mmc0):

 
STM32MP> load mmc 0:4 0xc0000000 publicKeyhash.bin
 32 bytes read in 50 ms (0 Bytes/s)

4.2.2 Register hash public key[edit]

First step to enable the authentication is to burn the OTP WORD 24 to 31 in BSEC with the corresponding public key hash (PKH, output file from STM32 KeyGen).

Make sure that a trusted image was programmed on your board, because below operation will not be possible with optee boot.

You can verify this PKH available in DDR:

 
STM32MP> stm32key read 0xc0000000                                       Read loaded key from DDR to confirm it is valid (without writing it in OTP)
 OTP value 24: 12345678
 OTP value 25: 12345678
 OTP value 26: 12345678
 OTP value 27: 12345678
 OTP value 28: 12345678
 OTP value 29: 12345678
 OTP value 30: 12345678
 OTP value 31: 12345678
Warning white.png Warning
If hash key is ok, the key in OTP can be fused
 
STM32MP> stm32key fuse 0xc0000000                                    Write and lock the key in OTP

The device now contains the hash to authenticate images. To read back the OTP, you can use NVMEM framework or the command stm32key:

 
STM32MP> stm32key read                                                   Read the key in OTP

4.3 Image signing[edit]

In a second step, FSBL binary must be signed. STM32 Signing tool allows to fill the STM32 binary header that is parsed by the embedded software to authenticate each binary.

4.3.1 STM32 Header[edit]

STM32 header.png

Each binary image (signed or not) loaded by ROM code needs to include a specific STM32 header added on top of the binary data. The header includes the authentication information.

Name Length Byte Offset Description
Magic number 32 bits 0 4 bytes in big endian:
'S', 'T', 'M', 0x32 = 0x53544D32
Image signature 512 bits 4 ECDSA signature for image authentication[Note 1]
Image checksum 32 bits 68 Checksum of the payload[Note 2]
Header version 32 bits 72 Header version v1.0 = 0x00010000
Byte0: reserved
Byte1:major version = 0x01
Byte2: minor version = 0x00
Byte3: reserved
Image length 32 bits 76 Length of image in bytes[Note 3]
Image entry Point 32 bits 80 Entry point of image
Reserved1 32 bits 84 Reserved
Load address 32 bits 88 Load address of image[Note 4]
Reserved2 32 bits 92 Reserved
Version number 32 bits 96 Image Version (monotonic number)[Note 5]
Option flags 32 bits 100 b0=1: no signature verification[Note 6]
ECDSA algorithm 32 bits 104 1: P-256 NIST ; 2: brainpool 256
ECDSA public key 512 bits 108 ECDSA public key to be used to verify the signature.[Note 7]
Padding 83 Bytes 172 Reserved padding bytes[Note 8]. Must all be set to 0
Binary type 1 Byte 255 Used to check the binary type
0x10-0x1F: TF-A
0x30: Copro
  1. Signature is calculated from first byte of header version field to last byte of image given by image length field.
  2. 32-bit sum of all payload bytes accessed as 8-bit unsigned numbers, discarding any overflow bits. Used to check the downloaded image integrity when signature is not used (if b0=1 in Option flags).
  3. Length is the length of the built image, it does not include the length of the STM32 header.
  4. This field is not used by ROM code.
  5. Image version number is an anti rollback monotonic counter. The ROM code checks that it is higher or equal to the monotonic counter stored in OTP.
  6. Enabling signature verification is mandatory on secure closed chips.
  7. This field is an extract of PEM public key file that only kept the ECC Point coordinates x and y in a raw binary format (RFC 5480). This field will be hashed with SHA-256 and compared to the Hash of pubKey that is stored in OTP.
  8. This padding forces STM32 header size to 256 bytes (0x100).


For STM32MP15x lines More info.png:

4.4 Image programming[edit]

Once the image is signed, it can be programmed into the flash on the target board with STM32CubeProgrammer.

4.5 PKH check[edit]

Before really starting the authentication process, the ROM code compares the hash of the public key carried in the STM32 header with the one that was provisioned in OTP.

4.6 Authentication[edit]

4.6.1 ROM code authentication[edit]

Using a signed binary, the ROM code authenticates and starts the FSBL.

At boot time on board, you must see the following line in TF-A trace:

NOTICE:  CPU: STM32MP157CAA Rev.?
NOTICE:  Model: STMicroelectronics STM32MP157C eval daughter on eval mother
NOTICE:  Board: MB1263 Var1.0 Rev.C-01
NOTICE:  Bootrom authentication succeeded
INFO:    Reset reason (0x15):
INFO:      Power-on Reset (rst_por)
INFO:    PMIC version = 0x10

On closed device, if the authentication fails, the ROM code enters into a serial boot loop indicated by the blinking Error LED (cf ROM code common debug and error cases).

The ROM code provides secure services to the FSBL for image authentication with the same ECC pair of keys, so there is no need to support ECDSA algorithm in FSBL.

4.7 Closing the device[edit]

Notice that this last step is not shown in the diagram above.

Without any other modification, the device is able to perform image authentication but non authenticated images can still be used and executed: the device is still opened, let's see this as a kind of test mode to check that the PKH is properly set.

As soon as the authentication process is confirmed, the device can be closed and the user is forced to use signed images.

OTP WORD0 bit 6 is the OTP bit that closes the device. Burning this bit will lock authentication processing and force authentication from the Boot ROM. Non signed binaries will not be supported anymore on the target.

To program this bit, the STM32CubeProgrammer or U-Boot command line interface can be used.

Here is how to proceed with U-Boot:

 
STM32MP> stm32key close

or if stm32key close is not supported, you can write bit 6 = 0x40 in OTP 0:

 
STM32MP> fuse prog 0 0x0 0x40

Warning white.png Warning
This must not be done on STM32MP15 part numbers without Secure boot enabled, otherwise the chip will be bricked and could not be used anymore

5 References[edit]


== Purpose ==
Secure boot is a key feature to guarantee a secure platform. <br><br/>

[[Boot_chain_overview#STM32MP_boot_sequence|STM32MP1 boot sequence]] supports a trusted boot chain that ensures that the loaded images are authenticated and checked in integrity before being used.
{{Warning| The secure boot feature availability is indicated in the ''security'' field of the chip [[STM32MP15_microprocessor#Part_number_codification|part number]].}}

== Authentication processing ==
STM32 MPU provides authentication processing with ECDSA <ref>https://en.wikipedia.org/wiki/Elliptic_Curve_Digital_Signature_Algorithm</ref> verification algorithm, based on  ECC <ref>https://en.wikipedia.org/wiki/Elliptic-curve_cryptography</ref>. ECDSA offers better result than RSA with a smaller key. STM32 MPU relies on a 256 bits ECDSA key.<br>


Two algorithms are supported for ECDSA calculation:
* P-256 NIST
* Brainpool 256
The algorithm selection is done via the signed binary header, as shown in [[#STM32_Header|STM32 header]] (subchapter in this same article).

The EDCSA verification follows the process below:<br>

[[File:Bootrom_Authentication.png|810px|center|link=]]

The [[BSEC internal peripheral|BSEC]] OTP used by secure boot are:
* the [[STM32MP15_ROM_code_overview#OTP WORD 24 to 31 - Public Key Hash (PKH)|OTP WORD 24 to 31]] for PKH
* the [[STM32MP15 ROM code overview#OTP WORD 0|OTP WORD0]] to close the device

== U-Boot command stm32key ==

OpenSTLinux embeds a <code>stm32key</code> tool that can be called from [[U-Boot_overview#U-Boot command line interface (CLI)|U-Boot command line interface]] to manage these OTP.

  {{U-Boot$}} help stm32key
  stm32key read [<addr>] : Read the hash stored at addr in memory or in OTP
  stm32key fuse [-y] <addr> : Fuse hash stored at addr in OTP
  stm32key close [-y] : Close the device, the hash stored in OTP

The optional option <code>-y</code> is used to skip the confirmation message.

Nota: the support of  <code>close</code> is available in {{EcosystemRelease | revision=3.1.0 | range=and after}}

In this article, this <code>stm32key</code> tool is used to illustrate and experiment the steps needed to activate the secure boot, but these OTP can also be updated directly by customer application or with [[Security_overview#Secure_Secret_Provisioning|Secure Secret Provisioning (SSP)]].

== Authentication steps ==

The expected sequence to test the secure boot on the device is
* [[#Key generation|Key generation]]

* [[ #Key registration| Key registration]]: update and lock PKH in OTP (<code>stm32key fuse</code>)

* [[#Authentication|Perform image authentication]] and check that the [[#ROM code authentication|ROM code accepted them]].

* [[#Closing the device|Close the device]], only signed binary will be accepted (<code>stm32key close</code>)

=== Key generation ===
First step is to generate the ECC pair of keys with [[KeyGen_tool|STM32 KeyGen tool]]. This is the key pair that will be used to sign the images. <br>

The tool also generates a third file containing the public key hash (PKH) that will be used to authenticate the public key on the target.

=== Key registration ===
{{Warning| Make sure that a device with Secure boot enabled is used: this is mentioned in the [[STM32MP15_microprocessor#Part_number_codification|part number]], otherwise the device will become permanently unusable.}}

==== Load hash public key ====

PKH file (publicKeyhash.bin) must be available in DDR before proceeding.

For example loaded from a filesystem partition on a storage device, like bootfs (partition 4)  on SD card (mmc0):

  {{U-Boot$}} load mmc 0:4 0xc0000000 publicKeyhash.bin
  32 bytes read in 50 ms (0 Bytes/s)

==== Register hash public key ====
First step to enable the authentication is to burn the [[STM32MP15_ROM_code_overview#OTP WORD 24 to 31 - Public Key Hash (PKH)|OTP WORD 24 to 31]] in [[BSEC internal peripheral|BSEC]] with the corresponding public key hash (PKH, output file from [[KeyGen_tool|STM32 KeyGen]]).

Make sure that a trusted image was programmed on your board, because below operation will not be possible with optee boot.

You can verify this PKH available in DDR:

  {{U-Boot$}} stm32key read 0xc0000000                                       {{highlight|Read loaded key from DDR to confirm it is valid (without writing it in OTP)}}
  OTP value 24: 12345678
  OTP value 25: 12345678
  OTP value 26: 12345678
  OTP value 27: 12345678
  OTP value 28: 12345678
  OTP value 29: 12345678
  OTP value 30: 12345678
  OTP value 31: 12345678

{{Warning| If hash key is ok, the key in OTP can be fused}}

  {{U-Boot$}} stm32key fuse 0xc0000000                                    {{highlight|Write and lock the key in OTP}}

The device now contains the hash to authenticate images. To read back the OTP, you can use [[NVMEM_overview|NVMEM framework]] or the command <code>stm32key</code>:

  {{U-Boot$}} stm32key read                                                   {{highlight|Read the key in OTP}}

=== Image signing ===
In a second step, FSBL binary must be signed. [[Signing_tool|STM32 Signing tool]] allows to fill the STM32 binary header that is parsed by the embedded software to authenticate each binary.

==== STM32 Header ==== 
{{:STM32 header for binary files}}

For {{MicroprocessorDevice | device=15}}:
* the monotonic counter is stored in [[STM32MP15_ROM_code_overview#OTP WORD 4 - Monotonic counter| OTP 4]]
* the Public Key Hash is stored in [[STM32MP15_ROM_code_overview#OTP WORD 24 to 31 - Public Key Hash (PKH)|OTP WORD 24 to 31]]

=== Image programming ===
Once the image is signed, it can be programmed into the flash on the target board with [[STM32CubeProgrammer]].

=== PKH check ===
Before really starting the authentication process, the ROM code compares the hash of the public key carried in the STM32 header with the one that was provisioned in OTP.

=== Authentication ===
==== ROM code authentication ====
Using a '''signed''' binary, the ROM code authenticates and starts the FSBL. 

At boot time on board, you must see the following line in TF-A trace: 
 NOTICE:  CPU: STM32MP157CAA Rev.?
 NOTICE:  Model: STMicroelectronics STM32MP157C eval daughter on eval mother
 NOTICE:  Board: MB1263 Var1.0 Rev.C-01
 {{highlight|NOTICE:  Bootrom authentication succeeded}}
 INFO:    Reset reason (0x15):
 INFO:      Power-on Reset (rst_por)
 INFO:    PMIC version = 0x10

On closed device, if the authentication fails, the ROM code enters into a serial boot loop indicated by the blinking Error LED (cf [[STM32MP15 ROM code overview#Common debug and error cases|ROM code common debug and error cases]]).

The [[STM32MP15 ROM code overview|ROM code]] provides secure services to the FSBL for image authentication with the same ECC pair of keys, so there is no need to support ECDSA algorithm in FSBL.

=== Closing the device ===
''Notice that this last step is not shown in the diagram above.''

Without any other modification, the device is able to perform image authentication but non authenticated images can still be used and executed: the device is still opened, let's see this as a kind of test mode to check that the PKH is properly set.

As soon as the authentication process is confirmed, the device can be closed and the user is forced to use signed images.

[[STM32MP15 ROM code overview#OTP WORD 0|OTP WORD0]] bit 6 is the OTP bit that closes the device. Burning this bit will lock authentication processing and force authentication from the Boot ROM.
Non signed binaries will not be supported anymore on the target.

To program this bit, the [[STM32CubeProgrammer_release_note|STM32CubeProgrammer]] or [[U-Boot_overview#U-Boot command line interface (CLI)|U-Boot command line interface]] can be used.

Here is how to proceed with U-Boot:
  {{U-Boot$}} stm32key close

or if <code>stm32key close</code> is not supported, you can write bit 6 = {{HighlightParam|0x40}} in OTP {{highlight|0}}:
  {{U-Boot$}} fuse prog 0 {{highlight|0x0}} {{highlightParam|0x40}}

{{Warning| This must not be done on [[STM32MP15_microprocessor#Security_and_Cortex-A7_frequency|STM32MP15 part numbers without Secure boot]] enabled, otherwise the chip will be bricked and could not be used anymore}}

== References ==<references/>

<noinclude>

[[Category:ROM code|02]]
{{PublicationRequestId | 10394  | 2019-01-30| BrunoB }}</noinclude>
Line 124: Line 124:
 
Without any other modification, the device is able to perform image authentication but non authenticated images can still be used and executed: the device is still opened, let's see this as a kind of test mode to check that the PKH is properly set.
 
Without any other modification, the device is able to perform image authentication but non authenticated images can still be used and executed: the device is still opened, let's see this as a kind of test mode to check that the PKH is properly set.
   
As soon as the authentication process is confirmed, the device can be closed and the user forced to use signed images.
+
As soon as the authentication process is confirmed, the device can be closed and the user is forced to use signed images.
   
 
[[STM32MP15 ROM code overview#OTP WORD 0|OTP WORD0]] bit 6 is the OTP bit that closes the device. Burning this bit will lock authentication processing and force authentication from the Boot ROM.
 
[[STM32MP15 ROM code overview#OTP WORD 0|OTP WORD0]] bit 6 is the OTP bit that closes the device. Burning this bit will lock authentication processing and force authentication from the Boot ROM.