Difference between revisions of "STM32 MPU Flash mapping"
[quality revision] | [checked revision] |
Philip Sage (talk | contribs)
|
Lionel Vitte (talk | contribs)
m (→Flash partitions)
|
Applicable for | STM32MP13x lines, STM32MP15x lines |
Contents
1 Supported Flash memory technologies[edit]
STM32MP15 boards STM32MP1 Series support the following types of Flash memory and the sub-bullets below show which interfaces are supported on STMicroelectronics boards:
- SD card on the SDMMC interface present on EVAL and DISCO boards
-
- used on STM32MP13 DISCO board
- used on STM32MP15 EVAL board
- used on STM32MP15 DISCO board
- e•MMC on the SDMMC interface present
-
- used on STM32MP15 EVAL board only
- Serial NOR Flash memory on the Dual QSPI interface present
-
- used on STM32MP15 EVAL board only
- NAND Flash memory on the FMC interface present
-
- used on STM32MP15 EVAL board only.
The next section lists all partitions used on STM32MP15 STM32MP1 boards (size, name, and content), and the following sections show how they are mapped on the different types of Flash memory.
2 Flash partitions[edit]
The tables below list the partitions defined for STMP32MP15 STMP32MP1 boards.
2.1 Minimal[edit]
Size | Component | Comment | |||
---|---|---|---|---|---|
Remaining area | userfs | The user file system contains user data and examples | |||
768 Mbytes | rootfs | Linux root file system contains all user space binaries (executable, libraries, and so on), and kernel modules | |||
16 Mbytes | vendorfs | This partition is preferred to the rootfs for third-party proprietary binaries, and ensures that they are not contaminated by any open source licence, such as GPL v3 | |||
64 Mbytes | bootfs or boot (NAND) |
The boot file system contains:
|
2 Mbytes | ssbl |
The
|
2 * 256 Kbytes (*) |
env
or uboot_config / uboot_config_r (NAND) |
This partition is used to store the U-Boot environment.
uboot_config_r is used for redundancy management with uboot_config, in NAND Flash.
|
|||
4 Mbytes | fip |
The TF-A firmware image package (FIP) is a binary file that encapsulates several binaries, and their certificates (optionally, for authentication), that will be loaded by TF-A]].
OpenSTLinux FIP contains:
|
|||
256 Kbytes to 512 Kbytes (*) | metadata |
Metadata are used by TF-A BL2 to localize the FIP copy to use, especially when the FIP is subject to update via FOTA.
|
|||
256 Kbytes to 512 Kbytes (*) | fsbl | The first stage boot loader is Arm Trusted Firmware (TF-A) or U-Boot Secondary Program Loader (SPL), with its device tree blob (dtb) appended at the end. At least two copies are embedded. Note: due to ROM code RAM needs, the FSBL payload is limited to 128 Kbytes on STM32MP13 and 247 Kbytes on STM32MP15. |
(*): The partition size depends on the Flash technology, to be aligned to the block erase size of the Flash memory present on the board: NOR (256 Kbytes) / NAND (512 Kbytes).
![]() |
Some boards can be equipped with multiple Flash devices, like the STM32MP15 EVAL board, where all of the Flash devices can be programmed with STM32CubeProgrammer. However, caution must be taken for the serial NOR/NAND and SLC NAND because a static bootable MTD partitioning is defined in U-Boot include/configs/stm32mp1.h (look for STM32MP_MTDPARTSdefault config (see MTD configuration for details), with the consequence that up to 6 Mbytes of space is lost at the beginning of each such device, even those which are not bootable. |
2.2 Optional[edit]
Size | Component | Comment |
---|---|---|
256 Kbytes (*) | env | This partition is used to store the U-Boot environment while booting from NOR Flash. For all other Flash devices, the U-Boot environment is stored either in an EXT4 bootfs partition (e•MMC, SD card), or UBI volumes (NAND). |
256 Kbytes to 512 Kbytes (*) | teeh | OP-TEE header |
256 Kbytes to 512 Kbytes (*) | teed | OP-TEE pageable code and data |
256 Kbytes to 512 Kbytes (*) | teex | OP-TEE pager |
(*): The partition size depends on the Flash technology, as it should be aligned to the block erase size of the Flash device present on the board (256 Kbytes for NOR and 512 Kbytes for NAND).
3 SD card memory mapping[edit]
The SD card has to be partitioned with GPT format in order to be recognized by the STM32MP15STM32MP1. The easiest way to achieve this is to use STM32CubeProgrammer.
The ROM code looks for the GPT entries whose name begins with "fsbl": fsbl1 and fsbl2 for example.
Note: The SD card can be unplugged from the board and inserted into a Linux host computer for direct partitioning with Linux utilities and access to the bootfs, rootfs and userfs partitions. The file system is Linux EXT4.
4 e•MMC memory mapping[edit]
The e•MMC embeds four physical partitions:
- Boot area partition 1: one copy of the FSBL
- Boot area partition 2: one copy of the FSBL
- User data area: formatted with GPT partitioning and used to store all remaining partitions
- Replay Protected Memory Block (RPMB): not shown in the figure below, since not involved in the current boot chain.
STM32CubeProgrammer has to be used to prepare the e•MMC with the layout shown below, and to populate each partition.
![]() |
The boot area partition used by the e•MMC boot sequence is selected via the EXT_CSD[179] register in the e•MMC. The STM32CubeProgrammer execution is concluded with the selection of the last written partition from the flashlayout file, typically partition 2. The other copy is never used as long as the user does not explicitly change the e•MMC EXT_CSD[179] register to select it. |
5 NOR memory mapping[edit]
As NOR Flash memory is expensive, its size is usually limited to the minimum needed to store only the bootloaders. The system files (bootfs, rootfs and userfs) are usually stored in another Flash memory, such as the SD card in OpenSTLinux distribution.
STM32CubeProgrammer must be used to prepare the NOR Flash and the SD card with the layout shown below, and to populate each partition.
It is possible to use an e•MMC card or NAND as second-level Flash memory, rather than an SD card. This requires the following aspects to be changed:
- The Flash memory layout, using STM32CubeProgrammer in order to write the rootfs and userfs to the targeted Flash memory
- The Linux kernel parameters, using U-Boot, in order to indicate where the rootfs and userfs have to be mounted.
6 NAND memory mapping[edit]
STM32CubeProgrammer has to be used to prepare the NAND Flash memory with the layout shown below, and to populate each partition.
__FORCETOC__{{ApplicableFor |MPUs list=STM32MP13x, STM32MP15x |MPUs checklist=STM32MP13x, STM32MP15x }} __FORCETOC__ == Supported Flash memory technologies ==STM32MP15 boards {{MicroprocessorDevice | device=1}} support the following types of Flash memory and the sub-bullets below show which interfaces are supported on STMicroelectronics boards: * SD card on the SDMMC interfacepresent :* used on [[:Category:Getting started with STM32MP1 boards|EVAL and DISCO boardsSTM32MP13 DISCO board]] :* used on [[:Category:Getting started with STM32MP1 boards|STM32MP15 EVAL board]] :* used on [[:Category:Getting started with STM32MP1 boards|STM32MP15 DISCO board]] * ''e''•MMC on the SDMMC interfacepresent :* used on [[:Category:Getting started with STM32MP1 boards|STM32MP15 EVAL board]] only * Serial NOR Flash memory on the Dual QSPI interfacepresent :* used on [[:Category:Getting started with STM32MP1 boards|STM32MP15 EVAL board]] only * NAND Flash memory on the FMC interfacepresent :* used on [[:Category:Getting started with STM32MP1 boards|STM32MP15 EVAL board]] only. The next section lists all partitions used on STM32MP15STM32MP1 boards (size, name, and content), and the following sections show how they are mapped on the different types of Flash memory. == Flash partitions == The tables below list the partitions defined for STMP32MP15STMP32MP1 boards.=== Minimal ===<br> {| class="st-table" |- ! Size !! Component !! Comment |- | Remaining area || userfs || The user file system contains user data and examples |- | 768 Mbytes || rootfs || Linux root file system contains all user space binaries (executable, libraries, and so on), and kernel modules |- | 16 Mbytes || vendorfs || This partition is preferred to the rootfs for third-party proprietary binaries, and ensures that they are not contaminated by any open source licence, such as GPL v3 |- | 64 Mbytes || bootfs <br>or<br>boot (NAND)|| The boot file system contains: * (option) the init RAM file system, which can be copied to the external RAM and used by Linux before mounting a fatter rootfs * Linux kernel device tree (can be in a Flattened Image Tree - FIT) * Linux kernel U-Boot image (can be in a Flattened Image Tree - FIT) * For all flashes except for NOR: the boot loader splash screen image, displayed by U-Boot * [[U-Boot_overview#Generic_Distro_configuration|U-Boot distro config file]] ''extlinux.conf''(can be in a Flattened Image Tree – FIT) |- | 2 Mbytes || ssbl || The second stage boot loader (SSBL) is U-Boot, with its device tree blob (dtb) appended at the end |- | 256 Kbytes to 512 Kbytes (*) || fsbl || The first stage boot loader is Arm Trusted Firmware (TF-A) or U-Boot Secondary Program Loader (SPL), with its device tree blob (dtb) appended at the end. At least two copies are embedded.<br> Note: due to ROM code RAM needs, the FSBL payload is limited to 247 Kbytes. |} (*): The partition size depends on the Flash technology, to be aligned to the block erase size of the Flash memory present on the board: NOR (256 Kbytes) / NAND (512 Kbytes). {{Info | Some boards can be equipped with multiple Flash devices, like the [[:Category:Getting started with STM32MP1 boards|EVAL board]], where all of the Flash devices can be programmed with [[STM32CubeProgrammer]]. However, caution must be taken for the serial NOR/NAND and SLC NAND because a '''static bootable MTD partitioning''' is defined in U-Boot {{CodeSource | U-Boot | include/configs/stm32mp1.h }} (look for ''STM32MP_MTDPARTS''), with the consequence that up to 6 Mbytes of space is lost at the beginning of each such device, '''even those which are not bootable'''.}} === Optional === {| class="st-table" |- ! Size !! Component !! Comment |- | 256 Kbytes (*) || env || This partition is used to store the U-Boot environment while booting from NOR Flash. For all other Flash devices, the U-Boot environment is stored either in an EXT4 bootfs partition (''e''•MMC, SD card), or UBI volumes (NAND). {{ReviewsComments|GeraldB: size to be increased to 512 Kbytes for release 2.0.0, due to redundancy|- | 2 * 256 Kbytes (*) || env<br>or uboot_config / uboot_config_r (NAND) || This partition is used to store the U-Boot environment.<br>uboot_config_r is used for redundancy management with uboot_config, in NAND Flash. {{ReviewsComments|-- [[User:Patrick Delaunay|Patrick Delaunay]] ([[User talk:Patrick Delaunay|talk]]) 17:58, 17 June 2022 (CEST)<br />env or u-boot-env ?}} {{ReviewsComments | [[User:Lionel Vitte|Lionel Vitte]] ([[User talk:Lionel Vitte|talk]]) 16:10, 21 June 2022 (CEST) - u-boot-env}} |- | 4 Mbytes || fip || The [[TF-A_overview#FIP|TF-A firmware image package (FIP)]] is a binary file that encapsulates several binaries, and their certificates (optionally, for authentication), that will be loaded by TF-A]].<br> OpenSTLinux FIP contains: * the second stage boot loader (SSBL): ** U-Boot binary ** U-Boot device tree blob * the OP-TEE {{ReviewsComments|-- [[User:Patrick Delaunay|Patrick Delaunay]] ([[User talk:Patrick Delaunay|talk]]) 17:49, 17 June 2022 (CEST)<br />Note: two partitions to have two different version when A/B (Seamless) FIP firmware update is activated in TF-A BL2: fip-a and fip-b.}} |- | 256 Kbytes to 512 Kbytes (*) || metadata || Metadata are used by TF-A BL2 to localize the FIP copy to use, especially when the FIP is subject to update via FOTA. {{ReviewsComments|-- [[User:Patrick Delaunay|Patrick Delaunay]] ([[User talk:Patrick Delaunay|talk]]) 17:49, 17 June 2022 (CEST)<br />/FIP copy/FIP version/ or slot ? copy is disturbing here}} {{ReviewsComments|-- [[User:Patrick Delaunay|Patrick Delaunay]] ([[User talk:Patrick Delaunay|talk]]) 17:23, 17 June 2022 (CEST)<br />s/to update via FOTA./to firmware update./ <br/> reason: "Over The Air" in not manadatory here}} {{ReviewsComments|-- [[User:Patrick Delaunay|Patrick Delaunay]] ([[User talk:Patrick Delaunay|talk]]) 17:49, 17 June 2022 (CEST)<br />s/, especially//<br/>reason: used only when firmware update is activated in TF-BL2}} {{ReviewsComments|-- [[User:Patrick Delaunay|Patrick Delaunay]] ([[User talk:Patrick Delaunay|talk]]) 17:49, 17 June 2022 (CEST)<br />Note: the metada are not used when the FIP firmware update is not activated in TF-A BL2; these partitions can be removed or is empty in this case.}} {{ReviewsComments|-- [[User:Patrick Delaunay|Patrick Delaunay]] ([[User talk:Patrick Delaunay|talk]]) 17:49, 17 June 2022 (CEST)<br />Note: The metatada update is failsafe against power loss during the FIP update process with two copies.}} |- | 256 Kbytes to 512 Kbytes (*) || teeh || OP-TEE header |- | 256 Kbytes to 512 Kbytes (*) || teed || OP-TEE pageable code and data |- | 256 Kbytes to 512 Kbytes (*) || teex || OP-TEE pagerfsbl || The first stage boot loader is Arm Trusted Firmware ([[TF-A_overview#BL2|TF-A]]). At least two copies are embedded.<br> Note: the FSBL payload is limited to 128 Kbytes on STM32MP13 and 247 Kbytes on STM32MP15. {{ReviewsComments|-- [[User:Patrick Delaunay|Patrick Delaunay]] ([[User talk:Patrick Delaunay|talk]]) 17:25, 17 June 2022 (CEST)<br />Note: The TF-A BL2 update is failsafe against power loss during the process with two copies.}}|} (*): The partition size depends on the Flash technology, as it should to be aligned to the block erase size of the Flash devicememory present on the board : NOR (256 Kbytes for NOR and 512 Kbytes for NAND).) / NAND (512 Kbytes). {{Info | Some boards can be equipped with multiple Flash devices, like the [[:Category:Getting started with STM32MP1 boards|STM32MP15 EVAL board]], where all of the Flash devices can be programmed with [[STM32CubeProgrammer]]. However, caution must be taken for the serial NOR/NAND and SLC NAND because a '''static bootable MTD partitioning''' is defined in U-Boot default config (see [[How_to_configure_U-Boot_for_your_board#MTD_partitions|MTD configuration ]] for details), with the consequence that up to 6 Mbytes of space is lost at the beginning of each such device, '''even those which are not bootable'''.}} == SD card memory mapping == The SD card has to be partitioned with GPT format in order to be recognized by the STM32MP15STM32MP1. The easiest way to achieve this is to use [[STM32CubeProgrammer]].<br /> The ROM code looks for the GPT entries whose name begins with "fsbl": fsbl1 and fsbl2 for example.<br/> Note: The SD card can be unplugged from the board and inserted into a Linux host computer for direct partitioning with Linux utilities and access to the '''bootfs''', '''rootfs''' and '''userfs''' partitions. The file system is Linux EXT4. [[Image:SD card mapping.png|center|link=]] == ''e''•MMC memory mapping == The ''e''•MMC embeds four physical partitions: * Boot area partition 1: one copy of the FSBL * Boot area partition 2: one copy of the FSBL * User data area: formatted with GPT partitioning and used to store all remaining partitions * Replay Protected Memory Block (RPMB): not shown in the figure below, since not involved in the current boot chain. [[STM32CubeProgrammer]] has to be used to prepare the ''e''•MMC with the layout shown below, and to populate each partition. {{Info | The boot area partition used by the ''e''•MMC boot sequence is selected via the EXT_CSD[179] register in the ''e''•MMC. The [[STM32CubeProgrammer]] execution is concluded with the selection of the last written partition from the flashlayout file, typically partition 2. The other copy is never used as long as the user does not explicitly change the ''e''•MMC EXT_CSD[179] register to select it.}} [[File:eMMC mapping.png|center|link=]] == NOR memory mapping == As NOR Flash memory is expensive, its size is usually limited to the minimum needed to store only the bootloaders. The system files (bootfs, rootfs and userfs) are usually stored in another Flash memory, such as the SD card in OpenSTLinux distribution.<br /> [[STM32CubeProgrammer]] must be used to prepare the NOR Flash and the SD card with the layout shown below, and to populate each partition.<br /><br> [[File:NOR mapping.png|center|link=]] It is possible to use an ''e''•MMC card or NAND as second-level Flash memory, rather than an SD card. This requires the following aspects to be changed: * The Flash memory layout, using [[STM32CubeProgrammer]] in order to write the rootfs and userfs to the targeted Flash memory * The Linux kernel parameters, using [[U-Boot overview|U-Boot]], in order to indicate where the rootfs and userfs have to be mounted.[[File:NOR mapping.png|center|link=]] == == NAND memory mapping == [[STM32CubeProgrammer]] has to be used to prepare the NAND Flash memory with the layout shown below, and to populate each partition.<br /> [[File:NAND mapping.png|center|link=]]<noinclude> [[Category:STM32MP15 platform configuration|1{{Warning|In the '''RAW/MTD area''', the number of copies to embed and the number of blocks to reserve at the end of each partition, for future bad blocks replacement, are a critical part of NAND based product dimensioning !<br> The strategy has to take into account many parameters such as: * the binaries sizes, * the read accesses to those partitions during product life, that may generate read disturb effect, * the capability of the product to refresh the partitions content when erroneous bits are detected, * the number of software updates estimated on this partition, * the selected NAND flash characteristics ST set foundations in the STM32MP1 device in order to allow the integration of NAND flash memories but the product definition remains the customer responsibility. Please, contact your memory provider for further advice.}}<noinclude> [[Category:Platform configuration]] {{PublicationRequestId | 14615 | 2020-01-15 |}}</noinclude>
(43 intermediate revisions by 4 users not shown) | |||
Line 1: | Line 1: | ||
+ | {{ApplicableFor |
||
+ | |MPUs list=STM32MP13x, STM32MP15x |
||
+ | |MPUs checklist=STM32MP13x, STM32MP15x |
||
+ | }} |
||
__FORCETOC__ |
__FORCETOC__ |
||
+ | |||
== Supported Flash memory technologies == |
== Supported Flash memory technologies == |
||
− | + |
{{MicroprocessorDevice | device=1}} support the following types of Flash memory and the sub-bullets below show which interfaces are supported on STMicroelectronics boards: |
|
− | * SD card on the SDMMC interface |
+ | * SD card on the SDMMC interface |
− | * ''e''•MMC on the SDMMC interface |
+ | :* used on [[:Category:Getting started with STM32MP1 boards|STM32MP13 DISCO board]] |
− | * Serial NOR Flash memory on the Dual QSPI interface |
+ |
:* used on [[:Category:Getting started with STM32MP1 boards|STM32MP15 EVAL board]]
|
− | * NAND Flash memory on the FMC interface |
+ |
:* used on [[:Category:Getting started with STM32MP1 boards|STM32MP15 DISCO board]] |
− | The next section lists all partitions used on |
+ | * ''e''•MMC on the SDMMC interface |
+ |
:* used on [[:Category:Getting started with STM32MP1 boards|STM32MP15 EVAL board]] only |
||
+ | * Serial NOR Flash memory on the Dual QSPI interface |
||
+ |
:* used on [[:Category:Getting started with STM32MP1 boards|STM32MP15 EVAL board]] only |
||
+ | * NAND Flash memory on the FMC interface |
||
+ |
:* used on [[:Category:Getting started with STM32MP1 boards|STM32MP15 EVAL board]] only. |
||
+ | The next section lists all partitions used on STM32MP1 boards (size, name, and content), and the following sections show how they are mapped on the different types of Flash memory. |
||
== Flash partitions == |
== Flash partitions == |
||
− | The tables below list the partitions defined for |
+ | The tables below list the partitions defined for STMP32MP1 boards. |
− | + | <br> |
|
{| class="st-table" |
{| class="st-table" |
||
|- |
|- |
||
Line 21: | Line 32: | ||
| 16 Mbytes || vendorfs || This partition is preferred to the rootfs for third-party proprietary binaries, and ensures that they are not contaminated by any open source licence, such as GPL v3 |
| 16 Mbytes || vendorfs || This partition is preferred to the rootfs for third-party proprietary binaries, and ensures that they are not contaminated by any open source licence, such as GPL v3 |
||
|- |
|- |
||
− | | 64 Mbytes || bootfs || The boot file system contains: |
+ | | 64 Mbytes || bootfs<br>or<br>boot (NAND)|| The boot file system contains: |
* (option) the init RAM file system, which can be copied to the external RAM and used by Linux before mounting a fatter rootfs |
* (option) the init RAM file system, which can be copied to the external RAM and used by Linux before mounting a fatter rootfs |
||
* Linux kernel device tree (can be in a Flattened Image Tree - FIT) |
* Linux kernel device tree (can be in a Flattened Image Tree - FIT) |
||
* Linux kernel U-Boot image (can be in a Flattened Image Tree - FIT) |
* Linux kernel U-Boot image (can be in a Flattened Image Tree - FIT) |
||
* For all flashes except for NOR: the boot loader splash screen image, displayed by U-Boot |
* For all flashes except for NOR: the boot loader splash screen image, displayed by U-Boot |
||
− | * U-Boot distro config file ''extlinux.conf'' |
+ | * [[U-Boot_overview#Generic_Distro_configuration|U-Boot distro config file]] ''extlinux.conf'' |
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
|- |
|- |
||
− | + | | 2 * 256 Kbytes (*) || env<br>or uboot_config / uboot_config_r (NAND) || This partition is used to store the U-Boot environment.<br>uboot_config_r is used for redundancy management with uboot_config, in NAND Flash. |
|
+ | {{ReviewsComments|-- [[User:Patrick Delaunay|Patrick Delaunay]] ([[User talk:Patrick Delaunay|talk]]) 17:58, 17 June 2022 (CEST)<br />env or u-boot-env ?}} |
||
+ | {{ReviewsComments | [[User:Lionel Vitte|Lionel Vitte]] ([[User talk:Lionel Vitte|talk]]) 16:10, 21 June 2022 (CEST) - u-boot-env}} |
||
|- |
|- |
||
− | | |
+ | | 4 Mbytes || fip || The [[TF-A_overview#FIP|TF-A firmware image package (FIP)]] is a binary file that encapsulates several binaries, and their certificates (optionally, for authentication), that will be loaded by TF-A]].<br>
|
− | {{ReviewsComments| |
+ | OpenSTLinux FIP contains: |
+ |
* the second stage boot loader (SSBL):
|
||
+ | ** U-Boot binary |
||
+ | ** U-Boot device tree blob |
||
+ | * the OP-TEE |
||
+ | {{ReviewsComments|-- [[User:Patrick Delaunay|Patrick Delaunay]] ([[User talk:Patrick Delaunay|talk]]) 17:49, 17 June 2022 (CEST)<br />Note: two partitions to have two different version when A/B (Seamless) FIP firmware update is activated in TF-A BL2: fip-a and fip-b.}} |
||
|- |
|- |
||
− | | 256 Kbytes to 512 Kbytes (*) || |
+ | | 256 Kbytes to 512 Kbytes (*) || metadata || Metadata are used by TF-A BL2 to localize the FIP copy to use, especially when the FIP is subject to update via FOTA.
|
− | |- |
+ |
{{ReviewsComments|-- [[User:Patrick Delaunay|Patrick Delaunay]] ([[User talk:Patrick Delaunay|talk]]) 17:49, 17 June 2022 (CEST)<br />/FIP copy/FIP version/ or slot ? copy is disturbing here}}
|
− | | |
+ |
{{ReviewsComments|-- [[User:Patrick Delaunay|Patrick Delaunay]] ([[User talk:Patrick Delaunay|talk]]) 17:23, 17 June 2022 (CEST)<br />s/to update via FOTA./to firmware update./ <br/> reason: "Over The Air" in not manadatory here}}
|
+ |
{{ReviewsComments|-- [[User:Patrick Delaunay|Patrick Delaunay]] ([[User talk:Patrick Delaunay|talk]]) 17:49, 17 June 2022 (CEST)<br />s/, especially//<br/>reason: used only when firmware update is activated in TF-BL2}}
|
||
+ |
{{ReviewsComments|-- [[User:Patrick Delaunay|Patrick Delaunay]] ([[User talk:Patrick Delaunay|talk]]) 17:49, 17 June 2022 (CEST)<br />Note: the metada are not used when the FIP firmware update is not activated in TF-A BL2; these partitions can be removed or is empty in this case.}}
|
||
+ |
{{ReviewsComments|-- [[User:Patrick Delaunay|Patrick Delaunay]] ([[User talk:Patrick Delaunay|talk]]) 17:49, 17 June 2022 (CEST)<br />Note: The metatada update is failsafe against power loss during the FIP update process with two copies.}}
|
||
|- |
|- |
||
− | | 256 Kbytes to 512 Kbytes (*) || |
+ | | 256 Kbytes to 512 Kbytes (*) || fsbl || The first stage boot loader is Arm Trusted Firmware ([[TF-A_overview#BL2|TF-A]]). At least two copies are embedded.<br>
|
+ | Note: the FSBL payload is limited to 128 Kbytes on STM32MP13 and 247 Kbytes on STM32MP15. |
||
+ | {{ReviewsComments|-- [[User:Patrick Delaunay|Patrick Delaunay]] ([[User talk:Patrick Delaunay|talk]]) 17:25, 17 June 2022 (CEST)<br />Note: The TF-A BL2 update is failsafe against power loss during the process with two copies.}} |
||
|} |
|} |
||
− | (*): The partition size depends on the Flash technology, |
+ | (*): The partition size depends on the Flash technology, to be aligned to the block erase size of the Flash memory present on the board: NOR (256 Kbytes) / NAND (512 Kbytes).
|
+ |
{{Info | Some boards can be equipped with multiple Flash devices, like the [[:Category:Getting started with STM32MP1 boards|STM32MP15 EVAL board]], where all of the Flash devices can be programmed with [[STM32CubeProgrammer]]. However, caution must be taken for the serial NOR/NAND and SLC NAND because a '''static bootable MTD partitioning''' is defined in U-Boot default config (see [[How_to_configure_U-Boot_for_your_board#MTD_partitions|MTD configuration ]] for details), with the consequence that up to 6 Mbytes of space is lost at the beginning of each such device, '''even those which are not bootable'''.}}
|
||
== SD card memory mapping == |
== SD card memory mapping == |
||
− | The SD card has to be partitioned with GPT format in order to be recognized by the |
+ | The SD card has to be partitioned with GPT format in order to be recognized by the STM32MP1. The easiest way to achieve this is to use [[STM32CubeProgrammer]].<br /> |
The ROM code looks for the GPT entries whose name begins with "fsbl": fsbl1 and fsbl2 for example.<br/> |
The ROM code looks for the GPT entries whose name begins with "fsbl": fsbl1 and fsbl2 for example.<br/> |
||
Note: The SD card can be unplugged from the board and inserted into a Linux host computer for direct partitioning with Linux utilities and access to the '''bootfs''', '''rootfs''' and '''userfs''' partitions. The file system is Linux EXT4. |
Note: The SD card can be unplugged from the board and inserted into a Linux host computer for direct partitioning with Linux utilities and access to the '''bootfs''', '''rootfs''' and '''userfs''' partitions. The file system is Linux EXT4. |
||
Line 69: | Line 83: | ||
== NOR memory mapping == |
== NOR memory mapping == |
||
As NOR Flash memory is expensive, its size is usually limited to the minimum needed to store only the bootloaders. The system files (bootfs, rootfs and userfs) are usually stored in another Flash memory, such as the SD card in OpenSTLinux distribution.<br /> [[STM32CubeProgrammer]] must be used to prepare the NOR Flash and the SD card with the layout shown below, and to populate each partition.<br /><br> |
As NOR Flash memory is expensive, its size is usually limited to the minimum needed to store only the bootloaders. The system files (bootfs, rootfs and userfs) are usually stored in another Flash memory, such as the SD card in OpenSTLinux distribution.<br /> [[STM32CubeProgrammer]] must be used to prepare the NOR Flash and the SD card with the layout shown below, and to populate each partition.<br /><br> |
||
+ | [[File:NOR mapping.png|center|link=]] |
||
+ | |||
It is possible to use an ''e''•MMC card or NAND as second-level Flash memory, rather than an SD card. This requires the following aspects to be changed: |
It is possible to use an ''e''•MMC card or NAND as second-level Flash memory, rather than an SD card. This requires the following aspects to be changed: |
||
* The Flash memory layout, using [[STM32CubeProgrammer]] in order to write the rootfs and userfs to the targeted Flash memory |
* The Flash memory layout, using [[STM32CubeProgrammer]] in order to write the rootfs and userfs to the targeted Flash memory |
||
* The Linux kernel parameters, using [[U-Boot overview|U-Boot]], in order to indicate where the rootfs and userfs have to be mounted. |
* The Linux kernel parameters, using [[U-Boot overview|U-Boot]], in order to indicate where the rootfs and userfs have to be mounted. |
||
− | |||
== NAND memory mapping == |
== NAND memory mapping == |
||
[[STM32CubeProgrammer]] has to be used to prepare the NAND Flash memory with the layout shown below, and to populate each partition.<br /> |
[[STM32CubeProgrammer]] has to be used to prepare the NAND Flash memory with the layout shown below, and to populate each partition.<br /> |
||
[[File:NAND mapping.png|center|link=]] |
[[File:NAND mapping.png|center|link=]] |
||
+ | {{Warning|In the '''RAW/MTD area''', the number of copies to embed and the number of blocks to reserve at the end of each partition, for future bad blocks replacement, are a critical part of NAND based product dimensioning !<br> |
||
+ | The strategy has to take into account many parameters such as: |
||
+ | * the binaries sizes, |
||
+ | * the read accesses to those partitions during product life, that may generate read disturb effect, |
||
+ | * the capability of the product to refresh the partitions content when erroneous bits are detected, |
||
+ | * the number of software updates estimated on this partition, |
||
+ | * the selected NAND flash characteristics |
||
+ | ST set foundations in the STM32MP1 device in order to allow the integration of NAND flash memories but the product definition remains the customer responsibility. Please, contact your memory provider for further advice.}} |
||
<noinclude> |
<noinclude> |
||
− | [[Category: |
+ | [[Category:Platform configuration]] |
{{PublicationRequestId | 14615 | 2020-01-15 |}} |
{{PublicationRequestId | 14615 | 2020-01-15 |}} |
||
</noinclude> |
</noinclude> |