Difference between revisions of "STM32MP15 Discovery kits - getting started"

[quality revision] [quality revision]
(Supported software distribution)
m
 

The STM32MP157x-DKx Discovery kits (STM32MP157A-DK1 and STM32MP157C-DK2) constitute a flexible and complete solution for evaluating the capabilities of the STM32MP15 microprocessor devices.

All the useful information in order to start with these boards is accessible through links provided here below.

1 Supported software distribution[edit]

Only one software distribution is supported in these boards:

For this distribution, three software Packages are delivered : the Starter Package, the Developer Package, the Distribution Package.
Note that the Which Package better suits your needs article provides hints for selecting the most appropriate Package.

The STM32MP157x-DKx Discovery kits include the software packages (image, source code) and the tools needed to get started.

ST logo.png STM32MPU Embedded Software distribution[1]
Starter Package Developer Package Distribution Package
  • to evaluate the board capabilities
  • to run examples
  • to modify the pieces of software delivered as source code in this Package (for example the Linux kernel...)
  • to add custom applications in the user space (delivered as binary in this Package)

Note: these developments require a host PC running the OpenSTLinux SDK, and optionally an IDE

  • to create custom distribution

2 Hardware description[edit]

A brief article (see link below) describes the board, and provides indications on how to:

  • assemble the board
  • configure hardware switches
  • connect the board to external material

It also contains a short introduction of the board hardware components and connectors.

Board description

STM32MP157x-DKx - hardware description
STM32MP157x-DKx - hardware description

3 References[edit]



The '''STM32MP157x-DKx Discovery kits''' (STM32MP157A-DK1 and STM32MP157C-DK2) constitute a flexible and complete solution for evaluating the capabilities of the STM32MP15 microprocessor devices.

All the useful information in order to start with these boards is accessible through links provided here below.
==Supported software distribution==
Only one software distribution is supported in these boards:
* The '''STM32MPU Embedded Software distribution'''<ref name="Embedded Software distribution">[[STM32MPU Embedded Software distribution]]</ref>. You might also take a look at the latest [[STM32MP15 ecosystem release note]].

For this distribution, three software Packages are delivered : the '''Starter Package''', the '''Developer Package''', the '''Distribution Package'''.<br>

Note that the [[Which Package better suits your needs]] article provides hints for selecting the most appropriate Package.

The STM32MP157x-DKx Discovery kits include the '''software packages''' (image, source code) and the '''tools''' needed to get started.

{|class="st-table"
|-
| colspan="3" | [[File:ST_logo.png | 50px |link=]] '''STM32MPU Embedded Software distribution'''<ref name="Embedded Software distribution" />

|-
| style="width:30%; text-align:center" | [[STM32MP15 Discovery kits - Starter Package|'''Starter Package''']]
| style="width:30%; text-align:center" | [[STM32MP1 Developer Package|'''Developer Package''']]
| style="width:30%; text-align:center" | [[STM32MP1 Distribution Package|'''Distribution Package''']]
|-
|
* to evaluate the board capabilities
* to run examples 
|
* to modify the pieces of software delivered as source code in this Package (for example the Linux kernel...)
* to add custom applications in the user space (delivered as binary in this Package)
Note: these developments require a host PC running the OpenSTLinux SDK, and optionally an IDE
|
* to create custom distribution
|}

==Hardware description==
A brief article (see link below) describes the board, and provides indications on how to:
* assemble the board
* configure hardware switches
* connect the board to external material

It also contains a short introduction of the board hardware components and connectors.

{|class="st-table"
|-
! '''Board description'''
|- style="text-align:center;"wikitable" style="text-align: left; border-color:#00C0FF; background: white ;" width="50%" cellspacing="0"
|-
! style="background:#00C0FF; text-align:left;" valign="top" | <font color=white >'''Board description'''</font>

|-
|style="border-color:#00C0FF;" align="center" |
[[File:STM32MP157X-DK2.png | 400px | link=STM32MP157X-DKX - hardware description|STM32MP157x-DKx - hardware description]]<br>[[STM32MP157X-DKX - hardware description|'''STM32MP157x-DKx - hardware description''']]
|}

==References==<references/>

<noinclude>

{{ReviewsComments|File to be reviewed by the marketing communication team}}
{{PublicationRequestId | 8421 | 2018-09-13 | BrunoB}}
[[Category:STM32MP15 Discovery kits|00]]</noinclude>
Line 38: Line 38:
 
It also contains a short introduction of the board hardware components and connectors.
 
It also contains a short introduction of the board hardware components and connectors.
   
{|class="wikitable" style="text-align: left; border-color:#00C0FF; background: white ;" width="50%" cellspacing="0"
+
{|class="st-table"
 
|-
 
|-
! style="background:#00C0FF; text-align:left;" valign="top" | <font color=white >'''Board description'''</font>
+
! '''Board description'''
|-
+
|- style="text-align:center;"
|style="border-color:#00C0FF;" align="center" |
+
| [[File:STM32MP157X-DK2.png | 400px | link=STM32MP157X-DKX - hardware description|STM32MP157x-DKx - hardware description]]<br>[[STM32MP157X-DKX - hardware description|'''STM32MP157x-DKx - hardware description''']]
[[File:STM32MP157X-DK2.png | 400px | link=STM32MP157X-DKX - hardware description|STM32MP157x-DKx - hardware description]]<br>[[STM32MP157X-DKX - hardware description|'''STM32MP157x-DKx - hardware description''']]
 
 
|}
 
|}
   

Attachments

Discussions