Difference between revisions of "STM32MP157x-DKx - board assembly"

[quality revision] [quality revision]
m (Jean Christophe Trotin moved page STM32MP157X-DKX - board assembly to STM32MP157x-DKx - board assembly without leaving a redirect)
m

Template:ArticleMainWriter Template:ReviewersList Template:ArticleApprovedVersion

This article explains how to assemble the STM32MP157xSTM32MP157X-DKxDKX STM32MP15 Discovery kits. It is valid both for the STM32MP157A-DK1 and STM32MP157C-DK2 Discovery kits: the part numbers are specified in the STM32MP15 microprocessor part numbers article. kit.

Warning.png To successfully start the board, it is recommended to go through the corresponding Starter Package article: Category:Starter Package

The STM32MP157x-DKx STM32MP15 Discovery kits kit packages (STM32MP157A-DK1 and STM32MP157C-DK2) are delivered assembled, and contain STM32MP157X-DKX) include the items listed below. A USB Type-C cable is also included.

Please note that;

  • the STM32MP157ASTM32MP157X-DK1 Discovery kit neither includes the "WLAN + Bluetooth" component (muRata LBEE5KL1DX), nor the MB1407 daughterboard DSI display
  • the STM32MP157CSTM32MP157X-DK2 Discovery kit includes the "WLAN + Bluetooth" component (muRata LBEE5KL1DX), and the MB1407 daughterboard DSI display

The different variants corresponding to STM32MP157X-DK1/2 are explained by the part number codification.


File:STM32MP157X-DKX split.png
Out of the STM32MP157X-DKX box
STM32MP157x-DKx
Position Description
1 MB1272 motherboard ("WLAN + Bluetooth" component included only for the STM32MP157CSTM32MP157X-DK2 Discovery kit)
2 MB1407 daughterboard DSI display (480x800 pixels): only for the STM32MP157CSTM32MP157X-DK2 Discovery kit
3 microSD card
4 DSI ribbon cable: only for the STM32MP157X-DK2 Discovery kit
assembled
STM32MP157C-DK2 shown here (picture not contractual)
(for the STM32MP157A-DK1, the element 2 is
5 Spacer for DSI display daughterboard: only for the STM32MP157X-DK2 Discovery kit
6 USB Type-C (power 5V-3A)


The following figures explain how to assemble the various items to obtain the STM32MP15 Discovery kit.

For STM32MP157X-DK1 kits, the assembly only consists in inserting the microSD card into the dedicated slot (step C in the below figures).

File:STM32MP157X-DKX assembly 1.png
Discovery kit assembly
Board name: STM32MP157X-DK2
File:STM32MP157X-DKX assembled.png
Discovery kit assembled
Board name: STM32MP157X-DK2 (for the STM32MP157X-DK1, the elements 2, 4 and 5 are not present)
<noinclude>

{{ArticleMainWriter|Jean-ChristopheT}}
{{ReviewersList | NathalieS, BernardP, GeraldB, LaurentB}}
{{ArticleApprovedVersion | Jean-ChristopheT | BernardP, GeraldB | No previous approved version | AnneJ - 07Aug'18 - 8427 | 09Aug'18}}
[[Category:Sub-articles]]
This article explains how to assemble the '''STM32MP157x-DKx''' Discovery kits. It is valid both for the STM32MP157A-DK1 and STM32MP157C-DK2 Discovery kits: the part numbers are specified in the [[STM32MP15 microprocessor#Part number codification|STM32MP15 microprocessor part numbers]] articleSTM32MP157X-DKX''' STM32MP15 Discovery kit.
{{Warning|To successfully start the board, it is recommended to go through the corresponding Starter Package article: [[:Category:Starter Package]]}}</noinclude>

The STM32MP157x-DKxSTM32MP15 Discovery kitskit packages (STM32MP157A-DK1 and STM32MP157C-DK2) are delivered assembled, and contain STM32MP157X-DKX) include the items listed below.A USB Type-C<sup>&trade;</sup> cable is also included.

Please note that;
* the '''STM32MP157A-STM32MP157X-'''DK1''' Discovery kit neither includes the  "WLAN + Bluetooth" component (muRata LBEE5KL1DX), nor the MB1407 daughterboard DSI display
* the '''STM32MP157C-STM32MP157X-'''DK2''' Discovery kit includes the  "WLAN + Bluetooth" component (muRata LBEE5KL1DX), and the MB1407 daughterboard DSI display
The different variants corresponding to STM32MP157'''X'''-DK1/2 are explained by the [[STM32MP15 microprocessor#Part number codification|part number codification]].

[[File: STM32MP157X-DKX_split.png|thumb|upright=4|left|link=|Out of the STM32MP157X-DKX box]]{|
|+ 
! Position !! Description                                               
|-
| 1 || [[MB1272]] motherboard ("WLAN + Bluetooth" component included only for the '''STM32MP157C-STM32MP157X-'''DK2''' Discovery kit)
|-
| 2 || [[MB1407]] daughterboard DSI display (480x800 pixels): only for the '''STM32MP157C-STM32MP157X-'''DK2''' Discovery kit
|-
| 3 || microSD card
|}<br clear=all>

[[File: STM32MP157x-DKx_assembled.png | thumb | upright=4 | center | link= | STM32MP157x-DKx Discovery kit assembled <br> '''STM32MP157C-DK2''' shown here (picture not contractual) <br> (for the STM32MP157A-DK1, the element 2 is -
| 4 || DSI ribbon cable: only for the STM32MP157X-'''DK2''' Discovery kit
|-
| 5 || Spacer for DSI display daughterboard: only for the STM32MP157X-'''DK2''' Discovery kit
|-
| 6 || USB Type-C (power 5V-3A)
|}
<br clear=all>

The following figures explain how to assemble the various items to obtain the STM32MP15 Discovery kit.

For STM32MP157X-'''DK1''' kits, the assembly only consists in inserting the microSD card into the dedicated slot (step '''C''' in the below figures).

[[File: STM32MP157X-DKX_assembly_1.png|thumb|upright=4|center|link=|Discovery kit assembly <br> Board name: '''STM32MP157X-DK2''']]
<div class="NavFrame collapsed">
<div class="NavHead">Detailed description of the assembly steps</div>
<div class="NavContent">

[[File: STM32MP157X-DKX_assembly_2.png|thumb|upright=4|center|link=|Discovery kit assembly: step A <br> Board name: '''STM32MP157X-DK2''']]
[[File: STM32MP157X-DKX_assembly_3.png|thumb|upright=4|center|link=|Discovery kit assembly: steps B and C <br> Board name: '''STM32MP157X-DK2''']]
[[File: STM32MP157X-DKX_assembly_4.png|thumb|upright=4|center|link=|Discovery kit assembly: step D <br> Board name: '''STM32MP157X-DK2''']]</div>
</div>


[[File: STM32MP157X-DKX_assembled.png|thumb|upright=4|center|link=|Discovery kit assembled <br> Board name: '''STM32MP157X-DK2''' (for the STM32MP157X-DK1, the elements 2, 4 and 5 are not present)]]
Line 1: Line 1:
 
<noinclude>
 
<noinclude>
{{ArticleMainWriter|Jean-ChristopheT}}
 
{{ReviewersList | NathalieS, BernardP, GeraldB, LaurentB}}
 
 
{{ArticleApprovedVersion | Jean-ChristopheT | BernardP, GeraldB | No previous approved version | AnneJ - 07Aug'18 - 8427 | 09Aug'18}}
 
{{ArticleApprovedVersion | Jean-ChristopheT | BernardP, GeraldB | No previous approved version | AnneJ - 07Aug'18 - 8427 | 09Aug'18}}
 
 
[[Category:Sub-articles]]
 
[[Category:Sub-articles]]
 
+
This article explains how to assemble the '''STM32MP157x-DKx''' Discovery kits. It is valid both for the STM32MP157A-DK1 and STM32MP157C-DK2 Discovery kits: the part numbers are specified in the [[STM32MP15 microprocessor#Part number codification|STM32MP15 microprocessor part numbers]] article.
This article explains how to assemble the '''STM32MP157X-DKX''' STM32MP15 Discovery kit.
 
 
{{Warning|To successfully start the board, it is recommended to go through the corresponding Starter Package article: [[:Category:Starter Package]]}}
 
{{Warning|To successfully start the board, it is recommended to go through the corresponding Starter Package article: [[:Category:Starter Package]]}}
 
</noinclude>
 
</noinclude>
The STM32MP15 Discovery kit packages (STM32MP157X-DKX) include the items listed below.
+
 
  +
The STM32MP157x-DKx Discovery kits packages (STM32MP157A-DK1 and STM32MP157C-DK2) are delivered assembled, and contain the items listed below. A USB Type-C<sup>&trade;</sup> cable is also included.
   
 
Please note that;
 
Please note that;
* the STM32MP157X-'''DK1''' Discovery kit neither includes the  "WLAN + Bluetooth" component (muRata LBEE5KL1DX), nor the MB1407 daughterboard DSI display
+
* the '''STM32MP157A-DK1''' Discovery kit neither includes the  "WLAN + Bluetooth" component (muRata LBEE5KL1DX), nor the MB1407 daughterboard DSI display
* the STM32MP157X-'''DK2''' Discovery kit includes the  "WLAN + Bluetooth" component (muRata LBEE5KL1DX), and the MB1407 daughterboard DSI display
+
* the '''STM32MP157C-DK2''' Discovery kit includes the  "WLAN + Bluetooth" component (muRata LBEE5KL1DX), and the MB1407 daughterboard DSI display
The different variants corresponding to STM32MP157'''X'''-DK1/2 are explained by the [[STM32MP15 microprocessor#Part number codification|part number codification]].
 
 
 
   
[[File: STM32MP157X-DKX_split.png|thumb|upright=4|left|link=|Out of the STM32MP157X-DKX box]]
 
 
{|
 
{|
 
|+  
 
|+  
 
! Position !! Description                                               
 
! Position !! Description                                               
 
|-
 
|-
| 1 || [[MB1272]] motherboard ("WLAN + Bluetooth" component included only for the STM32MP157X-'''DK2''' Discovery kit)
+
| 1 || [[MB1272]] motherboard ("WLAN + Bluetooth" component included only for the '''STM32MP157C-DK2''' Discovery kit)
 
|-
 
|-
| 2 || [[MB1407]] daughterboard DSI display (480x800 pixels): only for the STM32MP157X-'''DK2''' Discovery kit
+
| 2 || [[MB1407]] daughterboard DSI display (480x800 pixels): only for the '''STM32MP157C-DK2''' Discovery kit
 
|-
 
|-
 
| 3 || microSD card
 
| 3 || microSD card
|-
 
| 4 || DSI ribbon cable: only for the STM32MP157X-'''DK2''' Discovery kit
 
|-
 
| 5 || Spacer for DSI display daughterboard: only for the STM32MP157X-'''DK2''' Discovery kit
 
|-
 
| 6 || USB Type-C (power 5V-3A)
 
 
|}
 
|}
 
 
<br clear=all>
 
<br clear=all>
The following figures explain how to assemble the various items to obtain the STM32MP15 Discovery kit.
+
[[File: STM32MP157x-DKx_assembled.png | thumb | upright=4 | center | link= | STM32MP157x-DKx Discovery kit assembled <br> '''STM32MP157C-DK2''' shown here (picture not contractual) <br> (for the STM32MP157A-DK1, the element 2 is not present)]]
 
 
For STM32MP157X-'''DK1''' kits, the assembly only consists in inserting the microSD card into the dedicated slot (step '''C''' in the below figures).
 
 
 
[[File: STM32MP157X-DKX_assembly_1.png|thumb|upright=4|center|link=|Discovery kit assembly <br> Board name: '''STM32MP157X-DK2''']]
 
 
 
<div class="NavFrame collapsed">
 
  <div class="NavHead">Detailed description of the assembly steps</div>
 
  <div class="NavContent">
 
[[File: STM32MP157X-DKX_assembly_2.png|thumb|upright=4|center|link=|Discovery kit assembly: step A <br> Board name: '''STM32MP157X-DK2''']]
 
[[File: STM32MP157X-DKX_assembly_3.png|thumb|upright=4|center|link=|Discovery kit assembly: steps B and C <br> Board name: '''STM32MP157X-DK2''']]
 
[[File: STM32MP157X-DKX_assembly_4.png|thumb|upright=4|center|link=|Discovery kit assembly: step D <br> Board name: '''STM32MP157X-DK2''']]
 
  </div>
 
</div>
 
 
 
[[File: STM32MP157X-DKX_assembled.png|thumb|upright=4|center|link=|Discovery kit assembled <br> Board name: '''STM32MP157X-DK2''' (for the STM32MP157X-DK1, the elements 2, 4 and 5 are not present)]]
 

Attachments

Discussions