Last edited 2 months ago

STM32MP13 peripherals overview

Applicable for STM32MP13x lines

This article lists all internal peripherals embedded in STM32MP13x lines More info.png and shows the assignment possibilities to the execution contexts for each one of them.
From this article, you can also access to individual peripheral articles with information related to the overview and configuration aspects.

1. Internal peripherals overview[edit source]

The figure below shows all peripherals embedded in STM32MP13x lines More info.png, grouped per functional domains that are reused in many places of this wiki to structure the articles.

Several execution contexts exist on STM32MP13x lines More info.png[1], corresponding to the Arm Cortex-A7 security modes:

  •  Arm Cortex-A7 secure  (Trustzone), running ROM code and TF-A BL2 at boot time, and running OP-TEE at runtime
  •  Arm Cortex-A7 non secure , running U-Boot at boot time, and running Linux at runtime

Some peripherals can be strictly assigned to one execution context, this is the case for most of the peripherals, like USART or I2C.
Other ones can be shared between several execution contexts, this is the case for system peripherals like PWR or RCC.

The legend below shows how assigned and shared peripherals are identified in the assignment diagram that follows.

STM32MP13IPsOverview legend.png

Both the diagram below and the following summary table (in Internal peripherals runtime assignment and Internal peripherals boot time assignment chapters below) are clickable in order to jump to each peripheral overview article and get more detailed information (like the software frameworks used to control them). They list STMicroelectronics recommendations. The STM32MP13 reference manual [2] may expose more possibilities then what is shown here.


Cortex-A7STGENSYSCFGRTCEXTIGICIWDG1IWDG2DMAMUX1DMAMUX2DMAMUX2DMA1DMA2DMA3MDMASAESETZPCDDRMCEPKATZCRNGHASHTAMPCRYPCRCSYSRAMDDR via DDRCTRLBKPSRAMSRAM1SRAM2SRAM3DCMIPPLTDCTIMTIMLPTIMLPTIMGPIORCCPWRDTSDDRPERFMDBGMCUHDPBSECQUADSPIFMCSDMMCUSBHOTGUSBPHYCUSARTUSARTUSARTI2CI2CSPISPIFDCANETHVREFBUFDFSDMADCSPI I2SSPI I2SSPDIFRXSAI
STM32MP13 internal peripherals overview

2. Internal peripherals runtime assignment[edit source]

Click on How to.png to expand or collapse the legend...

STM32MP13 internal peripherals

Check boxes illustrate the possible peripheral allocations supported by STM32 MPU Embedded Software:

  • means that the peripheral can be assigned to the given runtime context.
  • means that the peripheral is assigned by default to the given runtime context and that the peripheral is mandatory for the STM32 MPU Embedded Software distribution.
  • means that the peripheral can be assigned to the given runtime context, but this configuration is not supported in STM32 MPU Embedded Software distribution.
  • is used for system peripherals that cannot be unchecked because they are hardware connected in the device.

Refer to How to assign an internal peripheral to an execution context for more information on how to assign peripherals manually or via STM32CubeMX.
The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possibilities might be described in STM32MP13 reference manuals.

Domain Peripheral Runtime allocation Comment How to.png
Instance Cortex-A7
secure
(OP-TEE)
Cortex-A7
non-secure
(Linux)
Analog ADC ADC1 Assignment (single choice)
ADC2 Assignment (single choice)
ADC2 can be used for system supplies monitoring
Analog DFSDM DFSDM Assignment (single choice)
Analog VREFBUF VREFBUF Assignment (single choice)
Audio SAI SAI1 Assignment (single choice)
SAI2 Assignment (single choice)
Audio SPDIFRX SPDIFRX Assignment (single choice)
Core RTC RTC RTC is mandatory to resynchronize STGEN after exiting low-power modes.
Core STGEN STGEN
Core SYSCFG SYSCFG
Core/DMA DMA DMA1 Assignment (single choice)
DMA2 Assignment (single choice)
DMA3 Assignment (single choice)
Core/DMA DMAMUX DMAMUX1 Assignment (single choice)
DMAMUX2 Assignment (single choice)
Core/DMA MDMA MDMA Shareable (multiple choices supported)
Core/Interrupts EXTI EXTI
Core/Interrupts GIC GIC
Core/IOs GPIO GPIOA-I The pins can individually be secured
Core/RAM BKPSRAM BKPSRAM Assignment (single choice)
Core/RAM DDRCTRL DDR
Core/RAM SRAM SRAM1 Assignment (between A7 S and A7 NS)
SRAM2 Assignment (between A7 S and A7 NS)
SRAM3 Assignment (between A7 S and A7 NS)
Core/RAM SYSRAM SYSRAM Shareable (multiple choices supported)

Secure section required for low power entry and exit

Core/Timers LPTIM LPTIM1
LPTIM2 Assignment (single choice)
LPTIM3 Assignment (single choice)
LPTIM3 can be used for HSE monitoring
LPTIM4
LPTIM5
Core/Timers TIM TIM1 (APB2 group)
TIM2 (APB1 group)
TIM3 (APB1 group)
TIM4 (APB1 group)
TIM5 (APB1 group)
TIM6 (APB1 group)
TIM7 (APB1 group)
TIM8 (APB2 group)
TIM12 (APB6 group) Assignment (single choice)
TIM12 or TIM15 can be used for HSI/CSI calibration[3]
TIM13 (APB6 group) Assignment (single choice)
TIM14 (APB6 group) Assignment (single choice)
TIM15 (APB6 group) Assignment (single choice)
TIM12 or TIM15 can be used for HSI/CSI calibration[3]
TIM16 (APB6 group) Assignment (single choice)
TIM17 (APB6 group) Assignment (single choice)
Core/Watchdog IWDG IWDG1 IWDG1 is secure programmable via ETZPC but this is not used / supported so not shown in STM32CubeMX
IWDG2 Shared (none or both):
  • Cortex-A7 non secure for reload
  • Cortex-A7 secure for early interrupt handling
High speed interface OTG (USB OTG) OTG (USB OTG) Assignment (single choice)
High speed interface USBH (USB Host) USBH (USB Host)
High speed interface USBPHYC (USB HS PHY controller) USBPHYC (USB HS PHY controller) Assignment (single choice)
Low speed interface I2C I2C1
I2C2
I2C3 Assignment (single choice)
I2C4 Assignment (single choice).
Used for PMIC control on ST boards.
I2C5 Assignment (single choice)
Low speed interface
or
audio
SPI SPI2S1
SPI2S2
SPI2S3
SPI2S4 Assignment (single choice)
SPI5 Assignment (single choice)
Low speed interface USART USART1 Assignment (single choice)
USART2 Assignment (single choice)
USART3
UART4
UART5
USART6
UART7
UART8
Mass storage FMC FMC Assignment (single choice)
Mass storage QUADSPI QUADSPI Assignment (single choice)
Mass storage SDMMC SDMMC1 Assignment (single choice)
SDMMC2 Assignment (single choice)
Networking ETH ETH1 Assignment (single choice)
ETH2 Assignment (single choice)
Networking FDCAN FDCAN1
FDCAN2
Power & Thermal DTS DTS
Power & Thermal PWR PWR
Power & Thermal RCC RCC
Security BSEC BSEC
Security CRC CRC
Security CRYP CRYP Assignment (single choice)
Security ETZPC ETZPC
Security HASH HASH Assignment (single choice)
Security DDRMCE DDRMCE
Security PKA PKA Assignment (single choice)
Security RNG RNG Assignment (single choice)
Security SAES SAES Assignment (single choice)
Security TAMP TAMP
Security TZC TZC
Trace & Debug DBGMCU DBGMCU
Trace & Debug DDRPERFM DDRPERFM
Trace & Debug HDP HDP
Visual DCMIPP DCMIPP
Visual LTDC LTDC Shareable (multiple choices supported)

3. Internal peripherals boot time assignment[edit source]

Click on How to.png to expand or collapse the legend...

Check boxes illustrate the possible peripheral allocations supported by STM32 MPU Embedded Software:

  • means that the peripheral can be assigned to the given boot time context.
  • means that the peripheral is assigned by default to the given boot time context and that the peripheral is mandatory for the STM32 MPU Embedded Software distribution.
  • means that the peripheral can be assigned to the given boot time context, but this configuration is not supported in STM32 MPU Embedded Software distribution.
  • is used for system peripherals that cannot be unchecked because they are hardware connected in the device.

The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possibilities might be described in STM32 MPU reference manuals.

Domain Peripheral Boot time allocation Comment How to.png
Instance Cortex-A7
secure
(ROM code)
Cortex-A7
secure
(TF-A BL2)
Cortex-A7
non-secure
(U-Boot)
Analog ADC Any instance
Analog VREFBUF VREFBUF
Core RTC RTC
Core STGEN STGEN
Core SYSCFG SYSCFG
Core/IOs GPIO GPIOA-I The pins can individually be secured
Core/RAM BKPSRAM BKPSRAM
Core/RAM DDRCTRL DDR
Core/RAM SRAM Any instance SRAM first used by ROM code, then TF-A BL2. After assignment free to user
Core/RAM SYSRAM SYSRAM
Core/Timers LPTIM LPTIM1
LPTIM2
LPTIM3
LPTIM4
LPTIM5
Core/Timers TIM TIMx (x = 1 to 8,
APB2 group)
TIMx (x = 2 to 7,
APB1 group)
TIMx (x = 12 to 17,
APB6 group)
Core/Watchdog IWDG Any instance
High speed interface OTG (USB OTG) OTG (USB OTG) The OTG can be used by ROM code, FSBL and SSBL in DFU mode to support serial boot.
It can be used also in U-boot with command line tools.
High speed interface USBH (USB Host) USBH (USB Host)
High speed interface USBPHYC (USB HS PHY controller) USBPHYC (USB HS PHY controller) The USBPHYC can be used by ROM code, FSBL and SSBL in DFU mode to support serial boot.
It can be used also in U-boot by OTG and USBH with command line tools.
Low speed interface I2C Any instance
Low speed interface USART Any instance
Mass storage FMC FMC
Mass storage QUADSPI QUADSPI
Mass storage SDMMC SDMMC1
SDMMC2
Networking ETH Any instance Assignment (single choice)
Power & Thermal PWR PWR
Power & Thermal RCC RCC
Security BSEC BSEC
Security CRYP CRYP ROM code allocation is managed with the bit 7 in OTP 9
Security ETZPC Any instance ETZPC configuration is set by OP-TEE
Security HASH HASH
Security DDRMCE DDRMCE
Security PKA PKA Assignment is mandatory only for secure boot
Security RNG RNG Required for DPA peripheral protection
Security SAES SAES ROM code allocation is managed with the bit 7 in OTP 9
Security TAMP TAMP
Security TZC TZC
Trace & Debug DBGMCU DBGMCU
Visual LTDC LTDC

4. References[edit source]