STM32MP13 HASH internal peripheral

Revision as of 19:23, 28 October 2021 by Lionel Debieve (talk | contribs)
(diff) ← Older revision | Latest revision (diff) | Newer revision → (diff)

Applicable for STM32MP13x lines

1 Article purpose[edit]

The purpose of this article is to:

  • briefly introduce the HASH peripheral and its main features
  • indicate the level of security supported by this hardware block
  • explain how each instance can be allocated to the three runtime contexts and linked to the corresponding software components
  • explain, when necessary, how to configure the HASH peripheral.

2 Peripheral overview[edit]

The HASH peripheral is used to compute a message digest.
Digest algorithms could be:

  • SHA[1] (1, 224, 256, 384, 512)
  • Keccak-based functions[2]
    • SHA3 (224, 256, 384, 512)
    • Shake
    • RawShake

The HASH peripheral is also able to give the HMAC[3] used for authentication using the same algorithm support.

2.1 Features[edit]

Refer to the STM32MP13 reference manuals for the complete list of features, and to the software components, introduced below, to see which features are implemented.

2.2 Security support[edit]

HASH is a secure peripheral (under ETZPC control)

3 Peripheral usage and associated software[edit]

3.1 Boot time[edit]

HASH instance is used as boot device to support binary authentication.

3.2 Runtime[edit]

3.2.1 Overview[edit]

HASH instance can be allocated to:

or


Chapter Peripheral assignment describes which peripheral instance can be assigned to which context.

3.2.2 Software frameworks[edit]

Domain Peripheral Software components Comment
OP-TEE Linux
Security HASH OP-TEE HASH driver Linux Crypto framework

3.2.3 Peripheral configuration[edit]

The configuration is applied by the firmware running in the context to which the peripheral is assigned. The configuration can be done alone via the STM32CubeMX tool for all internal peripherals, and then manually completed (particularly for external peripherals), according to the information given in the corresponding software framework article.

3.2.4 Peripheral assignment[edit]

Click on the right to expand the legend...

STM32MP13IPsOverview.png

Check boxes illustrate the possible peripheral allocations supported by STM32 MPU Embedded Software:

  • means that the peripheral can be assigned () to the given runtime context.
  • means that the peripheral can be assigned to the given runtime context, but this configuration is not supported in STM32 MPU Embedded Software distribution.
  • is used for system peripherals that cannot be unchecked because they are statically connected in the device.

Refer to How to assign an internal peripheral to a runtime context for more information on how to assign peripherals manually or via STM32CubeMX.
The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possiblities might be described in STM32MP13 reference manuals.

Domain Peripheral Runtime allocation Comment
Instance Cortex-A7
secure
(OP-TEE)
Cortex-A7
non-secure
(Linux)
Security HASH HASH Assignment (single choice)

4 References[edit]