STM32CubeProgrammer flashlayout

1 Article purpose

This article describes the FlashLayout file format.

This file is used as an input by STM32CubeProgrammer tool in order to:

  1. define the Flash memory partitions (see STM32MP15_Flash_mapping)
  2. select the files used to boot (see Boot chains overview) and then populate each partition.

The embedded programming service processes this file on the device and interacts with STM32CubeProgrammer to update the Flash memory.
This is done by the stm32prog command in U-Boot. This command is automatically executed for USB boot. However you can launch it manually from the U-boot console.

The next chapter:

FSBL and SSBL definitions can be found in the Boot chains overview.

2 FlashLayout file format

The FlashLayout is a text file with a tab-separated-value format (tsv). It includes the below elements:

The lines beginning with the '#' character are ignored and treated as comments.

The "Binary" last column is not used by U-Boot. It is used by STM32CubeProgrammer on the host computer to select the files to be sent to the target.

Several tabulations (<tab>) can be used to allow the correct column alignment in the editor. They are ignored by STM32CubeProgrammer and by U-Boot.

Empty fields are not allowed. The FlashLayout file format supports the 'none' reserved word.

2.1 Examples

Below some valid FlashLayout files:

#opt	Id	Name	Type		Device	Offset		Binary
P	0x01	fsbl1	Binary		mmc0	0x00004400	fsbl.stm32
P	0x02	fsbl2	Binary		mmc0	0x00044400	fsbl.stm32
P	0x03	ssbl	Binary		mmc0	0x00084400	ssbl.stm32
P	0x10	bootfs	System		mmc0	0x00284400	bootfs.ext4.bin
P	0x11	rootfs	FileSystem	mmc0	0x08284400	rootfs.ext4.bin
PE	0x12	userfs	FileSystem	mmc0	0x28284400	none

Above, the first line contains only header information. This is not mandatory, as shown below:

-	0x01	fsbl_boot	Binary		none	0x0	fsbl.stm32
-	0x03	ssbl_boot	Binary		none	0x0	ssbl.stm32
P	0x32	sdcard		RawImage	mmc0	0x0	sdcard.bin

2.2 Field1: Options

The Options field defines the operations to perform with a combination of characters: - P D E provided in any order;
First select the line of the FlashLayout with '-' or 'P':

  • '-' : none option, the partition or the device is not modified (mandatory if #Field5: Device = none)
  • 'P' : Program the partition or the device
U-Boot requests the binary to STM32CubeProgrammer and programs the partition or the Flash device.
On block devices (SD card or e•MMC), the GPT partitioning is performed if all partitions of the device are selected with 'P'.
For the 'P' option, two optional modifiers can be added:
  • 'E' : Empty partition or device, update is not requested (associated "Id" is skipped)
  • 'D' : Delete partition or device

The only supported combinations are the following (with character in any order):

  • '-'  : no action
  • 'P'  : update = program the partition or the flash device
  • 'PE'  : do not update (also 'EP') : allow GPT partitioning with empty partition for block device but equivalent to '-' for RAW flash device
  • 'PD'  : delete and update (also 'DP')
  • 'PDE' : delete and keep empty (also 'PED' / 'DPE' / 'DEP' / 'EPD' / 'EDP')

All other combinations are invalid.

2.3 Field2: Id

Id identifies in a unique way the "download phase" requested by the device to STM32CubeProgrammer.
It is used by the embedded programming service to identify the next binary that is downloaded to the device:

  • ROM code and FSBL: binary loaded in RAM
  • SSBL (U-Boot): binary populated in Flash memory

The FlashLayout supported ranges are :

Range Partition
0x01 to 0x0F Boot partitions with STM32 header: SSBL, FSBL, other (TEE, Cortex-M4 firmware)
0x10 to 0xF0 user partitions programmed without header (uimage, dtb, rootfs, vendorfs, userfs)

The Id 0x01 and 0x03 are reserved for FSBL and SSBL, respectively. They are loaded in RAM by ROM code and by FSBL.

2.3.1 Reserved Id

The reserved values are the following:

Code Partition
0x00 FlashLayout (used internally, cannot be used in FlashLayout file)
0x01 FSBL (first copy) : used by ROM code (load in RAM)
0x03 SSBL : used by FSBL=TF-A (load in RAM)
0xF1 to 0xFD "virtual partition": used internally
0xF1 Command GetPhase
0xF2 OTP
0xF3 SSP
0xF4 PMIC NVM
0xFE End of operation
0xFF Reset

2.3.2 Using Id for boot partition

In normal use cases, the same FSBL and SSBL binaries are loaded in RAM and programmed in Flash memory. A simple mapping is used:

Code Partition
0x01 (reserved) FSBL (first copy)
0x02 (default) FSBL (second copy)
0x03 (reserved) SSBL

However, in the FlashLayout file, any other Id lower than 0x10 (boot partition with STM32 header) can identify the FSBL and SSBL binaries to be programmed in Flash memory.
It enables having different binaries loaded in RAM and programed in Flash memory, for example when an updated feature is deactivated in the binaries to be programmed in Flash memory.

You can then use the boot partitions:

Code Partition
0x01 (reserved) FSBL to boot : load by ROM code
0x03 (reserved) SSBL to boot : loaded by FSBL
0x02 FSBL to program in Flash memory (first copy)
0x04 FSBL to program in Flash memory (second copy)
0x05 SSBL to program in Flash memory

2.4 Field3: Name

Name of the alternate setting of the USB DFU[1] for U-Boot enumeration. This is a string descriptor that indicates the target memory segment (see Interface Descriptor in DFU spec [2][3]).

This is also the name of the #GPT partition of block device: SD card / e•MMC.

The requirements for the GPT partition names are:

  • FSBL for SD card boot: the name must start with 'fsbl'= fsbl, fsbl1, fsbl2... (ROM code requirement)
  • SSBL for e•MMC/SD card boot: the name must be 'ssbl' (TF-A requirement)

These two requirements are not verified by U-Boot during the flash programming. If they are not fulfilled, the ROM code or TF-A does not find the boot stage binary and the boot from Flash memory fails.

2.5 Field4: Type

Type is only used in U-Boot to select the part of Flash memory to be updated:

The supported values are:

GPT MTD
Type SD card e•MMC NAND Flash memory NOR Flash memory
Binary x x x x
Binary(N) ssbl
FileSystem x x x x
System x x UBI UBI
RAWImage x user data x x

2.5.1 Block device GPT partition: SD card / e•MMC

Refer to GPT standard for details [4].

The supported values, with associated partition type GUID (globally unique identifiers[5]), are:

  • Binary : raw data / linux reserved
    (GUID = 8DA63339-0007-60C0-C436-083AC8230908)
  • FileSystem : Linux filesystem data
    (GUID = 0FC63DAF-8483-4772-8E79-3D69D8477DE4)
    ext2/ext4/fat file system
  • System : FileSystem partition marked as bootable and used by U-Boot to find extlinux.conf configuration file (normally only one in the device, generic DISTRO feature)

For a Block device, the GPT header is updated only if all the partitions of this device are selected with the 'P' option (full update).

2.5.2 Raw Flash device (NAND/NOR Flash memories) MTD partition

The supported values are:

  • Binary: raw data, skip bad block (partition erase is not needed)
  • Binary(N): raw data, skip bad block. The loaded binary is repeated N times.
    It is only supported for NAND Flash memories. It is used to avoid disturbances during the first boot (uncorrectable ECC errors).
    The first good block is read from NAND and duplicated N times in the same partition (write skip bad block).
  • FileSystem: unspecified File system, raw data
  • System: normally UBI volume, U-Boot erases all the blocks following the last data in the MTD partition to avoid mount errors.

2.5.3 Hardware device

Export the associated device as one alternate setting by using Type=RAWImage.

  • For SD card, NOR and NAND Flash memories: all the devices
  • For e•MMC: the user data area of e•MMC (see #Field6: Offset for access to the boot area partitions)

For RAWImage, Offset=0x0 and PartId >= 0x10

2.6 Field5: Device

Select the targeted device and the instance (starting at 0) as defined by U-Boot device tree:

  • mmc + instance : 'mmc0'
    It is used for e•MMC or SD card on SDMMC. In the below examples:
    • SD card = mmc0 (SDMMC1)
    • e•MMC = mmc1 (SDMMC2)
  • nor + instance : 'nor0'
    It is used for NOR on QUADSPI.
  • nand + instance : 'nand0'
    It is used for parallel NAND Flash memories on FMC or serial NAND memories on QUADSPI.
  • none for partition only used to load the binary in RAM
    It is allowed only for the reserved boot partition (FSBL=0x1 and SSBL=0x3). In this case, the only allowed fields are :
Type=Binary, Offset=0x0 and option='-'.

Several devices can be mixed in the same FlashLayout file.

2.7 Field6: Offset

The supported values are:

  • boot1: first boot area partition of e•MMC (offset is 0x0)
  • boot2: second boot area partition of e•MMC (offset is 0x0)
  • Offset in bytes: offset in Flash memory area (in the user data area for e•MMC)

Refer to #Partition sizes for offset constraints.

2.8 Field7: Binary

This file is used by STM32CubeProgrammer to find the file associated to each Id when it is requested by embedded programming service .

The file can be absent (Binary='none' in the tsv file) only for skipped partitions tagged with the 'E' option. In all other cases, this file is sent to U-Boot to update the Flash memory only for the partitions selected with the 'P' option.

2.9 GPT partuuid of rootfs partition

If #Field3: Name = "rootfs" for block device (SD card / e•MMC), U-Boot also sets a unique partition guid [5](PARTUUID) for each instance:

  • mmc0: PARTUUID = "e91c4e10-16e6-4c0e-bd0e-77becf4a3582"
  • mmc1: PARTUUID = "491f6117-415d-4f53-88c9-6e0de54deac6"
  • mmc2: PARTUUID = "fd58f1c7-be0d-4338-8ee9-ad8f050aeb18"

This partition PARTUUID is distinct from the filesystem UUID and it is persistent.

Refer to GPT standard for details. [4]

This value can be used with the "root" argument in the kernel bootargs to identify the partition used for the "Root filesystem". For instance, "root=PARTUID=e91c4e10-16e6-4c0e-bd0e-77becf4a3582" [6] starts with the partition named rootfs on mmc0.

2.10 Partition operations

To update only one partition, use the same FlashLayout file, keep the #Field1: Options='P' for the partition to update and change the others to '-'.
To update ssbl partition:

-	0x01	fsbl1	Binary		mmc0	0x00004400	fsbl.stm32
-	0x02	fsbl2	Binary		mmc0	0x00044400	fsbl.stm32
P	0x03	ssbl	Binary		mmc0	0x00084400	ssbl.stm32
-	0x10	bootfs	System		mmc0	0x00284400	bootfs.ext4.bin
-	0x11	rootfs	FileSystem	mmc0	0x08284400	rootfs.ext4.bin
-	0x12	userfs	FileSystem	mmc0	0x28284400	userfs.ext4.bin

To delete only one partition, add the 'DE' option on the corresponding line.
To delete ssbl partition:

-	0x01	fsbl1	Binary		mmc0	0x00004400	fsbl.stm32
-	0x02	fsbl2	Binary		mmc0	0x00044400	fsbl.stm32
PDE	0x03	ssbl	Binary		mmc0	0x00084400	ssbl.stm32
-	0x10	bootfs	System		mmc0	0x00284400	bootfs.ext4.bin
-	0x11	rootfs	FileSystem	mmc0	0x08284400	rootfs.ext4.bin
-	0x12	userfs	FileSystem	mmc0	0x28284400	userfs.ext4.bin

2.11 Partition sizes

The partitions are contiguous (no holes in Flash memory).
The last partition continues until the end of the selected Flash memory.

To reduce the size of the last partition, use an 'Empty' partition and leave it unused.

All the partitions need to be present in the FlashLayout file, even if they are not selected or empty.
Then the offset and size of each partition are compared with:

  • pre-existing GPT partitioning, for updates on block devices (e•MMC or SD card)
  • predefined partitioning for MTD devices (NOR and NAND): see mtdparts environment variable in U-Boot for more information.

In case of partition size error, compare the existing partition size in U-Boot with the offset in the FlashLayout file.

2.11.1 GPT partition sizes

Each GPT partition must be aligned to:

  • 512 bytes (LBA)
  • e•MMC erase group size

The first partition starts after 17 kbytes (default size of GPT header for 128 entries in U-Boot).

Prior to updating partitions in a block device, check the partition size by executing the U-Boot command "part list" on the selected device:

Board $> part list mmc 0

Partition Map for MMC device 0  --   Partition Type: EFI

Part	Start LBA	End LBA		Name
	Attributes
	Type GUID
	Partition GUID
  1	0x00000022	0x00000221	"fsbl1"
	attrs:	0x0000000000000000
	type:	ebd0a0a2-b9e5-4433-87c0-68b6b72699c7
	type:	data
	guid:	8ef917d1-2c6f-4bd0-a5b2-331a19f91cb2
  2	0x00000222	0x00000421	"fsbl2"
	attrs:	0x0000000000000000
	type:	ebd0a0a2-b9e5-4433-87c0-68b6b72699c7
	type:	data
	guid:	77877125-add0-4374-9e60-02cb591c9737
  3	0x00000422	0x00001821	"ssbl"
	attrs:	0x0000000000000000
	type:	ebd0a0a2-b9e5-4433-87c0-68b6b72699c7
	type:	data
	guid:	b4b84b8a-04e3-48ae-8536-aff5c9c495b1
  4	0x00001822	0x00021821	"bootfs"
	attrs:	0x0000000000000004
	type:	0fc63daf-8483-4772-8e79-3d69d8477de4
	type:	linux
	guid:	35219908-c613-4b08-9322-3391ff571e19
  5	0x00021822	0x00029821	"vendorfs"
	attrs:	0x0000000000000000
	type:	0fc63daf-8483-4772-8e79-3d69d8477de4
	type:	linux
	guid:	8e123a33-e3d3-4db9-92f4-d3ebd9b3224f
  6	0x00029822	0x001a9821	"rootfs"
	attrs:	0x0000000000000000
	type:	0fc63daf-8483-4772-8e79-3d69d8477de4
	type:	linux
	guid:	02a90af2-5d1c-4a29-9177-97a513e3cae4
  7	0x001a9822	0x003a9fdc	"userfs"
	attrs:	0x0000000000000000
	type:	0fc63daf-8483-4772-8e79-3d69d8477de4
	type:	linux
	guid:	3d5088db-a534-413e-836d-c757cb682814

Warning: Start and end are indicated in mutiple of LBA (512 bytes by default).

To check the e•MMC erase group size in U-Boot, select the mmc device (here 1) and use the command "mmc info" in U-Boot.

Board $> mmc dev 1

 switch to partitions #0, OK
 mmc1(part 0) is current device

Board $> mmc info

 Device: STM32 SDMMC2
 Manufacturer ID: 11
 OEM: 100
 Name: 004G6 
 Bus Speed: 52000000
 Mode : MMC High Speed (52MHz)
 Rd Block Len: 512
 MMC version 5.0
 High Capacity: Yes
 Capacity: 3.7 GiB
 Bus Width: 8-bit
 Erase Group Size: 512 KiB
 HC WP Group Size: 4 MiB
 User Capacity: 3.7 GiB WRREL
 Boot Capacity: 2 MiB ENH
 RPMB Capacity: 512 KiB ENH

2.11.2 MTD Partition sizes

Each MTD partition must be aligned to the device erase block size (NOR/NAND Flash memory).

In U-Boot command :

Board $> nand info

 Device 0: nand0, sector size 256 KiB
   Page size       4096 b
   OOB size         224 b
   Erase size    262144 b
   subpagesize     4096 b
   options     0x00084200
   bbt options 0x00060000

Board $> sf probe

 SF: Detected mx25l51235f with page size 256 Bytes, erase size 64 KiB, total 64 MiB

For MTD, the mtdparts variable is built dynamically (in board_mtdparts_default() under CONFIG_SYS_MTDPARTS_RUNTIME). Execute the U-Boot command mtparts to known the current value, for example when NOR and NAND Flash memories are supported:

Board $> mtdparts

SF: Detected mx25l51235f with page size 256 Bytes, erase size 64 KiB, total 64 MiB

device nor0 <nor0>, # parts = 5
 #: name		size		offset		mask_flags
 0: fsbl1               0x00040000	0x00000000	0
 1: fsbl2               0x00040000	0x00040000	0
 2: ssbl                0x00200000	0x00080000	0
 3: u-boot-env         0x00040000	0x00280000	0
 4: nor_user            0x03d40000	0x002c0000	0

device nand0 <nand0>, # parts = 4
 #: name		size		offset		mask_flags
 0: fsbl                0x00200000	0x00000000	0
 1: ssbl1               0x00200000	0x00200000	0
 2: ssbl2               0x00200000	0x00400000	0
 3: UBI                 0x3fa00000	0x00600000	0

active partition: nor0,0 - (fsbl1) 0x00040000 @ 0x00000000

defaults:
mtdids  : nor0=nor0,nand0=nand0
mtdparts: mtdparts=nor0:256k(fsbl1),256k(fsbl2),2m(ssbl),256k(u-boot-env),-(nor_user);nand0:2m(fsbl),2m(ssbl1),2m(ssbl2),-(UBI)

NOR Flash last partition, named 'nor_user', is a free MTD partition.

To change the MTD partitioning on NOR and NAND Flash memories, update this variable in U-Boot.

3 Typical FlashLayout file

This chapter describes the Layout file for the typical boot use cases based on STM32MP15_Flash_mapping when TEE is not used and associated partitions are absent (teeh, teed and teex).

Data are presented in tables for better readability despite the Layout file is plain text.

In the example, the trusted boot chain is used together with the following files:

  • FSBL = tf-a.stm32
  • SSBL = u-boot.stm32

3.1 Basic boot chain support

The layout in NVM is the same for the basic boot chain (see STM32MP15_Flash_mapping).

Warning.png The basic boot chain cannot be used for product development (see Boot chains overview for details).

The files that must be programmed in NVM for the basic boot chain are:

  • FSBL = u-boot-spl.stm32 (instead of tf-a.stm32)
  • SSBL = u-boot.img (instead of u-boot.stm32).

However, the basic boot chain does not support the STM32CubeProgrammer (use the trusted bootloaders to program the basic boot chain bootloaders in Flash memory) and the SSBL is programmed wihout STM32 header (with PhaseId ≥ 0x10).

3.2 NOR Flash memory and SD card

NOR Flash memory in RAW: Bootloaders = FSBL. It uses two copies (for failsafe update) and one copy for SSBL.
SD card using GPT: several user EXT4 partitions.

Opt Part Name Type Device Offset Binary
P 0x01 fsbl1 Binary nor0 0x0 tf-a.stm32
P 0x02 fsbl2 Binary nor0 0x40000 tf-a.stm32
P 0x03 ssbl Binary nor0 0x80000 u-boot.stm32
PE 0x20 u-boot-env Binary nor0 0x280000 none
PE 0x21 unused Binary nor0 0X2C0000 none
P 0x10 bootfs System mmc0 0x00004400 bootfs.ext4.bin
P 0x11 vendorfs FileSystem mmc0 0x04284400 vendorfs.ext4.bin
P 0x12 rootfs FileSystem mmc0 0x05284400 rootfs.ext4.bin
P 0x13 userfs FileSystem mmc0 0x35284400 userfs.ext4.bin

The PartId 0x20 is empty/free in nor0, no logo is provided.

The PartId 0x21 is an empty/free user partition associated to 'nor_user' MTD partition in U-Boot

3.3 NOR and NAND Flash memories

NOR Flash memory in RAW: TF-A uses several partitions for failsafe update, then U-Boot.
NAND Flash memory in UBI: only one large MTD partition for UBI volumes and UBIFS.

Opt Part Name Type Device Offset Binary
P 0x01 fsbl1 Binary nor0 0x0 tf-a.stm32
P 0x02 fsbl2 Binary nor0 0x40000 tf-a.stm32
P 0x03 ssbl Binary nor0 0x80000 u-boot.stm32
PE 0x20 u-boot-env Binary nor0 0x280000 none
PE 0x21 unused Binary nor0 0x2C0000 none
P 0x10 UBI FileSystem nand0 0x0 ubi.bin

The PartId 0x21 is an empty/free user partition associated to 'nor_user' MTD partition in U-Boot.

Warning: for compatility with NAND-only use case and U-Boot configuration on ST board, the offset of UBI in nand0 is set to 0x00600000.

3.4 NAND Flash memory

BootLoader using RAW and then file system in UBI volume.

3.4.1 FSBL:RAW & SSBL:UBI

FSBL (TF-A) uses two RAW copies to avoid NAND Flash memory disturbances inside one partition.

SSBL (U-Boot) is present in a RAW volume of the UBI partition.
The binary is also present in FlashLayout file to be loaded in RAM (Opt='-', Part=0x3, Device='none').

Opt Part Name Type Device Offset Binary
P 0x01 fsbl Binary(2) nand0 0x0 tf-a.stm32
- 0x03 ssbl Binary none 0x0 u-boot.stm32
P 0x10 UBI FileSystem nand0 0x00200000 ubi.bin

Warning: The MTD partitioning must be changed in U-Boot.

3.4.2 FSBL+SSBL:RAW

FSBL (TF-A) uses two copies in two partitions (for failsafe update) to avoid NAND Flash memory disturbances.

SSBL (U-Boot) uses two copies in two partitions (and not in a UBI volume).

One MTD partition for UBI with several volumes: boot, rootfs and userfs.

Opt Part Name Type Device Offset Binary
P 0x01 fsbl1 Binary(2) nand0 0x0 tf-a.stm32
P 0x02 fsbl2 Binary(2) nand0 0x100000 tf-a.stm32
P 0x03 ssbl1 Binary nand0 0x200000 u-boot.bin
P 0x04 ssbl2 Binary nand0 0x400000 u-boot.bin
P 0x10 UBI FileSystem nand0 0x600000 ubi.bin

3.5 e•MMC

TF-A copied in the two boot area partitions of e•MMC (hidden partition).

GPT partitioning is used on the user area. U-Boot starts just after the GPT header at 17-Kbyte offset.

The userfs partition is pre-populated with ext4 partition.

Opt Part Name Type Device Offset Binary
P 0x01 fsbl1 Binary mmc1 boot1 tf-a.stm32
P 0x02 fsbl2 Binary mmc1 boot2 tf-a.stm32
P 0x03 ssbl Binary mmc1 0x00080000 u-boot.stm32
P 0x10 bootfs System mmc1 0x00280000 bootfs.ext4.stm32
P 0x11 vendorfs FileSytem mmc1 0x04280000 vendorfs.ext4.bin
P 0x12 rootfs FileSytem mmc1 0x05280000 rootfs.ext4.bin
P 0x13 userfs FileSytem mmc1 0x35280000 userfs.ext4.bin

3.6 SD card

RAW partition: two TF-A partitions, then U-Boot. GPT partitioning is used so fsbl1 starts just after GPT header at 17-Kbyte offset.

Opt Part Name Type Device Offset Binary
P 0x01 fsbl1 Binary mmc0 0x4400 tf-a.stm32
P 0x02 fsbl2 Binary mmc0 0x00044400 tf-a.stm32
P 0x03 ssbl Binary mmc0 0x00084400 u-boot.stm32
P 0x10 bootfs System mmc0 0x00284400 bootfs.ext4.bin
P 0x11 vendorfs FileSytem mmc0 0x04284400 vendorfs.ext4.bin
P 0x12 rootfs FileSytem mmc0 0x05284400 rootfs.ext4.bin
P 0x13 userfs FileSytem mmc0 0x35284400 userfs.ext4.bin

4 Typical FlashLayout file with TEE

This chapter describes the Layout file with TEE partitions for the trusted typical boot use case based on STM32MP15_Flash_mapping.

Since TF-A binary for OPTEE does not yet support STM32CubeProgrammer, two different FSBL binaries are used:

  • to boot = tf-a.stm32 (no TEE support but programmer support)
  • to flash = tf-a-optee.stm32

Since the MTD partitionning is hardcoded in U-Boot, the optee variant is used : u-boot-optee.stm32.

4.1 NOR Flash memory and SD card with TEE

Opt Part Name Type Device Offset Binary
- 0x01 fsbl Binary none 0x0 tf-a.stm32
P 0x02 fsbl1 Binary nor0 0x0 tf-a-optee.stm32
P 0x04 fsbl2 Binary nor0 0x40000 tf-a-optee.stm32
P 0x03 ssbl Binary nor0 0x80000 u-boot-optee.stm32
PE 0x20 u-boot-env Binary nor0 0x280000 none
P 0x05 teeh Binary nor0 0x002C0000 tee-header.stm32
P 0x06 teed Binary nor0 0x00300000 tee-pageablee.stm32
P 0x07 teex Binary nor0 0x00340000 tee-pager.stm32
PE 0x21 unused Binary nor0 0x380000 none
P 0x10 bootfs System mmc0 0x00004400 bootfs.ext4.bin
P 0x11 vendorfs FileSystem mmc0 0x04284400 vendorfs.ext4.bin
P 0x12 rootfs FileSystem mmc0 0x05284400 rootfs.ext4.bin
P 0x13 userfs FileSystem mmc0 0x35284400 userfs.ext4.bin

4.2 NOR and NAND Flash memories with TEE

Opt Part Name Type Device Offset Binary
- 0x01 fsbl Binary none 0x0 tf-a.stm32
P 0x02 fsbl1 Binary nor0 0x0 tf-a-optee.stm32
P 0x04 fsbl2 Binary nor0 0x40000 tf-a-optee.stm32
P 0x03 ssbl Binary nor0 0x80000 u-boot-optee.stm32
PE 0x20 u-boot-env Binary nor0 0x280000 none
P 0x05 teeh Binary nor0 0x002C0000 tee-header.stm32
P 0x06 teed Binary nor0 0x00300000 tee-pageablee.stm32
P 0x07 teex Binary nor0 0x00340000 tee-pager.stm32
PE 0x21 unused Binary nor0 0x380000 none
P 0x10 UBI FileSystem nand0 0x0 ubi.bin

4.3 NAND Flash memory with TEE

4.3.1 FSBL:RAW & SSBL:UBI with TEE

Opt Part Name Type Device Offset Binary
- 0x01 fsbl Binary none 0x0 tf-a.stm32
P 0x02 fsbl Binary(2) nand0 0x0 tf-a-optee.stm32
- 0x03 ssbl Binary none 0x0 u-boot-optee.stm32
P 0x10 UBI FileSystem nand0 0x00200000 ubi.bin

4.3.2 FSBL+SSBL:RAW with TEE

WARNING: the 'tee' partitions are not duplicated in the next example (possible issue with NAND disturbance).

Opt Part Name Type Device Offset Binary
- 0x01 fsbl Binary none 0x0 tf-a.stm32
P 0x05 fsbl1 Binary(2) nand0 0x0 tf-a-optee.stm32
P 0x04 fsbl2 Binary(2) nand0 0x100000 tf-a-optee..stm32
P 0x03 ssbl1 Binary nand0 0x200000 u-boot-optee.bin
P 0x02 ssbl2 Binary nand0 0x400000 u-boot-optee.bin
P 0x06 teeh Binary nand0 0x600000 tee-header.stm32
P 0x07 teed Binary nand0 0x680000 tee-pageable.stm32
P 0x08 teex Binary nand0 0x700000 tee-pager.stm32
P 0x10 UBI FileSystem nand0 0x780000 ubi.bin

4.4 e•MMC with TEE

Opt Part Name Type Device Offset Binary
- 0x01 fsbl Binary none 0x0 tf-a.stm32
P 0x02 fsbl1 Binary mmc1 boot1 tf-a-optee.stm32
P 0x04 fsbl2 Binary mmc1 boot2 tf-a-optee.stm32
P 0x03 ssbl Binary mmc1 0x00080000 u-boot-optee.stm32
P 0x05 teeh Binary mmc1 0x00280000 tee-header.stm32
P 0x06 teed Binary mmc1 0x00300000 tee-pageable.stm32
P 0x07 teex Binary mmc1 0x00380000 tee-pager.stm32
P 0x10 bootfs System mmc1 0x00400000 bootfs.ext4.stm32
P 0x11 vendorfs FileSytem mmc1 0x04400000 vendorfs.ext4.bin
P 0x12 rootfs FileSytem mmc1 0x05400000 rootfs.ext4.bin
P 0x13 userfs FileSytem mmc1 0x35400000 userfs.ext4.bin

4.5 SD card with TEE

Opt Part Name Type Device Offset Binary
- 0x01 fsbl Binary none 0x0 tf-a.stm32
P 0x02 fsbl1 Binary mmc0 0x4400 tf-a-optee.stm32
P 0x04 fsbl2 Binary mmc0 0x00044400 tf-a-optee.stm32
P 0x03 ssbl Binary mmc0 0x00084400 u-boot-optee.stm32
P 0x05 teeh Binary mmc0 0x00284400 tee-header.stm32
P 0x06 teed Binary mmc0 0x00294400 tee-pageable.stm32
P 0x07 teex Binary mmc0 0x002C4400 tee-pager.stm32
P 0x10 bootfs System mmc0 0x00304400 bootfs.ext4.bin
P 0x11 vendorfs FileSytem mmc0 0x04304400 vendorfs.ext4.bin
P 0x12 rootfs FileSytem mmc0 0x05304400 rootfs.ext4.bin
P 0x13 userfs FileSytem mmc0 0x35304400 userfs.ext4.bin

5 Using provided FlashLayout files

The binary and the associated pre-defined FlashLayout file are provided by ST in the Discovery kit.

For example, in STM32MP15 Discovery kits, you can find the distribution images as well as the file FlashLayout_sdcard_stm32mp157c-ev1-trusted.tsv:

#Opt	Id	Name		Type		Device	Offset		Binary
P	0x01	fsbl1		Binary		mmc0	0x00004400	tf-a-stm32mp15c-ev1-trusted.stm32
P	0x02	fsbl2		Binary		mmc0	0x00044400	tf-a-stm32mp15c-ev1-trusted.stm32
P	0x03	ssbl		Binary		mmc0	0x00084400	u-boot-stm32mp15c-ev1-trusted.stm32
P	0x10	bootfs		System		mmc0	0x00294400	st-image-bootfs-openstlinux-weston-stm32mp1.ext4
P	0x11	vendorfs	FileSystem	mmc0	0x00294400	st-image-vendorfs-openstlinux-weston-stm32mp1.ext4
P	0x12	rootfs		FileSystem	mmc0	0x02294400	st-image-core-openstlinux-weston-stm32mp1.ext4
P	0x13	userfs		FileSystem	mmc0	0x22295800	st-image-userfs-openstlinux-weston-stm32mp1.ext4

You can use these FlashLayout files as a starting point and simply modify them:

5.1 Updating partitions

To update only some partitions, change the FlashLayout and only "select" the partitions that need to be updated:
Options field inside the FlashLayout is kept to 'P' for partition(s) that need to be updated, others are changed to '-'.
Then execute STM32CubeProgrammer as before.

Example to update only U-Boot binary and st-image-bootfs filesystem :

Opt Part Name Type Device Offset Binary
- 0x01 fsbl1 Binary mmc0 0x00004400 tf-a-stm32mp15c-ev1-trusted.stm32
- 0x02 fsbl2 Binary mmc0 0x00044400 tf-a-stm32mp15c-ev1-trusted.stm32
P 0x03 ssbl Binary mmc0 0x00084400 u-boot-stm32mp15c-ev1-trusted.stm32
P 0x10 bootfs System mmc0 0x00304400 st-image-bootfs-openstlinux-weston-stm32mp1.ext4
- 0x11 vendorfs FileSystem mmc0 0x04304400 st-image-vendorfs-openstlinux-weston-stm32mp1.ext4
- 0x12 rootfs FileSystem mmc0 0x05304400 st-image-core-openstlinux-weston-stm32mp1.ext4
- 0x13 userfs FileSystem mmc0 0x35304400 st-image-userfs-openstlinux-weston-stm32mp1.ext4

The associated text file becomes :

#Opt	Id	Name		Type		Device	Offset		Binary
-	0x01	fsbl1		Binary		mmc0	0x00004400	tf-a-stm32mp15c-ev1-trusted.stm32
-	0x02	fsbl2		Binary		mmc0	0x00044400	tf-a-stm32mp15c-ev1-trusted.stm32
P	0x03	ssbl		Binary		mmc0	0x00084400	u-boot-stm32mp15c-ev1-trusted.stm32
P	0x10	bootfs		System		mmc0	0x00294400	st-image-bootfs-openstlinux-weston-stm32mp1.ext4
-	0x11	vendorfs	FileSystem	mmc0	0x00294400	st-image-vendorfs-openstlinux-weston-stm32mp1.ext4
-	0x12	rootfs		FileSystem	mmc0	0x02294400	st-image-core-openstlinux-weston-stm32mp1.ext4
-	0x13	userfs		FileSystem	mmc0	0x22295800	st-image-userfs-openstlinux-weston-stm32mp1.ext4

5.2 Updating partitions using official ST bootloaders

If bootloader, FSBL or SSBL are modified, and the STM32CubeProgrammer support is lost for any reason (for example if the stm32prog command is removed), you can still program these new files by selecting the correct binary setting for the partitions 0x01 and 0x03 with Device='none' and change the Id for the binaries to program in flash, as indicated in chapter "Field2: Id".

For example, with ST board, you can flash Customer-modified binary by using ST original file. The new Layout file is:

Opt Part Name Type Device Offset Binary
- 0x01 fsbl-boot Binary none 0x0 tf-a-stm32mp15c-ev1-trusted.stm32
- 0x03 ssbl-boot Binary none 0x0 u-boot-stm32mp15c-ev1-trusted.stm32
P 0x02 fsbl2 Binary mmc0 0x00004400 <Customer-tf-a>.stm32
P 0x04 fsbl1 Binary mmc0 0x00044400 <Customer-tf-a>.stm32
P 0x05 ssbl Binary mmc0 0x00084400 <Customer-u-boot>.stm32
P 0x10 bootfs System mmc0 0x00304400 st-image-bootfs-openstlinux-weston-stm32mp1.ext4
P 0x11 vendorfs FileSystem mmc0 0x04304400 st-image-vendorfs-openstlinux-weston-stm32mp1.ext4
P 0x12 rootfs FileSystem mmc0 0x05304400 st-image-core-openstlinux-weston-stm32mp1.ext4
P 0x13 userfs FileSystem mmc0 0x35304400 st-image-userfs-openstlinux-weston-stm32mp1.ext4

The associated text file becomes :

#Opt	Id	Name		Type		Device	Offset		Binary
-	0x01	fsbl1		Binary		none	0x0		tf-a-stm32mp15c-ev1-trusted.stm32
-	0x03	ssbl		Binary		none	0x0		u-boot-stm32mp15c-ev1-trusted.stm32
P	0x02	fsbl1		Binary		mmc0	0x00004400	tf-a.stm32
P	0x04	fsbl2		Binary		mmc0	0x00044400	tf-a.stm32
P	0x05	ssbl		Binary		mmc0	0x00084400	u-boot.stm32
P	0x10	bootfs		System		mmc0	0x00294400	st-image-bootfs-openstlinux-weston-stm32mp1.ext4
P	0x11	vendorfs	System		mmc0	0x00294400	st-image-vendorfs-openstlinux-weston-stm32mp1.ext4
P	0x12	rootfs		FileSystem	mmc0	0x02294400	st-image-core-openstlinux-weston-stm32mp1.ext4
P	0x13	userfs		FileSystem	mmc0	0x22295800	st-image-userfs-openstlinux-weston-stm32mp1.ext4

6 Other FlashLayout examples

6.1 SD card: FAT

Below an example with FAT bootfs partition (kernel and RAMFS) and an empty userfs partition (deleted and formatted by Linux on first boot):

Opt Part Name Type Device Offset Binary
P 0x01 fsbl1 Binary mmc0 0x0 tf-a.stm32
P 0x02 fsbl2 Binary mmc0 0x40000 tf-a.stm32
P 0x03 ssbl Binary mmc0 0x80000 u-boot.stm32
P 0x10 bootfs System mmc0 0x200000 bootfs.vfat.bin
PED 0x11 userfs Empty mmc0 0x400000 none

6.2 Load and program different binaries

Same example as above with the first two partitions (named "2boot"). They are not programmed and only loaded in RAM.

Userfs is empty but not deleted.

Opt Part Name Type Device Offset Binary
- 0x01 fsbl2boot Binary none 0x0 tf-a2boot.stm32
- 0x03 ssbl2boot Binary none 0x0 u-boot2boot.stm32
P 0x02 fsbl1 Binary mmc0 0x40000 tf-a.stm32
P 0x04 fsbl2 Binary mmc0 0x0 tf-a.stm32
P 0x05 ssbl Binary mmc0 0x80000 u-boot.stm32
P 0x10 rootfs System mmc0 0x200000 rootfs.vfat.bin
PE 0x11 userfs FileSytem mmc0 0x400000 none

6.3 RAWImage

The SD card content is exported as RAW device and updated with the image.sdcard file:

Opt Part Name Type Device Offset Binary
- 0x01 fsbl Binary none 0x0 tf-a.stm32
- 0x03 ssbl Binary none 0x0 u-boot.stm32
P 0x10 sdcard RawImage mmc0 0x0 image.sdcard

You can also erase the device before performing the update, by adding 'D' in option.

6.4 Deleting device content

For example, NOR and NAND Flash memories are deleted with:

Opt Part Name Type Device Offset Binary
- 0x01 fsbl none none 0x0 tf-a.stm32
- 0x03 ssbl none none 0x0 u-boot.stm32
PDE 0x10 nor RawImage nor0 0x0 none
PDE 0x11 nand RawImage nand0 0x0 none

To erase all other devices, including the e•MMC boot partition, proceed as follows:

Opt Part Name Type Device Offset Binary
- 0x01 fsbl1 Binary none 0x0 tf-a.stm32
- 0x03 ssbl Binary none 0x0 u-boot.stm32
PDE 0x10 sdcard RawImage mmc0 0x0 none
PED 0x20 emmc_boot1 Binary mmc1 boot1 none
DPE 0x21 emmc_boot2 Binary mmc1 boot2 none
EPD 0x22 emmc RawImage mmc1 0x0 none
DPE 0x30 nand RawImage nand0 0x0 none
PDE 0x40 nor RawImage nor0 0x0 none

Warning: A timeout may occur in STM32CubeProgrammer since deleting NOR Flash memory might be slow. To avoid this issue you can delete only the used partitions (Option=PED), for example:

#Opt	Id	Name		Type		Device	Offset		Binary
-	0x01	fsbl_boot	Binary		none	0x0		fsbl.stm32
-	0x03	ssbl_boot	Binary		none	0x0		ssbl.stm32
#delete ALL devices
EPD	0x10	sdcard		RawImage	mmc0	0x0		none
PED	0x02	emmc_b1		Binary		mmc1	boot1		none
PED	0x04	emmc_b2		Binary		mmc1	boot2		none
PED	0x20	emmc		RawImage	mmc1	0x0		none
PED	0x30	nand		RawImage	nand0	0x0		none
# on NOR (slow device): delete ALL used partitions
PE	0x40	nor		RawImage	nor0	0x0		none
PED	0x41	fsbl1_nor	Binary		nor0	0x00000000	none
PED	0x42	fsbl2_nor	Binary		nor0	0x00040000	none
PED	0x43	ssbl_nor	Binary		nor0	0x00080000	none
PED	0x44	u-boot-env_nor	Binary		nor0	0x00280000	none
PE	0x45	unused		Binary		nor0	0x002C0000	none

6.5 Complex use case

Update SD card (mmc0 on SDMMC1). The GPT partition is created since all partitions are selected and Userfs is deleted and empty.

Erase all other devices, including e•MMC hidden boot partition.

Opt Part Name Type Device Offset Binary
P 0x01 fsbl1 Binary mmc0 0x04400 tf-a.stm32
P 0x02 fsbl2 Binary mmc0 0x44400 tf-a.stm32
P 0x03 ssbl Binary mmc0 0x84400 u-boot.stm32
P 0x10 bootfs System mmc0 0x284400 bootfs.stm32
P 0x11 rootfs FileSytem mmc0 0x08284400 rootfs.ext4.bin
DEP 0x12 userfs FileSytem mmc0 0x28284400 none
PED 0x60 emmc_boot1 Binary mmc1 boot1 none
DPE 0x61 emmc_boot2 Binary mmc1 boot2 none
EPD 0x62 emmc RawImage mmc1 0x0 none
D 0x10 nand RawImage nand0 0x0 none

7 Reference list


Attachments

Discussions