Difference between revisions of "STM32-CoPro-MPU plugin release note"

[quality revision] [quality revision]
m
 

More information can be found in the detailed release notes referenced later in this article.

SW4TM32 - System Workbench for STM32 2.9.0 - STM32-CoPro-MPU plugin[edit]

The STM32-CoPro-MPU plugin, based onto the System Workbench for STM32 (SW4STM32), targets the support of Cortex®-M core contained in the STM32MP1 Family.
It is included in System Workbench for STM32 from version 2.9.0.
It provides:

  • the target status widget,
  • the console management,
  • the project creation, compilation and debug in two modes:
    • Engineering Mode,
    • Production Mode, with Cortex®-M firmware download :
      • via Ethernet Network (LAN or Point-to-Point)
      • via Ethernet over USB
  • the remote system explorer configuration


It is available on Linux® and Windows® platforms.

Upgrading your System Workbench, STM32-CoPro-MPU plugin can be installed using the System Workbench for STM32 - Updates in menu Windows > Preferences > Install/Update > Available Software Site.
The installation is then the standard Eclipse one: Help > Install New Software...

In order to access to the Ac6 site, take care to configure proxy at Eclipse level: in Windows > Preferences > General > Network Connections; Active Provider set to Manual.
Then after selecting HTTP proxy entry, click Edit... and enter your proxy setup.


IDE for Linux® host PC IDE for Windows® host PC
Download

STM32-CoPro-MPU plugin in SW4STM32 2.9.0

  • Download the all-in-one Linux installer 2.9 install_sw4stm32_linux_64bits-v2.9.run from openstm32.org

STM32-CoPro-MPU plugin in SW4STM32 2.9.0

  • Download the all-in-one Windows installer 2.9 install_sw4stm32_win_64bits-v2.9.exe from openstm32.org
Installation
  • Run the installation script
$ chmod +x install_sw4stm32_linux_64bits-v2.9.run
$ ./install_sw4stm32_linux_64bits-v2.9.run

  • Run the installation exe
$ install_sw4stm32_win_64bits-v2.9.exe

Detailed release notes Details about the content of this tool version are available on openstm32.org

Details about the content of this tool version are available on openstm32.org




More information can be found in the detailed release notes referenced later in this article.

== SW4TM32 - System Workbench for STM32 2.9.0 - ''STM32-CoPro-MPU plugin''==

The '''STM32-CoPro-MPU''' plugin, based onto the ''System Workbench for STM32'' (SW4STM32), targets the support of Cortex<sup>&reg;</sup>-M core contained in the STM32MP1 Family. <br>

It is included in '''System Workbench for STM32''' from version 2.9.0. <br>

It provides:<br>

* the target status widget, 
* the console management, 
* the project creation, compilation and debug in two modes:
** '''Engineering Mode''', 
** '''Production Mode''', with Cortex<sup>&reg;</sup>-M firmware download :
***via Ethernet Network (LAN or Point-to-Point)
***via Ethernet over USB
*the remote system explorer configuration<br>

It is available on Linux<sup>&reg;</sup> and Windows<sup>&reg;</sup> platforms. <br>
<br>


Upgrading your System Workbench, '''STM32-CoPro-MPU''' plugin can be installed using the [http://www.ac6-tools.com/Eclipse-updates/org.openstm32.system-workbench.update-site-v2/ System Workbench for STM32 - Updates] 
in menu ''Windows > Preferences > Install/Update > Available Software Site''.  <br>

The installation is then the standard Eclipse one: ''Help > Install New Software...''  <br> 
<br>

In order to access to the Ac6 site, take care to configure proxy at Eclipse level: in ''Windows > Preferences > General > Network Connections''; Active Provider set to ''Manual''. <br>

Then after selecting ''HTTP'' proxy entry, click ''Edit...'' and enter your proxy setup.
<onlyinclude>

{| class="st-tablewikitable" width=98%
|-
!  !! style="text-align:center;"|IDE for Linux<sup>&reg;</sup> host PC!!style="text-align:center;"| IDE for Windows<sup>&reg;</sup> host PC
|-
| '''Download''' 
|| 
'''STM32-CoPro-MPU plugin in SW4STM32 2.9.0 '''
*Download the all-in-one Linux installer 2.9 '''install_sw4stm32_linux_64bits-v2.9.run''' from [http://www.openstm32.org/HomePage openstm32.org]
|| 
'''STM32-CoPro-MPU plugin in SW4STM32 2.9.0 '''
*Download the all-in-one Windows installer 2.9 '''install_sw4stm32_win_64bits-v2.9.exe''' from [http://www.openstm32.org/HomePage openstm32.org]
|-
| '''Installation''' 
|| 
* Run the installation script
 $ chmod +x install_sw4stm32_linux_64bits-v2.9.run
 $ ./install_sw4stm32_linux_64bits-v2.9.run
*Then follow instructions given on [http://www.openstm32.org/HomePage openstm32.org]
* '''When the installation is over''', to use the tool, you can follow instruction given in [[STM32-CoPro-MPU plugin for SW4STM32]] or in the detailed release note. 
||
* Run the installation exe
 $ install_sw4stm32_win_64bits-v2.9.exe
*Then follow instructions given on [http://www.openstm32.org/HomePage openstm32.org]
* '''When the installation is over''', to use the tool, you can follow instruction given in [[STM32-CoPro-MPU plugin for SW4STM32]] or in the detailed release note. 
|-
| '''Detailed release notes''' 
||Details about the content of this tool version are available on [http://www.openstm32.org/HomePage openstm32.org]
||
Details about the content of this tool version are available on [http://www.openstm32.org/HomePage openstm32.org]
|}</onlyinclude>

<noinclude>

{{PublicationRequestId | 8349 | 2018-08-14 | AlainF}}
[[Category:Release notes|5]]
[[Category:SW4STM32 IDE]]

{{UpdateNeededForNewRelease|
* Copy the current release (first chapter) in the "Archives" chapter
* Change the version of the tool
* Change the name of the archive file
* Change the download URLs
}}</noinclude>
Line 26: Line 26:
   
 
<onlyinclude>
 
<onlyinclude>
{| class="wikitable" width=98%
+
{| class="st-table" width=98%
 
|-
 
|-
!  !! IDE for Linux<sup>&reg;</sup> host PC!! IDE for Windows<sup>&reg;</sup> host PC
+
!  !! style="text-align:center;"|IDE for Linux<sup>&reg;</sup> host PC!!style="text-align:center;"| IDE for Windows<sup>&reg;</sup> host PC
 
|-
 
|-
 
| '''Download'''  
 
| '''Download'''  

Attachments

Discussions