Difference between revisions of "STM32-CoPro-MPU plugin release note"

[unchecked revision] [quality revision]
m

Template:ArticleMainWriter Template:ReviewersList Template:ArticleApprovedVersion

More information can be found in the detailed release notes referenced later in this article.

SW4TM32 - System Workbench for STM32 2.9.0 - STM32-CoPro-MPU plugin version 1.0.0[edit]

The STM32-CoPro-MPU plugin, based onto the System Workbench for STM32 (SW4STM32), targets the support of Cortex®-M core contained in the STM32MP1 Family.
It is included in System Workbench for STM32 from version 2.9.0.
It provides:

  • the target status widget,
  • the console management,
  • the project creation, compilation and debug in two modes:
    • Engineering Mode,
    • Production Mode, with Cortex®-M firmware download :
      • via Ethernet Network (LAN or Point-to-Point)
      • via Ethernet over USB
  • the remote system explorer configuration


It is available on Linux® and Windows® platforms.

Upgrading your System Workbench, STM32-CoPro-MPU plugin can be installed using the System Workbench for STM32 - Updates in menu Windows > Preferences > Install/Update > Available Software Site.
The installation is then the standard Eclipse one: Help > Install New Software...

In order to access to the Ac6 site, take care to configure proxy at Eclipse level: in Windows > Preferences > General > Network Connections; Active Provider set to Manual.
Then after selecting HTTP proxy entry, click Edit... and enter your proxy setup.


IDE for Linux® host PC IDE for Windows® host PC
Download

Version 1.0.0 STM32-CoPro-MPU plugin in SW4STM32 2.9.0

  • Download the all-in-one Linux installer 2.9 install_sw4stm32_linux_64bits-v2.9.run from openstm32.org

Version 1.0.0 STM32-CoPro-MPU plugin in SW4STM32 2.9.0

  • Download the all-in-one Windows installer 2.9 install_sw4stm32_win_64bits-v2.9.exe from openstm32.org
Installation
  • Run the installation script
$ chmod +x install_sw4stm32_linux_64bits-v2.9.run
$ ./install_sw4stm32_linux_64bits-v2.9.run
  • Run the installation exe
$ install_sw4stm32_win_64bits-v2.9.exe
Detailed release notes Details about the content of this tool version are available on openstm32.org

Details about the content of this tool version are available on openstm32.org




<noinclude>

{{ArticleMainWriter|LudovicR}}
{{ReviewersList|To be completed by LudovicR}}
{{ArticleApprovedVersion| LudovicR | BernardP | NathalieS - 29Aug'18 | AlainF - 14Aug'18 - 8349 | 21Nov'18}}

[[Category:Release notes|5]]
[[Category:SW4STM32 IDE]]

{{UpdateNeededForNewRelease|
* Copy the current release (first chapter) in the "Archives" chapter
* Change the version of the tool
* Change the name of the archive file
* Change the download URLs
}}</noinclude>


 {{ReviewsComments|ECO: The release 2.8.0 is not available anymore on AC6 web site. Now 2.9.0 }}
{{ReviewsComments|LVI: I copy comments from YCO made on the wrong Wiki page.
YCO 18-Feb-19 : Eclipse tool version 2.8 install_sw4stm32_linux_64bits-v2.8.run from openstm32.org not available<br>

YCO 19-Feb-19 : I have install the Eclipse tool version 2.8 for Linux "install_sw4stm32_linux_64bits-v2.8.run" from https://citools.st.com/snapshots/artifactory/webapp/#/artifacts/browse/tree/General/snapshots-stm32ide-codex-st-com/refs/tags/2.8.0/allinone/install_sw4stm32_linux_64bits.run <br>

We need to clarify the install process : <br>

- Do we need to desinstall a older version, according to the process described in AC6 (with the allinone installer), "NO" the workspace folder is overwritten, to be confirmed because I faced some troubles<br>

 > it is possible to upgrade the IDE as described here after <br>

- Can we open a project previously used with older IDE version ??, Not sure that the .cproject files are compatible <br>

 > yes, we can ;-) <br>

- Can we have two IDE version installed on the PC ?
 > Yes, in another directory but better to not share the workspace !! }} More information can be found in the detailed release notes referenced later in this article.

== SW4TM32 - System Workbench for STM32 2.9.0 - ''STM32-CoPro-MPU plugin version 1.0.0''==

The '''STM32-CoPro-MPU''' plugin, based onto the ''System Workbench for STM32'' (SW4STM32), targets the support of Cortex<sup>&reg;</sup>-M core contained in the STM32MP1 Family. <br>

It is included in '''System Workbench for STM32''' from version 2.9.0. <br>

It provides:<br>

* the target status widget, 
* the console management, 
* the project creation, compilation and debug in two modes:
** '''Engineering Mode''', 
** '''Production Mode''', with Cortex<sup>&reg;</sup>-M firmware download :
***via Ethernet Network (LAN or Point-to-Point)
***via Ethernet over USB
*the remote system explorer configuration<br>

It is available on Linux<sup>&reg;</sup> and Windows<sup>&reg;</sup> platforms. <br>
<br>


Upgrading your System Workbench, '''STM32-CoPro-MPU''' plugin can be installed using the [http://www.ac6-tools.com/Eclipse-updates/org.openstm32.system-workbench.update-site-v2/ System Workbench for STM32 - Updates] 
in menu ''Windows > Preferences > Install/Update > Available Software Site''.  <br>

The installation is then the standard Eclipse one: ''Help > Install New Software...''  <br> 
<br>

In order to access to the Ac6 site, take care to configure proxy at Eclipse level: in ''Windows > Preferences > General > Network Connections''; Active Provider set to ''Manual''. <br>

Then after selecting ''HTTP'' proxy entry, click ''Edit...'' and enter your proxy setup.
<onlyinclude>

{| class="wikitable" width=98%
|-
!  !! IDE for Linux<sup>&reg;</sup> host PC!! IDE for Windows<sup>&reg;</sup> host PC
|-
| '''Download''' 
|| 
'''Version 1.0.0STM32-CoPro-MPU plugin in SW4STM32 2.9.0 '''
*Download the all-in-one Linux installer 2.9 '''install_sw4stm32_linux_64bits-v2.9.run''' from [http://www.openstm32.org/HomePage openstm32.org]
|| 
'''Version 1.0.0STM32-CoPro-MPU plugin in SW4STM32 2.9.0 '''
*Download the all-in-one Windows installer 2.9 '''install_sw4stm32_win_64bits-v2.9.exe''' from [http://www.openstm32.org/HomePage openstm32.org]
|-
| '''Installation''' 
|| 
* Run the installation script
 $ chmod +x install_sw4stm32_linux_64bits-v2.9.run
 $ ./install_sw4stm32_linux_64bits-v2.9.run
*Then follow instructions given on [http://www.openstm32.org/HomePage openstm32.org]
* '''When the installation is over''', to use the tool, you can follow instruction given in [[STM32-CoPro-MPU plugin for SW4STM32]] or in the detailed release note. 
||
* Run the installation exe
 $ install_sw4stm32_win_64bits-v2.9.exe
*Then follow instructions given on [http://www.openstm32.org/HomePage openstm32.org]
* '''When the installation is over''', to use the tool, you can follow instruction given in [[STM32-CoPro-MPU plugin for SW4STM32]] or in the detailed release note. 
|-
| '''Detailed release notes''' 
||Details about the content of this tool version are available on [http://www.openstm32.org/HomePage openstm32.org]
||
Details about the content of this tool version are available on [http://www.openstm32.org/HomePage openstm32.org]
|}</onlyinclude>

<noinclude>

{{PublicationRequestId | 8349 | 2018-08-14 | AlainF}}
[[Category:Release notes|5]]
[[Category:SW4STM32 IDE]]

{{UpdateNeededForNewRelease|
* Copy the current release (first chapter) in the "Archives" chapter
* Change the version of the tool
* Change the name of the archive file
* Change the download URLs
}}</noinclude>
Line 1: Line 1:
<noinclude>
 
{{ArticleMainWriter|LudovicR}}
 
{{ReviewersList|To be completed by LudovicR}}
 
{{ArticleApprovedVersion| LudovicR | BernardP | NathalieS - 29Aug'18 | AlainF - 14Aug'18 - 8349 | 21Nov'18}}
 
 
[[Category:Release notes|5]]
 
[[Category:SW4STM32 IDE]]
 
 
{{UpdateNeededForNewRelease|
 
* Copy the current release (first chapter) in the "Archives" chapter
 
* Change the version of the tool
 
* Change the name of the archive file
 
* Change the download URLs
 
}}
 
</noinclude>
 
 
{{ReviewsComments|ECO: The release 2.8.0 is not available anymore on AC6 web site. Now 2.9.0 }}
 
{{ReviewsComments|LVI: I copy comments from YCO made on the wrong Wiki page.
 
YCO 18-Feb-19 : Eclipse tool version 2.8 install_sw4stm32_linux_64bits-v2.8.run from openstm32.org not available<br>
 
YCO 19-Feb-19 : I have install the Eclipse tool version 2.8 for Linux "install_sw4stm32_linux_64bits-v2.8.run" from https://citools.st.com/snapshots/artifactory/webapp/#/artifacts/browse/tree/General/snapshots-stm32ide-codex-st-com/refs/tags/2.8.0/allinone/install_sw4stm32_linux_64bits.run <br>
 
We need to clarify the install process : <br>
 
- Do we need to desinstall a older version, according to the process described in AC6 (with the allinone installer), "NO" the workspace folder is overwritten, to be confirmed because I faced some troubles<br>
 
> it is possible to upgrade the IDE as described here after <br>
 
- Can we open a project previously used with older IDE version ??, Not sure that the .cproject files are compatible <br>
 
> yes, we can ;-) <br>
 
- Can we have two IDE version installed on the PC ?
 
> Yes, in another directory but better to not share the workspace !! }}
 
 
More information can be found in the detailed release notes referenced later in this article.
 
More information can be found in the detailed release notes referenced later in this article.
   
== SW4TM32 - System Workbench for STM32 2.9.0 - ''STM32-CoPro-MPU plugin version 1.0.0''==
+
== SW4TM32 - System Workbench for STM32 2.9.0 - ''STM32-CoPro-MPU plugin''==
   
 
The '''STM32-CoPro-MPU''' plugin, based onto the ''System Workbench for STM32'' (SW4STM32), targets the support of Cortex<sup>&reg;</sup>-M core contained in the STM32MP1 Family. <br>
 
The '''STM32-CoPro-MPU''' plugin, based onto the ''System Workbench for STM32'' (SW4STM32), targets the support of Cortex<sup>&reg;</sup>-M core contained in the STM32MP1 Family. <br>
Line 59: Line 32:
 
| '''Download'''  
 
| '''Download'''  
 
||  
 
||  
'''Version 1.0.0 in SW4STM32 2.9.0 '''
+
'''STM32-CoPro-MPU plugin in SW4STM32 2.9.0 '''
 
*Download the all-in-one Linux installer 2.9 '''install_sw4stm32_linux_64bits-v2.9.run''' from [http://www.openstm32.org/HomePage openstm32.org]
 
*Download the all-in-one Linux installer 2.9 '''install_sw4stm32_linux_64bits-v2.9.run''' from [http://www.openstm32.org/HomePage openstm32.org]
 
||  
 
||  
'''Version 1.0.0 in SW4STM32 2.9.0 '''
+
'''STM32-CoPro-MPU plugin in SW4STM32 2.9.0 '''
 
*Download the all-in-one Windows installer 2.9 '''install_sw4stm32_win_64bits-v2.9.exe''' from [http://www.openstm32.org/HomePage openstm32.org]
 
*Download the all-in-one Windows installer 2.9 '''install_sw4stm32_win_64bits-v2.9.exe''' from [http://www.openstm32.org/HomePage openstm32.org]
 
|-
 
|-
Line 86: Line 59:
   
 
<noinclude>
 
<noinclude>
  +
{{PublicationRequestId | 8349 | 2018-08-14 | AlainF}}
  +
[[Category:Release notes|5]]
  +
[[Category:SW4STM32 IDE]]
  +
  +
{{UpdateNeededForNewRelease|
  +
* Copy the current release (first chapter) in the "Archives" chapter
  +
* Change the version of the tool
  +
* Change the name of the archive file
  +
* Change the download URLs
  +
}}
  +
</noinclude>

Attachments

Discussions