Difference between revisions of "STGEN internal peripheral"

[quality revision] [quality revision]
m
 

1 Article purpose[edit]

The purpose of this article is to:

  • briefly introduce the STGEN peripheral and its main features
  • indicate the level of security supported by this hardware block
  • explain how it can be allocated to the three runtime contexts and linked to the corresponding software components
  • explain, when necessary, how to configure the STGEN peripheral.

2 Peripheral overview[edit]

The STGEN peripheral provides the reference clock used by the Arm® Cortex®-A7 generic timer for its counters, including the system tick generation.

It is clocked by ACLK (the AXI bus clock), so caution is needed when this clock is changed; otherwise the operating system (running on the Cortex-A7) might run with a varying reference clock.

2.1 Features[edit]

Refer to the STM32MP15 reference manuals for the complete list of features, and to the software components, introduced below, to see which features are implemented.

2.2 Security support[edit]

The STGEN is a single-instance peripheral that can be accessed via the two following register sets:

  • STGENC for the control. That is, a secure port (under ETZPC control).
  • STGENR for the read-only access. That is, a non secure port.

3 Peripheral usage and associated software[edit]

3.1 Boot time[edit]

The STGEN is first initialized by the ROM code, then updated by the FSBL (see Boot chains chain overview) once the clock tree is set up.

3.2 Runtime[edit]

3.2.1 Overview[edit]

Linux® and OP-TEE use the Arm Cortex-A7 generic timer that gets its counter from the STGEN, but this is transparent at run time.

Hence there is no runtime allocation decision for this peripheral: both contexts are selected by default.

3.2.2 Software frameworks[edit]

Domain Peripheral Software frameworks Comment
Cortex-A7
secure
(OP-TEE)
Cortex-A7
non-secure
(Linux)
Cortex-M4

(STM32Cube)
Core STGEN see comment see comment Not applicable as the STGEN peripheral is configured at boot time and not accessed at runtime

3.2.3 Peripheral configuration[edit]

3.2.4 Peripheral assignment[edit]

Internal peripherals

Check boxes illustrate the possible peripheral allocations supported by STM32 MPU Embedded Software:

  • means that the peripheral can be assigned () to the given runtime context.
  • is used for system peripherals that cannot be unchecked because they are statically connected in the device.

Refer to How to assign an internal peripheral to a runtime context for more information on how to assign peripherals manually or via STM32CubeMX.
The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possiblities might be described in STM32MP15 reference manuals.

Domain Peripheral Runtime allocation Comment
Instance Cortex-A7
secure
(OP-TEE)
Cortex-A7
non-secure
(Linux)
Cortex-M4

(STM32Cube)
Core STGEN STGEN

4 How to go further[edit]

5 References[edit]




==Article purpose==
The purpose of this article is to:
* briefly introduce the STGEN peripheral and its main features
* indicate the level of security supported by this hardware block
* explain how it can be allocated to the three runtime contexts and linked to the corresponding software components
* explain, when necessary, how to configure the STGEN peripheral.

==Peripheral overview==
The STGEN peripheral provides the reference clock used by the Arm<sup>&reg;</sup> Cortex<sup>&reg;</sup>-A7 generic timer for its counters, including the system tick generation.

It is clocked by ACLK (the AXI bus clock), so caution is needed when this clock is changed; otherwise the operating system (running on the Cortex-A7) might run with a varying reference clock.

===Features===
Refer to the [[STM32MP15 resources#Reference manuals|STM32MP15 reference manuals]] for the complete list of features, and to the software components, introduced below, to see which features are implemented.

===Security support===
The STGEN is a single-instance peripheral that can be accessed via the two following register sets:

* STGEN'''C''' for the '''c'''ontrol. That is, a '''secure''' port (under [[ETZPC_internal_peripheral|ETZPC]] control).
* STGEN'''R''' for the '''r'''ead-only access. That is, a '''non secure''' port.

==Peripheral usage and associated software==
===Boot time===
The STGEN is first initialized by the [[STM32MP15 ROM code overview|ROM code]], then updated by the FSBL (see [[Boot chainschain overview]]) once the clock tree is set up.

===Runtime===

====Overview====
Linux<sup>&reg;</sup> and OP-TEE use the Arm Cortex-A7 generic timer that gets its counter from the STGEN, but this is transparent at run time. 

Hence there is no runtime allocation decision for this peripheral: '''both contexts are selected by default'''.

====Software frameworks====
{{:Internal_peripherals_software_table_template}}
 | Core
 | [[STGEN_internal_peripheral|STGEN]]
 | see comment
 | see comment
 | 
 | Not applicable as the STGEN peripheral is configured at boot time and not accessed at runtime
 |-
 |}

====Peripheral configuration====

====Peripheral assignment====
{{:Internal_peripherals_assignment_table_template}}<onlyinclude>

 | rowspan="1" | Core
 | rowspan="1" | [[STGEN_internal_peripheral|STGEN]]
 | STGEN
 | <span title="system peripheral" style="font-size:21px"></span>

 | <span title="system peripheral" style="font-size:21px"></span>

 |
 |
 |-</onlyinclude>

 |}

==How to go further==

==References==<references/>

<noinclude>

{{ArticleBasedOnModel| Internal peripheral article model}}
{{PublicationRequestId | 8348 | 2018-08-18 | PhilipS}}
[[Category:Core peripherals]]</noinclude>
Line 22: Line 22:
 
==Peripheral usage and associated software==
 
==Peripheral usage and associated software==
 
===Boot time===
 
===Boot time===
The STGEN is first initialized by the [[STM32MP15 ROM code overview|ROM code]], then updated by the FSBL (see [[Boot chains overview]]) once the clock tree is set up.
+
The STGEN is first initialized by the [[STM32MP15 ROM code overview|ROM code]], then updated by the FSBL (see [[Boot chain overview]]) once the clock tree is set up.
   
 
===Runtime===
 
===Runtime===