Difference between revisions of "SPI device tree configuration"

[quality revision] [pending revision]
m
m (Article purpose)
 
Template:ArticleMainWriter Template:ArticleMainWriter Template:ArticleApprovedVersion

1 Article purpose[edit]

This article explains how to configure the SPI internal peripheral[1] when the peripheral is assigned to Linux® OS, and in particular:

  • how to configure the STM32 SPI peripheral
  • how to configure the STM32 external SPI devices present either on the board or on a hardware extension.

The configuration is performed using the device tree mechanism[2].

It is used by the STM32 SPI Linux® driver that registers relevant information in the SPI framework.

If the peripheral is assigned to another execution context, refer to How to assign an internal peripheral to a runtime context article for guidelines on peripheral assignment and configuration.

2 DT bindings documentation[edit]

The SPI bus and its associated device are represented by:

  • The Generic device tree bindings for SPI buses[3]
  • The STM32 SPI controller device tree bindings[4]

3 DT configuration[edit]

This hardware description is a combination of the STM32 microprocessor device tree files (.dtsi extension) and board device tree files (.dts extension). See the Device tree for an explanation of the device tree file split.

STM32CubeMX can be used to generate the board device tree. Refer to How to configure the DT using STM32CubeMX for more details.

3.1 DT configuration (STM32 level)[edit]

At device level, each SPI controller is declared as follows:


spi1: spi@44004000 {
	#address-cells = <1>;
	#size-cells = <0>;
	compatible = "st,stm32h7-spi";
	reg = <0x44004000 0x400>;
	interrupts = <GIC_SPI 35 IRQ_TYPE_LEVEL_HIGH>;
	clocks = <&rcc SPI1_K>;
	resets = <&rcc SPI1_R>;
	dmas = <&dmamux1 37 0x400 0x05>,
	       <&dmamux1 38 0x400 0x05>;
	dma-names = "rx", "tx";
	power-domains = <&pd_core>;
	status = "disabled";
};

Warning.png This device tree part is related to STM32 microprocessors. It must be kept as is, without being modified by the end-user.

Refer to the DTS file: stm32mp157c.dtsi[5]

3.2 DT configuration (board level)[edit]


&spi1 {
	pinctrl-names = "default", "sleep";
	pinctrl-0 = <&spi1_pins_a>;
	pinctrl-1 = <&spi1_sleep_pins_a>;
	cs-gpios = <&gpioz 3 0>;
	status = "okay";

        foo@0 {
                compatible = "spi-foo";
                #address-cells = <1>;
                #size-cells = <0>;
                reg = <0>; /* CS #0 */
                spi-max-frequency = <10000000>;
        };
};


There are two levels of configuration:

  • Configuration of the SPI bus properties:
    • pinctrl-0&1 configuration depends on hardware board configuration and on how the SPI devices are connected to MOSI, MISO and Clk pins.
      More details about pin configuration are available here: Pinctrl device tree configuration
    • cs-gpios represents the list of GPIOs used as chip selects. Native controller chip select defined by a NULL value is not supported by STM32MP1 SPI driver.
      More details about GPIO configuration are available here: GPIO device tree configuration
    • dmas: by default, DMAs are specified for all SPI instances. This is up to the user to remove them if they are not needed. /delete-property/ is used to remove DMA usage for SPI. Both /delete-property/dma-names and /delete-property/dma have to be inserted to get rid of DMAs.
  • Configuration of the properties of the SPI device connected on the bus:
    • compatible represents the name of the SPI device driver.
    • reg represents the index of the gpio chip select associated to this SPI device.
    • spi-max-frequency represents the maximum SPI clocking speed for the device (in Hz).

For more information about SPI bus and SPI device bindings, please refer to spi-bus.txt[3]

3.3 DT configuration example[edit]

Example: of an external TPM device:

&spi1 {
	pinctrl-names = "default", "sleep";
	pinctrl-0 = <&spi1_pins_a>;
	pinctrl-1 = <&spi1_sleep_pins_a>;
	cs-gpios = <&gpioz 3 0>;
	status = "okay";

	st33zp24@0 {
		compatible = "st,st33htpm-spi";
		#address-cells = <1>;
		#size-cells = <0>;
		reg = <0>; /* CS #0 */
		spi-max-frequency = <10000000>;
	};
};

The above example registers a TPM device on spi1 bus, selected by chip select 0 also known as GPIO-Z3. This instance is compatible with the driver registered with the same compatible property (st,st33htpm-spi).

4 How to configure the DT using STM32CubeMX[edit]

The STM32CubeMX tool can be used to configure the STM32MPU device and get the corresponding platform configuration device tree files.
The STM32CubeMX may not support all the properties described in the above DT bindings documentation paragraph. If so, the tool inserts user sections in the generated device tree. These sections can then be edited to add some properties and they are preserved from one generation to another. Refer to STM32CubeMX user manual for further information.

5 References[edit]

Please refer to the following links for additional information:


<noinclude>

{{ArticleBasedOnModel | [[Peripheral or framework device tree configuration model]]}}
{{ArticleMainWriter | AmelieD}}
{{ArticleMainWriter | LoicP}}
{{ArticleApprovedVersion| LoicP | AmelieD, FabriceG | No previous approved version | AnneJ - 04Feb'19 - 10616 | 04Feb'19}}
[[Category:Device tree configuration]]
[[Category:SPI]]</noinclude>

== Article purpose ==
This article explains how to configure the ''SPI internal peripheral''<ref name="SPI internal peripheral"> [[SPI internal peripheral]] </ref> ''' when the peripheral is assigned to Linux<sup>&reg;</sup> OS''', and in particular:
* how to configure the STM32 SPI peripheral
* how to configure the STM32 external SPI devices present either on the board or on a hardware extension.

The configuration is performed using the '''device tree mechanism'''<ref> [[Device tree]]</ref>.

It is used by the ''STM32 SPI Linux<sup>&reg;</sup> driver'' that registers relevant information in the [[SPI overview|SPI]] framework.
If the peripheral is assigned to another execution context, refer to [[How to assign an internal peripheral to a runtime context]] article for guidelines on peripheral assignment and configuration.
== DT bindings documentation ==

The SPI bus and its associated device are represented by:
* The ''Generic device tree bindings for SPI buses''<ref name="spi-bus.txt">{{CodeSource | Linux kernel | Documentation/devicetree/bindings/spi/spi-bus.txt}}, Generic device tree bindings for SPI buses</ref>

* The ''STM32 SPI controller device tree bindings''<ref name="spi-stm32.txt ">{{CodeSource |Linux kernel | Documentation/devicetree/bindings/spi/spi-stm32.txt}}</ref>


== DT configuration ==
This hardware description is a combination of the '''STM32 microprocessor''' device tree files (''.dtsi'' extension) and '''board''' device tree files (''.dts'' extension). See the [[Device tree]] for an explanation of the device tree file split.

'''STM32CubeMX''' can be used to generate the board device tree. Refer to [[#How_to_configure_the_DT_using_STM32CubeMX|How to configure the DT using STM32CubeMX]] for more details.

===DT configuration (STM32 level) ===
At device level, each SPI controller is declared as follows:<pre class="brush:c; tab-size:8;gutter:true;">

spi1: spi@44004000 {
	#address-cells = <1>;
	#size-cells = <0>;
	compatible = "st,stm32h7-spi";
	reg = <0x44004000 0x400>;
	interrupts = <GIC_SPI 35 IRQ_TYPE_LEVEL_HIGH>;
	clocks = <&rcc SPI1_K>;
	resets = <&rcc SPI1_R>;
	dmas = <&dmamux1 37 0x400 0x05>,<&dmamux1 38 0x400 0x05>;
	dma-names = "rx", "tx";
	power-domains = <&pd_core>;
	status = "disabled";
};</pre>

{{Warning|This device tree part is related to STM32 microprocessors. It must be kept as is, without being modified by the end-user.}}

Refer to the DTS file: stm32mp157c.dtsi<ref name=DTS>{{CodeSource | Linux kernel | arch/arm/boot/dts/stm32mp157c.dtsi}}</ref>


=== DT configuration (board level) ==={{ReviewsComments|W1935: ABO: The properties #addess-cells and #size-cells are not required in the spi device. They are mandatory in the spi controller node, and in fact they are correctly present in stm32mp157c.dtsi, but not in the spi device. This is described in Documentation/devicetree/bindings/spi/spi-bus.txt }}<pre class="brush:c; tab-size:8;gutter:true;">

&spi1 {
	pinctrl-names = "default", "sleep";
	pinctrl-0 = <&spi1_pins_a>;
	pinctrl-1 = <&spi1_sleep_pins_a>;
	cs-gpios = <&gpioz 3 0>;
	status = "okay";

        foo@0 {
                compatible = "spi-foo";
                #address-cells = <1>;
                #size-cells = <0>;
                reg = <0>; /* CS #0 */
                spi-max-frequency = <10000000>;
        };
};
</pre>


There are two levels of configuration:
* Configuration of the SPI bus properties:
** '''{{highlight|pinctrl-0&1}}''' configuration depends on hardware board configuration and on how the SPI devices are connected to MOSI, MISO and Clk pins.<br/> More details about pin configuration are available here: [[Pinctrl device tree configuration]] 
** '''{{highlight|cs-gpios}}''' represents the list of GPIOs used as chip selects. Native controller chip select defined by a NULL value is not supported by STM32MP1 SPI driver.<br/>More details about GPIO configuration are available here: [[GPIO device tree configuration]]
** '''{{highlight|dmas}}''': by default, DMAs are specified for all SPI instances. This is up to the user to '''remove''' them if they are not needed. ''{{highlight|/delete-property/}}'' is used to remove DMA usage for SPI. Both '''{{highlight|/delete-property/dma-names}}''' and '''{{highlight|/delete-property/dma}}''' have to be inserted to get rid of DMAs.

* Configuration of the properties of the SPI device connected on the bus:
** '''{{highlight|compatible }}''' represents the name of the SPI device driver.
** '''{{highlight|reg}}''' represents the index of the gpio chip select associated to this SPI device.
** '''{{highlight|spi-max-frequency}}''' represents the maximum SPI clocking speed for the device (in Hz).

For more information about SPI bus and SPI device bindings, please refer to spi-bus.txt<ref name="spi-bus.txt"/>


=== DT configuration example ===
'''Example:''' of an external TPM device:
 &spi1 {
 	pinctrl-names = "default", "sleep";
 	pinctrl-0 = <&spi1_pins_a>;
 	pinctrl-1 = <&spi1_sleep_pins_a>;
 	cs-gpios = {{highlight|<&gpioz 3 0>}};
 	status = "okay";

 	st33zp24{{highlight|@0}} {
 		compatible = "st,st33htpm-spi";
 		#address-cells = <1>;
 		#size-cells = <0>;
 		reg = {{highlight|<0>}}; {{highlight|/* CS #0 */}}
 		spi-max-frequency = <10000000>;
 	};
 };

The above example registers a TPM device on spi1 bus, selected by chip select 0 also known as GPIO-Z3. This instance is compatible with the driver registered with the same compatible property (st,st33htpm-spi).<br/>


==How to configure the DT using STM32CubeMX==
The [[STM32CubeMX]] tool can be used to configure the STM32MPU device and get the corresponding [[Device_tree#STM32|platform configuration device tree]] files.<br />

The STM32CubeMX may not support all the properties described in the above [[#DT bindings documentation|DT bindings documentation]] paragraph. If so, the tool inserts '''user sections''' in the generated device tree. These sections can then be edited to add some properties and they are preserved from one generation to another. Refer to [[STM32CubeMX]] user manual for further information.

==References==
Please refer to the following links for additional information:
<references />

<noinclude>

[[Category:Device tree configuration]]
[[Category:SPI]]
{{ArticleBasedOnModel | Peripheral or framework device tree configuration model}}
{{PublicationRequestId | 10616 | 2019-02-04 | AnneJ}}</noinclude>
(2 intermediate revisions by 2 users not shown)
Line 1: Line 1:
<noinclude>
 
{{ArticleBasedOnModel | [[Peripheral or framework device tree configuration model]]}}
 
{{ArticleMainWriter | AmelieD}}
 
{{ArticleMainWriter | LoicP}}
 
{{ArticleApprovedVersion| LoicP | AmelieD, FabriceG | No previous approved version | AnneJ - 04Feb'19 - 10616 | 04Feb'19}}
 
[[Category:Device tree configuration]]
 
[[Category:SPI]]
 
</noinclude>
 
 
 
== Article purpose ==
 
== Article purpose ==
 
This article explains how to configure the ''SPI internal peripheral''<ref name="SPI internal peripheral"> [[SPI internal peripheral]] </ref> ''' when the peripheral is assigned to Linux<sup>&reg;</sup> OS''', and in particular:
 
This article explains how to configure the ''SPI internal peripheral''<ref name="SPI internal peripheral"> [[SPI internal peripheral]] </ref> ''' when the peripheral is assigned to Linux<sup>&reg;</sup> OS''', and in particular:
Line 16: Line 7:
   
 
It is used by the ''STM32 SPI Linux<sup>&reg;</sup> driver'' that registers relevant information in the [[SPI overview|SPI]] framework.
 
It is used by the ''STM32 SPI Linux<sup>&reg;</sup> driver'' that registers relevant information in the [[SPI overview|SPI]] framework.
  +
  +
If the peripheral is assigned to another execution context, refer to [[How to assign an internal peripheral to a runtime context]] article for guidelines on peripheral assignment and configuration.
   
 
== DT bindings documentation ==
 
== DT bindings documentation ==
Line 30: Line 23:
 
===DT configuration (STM32 level) ===
 
===DT configuration (STM32 level) ===
 
At device level, each SPI controller is declared as follows:
 
At device level, each SPI controller is declared as follows:
<pre class="brush:c; tab-size:8;gutter:true;">
+
<pre>
 
spi1: spi@44004000 {
 
spi1: spi@44004000 {
 
#address-cells = <1>;
 
#address-cells = <1>;
Line 51: Line 44:
   
 
=== DT configuration (board level) ===
 
=== DT configuration (board level) ===
<pre class="brush:c; tab-size:8;gutter:true;">
+
{{ReviewsComments|W1935: ABO: The properties #addess-cells and #size-cells are not required in the spi device. They are mandatory in the spi controller node, and in fact they are correctly present in stm32mp157c.dtsi, but not in the spi device. This is described in Documentation/devicetree/bindings/spi/spi-bus.txt }}
  +
<pre>
 
&spi1 {
 
&spi1 {
 
pinctrl-names = "default", "sleep";
 
pinctrl-names = "default", "sleep";
Line 111: Line 105:
   
 
<references />
 
<references />
  +
  +
<noinclude>
  +
[[Category:Device tree configuration]]
  +
[[Category:SPI]]
  +
{{ArticleBasedOnModel | Peripheral or framework device tree configuration model}}
  +
{{PublicationRequestId | 10616 | 2019-02-04 | AnneJ}}
  +
</noinclude>

Attachments

Discussions