Difference between revisions of "SPDIFRX device tree configuration"

[quality revision] [quality revision]
m (DT configuration (board level))
 
m
 
Template:ArticleMainWriter Template:ArticleApprovedVersion

1 Article purpose[edit]

This article explains how to configure the SPDIFRX internal peripheral when it is assigned to the Linux® OS. In that case, it is controlled by the ALSA framework.

The configuration is performed using the device tree mechanism that provides a hardware description of the SPDIFRX peripheral, used by the SPDFIRX linux driver.

If the peripheral is assigned to another execution context, refer to How to assign an internal peripheral to a runtime context article for guidelines on peripheral assignment and configuration.

2 DT bindings documentation[edit]

STM32 SPDIFRX device tree bindings [1] document describes all the required and optional configuration properties.

3 DT configuration[edit]

This hardware description is a combination of STM32 microprocessor [2] and board device tree files. See the Device tree for an explanation of the device tree file split.

STM32CubeMX can be used to generate the board device tree. Refer to How to configure the DT using STM32CubeMX for more details.

3.1 DT configuration (STM32 level)[edit]

The SPDIFRX node is declared in stm32mp157cstm32mp151.dtsi[2]. It describes the hardware parameters such as register addresses, interrupt, clock and DMA. This set of properties may not vary for a given STM32MPU.

Warning.png This device tree part is related to STM32 microprocessors. It must be kept as is, without being modified by the end-user.

3.2 DT configuration (board level)[edit]

The SPDIFRX is an audio peripheral, which can be used as a component of a soundcard through Linux® kernel ALSA framework. This part of the device tree allows the configuration of the SPDIFRX to implement a soundcard. Refer to soundcard configuration for examples of SPDIFRX configuration on various boards.

3.3 DT configuration examples[edit]

&spdifrx {
	pinctrl-names = "default", "sleep"; 
	pinctrl-0 = <&spdifrx_pins_a>;
	pinctrl-1 = <&spdifrx_sleep_pins_a>
	/* Use spdifrx_pins_a instead of spdifrx_sleep_pins_a configuration,
	to allow IEC958 status bits capture, when an audio stream record is
	not active. Note that sleep state has to be defined, to allow pin state
	recovery from low power modes. */

	spdifrx_port: port {
		spdifrx_endpoint: endpoint {
			remote-endpoint = <&spdif_in_endpoint>;
		};
	};
};

4 How to configure the DT using STM32CubeMX[edit]

The STM32CubeMX tool can be used to configure the STM32MPU device and get the corresponding platform configuration device tree files.
The STM32CubeMX may not support all the properties described in the above DT bindings documentation paragraph. If so, the tool inserts user sections in the generated device tree. These sections can then be edited to add some properties and they are preserved from one generation to another. Refer to STM32CubeMX user manual for further information.

5 References[edit]


<noinclude>

{{ArticleBasedOnModel | [[Peripheral or framework device tree configuration model]]}}
{{ArticleMainWriter | OlivierM}}
{{ArticleApprovedVersion | OlivierM | ArnaudP(Passed, W847.2) | No previous approved version |  AnneJ - 26Nov'18 - 9810  |  14Jan'19}} 
[[Category:Device tree configuration]]
[[Category:ALSA]]</noinclude>

== Article purpose ==
This article explains how to configure the [[SPDIFRX internal peripheral]] when it is assigned to the '''Linux® OS'''. In that case, it is controlled by the [[ALSA_overview|ALSA framework]].

The configuration is performed using the [[Device_tree|device tree]] mechanism that provides a hardware description of the SPDIFRX peripheral, used by the [[SPDIFRX_Linux_driver|SPDFIRX linux driver]].
If the peripheral is assigned to another execution context, refer to [[How to assign an internal peripheral to a runtime context]] article for guidelines on peripheral assignment and configuration.
== DT bindings documentation ==
STM32 SPDIFRX device tree bindings <ref name="spdifrx bindings">{{CodeSource | Linux kernel | Documentation/devicetree/bindings/sound/st,stm32-spdifrx.txtyaml}}</ref> document describes all the required and optional configuration properties.

== DT configuration ==
This hardware description is a combination of STM32 microprocessor <ref name="stm32mp157cstm32mp151.dtsi">{{CodeSource | Linux kernel | arch/arm/boot/dts/stm32mp157cstm32mp151.dtsi}}</ref> and board device tree files. See the [[Device tree]] for an explanation of the device tree file split.

'''STM32CubeMX''' can be used to generate the board device tree. Refer to [[#How_to_configure_the_DT_using_STM32CubeMX|How to configure the DT using STM32CubeMX]] for more details.

=== DT configuration (STM32 level) ===
The SPDIFRX node is declared in stm32mp157cstm32mp151.dtsi<ref name="stm32mp157cstm32mp151.dtsi">{{CodeSource | Linux kernel | arch/arm/boot/dts/stm32mp157cstm32mp151.dtsi}}</ref>. 
It describes the hardware parameters such as register addresses, interrupt, clock and DMA. This set of properties may not vary for a given STM32MPU.
{{Warning|This device tree part is related to STM32 microprocessors. It must be kept as is, without being modified by the end-user.}}

=== DT configuration (board level) ===

The SPDIFRX is an audio peripheral, which can be used as a component of a soundcard through Linux<sup>&reg;</sup> kernel [[ALSA overview|ALSA framework]]. This part of the device tree allows the configuration of the SPDIFRX to implement a soundcard. Refer to [[Soundcard configuration|soundcard configuration]] for examples of SPDIFRX configuration on various boards.

=== DT configuration examples ===

 &spdifrx {
 	pinctrl-names = "default", "sleep"; 
 	pinctrl-0 = <&spdifrx_pins_a>;
 	pinctrl-1 = <&spdifrx_sleep_pins_a>

 	{{highlight|/* Use spdifrx_pins_a instead of spdifrx_sleep_pins_a configuration,
 	to allow IEC958 status bits capture, when an audio stream record is
 	not active. Note that sleep state has to be defined, to allow pin state
 	recovery from low power modes. */}}

 	spdifrx_port: port {
 		spdifrx_endpoint: endpoint {
 			remote-endpoint = <&spdif_in_endpoint>;
 		};
 	};
 };

==How to configure the DT using STM32CubeMX==
The [[STM32CubeMX]] tool can be used to configure the STM32MPU device and get the corresponding [[Device_tree#STM32|platform configuration device tree]] files.<br />

The STM32CubeMX may not support all the properties described in the above [[#DT bindings documentation|DT bindings documentation]] paragraph. If so, the tool inserts '''user sections''' in the generated device tree. These sections can then be edited to add some properties and they are preserved from one generation to another. Refer to [[STM32CubeMX]] user manual for further information.

==References==
<references /><references />

<noinclude>

[[Category:Device tree configuration]]
[[Category:ALSA]]
{{ArticleBasedOnModel | Peripheral or framework device tree configuration model}}
{{PublicationRequestId | 9810| 2018-11-26 | AnneJ}}</noinclude>
(10 intermediate revisions by 4 users not shown)
Line 1: Line 1:
<noinclude>
 
{{ArticleBasedOnModel | [[Peripheral or framework device tree configuration model]]}}
 
{{ArticleMainWriter | OlivierM}}
 
{{ArticleApprovedVersion | OlivierM | ArnaudP(Passed, W847.2) | No previous approved version |  AnneJ - 26Nov'18 - 9810  |  14Jan'19}}
 
[[Category:Device tree configuration]]
 
[[Category:ALSA]]
 
</noinclude>
 
 
 
== Article purpose ==
 
== Article purpose ==
 
This article explains how to configure the [[SPDIFRX internal peripheral]] when it is assigned to the '''Linux® OS'''. In that case, it is controlled by the [[ALSA_overview|ALSA framework]].
 
This article explains how to configure the [[SPDIFRX internal peripheral]] when it is assigned to the '''Linux® OS'''. In that case, it is controlled by the [[ALSA_overview|ALSA framework]].
   
 
The configuration is performed using the [[Device_tree|device tree]] mechanism that provides a hardware description of the SPDIFRX peripheral, used by the [[SPDIFRX_Linux_driver|SPDFIRX linux driver]].
 
The configuration is performed using the [[Device_tree|device tree]] mechanism that provides a hardware description of the SPDIFRX peripheral, used by the [[SPDIFRX_Linux_driver|SPDFIRX linux driver]].
  +
  +
If the peripheral is assigned to another execution context, refer to [[How to assign an internal peripheral to a runtime context]] article for guidelines on peripheral assignment and configuration.
   
 
== DT bindings documentation ==
 
== DT bindings documentation ==
STM32 SPDIFRX device tree bindings <ref name="spdifrx bindings">{{CodeSource | Linux kernel | Documentation/devicetree/bindings/sound/st,stm32-spdifrx.txt}}</ref> document describes all the required and optional configuration properties.
+
STM32 SPDIFRX device tree bindings <ref name="spdifrx bindings">{{CodeSource | Linux kernel | Documentation/devicetree/bindings/sound/st,stm32-spdifrx.yaml}}</ref> document describes all the required and optional configuration properties.
   
 
== DT configuration ==
 
== DT configuration ==
This hardware description is a combination of STM32 microprocessor <ref name="stm32mp157c.dtsi">{{CodeSource | Linux kernel | arch/arm/boot/dts/stm32mp157c.dtsi}}</ref> and board device tree files. See the [[Device tree]] for an explanation of the device tree file split.
+
This hardware description is a combination of STM32 microprocessor <ref name="stm32mp151.dtsi">{{CodeSource | Linux kernel | arch/arm/boot/dts/stm32mp151.dtsi}}</ref> and board device tree files. See the [[Device tree]] for an explanation of the device tree file split.
   
 
'''STM32CubeMX''' can be used to generate the board device tree. Refer to [[#How_to_configure_the_DT_using_STM32CubeMX|How to configure the DT using STM32CubeMX]] for more details.
 
'''STM32CubeMX''' can be used to generate the board device tree. Refer to [[#How_to_configure_the_DT_using_STM32CubeMX|How to configure the DT using STM32CubeMX]] for more details.
   
 
=== DT configuration (STM32 level) ===
 
=== DT configuration (STM32 level) ===
The SPDIFRX node is declared in stm32mp157c.dtsi<ref name="stm32mp157c.dtsi">{{CodeSource | Linux kernel | arch/arm/boot/dts/stm32mp157c.dtsi}}</ref>.  
+
The SPDIFRX node is declared in stm32mp151.dtsi<ref name="stm32mp151.dtsi">{{CodeSource | Linux kernel | arch/arm/boot/dts/stm32mp151.dtsi}}</ref>.  
 
It describes the hardware parameters such as register addresses, interrupt, clock and DMA. This set of properties may not vary for a given STM32MPU.
 
It describes the hardware parameters such as register addresses, interrupt, clock and DMA. This set of properties may not vary for a given STM32MPU.
 
{{Warning|This device tree part is related to STM32 microprocessors. It must be kept as is, without being modified by the end-user.}}
 
{{Warning|This device tree part is related to STM32 microprocessors. It must be kept as is, without being modified by the end-user.}}
Line 28: Line 22:
   
 
The SPDIFRX is an audio peripheral, which can be used as a component of a soundcard through Linux<sup>&reg;</sup> kernel [[ALSA overview|ALSA framework]]. This part of the device tree allows the configuration of the SPDIFRX to implement a soundcard. Refer to [[Soundcard configuration|soundcard configuration]] for examples of SPDIFRX configuration on various boards.
 
The SPDIFRX is an audio peripheral, which can be used as a component of a soundcard through Linux<sup>&reg;</sup> kernel [[ALSA overview|ALSA framework]]. This part of the device tree allows the configuration of the SPDIFRX to implement a soundcard. Refer to [[Soundcard configuration|soundcard configuration]] for examples of SPDIFRX configuration on various boards.
  +
  +
=== DT configuration examples ===
  +
  +
&spdifrx {
  +
pinctrl-names = "default", "sleep";
  +
pinctrl-0 = <&spdifrx_pins_a>;
  +
pinctrl-1 = <&spdifrx_sleep_pins_a>
  +
{{highlight|/* Use spdifrx_pins_a instead of spdifrx_sleep_pins_a configuration,
  +
to allow IEC958 status bits capture, when an audio stream record is
  +
not active. Note that sleep state has to be defined, to allow pin state
  +
recovery from low power modes. */}}
  +
  +
spdifrx_port: port {
  +
spdifrx_endpoint: endpoint {
  +
remote-endpoint = <&spdif_in_endpoint>;
  +
};
  +
};
  +
};
   
 
==How to configure the DT using STM32CubeMX==
 
==How to configure the DT using STM32CubeMX==
Line 34: Line 46:
   
 
==References==
 
==References==
  +
<references />
   
<references />
+
<noinclude>
  +
[[Category:Device tree configuration]]
  +
[[Category:ALSA]]
  +
{{ArticleBasedOnModel | Peripheral or framework device tree configuration model}}
  +
{{PublicationRequestId | 9810| 2018-11-26 | AnneJ}}
  +
</noinclude>