Difference between revisions of "SDMMC internal peripheral"
[quality revision] | [quality revision] |
m
|
m
|
Contents
1 Article purpose[edit]
The purpose of this article is to
- briefly introduce the SDMMC peripheral and its main features
- indicate the level of security supported by this hardware block
- explain how each instance can be allocated to the three runtime contexts and linked to the corresponding software components
- explain, when necessary, how to configure the SDMMC peripheral.
2 Peripheral overview[edit]
The SDMMC peripheral is used to interconnect STM32 MPU to SD memory cards, SDIO and MMC devices.
2.1 Features[edit]
Refer to the STM32MP15 reference manuals for the complete list of features, and to the software components, introduced below, to see which features are implemented.
2.2 Security support[edit]
SDMMC1/2/3 instances are either non-secure or secure peripherals (under ETZPC control).
![]() |
|
3 Peripheral usage and associated software[edit]
3.1 Boot time[edit]
SDMMC1/2 instances can be used to support memory boot on SD or MMC Flash devices.
The SDMMC3 is not used at boot time.
![]() |
The SDMMC instances are ordered by address in the device tree arch/arm/boot/dts/stm32mp157c.dtsi file: sdmmc3: sdmmc@48004000 { ... sdmmc1: sdmmc@58005000 { ... sdmmc2: sdmmc@58007000 { By default, in OpenSTLinux distribution, sdmmc3 is disabled so the sdmmc1 (SD card on Evaluation boards and Discovery kits) and sdmmc2 (eMMC on Evaluation boards and Wifi on Discovery kits) are respectively aliased to mmc0 and mmc1. |
3.2 Runtime[edit]
3.2.1 Overview[edit]
SDMMC1/2/3 instances can be allocated to:
- the Arm® Cortex®-A7 non-secure core to be controlled in Linux® by the MMC framework
or
- the Arm® Cortex®-M4 to be controlled in STM32Cube MPU Package by STM32Cube SDMMC driver
Chapter #Peripheral assignment describes which peripheral instance can be assigned to which context.
3.2.2 Software frameworks[edit]
Internal peripherals software table template
| Mass storage | SDMMC | | Linux MMC framework | STM32Cube SDMMC driver | |- |}
3.2.3 Peripheral configuration[edit]
The configuration is applied by the firmware running in the context to which the peripheral is assigned. The configuration can be done alone via the STM32CubeMX tool for all internal peripherals, and then manually completed (particularly for external peripherals), according to the information given in the corresponding software framework article.
For Linux® kernel configuration, please refer to SDMMC device tree configuration.
3.2.4 Peripheral assignment[edit]
Internal peripherals assignment table template
| rowspan="3" | Mass storage | rowspan="3" | SDMMC | SDMMC1 | | ☐ | | |- | SDMMC2 | | ☐ | | |- | SDMMC3 | | ☐ | ☐ | Assignment (single choice) |-
|}
4 How to go further[edit]
5 References[edit]
==Article purpose== The purpose of this article is to * briefly introduce the SDMMC peripheral and its main features * indicate the level of security supported by this hardware block * explain how each instance can be allocated to the three runtime contexts and linked to the corresponding software components * explain, when necessary, how to configure the SDMMC peripheral. ==Peripheral overview== The '''SDMMC''' peripheral is used to interconnect STM32 MPU to SD memory cards, SDIO and MMC devices. ===Features=== Refer to the [[STM32MP15 resources#Reference manuals|STM32MP15 reference manuals]] for the complete list of features, and to the software components, introduced below, to see which features are implemented. ===Security support=== SDMMC1/2/3 instances are either '''non-secure''' or '''secure''' peripherals (under [[ETZPC_internal_peripheral|ETZPC]] control). {{Warning| * When an SDMMC instance is secure internal, the DMA cannot be used to perform data transfers. * STMicroelectronics does not provide secure MMC driver (see below chapter)}} ==Peripheral usage and associated software== ===Boot time=== SDMMC1/2 instances can be used to support memory boot on SD or MMC Flash devices. The SDMMC3 is not used at boot time. {{Info | The SDMMC instances are ordered by address in the [[Device tree|device tree]] {{CodeSource | Linux kernel | arch/arm/boot/dts/stm32mp157c.dtsi}} file: sdmmc3: sdmmc@48004000 { ... sdmmc1: sdmmc@58005000 { ... sdmmc2: sdmmc@58007000 { By default, in [[OpenSTLinux distribution]], '''sdmmc3 is disabled''' so the sdmmc1 (SD card on [[STM32MP157CSTM32MP157x-EV1_-_hardware_description|Evaluation boards]] and [[STM32MP157X-DKXSTM32MP157x-DKx_-_hardware_description|Discovery kits]]) and sdmmc2 (eMMC on [[STM32MP157CSTM32MP157x-EV1_-_hardware_description|Evaluation boards]] and Wifi on [[STM32MP157X-DKXSTM32MP157x-DKx_-_hardware_description|Discovery kits]]) are respectively aliased to mmc0 and mmc1.<br> '''If you enable sdmmc3''', it will take the mmc0 alias and the aliases above will shift, so don't forget to update the Linux kernel boot command accordingly!<br> For instance, 'root=/dev/mmcblk0p6' will become 'root=/dev/mmcblk1p6' to mount the rootfs from the sdmmc1 (SD card) when sdmmc3 is enabled.}} ===Runtime=== ====Overview==== SDMMC1/2/3 instances can be allocated to: * the Arm<sup>®</sup> Cortex<sup>®</sup>-A7 non-secure core to be controlled in Linux<sup>®</sup> by the [[MMC overview|MMC framework]] or * the Arm<sup>®</sup> Cortex<sup>®</sup>-M4 to be controlled in STM32Cube MPU Package by [[STM32CubeMP1 architecture|STM32Cube SDMMC driver]] Chapter [[#Peripheral assignment]] describes which peripheral instance can be assigned to which context. ====Software frameworks==== {{:Internal_peripherals_software_table_template}} | Mass storage | [[SDMMC internal peripheral|SDMMC]] | | [[MMC overview|Linux MMC framework]] | [[STM32CubeMP1 architecture|STM32Cube SDMMC driver]] | |- |} ====Peripheral configuration==== The configuration is applied by the firmware running in the context to which the peripheral is assigned. The configuration can be done alone via the [[STM32CubeMX]] tool for all internal peripherals, and then manually completed (particularly for external peripherals), according to the information given in the corresponding software framework article. For Linux<sup>®</sup> kernel configuration, please refer to [[SDMMC device tree configuration]]. ====Peripheral assignment==== {{:Internal_peripherals_assignment_table_template}}<onlyinclude> | rowspan="3" | Mass storage | rowspan="3" | [[SDMMC internal peripheral|SDMMC]] | SDMMC1 | | <span title="assignable peripheral" style="font-size:21px">☐</span> | | |- | SDMMC2 | | <span title="assignable peripheral" style="font-size:21px">☐</span> | | |- | SDMMC3 | | <span title="assignable peripheral" style="font-size:21px">☐</span> | <span title="assignable peripheral" style="font-size:21px">☐</span> | Assignment (single choice) |-</onlyinclude> |} ==How to go further== ==References==<references/> <noinclude> {{ArticleBasedOnModel | Internal peripheral article model}} {{PublicationRequestId | 8316 | 2018-08-06 | AnneJ}} [[Category:High speed interface peripherals]] [[Category:Mass storage peripherals]]</noinclude>
Line 30: | Line 30: | ||
... |
... |
||
sdmmc2: sdmmc@58007000 { |
sdmmc2: sdmmc@58007000 { |
||
− | By default, in [[OpenSTLinux distribution]], '''sdmmc3 is disabled''' so the sdmmc1 (SD card on [[ |
+ | By default, in [[OpenSTLinux distribution]], '''sdmmc3 is disabled''' so the sdmmc1 (SD card on [[STM32MP157x-EV1_-_hardware_description|Evaluation boards]] and [[STM32MP157x-DKx_-_hardware_description|Discovery kits]]) and sdmmc2 (eMMC on [[STM32MP157x-EV1_-_hardware_description|Evaluation boards]] and Wifi on [[STM32MP157x-DKx_-_hardware_description|Discovery kits]]) are respectively aliased to mmc0 and mmc1.<br> |
'''If you enable sdmmc3''', it will take the mmc0 alias and the aliases above will shift, so don't forget to update the Linux kernel boot command accordingly!<br> |
'''If you enable sdmmc3''', it will take the mmc0 alias and the aliases above will shift, so don't forget to update the Linux kernel boot command accordingly!<br> |
||
For instance, 'root=/dev/mmcblk0p6' will become 'root=/dev/mmcblk1p6' to mount the rootfs from the sdmmc1 (SD card) when sdmmc3 is enabled.}} |
For instance, 'root=/dev/mmcblk0p6' will become 'root=/dev/mmcblk1p6' to mount the rootfs from the sdmmc1 (SD card) when sdmmc3 is enabled.}} |