Difference between revisions of "SDMMC device tree configuration"

[quality revision] [quality revision]
m (DT configuration (board level))
 
m
 
Template:ArticleMainWriter Template:ArticleApprovedVersion

1 Article purpose[edit]

This article explains how to configure the SDMMC internal peripheral when it is assigned to the Linux® OS. In that case, it is controlled by the MMC framework.

The configuration is performed using the device tree mechanism that provides a hardware description of the SDMMC peripheral, used by the STM32 SDMMC Linux driver and by the MMC framework.

If the peripheral is assigned to another execution context, refer to How to assign an internal peripheral to a runtime context article for guidelines on peripheral assignment and configuration.

2 DT bindings documentation[edit]

The SDMMC device tree bindings are composed of:

  • generic MMC device tree bindings [1].
  • SDMMC MMC/SD/SDIO interface bindings [2].

3 DT configuration[edit]

This hardware description is a combination of the STM32 microprocessor device tree files (.dtsi extension) and board device tree files (.dts extension). See the Device tree for an explanation of the device tree file split.

STM32CubeMX can be used to generate the board device tree. Refer to How to configure the DT using STM32CubeMX for more details.

3.1 DT configuration (STM32 level)[edit]

The SDMMC peripheral node is located in stm32mp157cstm32mp151.dtsi[3] file.

   sdmmc1: sdmmc@58005000 {                                  Comments
       compatible = "arm,pl18x", "arm,primecell";
       arm,primecell-periphid = <0x00253180>;
       reg = <0x58005000 0x1000>,                            --> The controller register location 
             <0x58006000 0x1000>;                            --> The delay block register location
       interrupts = <GIC_SPI 49 IRQ_TYPE_LEVEL_HIGH>;        --> The interrupt number used
       interrupt-names = "cmd_irq";
       clocks = <&rcc SDMMC1_K>;
       clock-names = apb_pclk
       resets = <&rcc SDMMC1_R>;                      
       status = "disabled";
   };
Warning.png This device tree part is related to STM32 microprocessors. It should be kept as is, without being modified by the end-user.

3.2 DT configuration (board level)[edit]

The SDMMC peripheral may connect to one SD card, one e•MMC™ device or one SDIO card.

   &sdmmc1{                                                  Comments     
       pinctrl-names = "default", "opendrain", "sleep";      --> For pinctrl configuration, please refer to Pinctrl device tree configuration
       pinctrl-0 = <&sdmmc1_b4_pins_a &sdmmc1_dir_pins_a>;
       pinctrl-1 = <&sdmmc1_b4_od_pins_a &sdmmc1_dir_pins_a>;
       pinctrl-2 = <&sdmmc1_b4_sleep_pins_a &sdmmc1_dir_sleep_pins_a>;
       st,neg-edge;                                          --> Generate data and command on sdmmc clock falling edge
       st,sig-dir;                                           --> Allow to select direction polarity of an external transceiver
       st,use-ckin;                                          --> Use sdmmc_ckin pin from an external transceiver to sample the receive data
       bus-width = <4>;                                      --> Number of data lines, can be 1, 4 or 8
       vmmc-supply = <&vdd_sd>;                              --> Supply node for card's power
       vqmmc-supply = <&sd_switch>;                          --> Supply node for IO line power
       status = "okay";                                      --> Enable the node
   };

Below optional properties have to be used when an external transceiver is connected:

  • st,sig-dir: This property allows to select external transceiver direction signals polarity. When this property is set, the voltage transceiver IOs are driven as output when the direction signals are high. Without setting this property, the voltage transceiver IOs are driven as output when the direction signals are low.
  • st,use-ckin: By setting this property, the sdmmc_ckin pin from an external transceiver is used to sample the receive data.

3.3 DT configuration examples[edit]

Below example shows how to configure the SDMMC when an e•MMC™ is connected with 8 data lines [4].

   &sdmmc2{                                                  Comments     
       pinctrl-names = "default", "opendrain", "sleep";      
       pinctrl-0 = <&sdmmc2_b4_pins_a &sdmmc2_dir_pins_a>;
       pinctrl-1 = <&sdmmc2_b4_od_pins_a &sdmmc2_dir_pins_a>;
       pinctrl-2 = <&sdmmc2_b4_sleep_pins_a &sdmmc2_dir_sleep_pins_a>;             
       non-removable;                                        --> Non-removable slot, assume always present
       no-sd;                                                --> Avoid to send SD command during initialization
       no-sdio;                                              --> Avoid to send SDIO command during initialization
       st,neg-edge;                                           
       bus-width = <8>;                                    
       vmmc-supply = <&v3v3>;                      
       vqmmc-supply = <&vdd>;
       mmc-ddr-3_3v;                                         --> Host supports e•MMC™ DDR 3.3V                         
       status = "okay";                                     
   };

Below example shows how to configure the SDMMC to SD card (4 data lines) with an external transceiver [4].

   &sdmmc1{                                                  Comments     
       pinctrl-names = "default", "opendrain", "sleep";    
       pinctrl-0 = <&sdmmc1_b4_pins_a &sdmmc1_dir_pins_a>;
       pinctrl-1 = <&sdmmc1_b4_od_pins_a &sdmmc1_dir_pins_a>;
       pinctrl-2 = <&sdmmc1_b4_sleep_pins_a &sdmmc1_dir_sleep_pins_a>;               
       broken-cd;                                            --> use polling mode for card detection
       st,neg-edge;
       st,sig-dir;
       st,use-ckin;                                    
       bus-width = <4>;
       sd-uhs-sdr12;                                         --> sd modes supported [1]
       sd-uhs-sdr25;
       sd-uhs-sdr50;
       sd-uhs-ddr50;
       sd-uhs-sdr104;
       vmmc-supply = <&vdd_sd>;                      
       vqmmc-supply = <&sd_switch>;                          
       status = "okay";                                     
   };

4 How to configure the DT using STM32CubeMX[edit]

The STM32CubeMX tool can be used to configure the STM32MPU device and get the corresponding platform configuration device tree files.
The STM32CubeMX may not support all the properties described in the above DT bindings documentation paragraph. If so, the tool inserts user sections in the generated device tree. These sections can then be edited to add some properties and they are preserved from one generation to another. Refer to STM32CubeMX user manual for further information.

5 References[edit]

Please refer to the following links for additional information:


<noinclude>

{{ArticleBasedOnModel | [[Peripheral or framework device tree configuration model]]}}
{{ArticleMainWriter | LudovicB}}
{{ArticleApprovedVersion | LudovicB | GeraldB, ChristopheK (Passed, 18Oct'18) | No previous approved version | BrunoB - 26Oct'18 - 9408 | 26Oct'18}}

[[Category:Device tree configuration]]
[[Category:Mass storage]]</noinclude>

== Article purpose ==
This article explains how to configure the [[SDMMC internal peripheral|'''SDMMC''' internal peripheral]] when it is assigned to the Linux<sup>&reg;</sup> OS. In that case, it is controlled by the  [[MMC overview|MMC framework]].

The configuration is performed using the [[Device tree|device tree]] mechanism that provides a hardware description of the SDMMC peripheral, used by the STM32 SDMMC Linux driver and by  the MMC framework.
If the peripheral is assigned to another execution context, refer to [[How to assign an internal peripheral to a runtime context]] article for guidelines on peripheral assignment and configuration.
== DT bindings documentation ==
The SDMMC device tree bindings are composed of:

* generic MMC device tree bindings <ref name="mmc.txtyaml">{{CodeSource | Linux kernel | Documentation/devicetree/bindings/mmc/mmc.txt-controller.yaml}}</ref>.

* SDMMC MMC/SD/SDIO interface bindings <ref> {{CodeSource | Linux kernel | Documentation/devicetree/bindings/mmc/mmci.txt}} </ref>.

== DT configuration ==
This hardware description is a combination of the '''STM32 microprocessor''' device tree files (''.dtsi'' extension) and '''board''' device tree files (''.dts'' extension). See the [[Device tree]] for an explanation of the device tree file split.

'''STM32CubeMX''' can be used to generate the board device tree. Refer to [[#How_to_configure_the_DT_using_STM32CubeMX|How to configure the DT using STM32CubeMX]] for more details.

=== DT configuration (STM32 level) ===
The SDMMC peripheral node is located in ''stm32mp157cstm32mp151.dtsi''<ref>{{CodeSource | Linux kernel | arch/arm/boot/dts/stm32mp157cstm32mp151.dtsi}}</ref> file.

    sdmmc1: sdmmc@58005000 {                                  {{highlight|Comments}}
        compatible = "arm,pl18x", "arm,primecell";
        arm,primecell-periphid = <0x00253180>;
        reg = <0x58005000 0x1000>,                            {{highlight|--> The controller register location}} <0x58006000 0x1000>;                            {{highlight|--> The delay block register location}}
        interrupts = <GIC_SPI 49 IRQ_TYPE_LEVEL_HIGH>;        {{highlight|--> The interrupt number used}}
        interrupt-names = "cmd_irq";
        clocks = <&rcc SDMMC1_K>;
        clock-names = apb_pclk
        resets = <&rcc SDMMC1_R>;                      
        status = "disabled";
    };

{{Warning|This device tree part is related to STM32 microprocessors. It should be kept as is, without being modified by the end-user.}}

=== DT configuration (board level) ===
The SDMMC peripheral may connect to one SD card, one ''e''•MMC™ device or one SDIO card.

    &sdmmc1{                                                  {{highlight|Comments}}     
        pinctrl-names = "default", "opendrain", "sleep";      {{highlight|--> For pinctrl configuration, please refer to [[Pinctrl device tree configuration]]}}
        pinctrl-0 = <&sdmmc1_b4_pins_a &sdmmc1_dir_pins_a>;
        pinctrl-1 = <&sdmmc1_b4_od_pins_a &sdmmc1_dir_pins_a>;
        pinctrl-2 = <&sdmmc1_b4_sleep_pins_a &sdmmc1_dir_sleep_pins_a>;
        st,neg-edge;                                          {{highlight|--> Generate data and command on sdmmc clock falling edge}}
        st,sig-dir;                                           {{highlight|--> Allow to select direction polarity of an external transceiver}}
        st,use-ckin;                                          {{highlight|--> Use sdmmc_ckin pin from an external transceiver to sample the receive data}}
        bus-width = <4>;                                      {{highlight|--> Number of data lines, can be 1, 4 or 8}}
        vmmc-supply = <&vdd_sd>;                              {{highlight|--> Supply node for card's power}}
        vqmmc-supply = <&sd_switch>;                          {{highlight|--> Supply node for IO line power}}
        status = "okay";                                      {{highlight|--> Enable the node}}
    };

Below optional properties have to be used when an external transceiver is connected:
* st,sig-dir: This property allows to select external transceiver direction signals polarity. When this property is set, the voltage transceiver IOs are driven as output when the direction signals are high. Without setting this property, the voltage transceiver IOs are driven as output when the direction signals are low.
* st,use-ckin: By setting this property, the sdmmc_ckin pin from an external transceiver is used to sample the receive data.

=== DT configuration examples ===
Below example shows how to configure the SDMMC when an ''e''•MMC™ is connected with 8 data lines <ref name="ED1">{{CodeSource | Linux kernel | arch/arm/boot/dts/stm32mp157c-ed1.dtsstm32mp15xx-edx.dtsi}}</ref>.

    &sdmmc2{                                                  {{highlight|Comments}}     
        pinctrl-names = "default", "opendrain", "sleep";      
        pinctrl-0 = <&sdmmc2_b4_pins_a &sdmmc2_dir_pins_a>;
        pinctrl-1 = <&sdmmc2_b4_od_pins_a &sdmmc2_dir_pins_a>;
        pinctrl-2 = <&sdmmc2_b4_sleep_pins_a &sdmmc2_dir_sleep_pins_a>;             
        non-removable;                                        {{highlight|--> Non-removable slot, assume always present}}
        no-sd;                                                {{highlight|--> Avoid to send SD command during initialization}}
        no-sdio;                                              {{highlight|--> Avoid to send SDIO command during initialization}}
        st,neg-edge;                                           
        bus-width = <8>;                                    
        vmmc-supply = <&v3v3>;                      
        vqmmc-supply = <&vdd>;
        mmc-ddr-3_3v;                                         {{highlight|--> Host supports ''e''•MMC™ DDR 3.3V}}                         
        status = "okay";                                     
    };

Below example shows how to configure the SDMMC to SD card (4 data lines) with an external transceiver <ref name="ED1"/>.

    &sdmmc1{                                                  {{highlight|Comments}}     
        pinctrl-names = "default", "opendrain", "sleep";    
        pinctrl-0 = <&sdmmc1_b4_pins_a &sdmmc1_dir_pins_a>;
        pinctrl-1 = <&sdmmc1_b4_od_pins_a &sdmmc1_dir_pins_a>;
        pinctrl-2 = <&sdmmc1_b4_sleep_pins_a &sdmmc1_dir_sleep_pins_a>;               
        broken-cd;                                            {{highlight|--> use polling mode for card detection}}
        st,neg-edge;
        st,sig-dir;
        st,use-ckin;                                    
        bus-width = <4>;
        sd-uhs-sdr12;                                         {{highlight|--> sd modes supported <ref name="mmc.txtyaml"/>}}
        sd-uhs-sdr25;
        sd-uhs-sdr50;
        sd-uhs-ddr50;
        sd-uhs-sdr104;
        vmmc-supply = <&vdd_sd>;                      
        vqmmc-supply = <&sd_switch>;                          
        status = "okay";                                     
    };

==How to configure the DT using STM32CubeMX==
The [[STM32CubeMX]] tool can be used to configure the STM32MPU device and get the corresponding [[Device_tree#STM32|platform configuration device tree]] files.<br />

The STM32CubeMX may not support all the properties described in the above [[#DT bindings documentation|DT bindings documentation]] paragraph. If so, the tool inserts '''user sections''' in the generated device tree. These sections can then be edited to add some properties and they are preserved from one generation to another. Refer to [[STM32CubeMX]] user manual for further information.

==References==
Please refer to the following links for additional information:
<references /><references />

<noinclude>

[[Category:Device tree configuration]]
[[Category:Mass storage]]
{{PublicationRequestId | 9408 | 2018-10-26 | BrunoB}}
{{ArticleBasedOnModel | Peripheral or framework device tree configuration model}}</noinclude>
(3 intermediate revisions by 3 users not shown)
Line 1: Line 1:
<noinclude>
 
{{ArticleBasedOnModel | [[Peripheral or framework device tree configuration model]]}}
 
{{ArticleMainWriter | LudovicB}}
 
{{ArticleApprovedVersion | LudovicB | GeraldB, ChristopheK (Passed, 18Oct'18) | No previous approved version | BrunoB - 26Oct'18 - 9408 | 26Oct'18}}
 
 
[[Category:Device tree configuration]]
 
[[Category:Mass storage]]
 
</noinclude>
 
 
 
== Article purpose ==
 
== Article purpose ==
 
This article explains how to configure the [[SDMMC internal peripheral|'''SDMMC''' internal peripheral]] when it is assigned to the Linux<sup>&reg;</sup> OS. In that case, it is controlled by the  [[MMC overview|MMC framework]].
 
This article explains how to configure the [[SDMMC internal peripheral|'''SDMMC''' internal peripheral]] when it is assigned to the Linux<sup>&reg;</sup> OS. In that case, it is controlled by the  [[MMC overview|MMC framework]].
   
 
The configuration is performed using the [[Device tree|device tree]] mechanism that provides a hardware description of the SDMMC peripheral, used by the STM32 SDMMC Linux driver and by  the MMC framework.
 
The configuration is performed using the [[Device tree|device tree]] mechanism that provides a hardware description of the SDMMC peripheral, used by the STM32 SDMMC Linux driver and by  the MMC framework.
  +
  +
If the peripheral is assigned to another execution context, refer to [[How to assign an internal peripheral to a runtime context]] article for guidelines on peripheral assignment and configuration.
   
 
== DT bindings documentation ==
 
== DT bindings documentation ==
 
The SDMMC device tree bindings are composed of:
 
The SDMMC device tree bindings are composed of:
   
* generic MMC device tree bindings <ref name="mmc.txt">{{CodeSource | Linux kernel | Documentation/devicetree/bindings/mmc/mmc.txt}}</ref>.
+
* generic MMC device tree bindings <ref name="mmc.yaml">{{CodeSource | Linux kernel | Documentation/devicetree/bindings/mmc/mmc-controller.yaml}}</ref>.
   
 
* SDMMC MMC/SD/SDIO interface bindings <ref> {{CodeSource | Linux kernel | Documentation/devicetree/bindings/mmc/mmci.txt}} </ref>.
 
* SDMMC MMC/SD/SDIO interface bindings <ref> {{CodeSource | Linux kernel | Documentation/devicetree/bindings/mmc/mmci.txt}} </ref>.
Line 26: Line 19:
   
 
=== DT configuration (STM32 level) ===
 
=== DT configuration (STM32 level) ===
The SDMMC peripheral node is located in ''stm32mp157c.dtsi''<ref>{{CodeSource | Linux kernel | arch/arm/boot/dts/stm32mp157c.dtsi}}</ref> file.
+
The SDMMC peripheral node is located in ''stm32mp151.dtsi''<ref>{{CodeSource | Linux kernel | arch/arm/boot/dts/stm32mp151.dtsi}}</ref> file.
   
 
     sdmmc1: sdmmc@58005000 {                                  {{highlight|Comments}}
 
     sdmmc1: sdmmc@58005000 {                                  {{highlight|Comments}}
Line 65: Line 58:
   
 
=== DT configuration examples ===
 
=== DT configuration examples ===
Below example shows how to configure the SDMMC when an ''e''•MMC™ is connected with 8 data lines <ref name="ED1">{{CodeSource | Linux kernel | arch/arm/boot/dts/stm32mp157c-ed1.dts}}</ref>.
+
Below example shows how to configure the SDMMC when an ''e''•MMC™ is connected with 8 data lines <ref name="ED1">{{CodeSource | Linux kernel | arch/arm/boot/dts/stm32mp15xx-edx.dtsi}}</ref>.
   
 
     &sdmmc2{                                                  {{highlight|Comments}}     
 
     &sdmmc2{                                                  {{highlight|Comments}}     
Line 95: Line 88:
 
         st,use-ckin;                                     
 
         st,use-ckin;                                     
 
         bus-width = <4>;
 
         bus-width = <4>;
         sd-uhs-sdr12;                                        {{highlight|--> sd modes supported <ref name="mmc.txt"/>}}
+
         sd-uhs-sdr12;                                        {{highlight|--> sd modes supported <ref name="mmc.yaml"/>}}
 
         sd-uhs-sdr25;
 
         sd-uhs-sdr25;
 
         sd-uhs-sdr50;
 
         sd-uhs-sdr50;
Line 111: Line 104:
 
==References==
 
==References==
 
Please refer to the following links for additional information:
 
Please refer to the following links for additional information:
  +
<references />
   
<references />
+
<noinclude>
  +
[[Category:Device tree configuration]]
  +
[[Category:Mass storage]]
  +
{{PublicationRequestId | 9408 | 2018-10-26 | BrunoB}}
  +
{{ArticleBasedOnModel | Peripheral or framework device tree configuration model}}
  +
</noinclude>