Difference between revisions of "SAES device tree configuration"

[unchecked revision] [quality revision]
m (Nathalie Sangouard moved page SAES Device tree configuration to SAES device tree configuration without leaving a redirect: replace D by d in device)
m
Renaming.png This page is a candidate for renaming (move).
The requested new name is: SAES device tree configuration .
The supplied reason is: No upcase on device .
-- nicolas toromanoff (talk) 14:55, 19 May 2022 (CEST).
Wiki maintainers: remember to update the pages that link this page before renaming (moving) it.
Applicable for STM32MP13x lines

1 Article purpose[edit]

The purpose of this article is to explain how to configure the SAES using the device tree mechanism, relying on the bindings documentation, that is the description of the required and optional device-tree properties.

The peripheral can be assigned to different contexts/software components, depending on the final product needs. Refer to How to assign an internal peripheral to a runtime context article for guidelines on this configuration .

2 DT bindings documentation[edit]

The device tree binding documents are stored either in the given applicable components listed below, or in the Linux kernel repository:

3 DT configuration[edit]

This hardware description is a combination of the STM32 microprocessor device tree files (.dtsi extension) and board device tree files (.dts extension). See the Device tree for an explanation of the device-tree file organization.

STM32CubeMX can be used to generate the board device tree. Refer to How to configure the DT using STM32CubeMX for more details.

3.1 DT configuration (STM32/SoC level)[edit]

The SAES node is located in the device tree file for the software components, supporting the peripheral and listed in the above DT bindings documentation paragraph.

It is only included on SoC supporting cryptography.

Warning white.png Warning
This device tree part is related to STM32 microprocessors. It must be kept as is, without being modified by the end-user.

3.2 DT configuration (board level)[edit]

The objective of this chapter is to explain how to enable and configure the SAES DT nodes for a board.

Peripheral configuration should be done in specific board device tree files (board dts file).


3.3 DT configuration examples[edit]

   &saes {
        status = "okay";
   };

4 How to configure the DT using STM32CubeMX[edit]

The STM32CubeMX tool can be used to configure the STM32MPU device and get the corresponding platform configuration device tree files.
STM32CubeMX may not support all the properties described in DT binding files listed in the above DT bindings documentation paragraph. If so, the tool inserts user sections in the generated device tree. These sections can then be edited to add some properties, and they are preserved from one generation to another. Refer to STM32CubeMX user manual for further information.

5 References[edit]

Refer to the following links for additional information:



{{ArticleToRename | SAES device tree configuration | No upcase on device | [[User:Nicolas Toromanoff|Nicolas Toromanoff]] ([[User talk:Nicolas Toromanoff|talk]]) 14:55, 19 May 2022 (CEST)}}<noinclude>{{ApplicableFor
|MPUs list=STM32MP13x
|MPUs checklist=STM32MP13x
}}</noinclude>


== Article purpose ==
The purpose of this article is to explain how to configure the [[SAES_internal_peripheral|'''SAES''']] using the [[Device tree|device tree]] mechanism, relying on the bindings documentation, that is the description of the required and optional device-tree properties.

The peripheral can be assigned to different contexts/software components, depending on the final product needs. Refer to [[How to assign an internal peripheral to a runtime context]] article for guidelines on this configuration .

== DT bindings documentation ==

The device tree binding documents are stored either in the given applicable components listed below, or in the Linux kernel repository: <br>


* TF-A BL2, OP-TEE:
** SAES device tree bindings : {{CodeSource | OP-TEE_OS | documentation/devicetree/bindings/crypto/st,stm32-saes.yaml}}

== DT configuration ==
This hardware description is a combination of the '''STM32 microprocessor''' device tree files (''.dtsi'' extension) and '''board''' device tree files (''.dts'' extension). See the [[Device tree]] for an explanation of the device-tree file organization.

'''STM32CubeMX''' can be used to generate the board device tree. Refer to [[#How_to_configure_the_DT_using_STM32CubeMX|How to configure the DT using STM32CubeMX]] for more details.

===DT configuration (STM32/SoC level) ===

The [[SAES_internal_peripheral|'''SAES''']] node is located in the [[STM32 MPU device_tree#Device tree structure|device tree file]] for the software components, supporting the peripheral and listed in the above [[#DT bindings documentation|DT bindings documentation]] paragraph. 

It is only included on SoC supporting cryptography.

{{Warning|This device tree part is related to STM32 microprocessors. It must be kept as is, without being modified by the end-user.}}

=== DT configuration (board level) ===

The objective of this chapter is to explain how to enable and configure the [[SAES_internal_peripheral|'''SAES''']] DT nodes for a board.<br>


Peripheral configuration should be done in specific board device tree files (board dts file).<br>


=== DT configuration examples ===

    &saes {
         status = "okay";
    };

==How to configure the DT using STM32CubeMX==
The [[STM32CubeMX]] tool can be used to configure the STM32MPU device and get the corresponding [[Device_tree#STM32|platform configuration device tree]] files.<br />

STM32CubeMX may not support all the properties described in DT binding files listed in the above [[#DT bindings documentation|DT bindings documentation]] paragraph. If so, the tool inserts '''user sections''' in the generated device tree. These sections can then be edited to add some properties, and they are preserved from one generation to another. Refer to [[STM32CubeMX]] user manual for further information.

==References==
Refer to the following links for additional information:<references />

<noinclude>

{{ArticleBasedOnModel | Peripheral or framework device tree configuration model}}

[[Category:Device tree configuration]]
[[Category:OP-TEE Crypto]]</noinclude>
Line 1: Line 1:
{{ArticleToRename | SAES device tree configuration | No upcase on device | [[User:Nicolas Toromanoff|Nicolas Toromanoff]] ([[User talk:Nicolas Toromanoff|talk]]) 14:55, 19 May 2022 (CEST)}}
 
 
<noinclude>{{ApplicableFor
 
<noinclude>{{ApplicableFor
 
|MPUs list=STM32MP13x
 
|MPUs list=STM32MP13x