Approved version. Approved on: 15:33, 26 November 2021
- Last edited 5 months ago ago
Reserved memory
1 Article purpose[edit]
The Reserved-memory mechanism[1] allows reserving memory regions in the kernel. This mechanism is used by drivers to allocate buffers in specific memory regions (such as internal SRAM) or to get a dedicated memory pool that will not be managed by Linux® conventionnal memory allocator (in DDR).
2 Use cases[edit]
In OpenSTLinux, the reserved-memory is used:
- On STM32MP1 series by:
- the dmaengine driver to reserve the region where DMA buffers are allocated, typically in internal SRAM (STM32MP13 SRAM or STM32MP15 MCU SRAM).
- the remoteproc driver to reserve the regions in RETRAM and MCU SRAM where the coprocessor firmware will be loaded.
- the RPMsg driver to reserve the region where RPMsg buffers used for interprocess communication with the coprocessor, are allocated, typically MCU SRAM.
- the Vivante Gcnano driver to reserve the region where the GPU working memory is allocated, typically the DDR.