Difference between revisions of "QUADSPI device tree configuration"

[quality revision] [quality revision]
m
m
 

1 Article purpose[edit]

This article explains how to configure the QUADSPI internal peripheral when it is assigned to the Linux® OS. In that case, it is controlled by the MTD framework.

The configuration is performed using the device tree mechanism that provides a hardware description of the QUADSPI peripheral, used by the STM32 QUADSPI Linux driver and by the MTD framework.

If the peripheral is assigned to another execution context, refer to How to assign an internal peripheral to a runtime context article for guidelines on peripheral assignment and configuration.

2 DT bindings documentation[edit]

The QUADSPI device tree bindings are composed by:

  • generic SPI-NOR / SPI-NAND Flash memory bindings [1].
  • QUADSPI driver bindings [2].

3 DT configuration[edit]

This hardware description is a combination of the STM32 microprocessor device tree files (.dtsi extension) and board device tree files (.dts extension). See the Device tree for an explanation of the device tree file split.

STM32CubeMX can be used to generate the board device tree. Refer to How to configure the DT using STM32CubeMX for more details.

3.1 DT configuration (STM32 level)[edit]

The QUADSPI peripheral node is located in stm32mp157cstm32mp151.dtsi[3] file.

   qspi: spi@58003000 {                                      Comments
       compatible = "st,stm32f469-qspi";
       reg = <0x58003000 0x1000>,                            --> Register location
             <0x70000000 0x10000000>;                        --> Memory mapping address
       reg-names = "qspi", "qspi_mm";
       interrupts = <GIC_SPI 92 IRQ_TYPE_LEVEL_HIGH>;        --> The interrupt number used
       dmas = <&mdma1 22 0x10 0x100002 0x0 0x0 0x0>,         --> DMA specifiers [4]
              <&mdma1 22 0x10 0x100008 0x0 0x0 0x0>;
       dma-names = "tx", "rx";
       clocks = <&rcc QSPI_K>;
       resets = <&rcc QSPI_R>;   
       status = "disabled";
   };

Warning white.png Warning
This device tree part related to the STM32 should be kept as is, the customer should not modify it.

3.2 DT configuration (board level)[edit]

The QUADSPI peripheral may connect a maximum of 2 SPI-NOR Flash memories.

SPI-NOR Flash memory nodes [1] must be children of the QUADSPI peripheral node.

   &qspi {                                                   Comments
       pinctrl-names = "default", "sleep";                   --> For pinctrl configuration, please refer to Pinctrl device tree configuration
       pinctrl-0 = <&qspi_clk_pins_a &qspi_bk1_pins_a &qspi_bk2_pins_a>;
       pinctrl-1 = <&qspi_clk_sleep_pins_a &qspi_bk1_sleep_pins_a &qspi_bk2_sleep_pins_a>;
       reg = <0x58003000 0x1000>,
             <0x70000000 0x4000000>;                         --> Overwrite the memory map to the Flash device size, avoid the waste of virtual memory that will not be used
       #address-cells = <1>;
       #size-cells = <0>;
       status = "okay";                                      --> Enable the node

flash0: mx66l51235l@0 { compatible = "jdecjedec,spi-nor"; reg = <0>; --> Chip select number spi-rx-bus-width = <4>; --> The bus width (number of data wires used) spi-max-frequency = <108000000>; --> Maximum SPI clocking speed of device in Hz #address-cells = <1>; #size-cells = <1>; }; };

3.3 DT configuration example[edit]

The below example shows how to configure the QUADSPI peripheral when 1 SPI-NAND Flash and 1 SPI-NOR Flash memories are connected.

   &qspi {                                                    
       pinctrl-names = "default", "sleep";                    
       pinctrl-0 = <&qspi_clk_pins_a &qspi_bk1_pins_a &qspi_bk2_pins_a>;
       pinctrl-1 = <&qspi_clk_sleep_pins_a &qspi_bk1_sleep_pins_a &qspi_bk2_sleep_pins_a>;
       reg = <0x58003000 0x1000>,
             <0x70000000 0x4000000>;                          
       #address-cells = <1>;
       #size-cells = <0>;
       status = "okay";
flash0: mx66l51235l@0 { compatible = "jdecjedec,spi-nor"; reg = <0>; spi-rx-bus-width = <4>; spi-max-frequency = <108000000>; #address-cells = <1>; #size-cells = <1>; };
flash1: mt29f2g01abagd@1 { compatible = "spi-nand"; reg = <1>; spi-rx-bus-width = <4>; spi-tx-bus-width = <4>; spi-max-frequency = <133000000>; #address-cells = <1>; #size-cells = <1>; }; };

4 How to configure the DT using STM32CubeMX[edit]

The STM32CubeMX tool can be used to configure the STM32MPU device and get the corresponding platform configuration device tree files.
The STM32CubeMX may not support all the properties described in the above DT bindings documentation paragraph. If so, the tool inserts user sections in the generated device tree. These sections can then be edited to add some properties and they are preserved from one generation to another. Refer to STM32CubeMX user manual for further information.

5 References[edit]

Please refer to the following links for full description:



== Article purpose ==
This article explains how to configure the [[QUADSPI internal peripheral|'''QUADSPI''' internal peripheral]] when it is assigned to the Linux<sup>&reg;</sup> OS. In that case, it is controlled by the  [[MTD overview|MTD framework]].

The configuration is performed using the [[Device tree|device tree]] mechanism that provides a hardware description of the QUADSPI peripheral, used by the STM32 QUADSPI Linux driver and by  the MTD framework.

If the peripheral is assigned to another execution context, refer to [[How to assign an internal peripheral to a runtime context]] article for guidelines on peripheral assignment and configuration.

== DT bindings documentation ==

The QUADSPI device tree bindings are composed by:

* generic SPI-NOR / SPI-NAND Flash memory bindings <ref name="spi_busses_bindings">{{CodeSource | Linux kernel | Documentation/devicetree/bindings/spi/spi-bus.txtcontroller.yaml}}</ref>.

* QUADSPI driver bindings <ref> {{CodeSource | Linux kernel | Documentation/devicetree/bindings/spi/spi-st,stm32-qspi.txtyaml}} </ref>.

== DT configuration ==
This hardware description is a combination of the '''STM32 microprocessor''' device tree files (''.dtsi'' extension) and '''board''' device tree files (''.dts'' extension). See the [[Device tree]] for an explanation of the device tree file split.

'''STM32CubeMX''' can be used to generate the board device tree. Refer to [[#How_to_configure_the_DT_using_STM32CubeMX|How to configure the DT using STM32CubeMX]] for more details.

===DT configuration (STM32 level) ===
The QUADSPI peripheral node is located in ''stm32mp157cstm32mp151.dtsi''<ref>{{CodeSource | Linux kernel | arch/arm/boot/dts/stm32mp157cstm32mp151.dtsi}}</ref> file. 

    qspi: spi@58003000 {                                      {{highlight|Comments}}
        compatible = "st,stm32f469-qspi";
        reg = <0x58003000 0x1000>,                            {{highlight|--> Register location}}<0x70000000 0x10000000>;                        {{highlight|--> Memory mapping address}}
        reg-names = "qspi", "qspi_mm";
        interrupts = <GIC_SPI 92 IRQ_TYPE_LEVEL_HIGH>;        {{highlight|--> The interrupt number used}}
        dmas = <&mdma1 22 0x10 0x100002 0x0 0x0 0x0>,         {{highlight|--> DMA specifiers <ref>{{CodeSource | Linux kernel | Documentation/devicetree/bindings/dma/st,stm32-mdma.txtyaml}}</ref>}}<&mdma1 22 0x10 0x100008 0x0 0x0 0x0>;
        dma-names = "tx", "rx";
        clocks = <&rcc QSPI_K>;
        resets = <&rcc QSPI_R>;   
        status = "disabled";
    };

{{Warning|This device tree part related to the STM32 should be kept as is, the customer should not modify it.}}

=== DT configuration (board level) ===
The QUADSPI peripheral may connect a maximum of 2 SPI-NOR Flash memories.

SPI-NOR Flash memory nodes <ref name="spi_busses_bindings"/> must be children of the QUADSPI peripheral node.

    &qspi {                                                   {{highlight|Comments}}
        pinctrl-names = "default", "sleep";                   {{highlight|--> For pinctrl configuration, please refer to [[Pinctrl device tree configuration]]}}
        pinctrl-0 = <&qspi_clk_pins_a &qspi_bk1_pins_a &qspi_bk2_pins_a>;
        pinctrl-1 = <&qspi_clk_sleep_pins_a &qspi_bk1_sleep_pins_a &qspi_bk2_sleep_pins_a>;
        reg = <0x58003000 0x1000>,<0x70000000 0x4000000>;                         {{highlight|--> Overwrite the memory map to the Flash device size, avoid the waste of virtual memory that will not be used}}
        #address-cells = <1>;
        #size-cells = <0>;
        status = "okay";                                      {{highlight|--> Enable the node}}<br>

        flash0: mx66l51235l@0 {     
            compatible = "jdecjedec,spi-nor";                                  
            reg = <0>;                                        {{highlight|--> Chip select number}}
            spi-rx-bus-width = <4>;                           {{highlight|--> The bus width (number of data wires used)}}
            spi-max-frequency = <108000000>;                  {{highlight|--> Maximum SPI clocking speed of device in Hz}}
            #address-cells = <1>;
            #size-cells = <1>;
        };
    };

=== DT configuration example ===
The below example shows how to configure the QUADSPI peripheral when 1 SPI-NAND Flash and 1 SPI-NOR Flash memories are connected.

    &qspi {                                                    
        pinctrl-names = "default", "sleep";                    
        pinctrl-0 = <&qspi_clk_pins_a &qspi_bk1_pins_a &qspi_bk2_pins_a>;
        pinctrl-1 = <&qspi_clk_sleep_pins_a &qspi_bk1_sleep_pins_a &qspi_bk2_sleep_pins_a>;
        reg = <0x58003000 0x1000>,<0x70000000 0x4000000>;                          
        #address-cells = <1>;
        #size-cells = <0>;
        status = "okay";<br>

        flash0: mx66l51235l@0 {                                 
            compatible = "jdecjedec,spi-nor";
            reg = <0>;
            spi-rx-bus-width = <4>;
            spi-max-frequency = <108000000>;
            #address-cells = <1>;
            #size-cells = <1>;
        };<br>

        flash1: mt29f2g01abagd@1 {                             
            compatible = "spi-nand";
            reg = <1>;
            spi-rx-bus-width = <4>;
            spi-tx-bus-width = <4>;
            spi-max-frequency = <133000000>;
            #address-cells = <1>;
            #size-cells = <1>;
        };
    };

==How to configure the DT using STM32CubeMX==
The [[STM32CubeMX]] tool can be used to configure the STM32MPU device and get the corresponding [[Device_tree#STM32|platform configuration device tree]] files.<br />

The STM32CubeMX may not support all the properties described in the above [[#DT bindings documentation|DT bindings documentation]] paragraph. If so, the tool inserts '''user sections''' in the generated device tree. These sections can then be edited to add some properties and they are preserved from one generation to another. Refer to [[STM32CubeMX]] user manual for further information.

==References==
Please refer to the following links for full description:
<references />

<noinclude>

{{ArticleBasedOnModel | Peripheral or framework device tree configuration model}}
{{PublicationRequestId | 8899 |2018-10-10 |  AlainF}}
[[Category:Device tree configuration]]
[[Category:Mass storage]]</noinclude>
(3 intermediate revisions by 2 users not shown)
Line 10: Line 10:
 
The QUADSPI device tree bindings are composed by:
 
The QUADSPI device tree bindings are composed by:
   
* generic SPI-NOR / SPI-NAND Flash memory bindings <ref name="spi_busses_bindings">{{CodeSource | Linux kernel | Documentation/devicetree/bindings/spi/spi-bus.txt}}</ref>.
+
* generic SPI-NOR / SPI-NAND Flash memory bindings <ref name="spi_busses_bindings">{{CodeSource | Linux kernel | Documentation/devicetree/bindings/spi/spi-controller.yaml}}</ref>.
   
* QUADSPI driver bindings <ref> {{CodeSource | Linux kernel | Documentation/devicetree/bindings/spi/spi-stm32-qspi.txt}} </ref>.
+
* QUADSPI driver bindings <ref> {{CodeSource | Linux kernel | Documentation/devicetree/bindings/spi/st,stm32-qspi.yaml}} </ref>.
   
 
== DT configuration ==
 
== DT configuration ==
Line 20: Line 20:
   
 
===DT configuration (STM32 level) ===
 
===DT configuration (STM32 level) ===
The QUADSPI peripheral node is located in ''stm32mp157c.dtsi''<ref>{{CodeSource | Linux kernel | arch/arm/boot/dts/stm32mp157c.dtsi}}</ref> file.  
+
The QUADSPI peripheral node is located in ''stm32mp151.dtsi''<ref>{{CodeSource | Linux kernel | arch/arm/boot/dts/stm32mp151.dtsi}}</ref> file.  
   
 
     qspi: spi@58003000 {                                      {{highlight|Comments}}
 
     qspi: spi@58003000 {                                      {{highlight|Comments}}
Line 28: Line 28:
 
         reg-names = "qspi", "qspi_mm";
 
         reg-names = "qspi", "qspi_mm";
 
         interrupts = <GIC_SPI 92 IRQ_TYPE_LEVEL_HIGH>;        {{highlight|--> The interrupt number used}}
 
         interrupts = <GIC_SPI 92 IRQ_TYPE_LEVEL_HIGH>;        {{highlight|--> The interrupt number used}}
         dmas = <&mdma1 22 0x10 0x100002 0x0 0x0 0x0>,        {{highlight|--> DMA specifiers <ref>{{CodeSource | Linux kernel | Documentation/devicetree/bindings/dma/stm32-mdma.txt}}</ref>}}
+
         dmas = <&mdma1 22 0x10 0x100002 0x0 0x0 0x0>,        {{highlight|--> DMA specifiers <ref>{{CodeSource | Linux kernel | Documentation/devicetree/bindings/dma/st,stm32-mdma.yaml}}</ref>}}
 
               <&mdma1 22 0x10 0x100008 0x0 0x0 0x0>;
 
               <&mdma1 22 0x10 0x100008 0x0 0x0 0x0>;
 
         dma-names = "tx", "rx";
 
         dma-names = "tx", "rx";
Line 53: Line 53:
 
         status = "okay";                                      {{highlight|--> Enable the node}}<br>
 
         status = "okay";                                      {{highlight|--> Enable the node}}<br>
 
         flash0: mx66l51235l@0 {     
 
         flash0: mx66l51235l@0 {     
             compatible = "jdec,spi-nor";                                   
+
             compatible = "jedec,spi-nor";                                   
 
             reg = <0>;                                        {{highlight|--> Chip select number}}
 
             reg = <0>;                                        {{highlight|--> Chip select number}}
 
             spi-rx-bus-width = <4>;                          {{highlight|--> The bus width (number of data wires used)}}
 
             spi-rx-bus-width = <4>;                          {{highlight|--> The bus width (number of data wires used)}}
Line 75: Line 75:
 
         status = "okay";<br>
 
         status = "okay";<br>
 
         flash0: mx66l51235l@0 {                                 
 
         flash0: mx66l51235l@0 {                                 
             compatible = "jdec,spi-nor";
+
             compatible = "jedec,spi-nor";
 
             reg = <0>;
 
             reg = <0>;
 
             spi-rx-bus-width = <4>;
 
             spi-rx-bus-width = <4>;