Last edited 3 days ago

Pose estimation

Applicable for STM32MP23x lines, STM32MP25x lines

This article explains how to use the stai_mpu API for human pose estimation applications supporting OpenVX [1] back-end.

1. Description[edit | edit source]

The human pose estimation neural network model allows localization and estimation the pose of a person from an input image or video by predicting the spatial locations of key body joints known as keypoints. Common pose estimation neural network models are able to detect 17 keypoints of a human body.

Human Pose estimation application

The application demonstrates a computer vision use case for human pose estimation where frames are grabbed from a camera input (/dev/videox) and analyzed by a neural network model interpreted by OpenVX framework.
A Gstreamer pipeline is used to stream camera frames (using v4l2src), to display a preview (using gtkwaylandsink) and to execute neural network inference (using appsink).
The result of the inference is displayed in the preview. The overlay is done using GtkWidget with cairo.

The model used with this application is the ST YoloV8n-pose downloaded from the stm32-hotspot ultralytics github fork[2]

Info white.png Information
For this application, an TensorFlow Lite per-tensor asymmetric quantized model is used, which is accelerated using the neural processing unit (NPU). Then, the model has been converted to NBG format using ST Edge AI tool. For more information about this tool, refer to the dedicated article.

2. Installation[edit | edit source]

2.1. Install from the OpenSTLinux AI package repository[edit | edit source]

Warning white.png Warning
The software package is provided AS IS, and by downloading it, you agree to be bound to the terms of the software license agreement (SLA0048). The detailed content licenses can be found here.

After having configured the AI OpenSTLinux package you can install X-LINUX-AI components for human pose estimation application:

2.1.1. Install on STM32MP2x board with AI hardware accelerator[edit | edit source]

The OpenVX application will be installed to take advantage of the neural processing unit (NPU) and graphics processing unit (GPU). The application is only available in Python and on STM32MP2x boards with AI hardware accelerator.

  • To install this application, please use the following command:
x-linux-ai -i stai-mpu-pose-estimation-python-ovx-npu
Warning DB.png Important
Human pose estimation application is only provided for STM32MP2x with AI hardware accelerator as a python application based on OpenVX back-end


  • Then, restart the demo launcher:
systemctl restart weston-graphical-session.service

2.2. Source code location[edit | edit source]

  • in the OpenSTLinux Distribution with X-LINUX-AI Expansion Package:
<Distribution Package installation directory>/layers/meta-st/meta-st-x-linux-ai/recipes-samples/pose-estimation/files/stai_mpu
  • on the target:
/usr/local/x-linux-ai/pose-estimation/stai_mpu_pose_estimation.py
  • on GitHub:
recipes-samples/pose-estimation/files/stai-mpu


3. How to use the application[edit | edit source]

3.1. Launching via the demo launcher[edit | edit source]

You can click on the icon to run Python OpenVX application installed on your STM32MP2x board with AI hardware accelerator.

Demo launcher

3.2. Executing with the command line[edit | edit source]

The pose estimation Python application is located in the userfs partition:

/usr/local/x-linux-ai/pose-estimation/stai_mpu_pose_estimation.py

It accepts the following input parameters:

 
usage: stai_mpu_pose_estimation.py [-h] [-m MODEL_FILE] [-i IMAGE] 
                                    [-v VIDEO_DEVICE] [--conf_threshold CONF_THRESHOLD] [--iou_threshold IOU_THRESHOLD] 
                                    [--frame_width FRAME_WIDTH] [--frame_height FRAME_HEIGHT] [--framerate FRAMERATE] 
                                    [--input_mean INPUT_MEAN] [--input_std INPUT_STD] [--normalize NORMALIZE] 
                                    [--validation] [--val_run VAL_RUN]
options:
  -h, --help  show this help message and exit
  -m MODEL_FILE, --model_file MODEL_FILE Neural network model to be executed
  -i IMAGE, --image IMAGE image directory with image to be classified
  -v VIDEO_DEVICE, --video_device VIDEO_DEVICE video device ex: video0
  --conf_threshold CONF_THRESHOLD Confidence threshold
  --iou_threshold IOU_THRESHOLD IoU threshold, used to compute NMS
  --frame_width FRAME_WIDTH width of the camera frame (default is 640)
  --frame_height FRAME_HEIGHT height of the camera frame (default is 480)
  --framerate FRAMERATE framerate of the camera (default is 15fps)
  --input_mean INPUT_MEAN input mean
  --input_std INPUT_STD input standard deviation
  --normalize NORMALIZE input standard deviation
  --validation enable the validation mode
  --val_run VAL_RUN set the number of draws in the validation mode

4. Testing with Yolov8n-pose on STM32MP2x with AI hardware accelerator[edit | edit source]

The model used for testing is the yolov8n_256_quant_pt_uf_pose_coco-st.nb

Info white.png Information
Yolov8n-pose is a multi-pose estimation neural network, it means that the model is able to perform pose estimation on several

persons which stands in the field of view of the camera.

To ease launching of the application, two shell scripts are available for Python application on the board:

  • launch pose estimation based on camera frame inputs:
/usr/local/x-linux-ai/pose-estimation/launch_python_pose_estimation.sh
  • launch pose estimation based on the pictures located in /usr/local/x-linux-ai/pose-estimation/models/yolov8n_pose/testdata directory
/usr/local/x-linux-ai/pose-estimation/launch_python_pose_estimation_testdata.sh
Warning DB.png Important
Note that you need to populate the testdata directory with your own data sets. The pictures are then randomly read from the testdata directory

5. Going further[edit | edit source]

The two shell scripts described before offers the possibility to select the framework automatically depending on the model provided or by specifying it. To be able to run the application using a specify frameworks, the models for each frameworks must be available in the /usr/local/x-linux-ai/pose-estimation/models/yolov8n_pose/ directory. Then, you will need to specify the framework as an argument of the launch scripts as follow.

Warning DB.png Important
For application like pose estimation that targets STM32MP2x board with NPU acceleration, only NBG model is provided as example. But you can still add TFLite or ONNX models yourself and run the application on the CPU.
  • Run pose estimation based on camera input with the chosen framework. Available framework option is : nbg
/usr/local/x-linux-ai/pose-estimation/launch_python_pose_estimation.sh nbg
  • Run pose estimation based on picture located in the /usr/local/x-linux-ai/pose-estimation/models/yolov8n_pose/testdata directory with the chosen framework. Available framework option is: nbg.
/usr/local/x-linux-ai/pose-estimation/launch_python_pose_estimation_testdata.sh nbg
Warning DB.png Important
Note that you need to populate the testdata directory with your own data sets. The pictures are then randomly read from the testdata directory

6. References[edit | edit source]