Difference between revisions of "Pinctrl device tree configuration"
[quality revision] | [quality revision] |
m
|
m
|
Applicable for | STM32MP13x lines, STM32MP15x lines |
Contents
1 Purpose[edit]
The purpose of this article is to explain how to configure the GPIO internal peripheral through the pin controller (pinctrl) framework, when this peripheral is assigned to Linux® OS (Cortex-A). The configuration is performed using the Device tree.
To better understand I/O management, it is recommended to read the Overview of GPIO pins article.
This article also provides an example explaining how to add a new pin in the device tree.
If the peripheral is assigned to another execution context, refer to How to assign an internal peripheral to a runtime context article for guidelines on peripheral assignment and configuration.
2 DT bindings documentation[edit]
The Pinctrl device tree bindings are composed of:
- generic DT bindings[1] used by the pinctrl framework.
- vendor pinctrl DT bindings[2] used by the stm32-pinctrl driver: this binding document explains how to write device tree files for pinctrl.
3 DT configuration[edit]
3.1 DT configuration (STM32 level)[edit]
The pin controller node is composed of several parts:
3.1.1 STM32 pin controller information[edit]
The pin controller node is located in the SOC dtsi file
For example:
pinctrl: pin-controller@50002000pinctrl@50002000 { Comments #address-cells = <1>; #size-cells = <1>; ranges = <0 0x50002000 0xa400>; -->Provides IP start address and memory map device size interrupt-parent = <&exti>; -->Provides interrupt parent controller (used when the GPIO is configured as an external interrupt) st,syscfg = <&exti 0x60 0xff>; -->Provides phandle for IRQ mux selection pins-are-numbered; ... };
![]() |
This device tree part is related to STM32 microprocessors. It must be kept as is, without being modified by the end-user. |
3.1.2 GPIO bank information[edit]
The GPIO bank information nodes are located in the SOC dtsi file
For example:
pinctrl: pin-controller@50002000pinctrl@50002000 { Comments ... gpioa: gpio@50002000 { gpio-controller; #gpio-cells = <2>; interrupt-controller; -->Indicates that this GPIO bank can be used as interrupt controller #interrupt-cells = <2>; reg = <0x0 0x400>; -->Provides offset in pinctrl addres map for the GPIO bank clocks = <&rcc GPIOA>; -->phandle on GPIO bank clock st,bank-name = "GPIOA"; status = "disabled"; }; gpiob: gpio@50003000 { gpio-controller; #gpio-cells = <2>; interrupt-controller; #interrupt-cells = <2>; reg = <0x1000 0x400>; clocks = <&rcc GPIOB>; st,bank-name = "GPIOB"; status = "disabled"; }; ... };
The GPIO bank definition may be completed by the pinctrl package dtsi files, as, for example for STM32MP15x lines stm32mp15xxaa-pinctrl.dtsi[5].
&pinctrl { st,package = <STM32MP_PKG_AA>; gpioa: gpio@50002000 { status = "okay"; ngpios = <16>; gpio-ranges = <&pinctrl 0 0 16>; }; gpiob: gpio@50003000 { status = "okay"; ngpios = <16>; gpio-ranges = <&pinctrl 0 16 16>; };
![]() |
This device tree part is related to STM32 microprocessors. It must be kept as is, without being modified by the end-user. |
3.1.3 Pin state definition[edit]
The pin states are defined in the pinctrl dtsi file
For example:
&pinctrl { ... usart3_pins_a: usart3@0 { Comments pins1 { pinmux = <STM32_PINMUX('B', 10, AF7)>, /* USART3_TX */ -->Pin muxing information: AF7 (alternate function 7) selected on PB10 pin <STM32_PINMUX('G', 8, AF8)>; /* USART3_RTS */ -->Pin muxing information: AF8 (alternate function 8) selected on PG8 pin bias-disable; -->Generic bindings corresponding to "no pull-up" and "no pull-down" drive-push-pull; -->Generic bindings to select pin driving information slew-rate = <0>; -->Generic bindings to select pin speed }; pins2 { pinmux = <STM32_PINMUX('B', 12, AF8)>, /* USART3_RX */ <STM32_PINMUX('I', 10, AF8)>; /* USART3_CTS_NSS */ bias-disable; }; }; ... };
- - Refer to GPIO internal peripheral for more details on hardware pin configuration.
3.2 DT configuration (board level)[edit]
3.2.1 Pin state selection[edit]
As seen in Pin controller configuration (pin state definition part), all pin states are defined inside the pin controller node.
Each device that requires pins has to select the desired pin state phandle inside the board device tree file (see Device tree for more explanations about device tree file split).
The STM32MP1 devices feature a lot of possible pin combinations for a given internal peripheral. From one board to another, different sets of pins can consequently be used for an internal peripheral. Note that "_a", "_b" suffixes are used to identify pin muxing combinations in the device tree pinctrl file. The right suffixed combination must then be used in the device tree board file.
- Example:
&usart3 { ... pinctrl-names = "default","sleep"; pinctrl-0 = <&usart3_pins_a>; pinctrl-1 = <&usart3_sleep_pins_a>; ... };
3.2.2 GPIO bank secure information (OP-TEE device tree)[edit]
The secure aware GPIO banks (see Security support) may contain some specific secure settings. A peripheral set as secure MUST use secure GPIOs.
The specific st,protreg binding defined in the OP-TEE device tree sets the security at boot time and prevents non secure peripherals from using pins.
For example:
&gpiob {
st,protreg = <TZPROT(1)|TZPROT(6)>; --> pins 1 and 6 are configured as secure
};
![]() |
If this property is not defined, all the GPIOs of the bank are set as non secure, so not compatible with a secure peripheral |
3.3 DT configuration examples[edit]
3.3.1 How to add new pin states[edit]
To add new pin states and affect them to a foo_device, proceed as follows:
- 1. Find the pins you need:
- In the example below, the foo_device needs to configure PC13, PG8 and PI2.
- AF2 is selected as alternate function on PC13, and AF5 on PG8 and PI2.
- Each pin requires an internal pull-up.
- 2. Write your pin state phandle in stm32mp15-pinctrl.dtsi.
&pinctrl { ... foo_pins_a: foo@0 { pins { pinmux = <STM32_PINMUX('C', 13, AF2)>, <STM32_PINMUX('G', 8, AF5)>, <STM32_PINMUX('I', 2, AF5)>; bias-pull-up; }; }; ... };
-
- All the possible settings are described in GPIO internal peripheral.
- 3. Select the pin state phandle required for your device in the board file.
&foo { ... pinctrl-names = "default"; pinctrl-0 = <&foo_pins_a>; ... };
4 How to configure GPIOs using STM32CubeMX[edit]
The STM32CubeMX tool can be used to configure the STM32MPU device and get the corresponding platform configuration device tree files.
The STM32CubeMX may not support all the properties described in the above DT bindings documentation paragraph. If so, the tool inserts user sections in the generated device tree. These sections can then be edited to add some properties and they are preserved from one generation to another. Refer to STM32CubeMX user manual for further information.
5 References[edit]
Please refer to the following links for additional information:
- ↑ Documentation/devicetree/bindings/pinctrl/pinctrl-bindings.txt , Generic pinctrl device tree bindings
- ↑ Documentation/devicetree/bindings/pinctrl/st,stm32-pinctrl.yaml , STM32 pinctrl device tree bindings
- ↑ 3.03.1 stm32mp131.dtsi STM32MP13 SOC device tree file
- ↑ 4.04.1 stm32mp151.dtsi STM32MP15 SOC device tree file
- ↑ stm32mp15xxaa-pinctrl.dtsi STM32MP15 Pinctrl device tree file
- ↑ stm32mp13-pinctrl.dtsi STM32MP13 pinctrl device tree file
- ↑ stm32mp15-pinctrl.dtsi STM32MP15 pinctrl device tree file
<noinclude>{{ApplicableFor |MPUs list=STM32MP13x, STM32MP15x |MPUs checklist=STM32MP13x,STM32MP15x }}</noinclude> == Purpose == The purpose of this article is to explain how to configure the [[GPIO internal peripheral]] through '''the pin controller (pinctrl) framework''', '''when this peripheral is assigned to Linux<sup>®</sup> OS (Cortex-A)'''. The configuration is performed using the [[Device tree]]. To better understand I/O management, it is recommended to read the [[Overview of GPIO pins]] article. This article also provides an example explaining how to add a new pin in the device tree. If the peripheral is assigned to another execution context, refer to [[How to assign an internal peripheral to a runtime context]] article for guidelines on peripheral assignment and configuration. == DT bindings documentation == The Pinctrl device tree bindings are composed of: *generic DT bindings<ref>{{CodeSource | Linux kernel | Documentation/devicetree/bindings/pinctrl/pinctrl-bindings.txt | Documentation/devicetree/bindings/pinctrl/pinctrl-bindings.txt}}, Generic pinctrl device tree bindings</ref> used by the pinctrl framework. *vendor pinctrl DT bindings<ref>{{CodeSource | Linux kernel | Documentation/devicetree/bindings/pinctrl/st,stm32-pinctrl.yaml | Documentation/devicetree/bindings/pinctrl/st,stm32-pinctrl.yaml}}, STM32 pinctrl device tree bindings</ref> used by the stm32-pinctrl driver: this binding document explains how to write device tree files for pinctrl. == DT configuration == === DT configuration (STM32 level) === The pin controller node is composed of several parts: ==== STM32 pin controller information ==== The pin controller node is located in the SOC dtsi file * for {{MicroprocessorDevice | device=13}} ''stm32mp131.dtsi''<ref name="stm32mp131_dtsi">{{CodeSource | Linux kernel | arch/arm/boot/dts/stm32mp131.dtsi | stm32mp131.dtsi}} STM32MP13 SOC device tree file</ref> * for {{MicroprocessorDevice | device=15}} ''stm32mp151.dtsi''<ref name="stm32mp151_dtsi">{{CodeSource | Linux kernel | arch/arm/boot/dts/stm32mp151.dtsi | stm32mp151.dtsi}} STM32MP15 SOC device tree file</ref> For example: pinctrl: pin-controller@50002000pinctrl@50002000 { {{Highlight|Comments}} #address-cells = <1>; #size-cells = <1>; ranges = <0 0x50002000 0xa400>; {{Highlight|-->Provides IP start address and memory map device size}} interrupt-parent = <&exti>; {{Highlight|-->Provides interrupt parent controller (used when the GPIO is configured as an external interrupt)}} st,syscfg = <&exti 0x60 0xff>; {{Highlight|-->Provides phandle for IRQ mux selection}} pins-are-numbered; ... }; {{Warning|This device tree part is related to STM32 microprocessors. It must be kept as is, without being modified by the end-user.}} ==== GPIO bank information ==== The GPIO bank information nodes are located in the SOC dtsi file * for {{MicroprocessorDevice | device=13}} ''stm32mp131.dtsi''<ref name="stm32mp131_dtsi">{{CodeSource | Linux kernel | arch/arm/boot/dts/stm32mp131.dtsi | stm32mp131.dtsi}} STM32MP13 SOC device tree file</ref> * for {{MicroprocessorDevice | device=15}} ''stm32mp151.dtsi''<ref name="stm32mp151_dtsi">{{CodeSource | Linux kernel | arch/arm/boot/dts/stm32mp151.dtsi | stm32mp151.dtsi}} STM32MP15 SOC device tree file</ref> For example: pinctrl: pin-controller@50002000pinctrl@50002000 { {{Highlight|Comments}} ... gpioa: gpio@50002000 { gpio-controller; #gpio-cells = <2>; interrupt-controller; {{Highlight|-->Indicates that this GPIO bank can be used as interrupt controller}} #interrupt-cells = <2>; reg = <0x0 0x400>; {{Highlight|-->Provides offset in pinctrl addres map for the GPIO bank}} clocks = <&rcc GPIOA>; {{Highlight|-->phandle on GPIO bank clock}} st,bank-name = "GPIOA"; status = "disabled"; }; gpiob: gpio@50003000 { gpio-controller; #gpio-cells = <2>; interrupt-controller; #interrupt-cells = <2>; reg = <0x1000 0x400>; clocks = <&rcc GPIOB>; st,bank-name = "GPIOB"; status = "disabled"; }; ... }; The GPIO bank definition may be completed by the pinctrl package dtsi files, as, for example for {{MicroprocessorDevice | device=15}} ''stm32mp15xxaa-pinctrl.dtsi''<ref name="stm32mp15_pin_package_dtsi">{{CodeSource | Linux kernel | arch/arm/boot/dts/stm32mp15xxaa-pinctrl.dtsi | stm32mp15xxaa-pinctrl.dtsi}} STM32MP15 Pinctrl device tree file</ref>. &pinctrl { st,package = <STM32MP_PKG_AA>; gpioa: gpio@50002000 { status = "okay"; ngpios = <16>; gpio-ranges = <&pinctrl 0 0 16>; }; gpiob: gpio@50003000 { status = "okay"; ngpios = <16>; gpio-ranges = <&pinctrl 0 16 16>; }; {{Warning|This device tree part is related to STM32 microprocessors. It must be kept as is, without being modified by the end-user.}} ==== Pin state definition ==== The pin states are defined in the pinctrl dtsi file * for {{MicroprocessorDevice | device=13}} ''stm32mp13-pinctrl.dtsi'' <ref name="stm32mp13_pin_dtsi">{{CodeSource | Linux kernel | arch/arm/boot/dts/stm32mp13-pinctrl.dtsi | stm32mp13-pinctrl.dtsi}} STM32MP13 pinctrl device tree file</ref> * for {{MicroprocessorDevice | device=15}} ''stm32mp15-pinctrl.dtsi'' <ref name="stm32mp15_pin_dtsi">{{CodeSource | Linux kernel | arch/arm/boot/dts/stm32mp15-pinctrl.dtsi | stm32mp15-pinctrl.dtsi}} STM32MP15 pinctrl device tree file</ref> For example: &pinctrl { ... usart3_pins_a: usart3@0 { {{Highlight|Comments}} pins1 { pinmux = <STM32_PINMUX('B', 10, AF7)>, /* USART3_TX */ {{Highlight|-->Pin muxing information: AF7 (alternate function 7) selected on PB10 pin}}<STM32_PINMUX('G', 8, AF8)>; /* USART3_RTS */ {{Highlight|-->Pin muxing information: AF8 (alternate function 8) selected on PG8 pin}} bias-disable; {{Highlight|-->Generic bindings corresponding to "no pull-up" and "no pull-down"}} drive-push-pull; {{Highlight|-->Generic bindings to select pin driving information}} slew-rate = <0>; {{Highlight|-->Generic bindings to select pin speed}} }; pins2 { pinmux = <STM32_PINMUX('B', 12, AF8)>, /* USART3_RX */<STM32_PINMUX('I', 10, AF8)>; /* USART3_CTS_NSS */ bias-disable; }; }; ... }; :- Refer to [[GPIO internal peripheral]] for more details on hardware pin configuration. === DT configuration (board level) === ==== Pin state selection ==== As seen in [[Pinctrl_device_tree_configuration#Pin state definition|Pin controller configuration]] (pin state definition part), all pin states are defined inside the pin controller node. Each device that requires pins has to select the desired pin state phandle inside the board device tree file (see [[Device tree]] for more explanations about device tree file split). The STM32MP1 devices feature a lot of possible pin combinations for a given internal peripheral. From one board to another, different sets of pins can consequently be used for an internal peripheral. Note that "_a", "_b" suffixes are used to identify pin muxing combinations in the device tree pinctrl file. The right suffixed combination must then be used in the device tree board file. *Example:<pre> &usart3 { ... pinctrl-names = "default","sleep"; pinctrl-0 = <&usart3_pins_a>; pinctrl-1 = <&usart3_sleep_pins_a>; ... };</pre> ==== GPIO bank secure information (OP-TEE device tree) ==== The secure aware GPIO banks (see [[GPIO internal peripheral#Security_support|Security support]]) may contain some specific secure settings. A peripheral set as secure '''MUST''' use secure GPIOs. The specific '''st,protreg''' binding defined in the [[OP-TEE_overview|OP-TEE]] device tree sets the security at boot time and prevents non secure peripherals from using pins. For example: &gpiob { st,protreg = <TZPROT(1)|TZPROT(6)>; {{Highlight|--> pins 1 and 6 are configured as secure}} }; {{Warning|If this property is not defined, all the GPIOs of the bank are set as non secure, so not compatible with a secure peripheral}} === DT configuration examples === ====How to add new pin states==== To add new pin states and affect them to a foo_device, proceed as follows: :1. Find the pins you need: ::In the example below, the foo_device needs to configure PC13, PG8 and PI2. ::AF2 is selected as alternate function on PC13, and AF5 on PG8 and PI2. ::Each pin requires an internal pull-up. :2. Write your pin state phandle in ''stm32mp15-pinctrl.dtsi''.<pre> &pinctrl { ... foo_pins_a: foo@0 { pins { pinmux = <STM32_PINMUX('C', 13, AF2)>,<STM32_PINMUX('G', 8, AF5)>,<STM32_PINMUX('I', 2, AF5)>; bias-pull-up; }; }; ... };</pre> ::All the possible settings are described in [[GPIO internal peripheral]]. :3. Select the pin state phandle required for your device in the board file. <pre> &foo { ... pinctrl-names = "default"; pinctrl-0 = <&foo_pins_a>; ... };</pre> ==How to configure GPIOs using STM32CubeMX== The [[STM32CubeMX]] tool can be used to configure the STM32MPU device and get the corresponding [[Device_tree#STM32|platform configuration device tree]] files.<br /> The STM32CubeMX may not support all the properties described in the above [[#DT bindings documentation|DT bindings documentation]] paragraph. If so, the tool inserts '''user sections''' in the generated device tree. These sections can then be edited to add some properties and they are preserved from one generation to another. Refer to [[STM32CubeMX]] user manual for further information. ==References== Please refer to the following links for additional information:<references /> <noinclude> [[Category:Device tree configuration]] [[Category:IOs pin management|2]] {{PublicationRequestId | 8781 | 2018-09-20 | AnneJ}} {{ArticleBasedOnModel|Peripheral or framework device tree configuration model}}</noinclude>
Line 30: | Line 30: | ||
* for {{MicroprocessorDevice | device=15}} ''stm32mp151.dtsi''<ref name="stm32mp151_dtsi">{{CodeSource | Linux kernel | arch/arm/boot/dts/stm32mp151.dtsi | stm32mp151.dtsi}} STM32MP15 SOC device tree file</ref> |
* for {{MicroprocessorDevice | device=15}} ''stm32mp151.dtsi''<ref name="stm32mp151_dtsi">{{CodeSource | Linux kernel | arch/arm/boot/dts/stm32mp151.dtsi | stm32mp151.dtsi}} STM32MP15 SOC device tree file</ref> |
||
For example: |
For example: |
||
− | pinctrl: |
+ | pinctrl: pinctrl@50002000 { {{Highlight|Comments}} |
#address-cells = <1>; |
#address-cells = <1>; |
||
#size-cells = <1>; |
#size-cells = <1>; |
||
Line 48: | Line 48: | ||
* for {{MicroprocessorDevice | device=15}} ''stm32mp151.dtsi''<ref name="stm32mp151_dtsi">{{CodeSource | Linux kernel | arch/arm/boot/dts/stm32mp151.dtsi | stm32mp151.dtsi}} STM32MP15 SOC device tree file</ref> |
* for {{MicroprocessorDevice | device=15}} ''stm32mp151.dtsi''<ref name="stm32mp151_dtsi">{{CodeSource | Linux kernel | arch/arm/boot/dts/stm32mp151.dtsi | stm32mp151.dtsi}} STM32MP15 SOC device tree file</ref> |
||
For example: |
For example: |
||
− | pinctrl: |
+ | pinctrl: pinctrl@50002000 { {{Highlight|Comments}} |
... |
... |
||