Difference between revisions of "Package repository for OpenSTLinux distribution"
[quality revision] | [quality revision] |
m (Update for DV-2.1)
|
m (Add warning to explain errors that may occurs with stm32mp13 boards)
|
Applicable for | STM32MP13x lines, STM32MP15x lines |
Contents
1 Disclaimers[edit]
STMicroelectronics packages repository service is provided for evaluation purpose only, and therefore not approved for use in production.
The package licenses hosted in these repositories can be found here: OpenSTLinux licenses.
Command outputs described in this document may slightly vary depending on tools version.
1.1 Description[edit]
OpenSTLinux provides a package repository service hosted at the non-browsable URL http://packages.openstlinux.st.com. The package repository service is designed for STM32MP157C-DK2 STM32MP157x-DKx , STM32MP157x-EV1
and STM32MP135F-DK
boards and is enabled by default in the Starter Package.
1.2 Organization[edit]
Within each repository, packages are organized in two three groups (a.k.a components in the APT terminology):
- the main group contains a wide selection of packages whose installation is automatically tested by STMicroelectronics
- the untested group contains all the other packages that can be built using the
bitbake world
command. However their installation is not guaranteed.
- the updates group contains additional packages not included in the OpenSTLinux distribution releases and updated packages. This group is managed by a dedicated layer available through github®. Further details are available by following the github® link: https://github.com/STMicroelectronics/meta-st-pkgrepo-updates.
1.3 Limitations[edit]
Packages repository service doesn't include the packages that are shipped in the rootfs image, nor the BSP components (TF-A, U-Boot, Linux and OP-TEE). They can be installed only from the Starter Package using the STM32CubeProgrammer.
rootfs available space is about 60MB by default. For a better experience it is recommended to flash the Starter Package using the "extensible" flashlayout (*-extensible.tsv).
Extensible flashlayout does not flash userfs partition to extend the rootfs partition to the size of the sdcard.
2 Usage[edit]
2.1 Prequisite[edit]
We assume your board has an internet connection either through the network cable or through a WiFi connection.
2.2 Apt[edit]
OpenSTLinux packages can be handled using apt-*
utilities, which are the same utilities used on a Debian system. The first apt-*
command that must be run before any other is:
apt-get update The software package is provided AS IS, and by downloading it, you agree to be bound to the terms of the software license agreement (SLA). The detailed content licenses can be found at https://wiki.st.com/stm32mpu/wiki/OpenSTLinux_licenses. Get:1 http://packages.openstlinux.st.com/24.10 dunfell InRelease [34583459 B] Get:2 http://packages.openstlinux.st.com/24.10 dunfell/main armhf Packages [1040 kB682kB] Get:3 http://packages.openstlinux.st.com/24.10 dunfell/updates armhf Packages [2664.6 kB2kB] Get:4 http://packages.openstlinux.st.com/24.10 dunfell/untested armhf Packages [1627 kB1223kB] Fetched 26971973 kB in 4s3s (585626 kB/s) Reading package lists... Done
This command synchronizes the local packages index from the repositories enumerated in /etc/apt/sources.list{,.d}
. Once it is updated, apt-cache
can be used to get the list of all available packages:
apt-cache search . a52dec - ATSC A/52 surround sound stream decoder a52dec-doc - ATSC A/52 surround sound stream decoder acl - Utilities for managing POSIX Access Control Lists ... xserverxkeyboard-xorgconfig - TheKeyboard X.Orgconfiguration X server xserver-xorg-xwayland - The X.Org X server xterm - xterm is the standard terminal emulator for the database for X Window System xxhash xvinfo - PrintExtremely outfast Xnon-Videocryptographic extensionhash adaptoralgorithm information xz - Utilities for managing LZMA compressed files
It is possible to list only packages that match a given pattern, for example:
apt-cache search emacs
libreadline-doc - Library for editing typed command lines - Documentation files
libreadline-src - Library for editing typed command lines - Source files
emacs-base - Emacs is the extensible, customizable, self-documenting real-time display editor
emacs-doc - Emacs is the extensible, customizable, self-documenting real-time display editor - Documentation files
emacs-full - Emacs is the extensible, customizable, self-documenting real-time display editor
emacs-minimal - Emacs is the extensible, customizable, self-documenting real-time display editor
gpm - Console mouse driver
gpm-doc - Console mouse driver - Documentation files
zile - Zile is lossy Emacs
zile-doc - Zile is lossy Emacs - Documentation files
libreadline8 - Library for editing typed command lines
The desired package(s) can then be easily installed:
apt-get install zile Reading package lists... Done Building dependency tree Reading state information... Done The following additional packages will be installed: bdwgc The following NEW packages will be installed: bdwgc zile 0 upgraded, 2 newly installed, 0 to remove and 03 not upgraded. Need to get 149150 kB of archives. After this operation, 0 B of additional disk space will be used. Do you want to continue? [Y/n] Get:1 http://packages.openstlinux.st.com/24.10 dunfell/untested armhf bdwgc armhf 8.2.0.4-r0 [6970.29 kB] Get:2 http://packages.openstlinux.st.com/24.10 dunfell/untested armhf zile armhf 2.4.1415-r0 [79.31 kB] Fetched 149150 kB in 0s1s (329287 kB/s) The software package is provided AS IS, and by downloading it, you agree to be bound to the terms of the software license agreement (SLA). The detailed content licenses can be found at https://wiki.st.com/stm32mpu/wiki/OpenSTLinux_licenses. Selecting previously unselected package bdwgc. (Reading database ... 1408514860 files and directories currently installed.) Preparing to unpack .../bdwgc_8.2.0.4-r0_armhf.deb ... Unpacking bdwgc (8.2.0.4-r0) ... Selecting previously unselected package zile. Preparing to unpack .../zile_2.4.1415-r0_armhf.deb ... Unpacking zile (2.4.1415-r0) ... Setting up bdwgc (8.2.0.4-r0) ... Setting up zile (2.4.1415-r0) ...
... or removed:
apt-get remove zile Reading package lists... Done Building dependency tree Reading state information... Done The following package was automatically installed and is no longer required: bdwgc Use 'apt autoremove' to remove it. The following packages will be REMOVED: zile 0 upgraded, 0 newly installed, 1 to remove and 03 not upgraded. After this operation, 0 B of additional disk space will be used. Do you want to continue? [Y/n] The software package is provided AS IS, and by downloading it, you agree to be bound to the terms of the software license agreement (SLA). The detailed content licenses can be found at https://wiki.st.com/stm32mpu/wiki/OpenSTLinux_licenses. (Reading database ... 1409014865 files and directories currently installed.) Removing zile (2.4.1415-r0) ...
This command only removes the files that were installed from this package. It does not remove the package from the apt
download cache. If there is not enough space available on the system, it is recommended to clean the cache:
apt-get clean
Likewise, some packages may have been automatically installed to respect dependencies with other packages. If they are no longer required, they can be removed to free space:
apt-get autoremove Reading package lists... Done Building dependency tree Reading state information... Done The following packages will be REMOVED: bdwgc 0 upgraded, 0 newly installed, 1 to remove and 03 not upgraded. After this operation, 0 B of additional disk space will be used. Do you want to continue? [Y/n] The software package is provided AS IS, and by downloading it, you agree to be bound to the terms of the software license agreement (SLA). The detailed content licenses can be found at https://wiki.st.com/stm32mpu/wiki/OpenSTLinux_licenses. (Reading database ... 1408914864 files and directories currently installed.) Removing bdwgc (8.2.0.4-r0) ...
3 How to activate a local package repository[edit]
3.1 Prerequisite[edit]
Even if Package repository for OpenSTLinux offers lots of and various packages, you may need to use a local and personnal package repository. To use Using a local and personnal personal package repository is a 'smart' and 'quick' way to update the STM32MP15_Discovery_kits_-_Starter _ Package with your developments.
A local package repository is a collection of *.deb organized such apt
needs it. The local repository should provide Packages metafiles.
Natively OpenEmbedded/Yocto build system is able to generate a valid package repository (by using bitbake package-index
command listed below). So first Install the STM32MP1 OpenSTLinux distribution.
3.2 Update the repo package indexes[edit]
Execute the bitbake package-index
command:
cd [your STM32MP1 Distribution path]/build-<DISTRO>-<MACHINE> bitbake package-index
3.3 HTTP server execution on the computer[edit]
SimpleHTTPserver python application is already installed on the board with the OpenSTLinux distribution. You just need to launch this application on your host computer, in the "[your STM32MP1 Distribution path]/build-<DISTRO>-<MACHINE>/tmp-glibc/deploy/deb" folder:
cd [your STM32MP1 Distribution path]/build-<DISTRO>-<MACHINE>/tmp-glibc/deploy/deb python -m SimpleHTTPServer&
3.4 How to use the local OpenSTLinux Distribution[edit]
We use the physical IP address of the HTTP server we launched above to configure APT. That means this {{<IP>}} address should be defined as static on the host computer.
You can now configure the APT tool directly on the target via a Linux console:
echo "deb [trusted=yes] http://<IP>:8000/stm32mp1 /" > /etc/apt/sources.list.d/my_custom.list
echo "deb [trusted=yes] http://<IP>:8000/all /" >> /etc/apt/sources.list.d/my_custom.list
echo "deb [trusted=yes] http://<IP>:8000/cortexa7t2hf-neon-vfpv4 /" >> /etc/apt/sources.list.d/my_custom.list
echo "deb [trusted=yes] http://<IP>:8000/cortexa7hf-neon-vfpv4 /" >> /etc/apt/sources.list.d/my_custom.list
In the above example, [trusted=yes] has been specified because the package manifest Release is not signed.
Then you can run the command to synchronize the local packages index:
apt-get update The software package is provided AS IS, and by downloading it, you agree to be bound to the terms of the software license agreement (SLA). The detailed content licenses can be found at https://wiki.st.com/stm32mpu/wiki/OpenSTLinux_licenses. Ign:1 http://<IP>:8000/allstm32mp1 InRelease Ign:2 http://<IP>:8000/stm32mp1all InRelease Ign:3 http://<IP>:8000/cortexa7t2hf-neon-vfpv4 InRelease Ign:4 http://<IP>:8000/cortexa7hf-neon-vfpv4 InRelease Get:5 http://<IP>:8000/stm32mp1 Release [1088 Get:4B] Get:6 http://<IP>:8000/all Release [12131083 B] Get:5Get:7 http://<IP>:8000/stm32mp1cortexa7t2hf-neon-vfpv4 Release [12181115 B] Get:6Get:8 http://<IP>:8000/cortexa7t2hfcortexa7hf-neon-vfpv4 Release [12331097 B] Ign:9 http://<IP>:8000/stm32mp1 Ign:7Release.gpg Ign:10 http://<IP>:8000/all Release.gpg Ign:8Ign:11 http://<IP>:8000/stm32mp1cortexa7t2hf-neon-vfpv4 Release.gpg Ign:9Ign:12 http://<IP>:8000/cortexa7t2hfcortexa7hf-neon-vfpv4 Release.gpg Get:13 http://<IP>:8000/stm32mp1 Packages [165 Get:10kB] Get:14 http://<IP>:8000/all Packages [82.8109 kB] Get:11Get:15 http://<IP>:8000/stm32mp1cortexa7t2hf-neon-vfpv4 Packages [1732775 kB] Get:12Get:16 http://<IP>:8000/cortexa7t2hfcortexa7hf-neon-vfpv4 Packages [173420.5 kB] Fetched 1994Fetched 3073 kB in 3s7s (662463 kB/s) Reading package lists... Done
The other apt-*
commands are now available as described above.
4 Support[edit]
Bug reports, request for new packages, or any other kind of support requests can be submitted through https://community.st.com.
5 Further readings[edit]
- Dpkg
- https://manpages.debian.org/stable/apt/apt-get.8.en.html
- https://manpages.debian.org/stable/apt/sources.list.5.en.html
- https://manpages.debian.org/stable/apt/apt-cache.8.en.html
- https://wiki.debian.org/DebianRepository/Setup
- https://wiki.debian.org/DebianRepository/SetupWithReprepro
- https://wiki.debian.org/SecureApt
- STM32MP15 Discovery kits - Starter Package
- STM32MP15 _ Evaluation boards - Starter Package
- STM32MP1 Developer Package
=={{ApplicableFor |MPUs list=STM32MP13x, STM32MP15x |MPUs checklist=STM32MP13x, STM32MP15x }}<noinclude> </noinclude> ==Disclaimers== STMicroelectronics packages repository service is provided for evaluation purpose only, and therefore not approved for use in production.<br/> The package licenses hosted in these repositories can be found here: [[OpenSTLinux_licenses|OpenSTLinux licenses]].<br/> Command outputs described in this document may slightly vary depending on tools version. ===Description=== OpenSTLinux provides a package repository service hosted at the non-browsable URL <nowiki>http://packages.openstlinux.st.com</nowiki>. The package repository service is designed for ''STM32MP157C-DK2'' {{Board | type=157x-DKx | name=short}}'', ''{{Board | type=157x-EV1 | name=short}}'' and {{Board | type=135F-DK | name=short}} boards and is enabled by default in the [[STM32MP15_Discovery_kits_-_:Category:Starter_Package|Starter Package]]. ==={{Warning| Some packages provided in the OpenSTLinux distribution can't be installed or run onto the {{Board | type=135F-DK | name=short}} board. This mainly concerns graphical and related packages because of hardware technical characteristics which differ from ''{{Board | type=157x-DKx | name=short}}'' and ''{{Board | type=157x-EV1 | name=short}}'' boards.}} ===Organization=== Within each repository, packages are organized in twothree groups (a.k.a ''components'' in the APT terminology): * the '''main''' group contains a wide selection of packages whose installation is automatically tested by STMicroelectronics * the '''untested''' group contains all the other packages that can be built using the <code>bitbake world</code> command. However their installation is not guaranteed. A third group named '''updates''' is reserved for future use. * the '''updates''' group contains additional packages not included in the [[OpenSTLinux_distribution|OpenSTLinux distribution releases]] and updated packages. This group is managed by a dedicated layer available through github®. Further details are available by following the github® link: https://github.com/STMicroelectronics/meta-st-pkgrepo-updates. ===Limitations=== Packages repository service doesn't include the packages that are shipped in the rootfs image, nor the BSP components (TF-A, U-Boot, Linux and OP-TEE). They can be installed only from the [[STM32MP15_Discovery_kits_-_:Category:Starter_Package|Starter Package]] using the [[STM32CubeProgrammer]]. ''rootfs'' available space is about 60MB by default. For a better experience it is recommended to [[STM32CubeProgrammer#How_to_flash_with_STM32CubeProgrammer|flash]] the [[STM32MP15_Discovery_kits_-_:Category:Starter_Package|Starter Package]] using the "extensible" flashlayout (''*-extensible.tsv'').<br/> {{Grey|'''''Extensible flashlayout''''' does not flash userfs partition to extend the rootfs partition to the size of the sdcard.}} ==Usage== ===Prequisite=== We assume your board has an internet connection either through the network cable or through a WiFi connection. {{InternalInfo| If your internet access depends on a proxy server, you should define the http_proxy environment variable with the following command before any <code>apt-*</code> commands: {{Board$}} export http_proxy='http://<proxy url>:<proxy port>/' }} ===Apt === OpenSTLinux packages can be handled using <code>apt-*</code> utilities, which are the same utilities used on a [https://manpages.debian.org/stable/apt/apt-get.8.en.html Debian system]. The first <code>apt-*</code> command that must be run before any other is: {{Board$}} apt-get update The software package is provided AS IS, and by downloading it, you agree to be bound to the terms of the software license agreement (SLA). The detailed content licenses can be found at<nowiki>https://wiki.st.com/stm32mpu/wiki/OpenSTLinux_licenses</nowiki>. Get:1 <nowiki>http://packages.openstlinux.st.com/2.14.0</nowiki> dunfell InRelease [34583459 B] Get:2 <nowiki>http://packages.openstlinux.st.com/2.14.0</nowiki> dunfell/main armhf Packages [1040 kB682kB] Get:3 <nowiki>http://packages.openstlinux.st.com/2.14.0</nowiki> dunfell/updates armhf Packages [26.6 kB64.2kB] Get:4 <nowiki>http://packages.openstlinux.st.com/2.14.0</nowiki> dunfell/untested armhf Packages [1627 kB1223kB] Fetched 26971973 kB in 4s (5853s (626 kB/s) Reading package lists... Done This command synchronizes the local packages index from the repositories enumerated in [https://manpages.debian.org/stable/apt/sources.list.5.en.html <code>/etc/apt/sources.list{,.d}</code>]. Once it is updated, [https://manpages.debian.org/stable/apt/apt-cache.8.en.html <code>apt-cache</code>] can be used to get the list of all available packages: {{Board$}} apt-cache search . a52dec - ATSC A/52 surround sound stream decoder a52dec-doc - ATSC A/52 surround sound stream decoder acl - Utilities for managing POSIX Access Control Lists ...xserver-xorg - The X.Org X server xserver-xorg-xwayland - The X.Org X server xterm - xterm is the standard terminal emulator for the X Window System xvinfo - Print out X-Video extension adaptor informationxkeyboard-config - Keyboard configuration database for X Window xxhash - Extremely fast non-cryptographic hash algorithmxz - Utilities for managing LZMA compressed files It is possible to list only packages that match a given pattern, for example: {{Board$}} apt-cache search emacs libreadline-doc - Library for editing typed command lines - Documentation fileslibreadline-src - Library for editing typed command lines - Source files emacs-base - Emacs is the extensible, customizable, self-documenting real-time display editor emacs-doc - Emacs is the extensible, customizable, self-documenting real-time display editor - Documentation files emacs-full - Emacs is the extensible, customizable, self-documenting real-time display editor emacs-minimal - Emacs is the extensible, customizable, self-documenting real-time display editorgpm - Console mouse driver gpm-doc - Console mouse driver - Documentation files zile - Zile is lossy Emacs zile-doc - Zile is lossy Emacs - Documentation files libreadline8 - Library for editing typed command lines The desired package(s) can then be easily installed: {{Board$}} apt-get install zile Reading package lists... Done Building dependency tree Reading state information... Done The following additional packages will be installed: bdwgc The following NEW packages will be installed: bdwgc zile 0 upgraded, 2 newly installed, 0 to remove and 03 not upgraded. Need to get 149150 kB of archives. After this operation, 0 B of additional disk space will be used. Do you want to continue? [Y/n] Get:1 <nowiki>http://packages.openstlinux.st.com/2.14.0</nowiki> dunfell/untested armhf bdwgc armhf 8.2.0.4-r0 [69.270.9 kB] Get:2 <nowiki>http://packages.openstlinux.st.com/2.14.0</nowiki> dunfell/untested armhf zile armhf 2.4.1415-r0 [79.31 kB] Fetched 149150 kB in 0s (3291s (287 kB/s) The software package is provided AS IS, and by downloading it, you agree to be bound to the terms of the software license agreement (SLA). The detailed content licenses can be found at<nowiki>https://wiki.st.com/stm32mpu/wiki/OpenSTLinux_licenses</nowiki>. Selecting previously unselected package bdwgc. (Reading database ... 1408514860 files and directories currently installed.) Preparing to unpack .../bdwgc_8.2.0.4-r0_armhf.deb ... Unpacking bdwgc (8.2.0.4-r0) ... Selecting previously unselected package zile. Preparing to unpack .../zile_2.4.1415-r0_armhf.deb ... Unpacking zile (2.4.1415-r0) ... Setting up bdwgc (8.2.0.4-r0) ... Setting up zile (2.4.1415-r0) ... ... or removed: {{Board$}} apt-get remove zile Reading package lists... Done Building dependency tree Reading state information... Done The following package was automatically installed and is no longer required: bdwgc Use 'apt autoremove' to remove it. The following packages will be REMOVED: zile 0 upgraded, 0 newly installed, 1 to remove and 03 not upgraded. After this operation, 0 B of additional disk space will be used. Do you want to continue? [Y/n] The software package is provided AS IS, and by downloading it, you agree to be bound to the terms of the software license agreement (SLA). The detailed content licenses can be found at<nowiki>https://wiki.st.com/stm32mpu/wiki/OpenSTLinux_licenses</nowiki>. (Reading database ... 1409014865 files and directories currently installed.) Removing zile (2.4.1415-r0) ... This command only removes the files that were installed from this package. It does not remove the package from the <code>apt</code> download cache. If there is not enough space available on the system, it is recommended to clean the cache: {{Board$}} apt-get clean Likewise, some packages may have been automatically installed to respect dependencies with other packages. If they are no longer required, they can be removed to free space: {{Board$}} apt-get autoremove Reading package lists... Done Building dependency tree Reading state information... Done The following packages will be REMOVED: bdwgc 0 upgraded, 0 newly installed, 1 to remove and 03 not upgraded. After this operation, 0 B of additional disk space will be used. Do you want to continue? [Y/n] The software package is provided AS IS, and by downloading it, you agree to be bound to the terms of the software license agreement (SLA). The detailed content licenses can be found at<nowiki>https://wiki.st.com/stm32mpu/wiki/OpenSTLinux_licenses</nowiki>. (Reading database ... 1408914864 files and directories currently installed.) Removing bdwgc (8.2.0.4-r0) ... == How to activate a local package repository == ===Prerequisite=== Even if ''Package repository for OpenSTLinux'' offers lots of and various packages, you may need to use a local and personnal package repository. To use Using a local and personnalpersonal package repository is a 'smart' and 'quick' way to update the [[STM32MP15_Discovery_kits_-_Starter_Package:Category:Starter_Package|Starter Package]] with your developments. A local package repository is a collection of *.deb organized such <code>apt</code> needs it. The local repository should provide ''Packages'' metafiles. Natively OpenEmbedded/Yocto build system is able to generate a valid package repository (by using <code>bitbake package-index</code> command listed below). So first [[STM32MP1 Distribution Package - OpenSTLinux distribution#Download|Install the STM32MP1 OpenSTLinux distribution]]. ===Update the repo package indexes=== Execute the <code>bitbake package-index</code> command: {{PC$}} cd [your STM32MP1 Distribution path]/build-<DISTRO>-<MACHINE> {{PC$}} bitbake package-index ===HTTP server execution on the computer=== '''SimpleHTTPserver''' python application is already installed on the board with the OpenSTLinux distribution. You just need to launch this application on your host computer, in the "[your STM32MP1 Distribution path]/build-<DISTRO>-<MACHINE>/tmp-glibc/deploy/deb" folder: {{PC$}} cd [your STM32MP1 Distribution path]/build-<DISTRO>-<MACHINE>/tmp-glibc/deploy/deb {{PC$}} python -m SimpleHTTPServer& ===How to use the local OpenSTLinux Distribution=== We use the physical IP address of the HTTP server we launched above to configure APT. That means this {{<IP>}} address should be defined as static on the host computer.<br/> You can now configure the APT tool directly on the target via a Linux console: {{Board$}} echo "deb [trusted=yes] http://<IP>:8000/stm32mp1 /" > /etc/apt/sources.list.d/my_custom.list {{Board$}} echo "deb [trusted=yes] http://<IP>:8000/all /" >> /etc/apt/sources.list.d/my_custom.list {{Board$}} echo "deb [trusted=yes] http://<IP>:8000/cortexa7t2hf-neon-vfpv4 /" >> /etc/apt/sources.list.d/my_custom.list{{Board$}} echo "deb [trusted=yes] http://<IP>:8000/cortexa7hf-neon-vfpv4 /" >> /etc/apt/sources.list.d/my_custom.list In the above example, '''[trusted=yes]''' has been specified because the package manifest '''Release''' is not signed.<br/> Then you can run the command to synchronize the local packages index: {{Board$}} apt-get update The software package is provided AS IS, and by downloading it, you agree to be bound to the terms of the software license agreement (SLA). The detailed content licenses can be found at<nowiki>https://wiki.st.com/stm32mpu/wiki/OpenSTLinux_licenses</nowiki>. Ign:1 http://<IP>:8000/allstm32mp1 InRelease Ign:2 http://<IP>:8000/stm32mp1all InRelease Ign:3 http://<IP>:8000/cortexa7t2hf-neon-vfpv4 InRelease Get:4Ign:4 http://<IP>:8000/cortexa7hf-neon-vfpv4 InRelease Get:5 http://<IP>:8000/stm32mp1 Release [1088 B] Get:6 http://<IP>:8000/all Release [12131083 B] Get:5 http://<IP>:8000/stm32mp1 Release [1218 B] Get:6 http://<IP>:8000/cortexa7t2hf-neon-vfpv4 Release [1233 B] Ign:7Get:7 http://<IP>:8000/cortexa7t2hf-neon-vfpv4 Release [1115 B] Get:8 http://<IP>:8000/cortexa7hf-neon-vfpv4 Release [1097 B] Ign:9 http://<IP>:8000/stm32mp1 Release.gpg Ign:10 http://<IP>:8000/all Release.gpg Ign:8 http://<IP>:8000/stm32mp1 Release.gpg Ign:9 http://<IP>:8000/cortexa7t2hfIgn:11 http://<IP>:8000/cortexa7t2hf-neon-vfpv4 Release.gpg Ign:12 http://<IP>:8000/cortexa7hf-neon-vfpv4 Release.gpg Get:10Get:13 http://<IP>:8000/stm32mp1 Packages [165 kB] Get:14 http://<IP>:8000/all Packages [82.8109 kB] Get:11 http://<IP>:8000/stm32mp1 Packages [173 kB] Get:12 http://<IP>:8000/cortexa7t2hf-neon-vfpv4 Packages [1734 kB] Fetched 1994 kB in 3s (662 kB/s) Get:15 http://<IP>:8000/cortexa7t2hf-neon-vfpv4 Packages [2775 kB] Get:16 http://<IP>:8000/cortexa7hf-neon-vfpv4 Packages [20.5 kB] Fetched 3073 kB in 7s (463 kB/s)Reading package lists... Done The other <code>apt-*</code> commands are now available as described above. ==Support== Bug reports, request for new packages, or any other kind of support requests can be submitted through https://community.st.com. ==Further readings== * [[Dpkg]] * https://manpages.debian.org/stable/apt/apt-get.8.en.html * https://manpages.debian.org/stable/apt/sources.list.5.en.html * https://manpages.debian.org/stable/apt/apt-cache.8.en.html * https://wiki.debian.org/DebianRepository/Setup * https://wiki.debian.org/DebianRepository/SetupWithReprepro * https://wiki.debian.org/SecureApt * [[STM32MP15 Discovery kits - Starter Package]] * [[STM32MP15_Evaluation boards - Starter Package | STM32MP15 Evaluation boards - Starter Package]] * [[STM32MP1 Developer Package]] <noinclude> [[Category:Services]] {{PublicationRequestId | 14914 | 2020-02-12 |AnneJ}}</noinclude>
(26 intermediate revisions by 4 users not shown) | |||
Line 1: | Line 1: | ||
+ | {{ApplicableFor |
||
+ | |MPUs list=STM32MP13x, STM32MP15x |
||
+ | |MPUs checklist=STM32MP13x, STM32MP15x |
||
+ | }} |
||
+ | <noinclude> |
||
+ | |||
+ | </noinclude> |
||
==Disclaimers== |
==Disclaimers== |
||
STMicroelectronics packages repository service is provided for evaluation purpose only, and therefore not approved for use in production.<br/> |
STMicroelectronics packages repository service is provided for evaluation purpose only, and therefore not approved for use in production.<br/> |
||
Line 6: | Line 13: | ||
===Description=== |
===Description=== |
||
OpenSTLinux provides a package repository service hosted at the non-browsable URL <nowiki>http://packages.openstlinux.st.com</nowiki>. |
OpenSTLinux provides a package repository service hosted at the non-browsable URL <nowiki>http://packages.openstlinux.st.com</nowiki>. |
||
+ | The package repository service is designed for ''{{Board | type=157x-DKx | name=short}}'', ''{{Board | type=157x-EV1 | name=short}}'' and {{Board | type=135F-DK | name=short}} boards and is enabled by default in the [[:Category:Starter_Package|Starter Package]]. |
||
− | + |
{{Warning| Some packages provided in the OpenSTLinux distribution can't be installed or run onto the {{Board | type=135F-DK | name=short}} board. This mainly concerns graphical and related packages because of hardware technical characteristics which differ from ''{{Board | type=157x-DKx | name=short}}'' and ''{{Board | type=157x-EV1 | name=short}}'' boards.}}
|
|
− | |||
===Organization=== |
===Organization=== |
||
− | Within each repository, packages are organized in |
+ | Within each repository, packages are organized in three groups (a.k.a ''components'' in the APT terminology): |
* the '''main''' group contains a wide selection of packages whose installation is automatically tested by STMicroelectronics |
* the '''main''' group contains a wide selection of packages whose installation is automatically tested by STMicroelectronics |
||
* the '''untested''' group contains all the other packages that can be built using the <code>bitbake world</code> command. However their installation is not guaranteed. |
* the '''untested''' group contains all the other packages that can be built using the <code>bitbake world</code> command. However their installation is not guaranteed. |
||
− | + |
* the '''updates''' group contains additional packages not included in the [[OpenSTLinux_distribution|OpenSTLinux distribution releases]] and updated packages. This group is managed by a dedicated layer available through github®. Further details are available by following the github® link: https://github.com/STMicroelectronics/meta-st-pkgrepo-updates. |
|
− | |||
===Limitations=== |
===Limitations=== |
||
− | Packages repository service doesn't include the packages that are shipped in the rootfs image, nor the BSP components (TF-A, U-Boot, Linux and OP-TEE). They |
+ | Packages repository service doesn't include the packages that are shipped in the rootfs image, nor the BSP components (TF-A, U-Boot, Linux and OP-TEE). They can be installed only from the [[:Category:Starter_Package|Starter Package]] using the [[STM32CubeProgrammer]]. |
− | ''rootfs'' available space is about 60MB by default. For a better experience it is recommended to [[STM32CubeProgrammer#How_to_flash_with_STM32CubeProgrammer|flash]] the [[ |
+ | ''rootfs'' available space is about 60MB by default. For a better experience it is recommended to [[STM32CubeProgrammer#How_to_flash_with_STM32CubeProgrammer|flash]] the [[:Category:Starter_Package|Starter Package]] using the "extensible" flashlayout (''*-extensible.tsv'').<br/> |
{{Grey|'''''Extensible flashlayout''''' does not flash userfs partition to extend the rootfs partition to the size of the sdcard.}} |
{{Grey|'''''Extensible flashlayout''''' does not flash userfs partition to extend the rootfs partition to the size of the sdcard.}} |
||
− | |||
==Usage== |
==Usage== |
||
Line 44: | Line 49: | ||
<nowiki>https://wiki.st.com/stm32mpu/wiki/OpenSTLinux_licenses</nowiki>. |
<nowiki>https://wiki.st.com/stm32mpu/wiki/OpenSTLinux_licenses</nowiki>. |
||
− | Get:1 <nowiki>http://packages.openstlinux.st.com/ |
+ | Get:1 <nowiki>http://packages.openstlinux.st.com/4.0</nowiki> dunfell InRelease [3459 B] |
− | Get:2 <nowiki>http://packages.openstlinux.st.com/ |
+ | Get:2 <nowiki>http://packages.openstlinux.st.com/4.0</nowiki> dunfell/main armhf Packages [682kB] |
− | Get:3 <nowiki>http://packages.openstlinux.st.com/ |
+ | Get:3 <nowiki>http://packages.openstlinux.st.com/4.0</nowiki> dunfell/updates armhf Packages [64.2kB] |
− | Get:4 <nowiki>http://packages.openstlinux.st.com/ |
+ | Get:4 <nowiki>http://packages.openstlinux.st.com/4.0</nowiki> dunfell/untested armhf Packages [1223kB] |
− | Fetched |
+ | Fetched 1973 kB in 3s (626 kB/s) |
Reading package lists... Done |
Reading package lists... Done |
||
Line 58: | Line 63: | ||
acl - Utilities for managing POSIX Access Control Lists |
acl - Utilities for managing POSIX Access Control Lists |
||
... |
... |
||
− | + | xkeyboard-config - Keyboard configuration database for X Window |
|
− | + | xxhash - Extremely fast non-cryptographic hash algorithm
|
|
− | |||
− | |||
xz - Utilities for managing LZMA compressed files |
xz - Utilities for managing LZMA compressed files |
||
Line 68: | Line 71: | ||
{{Board$}} apt-cache search emacs |
{{Board$}} apt-cache search emacs |
||
libreadline-doc - Library for editing typed command lines - Documentation files |
libreadline-doc - Library for editing typed command lines - Documentation files |
||
+ | libreadline-src - Library for editing typed command lines - Source files |
||
+ | emacs-base - Emacs is the extensible, customizable, self-documenting real-time display editor |
||
+ | emacs-doc - Emacs is the extensible, customizable, self-documenting real-time display editor - Documentation files |
||
+ | emacs-full - Emacs is the extensible, customizable, self-documenting real-time display editor |
||
+ | emacs-minimal - Emacs is the extensible, customizable, self-documenting real-time display editor |
||
gpm - Console mouse driver |
gpm - Console mouse driver |
||
gpm-doc - Console mouse driver - Documentation files |
gpm-doc - Console mouse driver - Documentation files |
||
Line 84: | Line 92: | ||
The following NEW packages will be installed: |
The following NEW packages will be installed: |
||
bdwgc zile |
bdwgc zile |
||
− | 0 upgraded, 2 newly installed, 0 to remove and |
+ | 0 upgraded, 2 newly installed, 0 to remove and 3 not upgraded. |
− | Need to get |
+ | Need to get 150 kB of archives. |
After this operation, 0 B of additional disk space will be used. |
After this operation, 0 B of additional disk space will be used. |
||
Do you want to continue? [Y/n] |
Do you want to continue? [Y/n] |
||
− | Get:1 <nowiki>http://packages.openstlinux.st.com/ |
+ | Get:1 <nowiki>http://packages.openstlinux.st.com/4.0</nowiki> dunfell/untested armhf bdwgc armhf 8.2.0-r0 [70.9 kB] |
− | Get:2 <nowiki>http://packages.openstlinux.st.com/ |
+ | Get:2 <nowiki>http://packages.openstlinux.st.com/4.0</nowiki> dunfell/untested armhf zile armhf 2.4.15-r0 [79.1 kB] |
− | Fetched |
+ | Fetched 150 kB in 1s (287 kB/s) |
The software package is provided AS IS, and by downloading it, you agree to be |
The software package is provided AS IS, and by downloading it, you agree to be |
||
Line 98: | Line 106: | ||
Selecting previously unselected package bdwgc. |
Selecting previously unselected package bdwgc. |
||
− | (Reading database ... |
+ | (Reading database ... 14860 files and directories currently installed.) |
− | Preparing to unpack .../bdwgc_8.0 |
+ | Preparing to unpack .../bdwgc_8.2.0-r0_armhf.deb ... |
− | Unpacking bdwgc (8.0 |
+ | Unpacking bdwgc (8.2.0-r0) ... |
Selecting previously unselected package zile. |
Selecting previously unselected package zile. |
||
− | Preparing to unpack .../zile_2.4. |
+ | Preparing to unpack .../zile_2.4.15-r0_armhf.deb ... |
− | Unpacking zile (2.4. |
+ | Unpacking zile (2.4.15-r0) ... |
− | Setting up bdwgc (8.0 |
+ | Setting up bdwgc (8.2.0-r0) ... |
− | Setting up zile (2.4. |
+ | Setting up zile (2.4.15-r0) ... |
... or removed: |
... or removed: |
||
Line 118: | Line 126: | ||
The following packages will be REMOVED: |
The following packages will be REMOVED: |
||
zile |
zile |
||
− | 0 upgraded, 0 newly installed, 1 to remove and |
+ | 0 upgraded, 0 newly installed, 1 to remove and 3 not upgraded. |
After this operation, 0 B of additional disk space will be used. |
After this operation, 0 B of additional disk space will be used. |
||
Do you want to continue? [Y/n] |
Do you want to continue? [Y/n] |
||
Line 127: | Line 135: | ||
<nowiki>https://wiki.st.com/stm32mpu/wiki/OpenSTLinux_licenses</nowiki>. |
<nowiki>https://wiki.st.com/stm32mpu/wiki/OpenSTLinux_licenses</nowiki>. |
||
− | (Reading database ... |
+ | (Reading database ... 14865 files and directories currently installed.) |
− | Removing zile (2.4. |
+ | Removing zile (2.4.15-r0) ... |
Line 143: | Line 151: | ||
The following packages will be REMOVED: |
The following packages will be REMOVED: |
||
bdwgc |
bdwgc |
||
− | 0 upgraded, 0 newly installed, 1 to remove and |
+ | 0 upgraded, 0 newly installed, 1 to remove and 3 not upgraded. |
After this operation, 0 B of additional disk space will be used. |
After this operation, 0 B of additional disk space will be used. |
||
Do you want to continue? [Y/n] |
Do you want to continue? [Y/n] |
||
Line 152: | Line 160: | ||
<nowiki>https://wiki.st.com/stm32mpu/wiki/OpenSTLinux_licenses</nowiki>. |
<nowiki>https://wiki.st.com/stm32mpu/wiki/OpenSTLinux_licenses</nowiki>. |
||
− | (Reading database ... |
+ | (Reading database ... 14864 files and directories currently installed.) |
− | Removing bdwgc (8.0 |
+ | Removing bdwgc (8.2.0-r0) ... |
− | |||
== How to activate a local package repository == |
== How to activate a local package repository == |
||
===Prerequisite=== |
===Prerequisite=== |
||
− | Even if ''Package repository for OpenSTLinux'' offers lots of and various packages, you may need to use a local and personnal package repository. |
+ | Even if ''Package repository for OpenSTLinux'' offers lots of and various packages, you may need to use a local and personnal package repository. Using a local and personal package repository is a 'smart' and 'quick' way to update the [[:Category:Starter_Package|Starter Package]] with your developments. |
A local package repository is a collection of *.deb organized such <code>apt</code> needs it. The local repository should provide ''Packages'' metafiles. |
A local package repository is a collection of *.deb organized such <code>apt</code> needs it. The local repository should provide ''Packages'' metafiles. |
||
Line 184: | Line 191: | ||
{{Board$}} echo "deb [trusted=yes] http://<IP>:8000/all /" >> /etc/apt/sources.list.d/my_custom.list |
{{Board$}} echo "deb [trusted=yes] http://<IP>:8000/all /" >> /etc/apt/sources.list.d/my_custom.list |
||
{{Board$}} echo "deb [trusted=yes] http://<IP>:8000/cortexa7t2hf-neon-vfpv4 /" >> /etc/apt/sources.list.d/my_custom.list |
{{Board$}} echo "deb [trusted=yes] http://<IP>:8000/cortexa7t2hf-neon-vfpv4 /" >> /etc/apt/sources.list.d/my_custom.list |
||
+ | {{Board$}} echo "deb [trusted=yes] http://<IP>:8000/cortexa7hf-neon-vfpv4 /" >> /etc/apt/sources.list.d/my_custom.list |
||
In the above example, '''[trusted=yes]''' has been specified because the package manifest '''Release''' is not signed.<br/> |
In the above example, '''[trusted=yes]''' has been specified because the package manifest '''Release''' is not signed.<br/> |
||
Line 194: | Line 202: | ||
The detailed content licenses can be found at |
The detailed content licenses can be found at |
||
<nowiki>https://wiki.st.com/stm32mpu/wiki/OpenSTLinux_licenses</nowiki>. |
<nowiki>https://wiki.st.com/stm32mpu/wiki/OpenSTLinux_licenses</nowiki>. |
||
− | Ign:1 http://<IP>:8000/ |
+ | Ign:1 http://<IP>:8000/stm32mp1 InRelease |
− | Ign:2 http://<IP>:8000/ |
+ | Ign:2 http://<IP>:8000/all InRelease |
− | Ign:3 http://<IP>:8000/cortexa7t2hf-neon-vfpv4 InRelease |
+ | Ign:3 http://<IP>:8000/cortexa7t2hf-neon-vfpv4 InRelease |
− | Get: |
+ | Ign:4 http://<IP>:8000/cortexa7hf-neon-vfpv4 InRelease |
− | Get: |
+ | Get:5 http://<IP>:8000/stm32mp1 Release [1088 B]
|
− | Get: |
+ |
Get:6 http://<IP>:8000/all Release [1083 B] |
− | Ign: |
+ | Get:7 http://<IP>:8000/cortexa7t2hf-neon-vfpv4 Release [1115 B] |
− | Ign: |
+ | Get:8 http://<IP>:8000/cortexa7hf-neon-vfpv4 Release [1097 B] |
− | Ign: |
+ | Ign:9 http://<IP>:8000/stm32mp1 Release.gpg
|
− | Get: |
+ |
Ign:10 http://<IP>:8000/all Release.gpg |
− | Get: |
+ | Ign:11 http://<IP>:8000/cortexa7t2hf-neon-vfpv4 Release.gpg |
− | Get: |
+ | Ign:12 http://<IP>:8000/cortexa7hf-neon-vfpv4 Release.gpg |
− | Fetched |
+ | Get:13 http://<IP>:8000/stm32mp1 Packages [165 kB]
|
+ |
Get:14 http://<IP>:8000/all Packages [109 kB] |
||
+ | Get:15 http://<IP>:8000/cortexa7t2hf-neon-vfpv4 Packages [2775 kB] |
||
+ | Get:16 http://<IP>:8000/cortexa7hf-neon-vfpv4 Packages [20.5 kB] |
||
+ | Fetched 3073 kB in 7s (463 kB/s) |
||
Reading package lists... Done |
Reading package lists... Done |
||
Line 227: | Line 239: | ||
* https://wiki.debian.org/SecureApt |
* https://wiki.debian.org/SecureApt |
||
* [[STM32MP15 Discovery kits - Starter Package]] |
* [[STM32MP15 Discovery kits - Starter Package]] |
||
− | * [[STM32MP15_Evaluation boards - Starter Package]] |
+ | * [[STM32MP15_Evaluation boards - Starter Package | STM32MP15 Evaluation boards - Starter Package]] |
* [[STM32MP1 Developer Package]] |
* [[STM32MP1 Developer Package]] |
||