Difference between revisions of "OpenSTLinux distribution"
[unchecked revision] | [quality revision] |
m
|
m
|
Applicable for | STM32MP13x lines, STM32MP15x lines |
Contents
1 What is the OpenSTLinux distribution?[edit]
The OpenSTLinux distribution, running on the Arm® Cortex®-A processor(s), is a sub-part of the STM32MPU Embedded Software distribution.
OpenSTLinux is a Linux® distribution based on the OpenEmbedded build framework.
It includes the following collection of software components:
- OpenSTLinux BSP (OP-TEE secure OS, boot chain and Linux kernel)
- Application frameworks such as the following Linux application frameworks (non-exhaustive list):
- Wayland-Weston as a display/graphic framework
- Gstreamer as a multimedia framework
- Advanced Linux Sound Architecture (ALSA) libraries
As explained in the OpenEmbedded article, the files used to build an image are stored in layers that come from different sources, and that are configured for this image.
Only layers specific to the OpenSTLinux distribution (for example the OpenSTLinux Board Support Package layer) are detailed in the Layers chapter below. Community layers referenced in this article are not listed.
The Machines chapter introduces the machine metadata (the information needed to build a kernel for specific target boards), while the Images chapter specifies the images that contain the information needed to build the user space. The Distros chapter describes the available distros configurations.
2 Software architecture overview[edit]
The figure below gives an overview of the OpenSTLinux architecture. You can obtain more details by clicking on one of the sub-levels.
The Linux application frameworks (or Linux user space components) that rely on the OpenSTLinux BSP, mainly come from open-source communities.
OpenEmbedded core components (community layers) combined with STMicroelectronics-specific layers (for example the BSP layer) give a consistent starting point to develop customer applications based on a standardized interface.

3 OpenSTLinux concept[edit]
To build an OpenSTLinux based software, a combination of machine, image and distro must be selected.
Available machines, images and distros are listed below.
More information on how to compile and use an OpenSTLinux distribution can be found in the Distribution Package articles.
3.1 Layers[edit]
This chapter describes the layers developed by STMicroelectonics.
STMicroelectronics' strategy is to organize the layers in order to split BSP descriptions from applications and frameworks.
By doing this, any BSP can be combined with any framework, or no framework at all.
Layer | Description |
---|---|
meta-st-stm32mp | BSP Layer for stm32mp |
meta-st-openstlinux | OpenSTLinux layer - framework/image settings |
For the detailed content of the layers, please check:
-
STM32_MPU_OpenSTLinux_release_note#Detailed delivery content for STM32MP15x lines
lines
-
STM32_MPU_OpenSTLinux_release_note#Detailed delivery content for STM32MP13x lines
lines
In addition, in OpenSTLinux distribution, a layer (meta-st-stm32mp-addons) has been created to manage STM32CubeMX integration.
If necessary, you can also create your own layer. The procedure to do so is explained in How_to_create_a_new_open_embedded_layer.
Layer | Description |
---|---|
meta-st-stm32mp-addons | BSP Layer addons for stm32mp (CubeMX Machine) |
meta-my-custo-layer | framework addons/customization |
3.2 Machines[edit]
3.3 Images[edit]
Image | Description |
---|---|
Official images | |
st-image-weston | OpenSTLinux weston image with basic Wayland support (if enabled in distro) |
Supported images | |
st-image-core | OpenSTLinux core image |
Images, proposed as example only | |
st-example-image-qt | ST example of image based on QT framework |
st-example-image-qtwayland | ST example of image based on QT framework (available for ecosystem release ≥ v2.1.0 ) |
3.4 Distros[edit]
For further details on distributions (distros), read "Creating a distribution" [1]
Distro | Description |
---|---|
openstlinux-eglfs | OpenSTLinux featuring eglfs - no X11, no Wayland |
openstlinux-weston | OpenSTLinux featuring Weston/Wayland |
nodistro | *** DEFAULT OPENEMBEDDED SETTING : DISTRO is not defined *** |
3.5 Reference source code[edit]
By default, Yocto recipes to get the TF-A, U-Boot and OP-TEE components have been configured to use official GitHub® repository of their respective community + ST patches for source code, and tarball + patches for kernel component source code.
If you prefer to use ST GitHub® as a source code reference for these BSPs components, you need to update your local.conf file
Refer to the section ‘Configure STM32MP default version to github’ in local.conf :
# ========================================================================= # Configure STM32MP default version to github # ========================================================================= #STM32MP_SOURCE_SELECTION_pn-linux-stm32mp = "github" #STM32MP_SOURCE_SELECTION_pn-optee-os-stm32mp = "github" #STM32MP_SOURCE_SELECTION_pn-tf-a-stm32mp = "github" #STM32MP_SOURCE_SELECTION_pn-u-boot-stm32mp = "github"
Then just uncomment the line to switch the component to github® for source code.
4 How to get the software for this distribution[edit]
The OpenSTLinux distribution is available through the three Packages (Starter, Developer, and Distribution) of the STM32MPU Embedded Software distribution.
5 References[edit]
{{ApplicableFor |MPUs list=STM32MP13x, STM32MP15x |MPUs checklist=STM32MP13x, STM32MP15x }}<noinclude></noinclude> ==What is the OpenSTLinux distribution?== The OpenSTLinux distribution, running on the Arm<sup>®</sup> Cortex<sup>®</sup>-A processor(s), is a sub-part of the [[STM32MPU Embedded Software distribution]]. [[File:OpenSTLinux distribution.png|thumb|200px|link=]] OpenSTLinux is a Linux<sup>®</sup> distribution based on the [[OpenEmbedded]] build framework.<br> It includes the following collection of software components: * [[OpenSTLinux BSP architecture overview|OpenSTLinux BSP]] (OP-TEE secure OS, boot chain and Linux kernel) * Application frameworks such as the following Linux application frameworks (non-exhaustive list): ** [[Wayland Weston overview|Wayland-Weston]] as a display/graphic framework ** [[GStreamer_overview|Gstreamer]] as a multimedia framework ** [[ALSA overview|Advanced Linux Sound Architecture (ALSA)]] libraries As explained in the [[OpenEmbedded]] article, the files used to build an image are stored in layers that come from different sources, and that are configured for this image. <br> Only layers specific to the OpenSTLinux distribution (for example the OpenSTLinux Board Support Package layer) are detailed in the [[#Layers|Layers]] chapter below. Community layers referenced in this article are not listed. The [[#Machines|Machines]] chapter introduces the machine metadata (the information needed to build a kernel for specific target boards), while the [[#Images|Images]] chapter specifies the images that contain the information needed to build the user space. The [[#Distros|Distros]] chapter describes the available distros configurations. ==Software architecture overview== The figure below gives an overview of the [[OpenSTLinux architecture overview|OpenSTLinux architecture]]. You can obtain more details by clicking on one of the sub-levels.<br> The '''Linux application frameworks''' (or Linux user space components) that rely on the [[OpenSTLinux BSP architecture overview|OpenSTLinux BSP]], mainly come from open-source communities. OpenEmbedded core components (community layers) combined with STMicroelectronics-specific layers (for example the BSP layer) give a consistent starting point to develop customer applications based on a standardized interface. {{:OpenSTLinux architecture overview}} ==OpenSTLinux concept== To build an OpenSTLinux based software, a combination of machine, image and distro must be selected.<br> Available machines, images and distros are listed below. More information on how to compile and use an OpenSTLinux distribution can be found in the [[:category:Distribution Package | '''Distribution Package''' articles]]. ===Layers=== This chapter describes the layers developed by STMicroelectonics. STMicroelectronics' strategy is to organize the layers in order to split BSP descriptions from applications and frameworks.<br> By doing this, any BSP can be combined with any framework, or no framework at all. {| class="st-table" style="text-align: left; " |- ! align="center" valign="center"| Layer ! align="center" valign="center"| Description |- | [https://github.com/STMicroelectronics/meta-st-stm32mp/ meta-st-stm32mp] || BSP Layer for stm32mp |- | [https://github.com/STMicroelectronics/meta-st-openstlinux/ meta-st-openstlinux] || OpenSTLinux layer - framework/image settings |} For the detailed content of the layers, please check: {{ReviewsComments|-- [[User:Nathalie Sangouard|Nathalie Sangouard]] ([[User talk:Nathalie Sangouard|talk]]) 15:48, 17 June 2022 (CEST)<br />To rework after changes of release note name and rework. is there some aprt dedicated to MP13 et MP15?}} * [[STM32_MPU_OpenSTLinux_release_note#Detailed delivery content]] for {{MicroprocessorDevice | device=15}} lines * [[STM32_MPU_OpenSTLinux_release_note#Detailed delivery content]] for {{MicroprocessorDevice | device=13}} lines In addition, in OpenSTLinux distribution, a layer ('''meta-st-stm32mp-addons''') has been created to manage STM32CubeMX integration.<br> If necessary, you can also create your own layer. The procedure to do so is explained in [[How_to_create_a_new_open_embedded_layer]]. {| class="st-table" style="text-align: left; " |- ! align="center" valign="center"| Layer ! align="center" valign="center"| Description |- | [https://github.com/STMicroelectronics/meta-st-stm32mp-addons/ meta-st-stm32mp-addons] || BSP Layer addons for stm32mp (CubeMX Machine) |- | meta-{{HighlightParam|''my-custo-layer''}} || framework addons/customization |} ===Machines=== {| class="st-table" style="text-align: left; " |- ! align="center" valign="center"| Machine ! align="center" valign="center"| Description |- | style="width: 22%" | stm32mp1 || Machine configuration for STM32MP1 microprocessor device boards |- | style="width: 22%" | '''stm32mp13-disco''' || Machine Example of machine configuration for STM32MP13 disco board ({{Board | type=135D-DK | name=short}} and {{Board | type=135F-DK | name=short}} in OP-TEE boot mode on SDCard) |- | style="width: 22%" | '''stm32mp15-disco''' || Machine Example of machine configuration for STM32MP1 disco board (Only {{Board | type=157C-DK2 | name=short}} in OP-TEE boot mode on SDCard) |- | style="width: 22%" | '''stm32mp15-eval''' || Machine Example of machine configuration for STM32MP1 evaluation board (Only {{Board | type=157C-EV1 | name=short}} in trusted boot mode on SDCard) |} ===Images=== {| class="st-table" style="text-align: left; " |- ! align="center" valign="center "| Image ! align="center" valign="center "| Description |- !! colspan="2" | '''Official images''' |- | st-image-weston || OpenSTLinux weston image with basic Wayland support (if enabled in distro) |- !! colspan="2" | '''Supported images''' |- | st-image-core || OpenSTLinux core image |- !! colspan="2" | '''Images, proposed as example only''' |- | st-example-image-qt || ST example of image based on QT framework |- | st-example-image-qtwayland || ST example of image based on QT framework (available for {{EcosystemRelease | revision=2.1.0 | range=and after}}) |} ===Distros=== For further details on distributions (distros), read "Creating a distribution" <ref>{{DocSource | domain=Yocto Project | path=mega-manual/mega-manual.html#creating-your-own-distribution | text=Creating a distribution}}</ref> {| class="st-table" style="text-align: left;" |- ! align="center" valign="center "| Distro ! align="center" valign="center "| Description |- | openstlinux-eglfs || OpenSTLinux featuring eglfs - no X11, no Wayland |- | openstlinux-weston || OpenSTLinux featuring Weston/Wayland |- | nodistro || *** DEFAULT OPENEMBEDDED SETTING : DISTRO is not defined *** |} ===Reference source code=== By default, Yocto recipes to get the TF-A, U-Boot and OP-TEE components have been configured to use '''official GitHub<sup>®</sup> repository of their respective community + ST patches''' for source code, and '''tarball + patches''' for kernel component source code. If you prefer to use '''ST GitHub'''<sup>®</sup> as a source code reference for these BSPs components, you need to update your local.conf file Refer to the section ‘Configure STM32MP default version to github’ in local.conf : # ========================================================================= # Configure STM32MP default version to github # ========================================================================= #STM32MP_SOURCE_SELECTION_pn-linux-stm32mp = "github" #STM32MP_SOURCE_SELECTION_pn-optee-os-stm32mp = "github" #STM32MP_SOURCE_SELECTION_pn-tf-a-stm32mp = "github" #STM32MP_SOURCE_SELECTION_pn-u-boot-stm32mp = "github" Then just uncomment the line to switch the component to github<sup>®</sup> for source code. ==How to get the software for this distribution== The OpenSTLinux distribution is available through the three Packages (Starter, Developer, and Distribution) of the [[STM32MPU Embedded Software distribution|STM32MPU Embedded Software distribution]]. ==References==<references/> <noinclude> [[Category:OpenSTLinux distribution|00]] {{PublicationRequestId | 8358 | 2018-06-18 | PhilipS}}</noinclude>
Line 55: | Line 55: | ||
|} |
|} |
||
− | |||
− | |||
− | |||
− | |||
− | In addition, in OpenSTLinux distribution, a layer (meta-st-stm32mp-addons) has been created to manage STM32CubeMX integration.<br> |
+ | In addition, in OpenSTLinux distribution, a layer ('''meta-st-stm32mp-addons''') has been created to manage STM32CubeMX integration.<br> |
If necessary, you can also create your own layer. The procedure to do so is explained in [[How_to_create_a_new_open_embedded_layer]]. |
If necessary, you can also create your own layer. The procedure to do so is explained in [[How_to_create_a_new_open_embedded_layer]]. |
||
Line 81: | Line 77: | ||
| style="width: 22%" | stm32mp1 || Machine configuration for STM32MP1 microprocessor device boards |
| style="width: 22%" | stm32mp1 || Machine configuration for STM32MP1 microprocessor device boards |
||
|- |
|- |
||
− | | style="width: 22%" | '''stm32mp13-disco''' || |
+ | | style="width: 22%" | '''stm32mp13-disco''' || Example of machine configuration for STM32MP13 disco board ({{Board | type=135D-DK | name=short}} and {{Board | type=135F-DK | name=short}} in OP-TEE boot mode on SDCard) |
|- |
|- |
||
− | | style="width: 22%" | '''stm32mp15-disco''' || |
+ | | style="width: 22%" | '''stm32mp15-disco''' || Example of machine configuration for STM32MP1 disco board (Only {{Board | type=157C-DK2 | name=short}} in OP-TEE boot mode on SDCard) |
|- |
|- |
||
− | | style="width: 22%" | '''stm32mp15-eval''' || |
+ | | style="width: 22%" | '''stm32mp15-eval''' || Example of machine configuration for STM32MP1 evaluation board (Only {{Board | type=157C-EV1 | name=short}} in trusted boot mode on SDCard) |
|} |
|} |
||