Difference between revisions of "OpenSTLinux architecture overview"

[quality revision] [unchecked revision]
m
m

The OpenSTLinux distribution encompasses the following components:

  • The OpenSTLinux BSP that offers services, to the application frameworks in the same context, from:
    • The boot chain based on TF-A and U-Boot
    • The OP-TEE secure OS running on the Cortex-A in secure mode
    • The Linux® kernel running on the Arm® Cortex®-A in non-secure mode
  • The Application frameworks that rely on the services provided by the OpenSTLinux BSP, to provide particular functionalities (code libraries, APIs, tool sets...) to facilitate the development of software applications:
    • The Linux application frameworks (aka Linux middlewares) running on the user space of the Linux OS: e.g. libusb C library for a generic access to USB devices, ALSA user-space bundle for audio functionalities, GStreamer multimedia framework...
    • The OP-TEE application frameworks running on the user space of the secure OS: e.g. TEE Internal core API for the development of Trusted Applications (TA)
    • The U-Boot application frameworks: e.g. configuration scripts

The figure below is clickable so that the user can directly jump to one of the sub-levels listed above.

Zoom out to STM32MPU Embedded Software


OP-TEE overview OP-TEE overview TF-A overview U-Boot overview STM32MP15 Linux kernel overview Boot chain overview OpenSTLinux BSP architecture overview Linux application frameworks overview
OpenSTLinux architecture overview



The '''OpenSTLinux distribution''' encompasses the following components:
* The '''OpenSTLinux BSP''' that offers services, to the application frameworks in the same context, from:
** The '''boot chain''' based on '''TF-A''' and '''U-Boot'''
** The '''OP-TEE secure OS''' running on the Cortex-A in secure mode
** The '''Linux<sup>&reg;</sup> kernel''' running on the Arm<sup>&reg;</sup> Cortex<sup>&reg;</sup>-A in non-secure mode
* The '''Application frameworks''' that rely on the services provided by the OpenSTLinux BSP, to provide particular functionalities (code libraries, APIs, tool sets...) to facilitate the development of software applications:
** The '''Linux application frameworks''' (aka Linux middlewares) running on the user space of the Linux OS: e.g. libusb C library for a generic access to USB devices, ALSA user-space bundle for audio functionalities, GStreamer multimedia framework...
** The '''OP-TEE application frameworks''' running on the user space of the secure OS: e.g. TEE Internal core API for the development of Trusted Applications (TA)
** The '''U-Boot application frameworks''': e.g. configuration scripts

The figure below is clickable so that the user can directly jump to one of the sub-levels listed above.<br>


[[File: STM32MPU Embedded Software architecture overview.png|link=STM32MPU Embedded Software architecture overview|thumb|Zoom out to STM32MPU Embedded Software]]<onlyinclude>

{{ImageMap|Image: OpenSTLinux architecture overview.png{{!}} frame {{!}} center {{!}} OpenSTLinux architecture overview
rect 40 62 137 123 [[OP-TEE overview]]
rect 40 229 137 286 [[OP-TEE overview]]
rect 144 229 239 286 [[TF-A overview]]
rect 260 229 356 286 [[U-Boot overview]]
rect 364 229 461 287 [[STM32MP15 Linux kernel overview]]
poly 255 203 359 203 359 289 140 289 140 224 255 224 [[Boot_chain_overview|Boot chain overview]]
rect 32 198 469 296 [[OpenSTLinux BSP architecture overview]]
rect 364 62 461 121 [[Linux application frameworks overview]]
}}<br>
</onlyinclude>

</onlyinclude>

{{ReviewsComments|-- [[User:Gerald Baeza|Gerald Baeza]] ([[User talk:Gerald Baeza|talk]]) 14:30, 5 March 2021 (CET)<br />Remove OP-TEE application framework (there is nothing here) and corresponding clickable area}} <noinclude>

{{PublicationRequestId | 5963 | 2018-01-25 | AlainF}}
[[Category:Architecture overview|02]]</noinclude>
Line 23: Line 23:
 
rect 364 62 461 121 [[Linux application frameworks overview]]
 
rect 364 62 461 121 [[Linux application frameworks overview]]
 
}}
 
}}
<br>
 
 
</onlyinclude>
 
</onlyinclude>
 
+
{{ReviewsComments|-- [[User:Gerald Baeza|Gerald Baeza]] ([[User talk:Gerald Baeza|talk]]) 14:30, 5 March 2021 (CET)<br />Remove OP-TEE application framework (there is nothing here) and corresponding clickable area}}
 
<noinclude>
 
<noinclude>
 
{{PublicationRequestId | 5963 | 2018-01-25 | AlainF}}
 
{{PublicationRequestId | 5963 | 2018-01-25 | AlainF}}
 
[[Category:Architecture overview|02]]
 
[[Category:Architecture overview|02]]
 
</noinclude>
 
</noinclude>