Difference between revisions of "Netstat"
[unchecked revision] | [quality revision] |
m
|
Contents
1 Article purpose[edit]
This article provides the basic information needed to start using the Linux tool: netstat [1].
2 Introduction[edit]
The following table provides a brief description of the tool, as well as its availability depending on the software packages:
: this tool is either present (ready to use or to be activated), or can be integrated and activated on the software package.
: this tool is not present and cannot be integrated, or it is present but cannot be activated on the software package.
Tool | STM32MPU Embedded Software distribution | STM32MPU Embedded Software distribution for Android™ | ||||||
---|---|---|---|---|---|---|---|---|
Name | Category | Purpose | Starter Package | Developer Package | Distribution Package | Starter Package | Developer Package | Distribution Package |
netstat | Monitoring tools | netstat[1] prints network connections, routing tables, interface statistics, masquerade connections, and multicast membership information. | ![]() |
![]() |
![]() |
![]() |
![]() |
![]() |
3 Installing the trace and debug tool on your target board[edit]
3.1 Using the STM32MPU Embedded Software distribution[edit]
netstat is installed by default and ready to be used with all STM32MPU Embedded Software Packages.
It comes through the busybox:
Board $> which netstat | xargs ls -la /bin/netstat -> /bin/busybox.nosuid
3.2 Using the STM32MPU Embedded Software distribution for Android™[edit]
netstat is installed by default and ready to be used with all STM32MPU Embedded Software Packages for Android™.
It comes with the toybox:
Board $> which netstat | xargs ls -la /system/bin/netstat -> toybox
4 Getting started[edit]
Here are basic commands to start with netstat:
- Display kernel routing information
Board $> netstat -rn Kernel IP routing table Destination Gateway Genmask Flags MSS Window irtt Iface 0.0.0.0 10.99.3.254 0.0.0.0 UG 0 0 0 eth0 10.99.0.0 0.0.0.0 255.255.252.0 U 0 0 0 eth0 10.99.3.254 0.0.0.0 255.255.255.255 UH 0 0 0 eth0
- List out listening-only connections
Board $> netstat -tnl Active Internet connections (only servers) Proto Recv-Q Send-Q Local Address Foreign Address State tcp 0 0 0.0.0.0:19999 0.0.0.0:* LISTEN tcp 0 0 0.0.0.0:5355 0.0.0.0:* LISTEN tcp 0 0 10.99.1.237:53 0.0.0.0:* LISTEN tcp 0 0 127.0.0.1:53 0.0.0.0:* LISTEN tcp 0 0 127.0.0.1:953 0.0.0.0:* LISTEN tcp 0 0 0.0.0.0:1534 0.0.0.0:* LISTEN tcp 0 0 :::19999 :::* LISTEN tcp 0 0 :::5355 :::* LISTEN tcp 0 0 :::53 :::* LISTEN tcp 0 0 :::22 :::* LISTEN
5 To go further[edit]
Additional documentation is available on Internet about netstat. See References.
Refer to Linux® Template:Sup man page[1] for more details on command options.
6 References[edit]
- Useful external links
Document link | Document Type | Description |
---|---|---|
netstat (wikipedia.org) | Standard | wikipedia.org |
netstat examples | User Guide | binarytides.com |
netstat main commands | User Guide | geekflare.com |
==Article purpose== This article provides the basic information needed to start using the Linux tool: '''netstat''' <ref name=netstatmanpage/>. ==Introduction== {{:Trace_and_debug_tools_assignment_table_template}}<onlyinclude> | [[Netstat|netstat]] | [[:Category:Monitoring tools|Monitoring tools]] | style="text-align:left;" | '''netstat'''<ref name=netstatmanpage>https://linux.die.net/man/8/netstat</ref> prints network connections, routing tables, interface statistics, masquerade connections, and multicast membership information. || {{Y}} || {{Y}} || {{Y}} || {{Y}} || {{Y}} || {{Y}} |-</onlyinclude> |} == Installing the trace and debug tool on your target board == === Using the STM32MPU Embedded Software distribution === '''netstat''' is installed by default and ready to be used with all STM32MPU Embedded Software Packages. It comes through the '''busybox''': {{Board$}} which netstat | xargs ls -la /bin/netstat -> /bin/busybox.nosuid === Using the STM32MPU Embedded Software distribution for Android™ === '''netstat''' is installed by default and ready to be used with all STM32MPU Embedded Software Packages for Android™. It comes with the '''toybox''': {{Board$}} which netstat | xargs ls -la /system/bin/netstat -> toybox ==Getting started== Here are basic commands to start with netstat: * Display kernel routing information {{Board$}} netstat -rn Kernel IP routing table Destination Gateway Genmask Flags MSS Window irtt Iface 0.0.0.0 10.99.3.254 0.0.0.0 UG 0 0 0 eth0 10.99.0.0 0.0.0.0 255.255.252.0 U 0 0 0 eth0 10.99.3.254 0.0.0.0 255.255.255.255 UH 0 0 0 eth0 * List out listening-only connections {{Board$}} netstat -tnl Active Internet connections (only servers) Proto Recv-Q Send-Q Local Address Foreign Address State tcp 0 0 0.0.0.0:19999 0.0.0.0:* LISTEN tcp 0 0 0.0.0.0:5355 0.0.0.0:* LISTEN tcp 0 0 10.99.1.237:53 0.0.0.0:* LISTEN tcp 0 0 127.0.0.1:53 0.0.0.0:* LISTEN tcp 0 0 127.0.0.1:953 0.0.0.0:* LISTEN tcp 0 0 0.0.0.0:1534 0.0.0.0:* LISTEN tcp 0 0 :::19999 :::* LISTEN tcp 0 0 :::5355 :::* LISTEN tcp 0 0 :::53 :::* LISTEN tcp 0 0 :::22 :::* LISTEN == To go further == Additional documentation is available on Internet about '''netstat'''. See [[#References|References]]. Refer to Linux{{sup|®</sup>}} man page<ref name=netstatmanpage/> for more details on command options. == References ==<references /> * Useful external links {| ! scope=col | Document link ! scope=col | Document Type ! scope=col | Description |- | [https://en.wikipedia.org/wiki/Netstat netstat (wikipedia.org)] | Standard | wikipedia.org |- | [http://www.binarytides.com/linux-netstat-command-examples netstat examples] | User Guide | binarytides.com |- | [https://geekflare.com/netstat/ netstat main commands] | User Guide | geekflare.com |} <noinclude> {{ ArticleBasedOnModel | Trace and debug tools article model }} {{ PublicationRequestId | 9039 | 08Oct'18 }} [[Category:Linux monitoring tools]] </noinclude>
Line 58: | Line 58: | ||
Additional documentation is available on Internet about '''netstat'''. See [[#References|References]]. |
Additional documentation is available on Internet about '''netstat'''. See [[#References|References]]. |
||
− | Refer to Linux |
+ | Refer to Linux<sup>®</sup> man page<ref name=netstatmanpage/> for more details on command options. |
== References == |
== References == |
||
Line 83: | Line 83: | ||
|} |
|} |
||
+ | <noinclude> |
||
{{ ArticleBasedOnModel | Trace and debug tools article model }} |
{{ ArticleBasedOnModel | Trace and debug tools article model }} |
||
{{ PublicationRequestId | 9039 | 08Oct'18 }} |
{{ PublicationRequestId | 9039 | 08Oct'18 }} |
||
− | |||
[[Category:Linux monitoring tools]] |
[[Category:Linux monitoring tools]] |
||
+ | </noinclude> |