Difference between revisions of "Modify, rebuild and reload the Linux® kernel"

[unchecked revision] [quality revision]
m (Download the the Linux® kernel source code)
m

Template:ArticleMainWriter


1 Overview[edit]

This stage explains how modify, rebuild and reload the Linux® kernel.
You will first be guided to install the Linux® kernel source code in the Developer Package directory. Then step by step you will execute procedures to modify, rebuild and reload the Linux® kernel.

2 Download the the Linux® kernel source code[edit]

  • Download the STM32MP15-Ecosystem-v1.0.0 Developer Package Sources to the following directory:
    $HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v1.0.0/Developer-Package
  • Uncompress the tarball file to get the Linux® kernel tarball, the ST patches and the ST configuration fragments
PC $> cd $HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v1.0.0/Developer-Package
PC $> tar xvf en.SOURCES-kernel-stm32mp1-openstlinux-4.19-thud-mp1-19-02-20.tar.xz

3 Prepare the Linux® kernel source code[edit]

  • Extract the Linux® kernel source
PC $> cd stm32mp1-openstlinux-4.19-thud-mp1-19-02-20/sources/arm-openstlinux_weston-linux-gnueabi/linux-stm32mp-4.19-r0
PC $> tar xvf linux-4.19.9.tar.xz
  • Apply the ST patches
PC $> cd linux-4.19.9/
PC $> for p in `ls -1 ../*.patch`; do patch -p1 < $p; done
  • Apply fragments
PC $> make multi_v7_defconfig fragment*.config
PC $> for f in `ls -1 ../fragment*.config`; do scripts/kconfig/merge_config.sh -m -r .config $f; done
PC $> yes '' | make oldconfig

4 Build the Linux® kernel source code for the first time[edit]

Info.png The first time the kernel is build it could take several minutes.
  • Build kernel images (uImage and vmlinux) and device tree (dtbs)
PC $> make uImage vmlinux dtbs LOADADDR=0xC2000040
  • Build kernel module
PC $> make modules
  • Generate output build artifacts
PC $> mkdir -p $PWD/install_artifact/
PC $> make INSTALL_MOD_PATH="$PWD/install_artifact" modules_install

5 Deploy the Linux® kernel on the board[edit]

5.1 Push the Linux® kernel into the board[edit]

PC $> scp arch/arm/boot/uImage root@<board ip address>:/boot

5.2 Push the devicetree into the board[edit]

PC $> scp arch/arm/boot/dts/stm32mp157*.dtb root@<board ip address>:/boot

5.3 Push the kernel modules into the board[edit]

  • Remove the link created inside the install_artifact/lib/modules/4.19.9 directory
PC $> rm install_artifact/lib/modules/4.19.9/build install_artifact/lib/modules/4.19.9/source
  • Optionally, strip kernel modules (to reduce the size of each kernel modules)
PC $> find install_artifact/ -name "*.ko" | xargs $STRIP --strip-debug --remove-section=.comment --remove-section=.note --preserve-dates
  • Copy Kernel modules
PC $> scp -r install_artifact/lib/modules/* root@<ip of board>:/lib/modules
  • Using the Linux console, re-generate the list of module dependencies (modules.dep) and the list of symbols provided by modules (modules.symbols)
Board $> /sbin/depmod -a
  • Synchronize data on disk with memory
Board $> sync

5.4 Reboot the board[edit]

Board $> reboot

6 Modifying a built-in Linux kernel device driver[edit]

This simple example adds unconditional log information when the display driver is probed.

  • Using the Linux console, check that there is no log information when the display driver is probed
Board $> dmesg | grep -i stm_drm_platform_probe
Board $>

  • Go to the Linux® kernel source directory
PC $> cd $HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v1.0.0/Developer-Package/stm32mp1-openstlinux-4.19-thud-mp1-19-02-20/sources/arm-openstlinux_weston-linux-gnueabi/linux-stm32mp-4.19-r0/linux-4.19.9
  • Edit the ./drivers/gpu/drm/stm/drv.c source file
  • Add a log information in the stm_drm_platform_probe function as follow
static int stm_drm_platform_probe(struct platform_device *pdev)
{
	struct device *dev = &pdev->dev;
	struct drm_device *ddev;
	int ret;
	[...]

	DRM_INFO("Simple example - %s\n", __func__);

	return 0;
	[...]
}
  • Save the file
  • Rebuitd the Linux® kernel
PC $> make uImage LOADADDR=0xC2000040
  • Update the Linux kernel image into board
PC $> scp arch/arm/boot/uImage root@<board ip address>:/boot
  • Reboot the board
Board $> reboot
  • Check that there is now log information when the display driver is probed
Board $> dmesg | grep -i stm_drm_platform_probe
[    2.764080] [drm] Simple example - stm_drm_platform_probe
<noinclude>

{{ArticleMainWriter | VincentA}}
[[Category:Sub-articles]]
__NOTOC__</noinclude>

==Overview==
This stage explains how modify, rebuild and reload the Linux® kernel.<br>

You will first be guided to install the Linux® kernel source code in the Developer Package directory. Then step by step you will execute procedures to modify, rebuild and reload the Linux® kernel.

==Download the the Linux® kernel source code==
* Download the [https://www.st.com/content/ccc/resource/technical/sw-updater/firmware2/group0/d1/01/38/fc/a8/61/4f/e9/STM32cube_Standard_A7_BSP_components_kernel/files/SOURCES-kernel-stm32mp1-openstlinux-4.19-thud-mp1-19-02-20.tar.xz/jcr:content/translations/en.SOURCES-kernel-stm32mp1-openstlinux-4.19-thud-mp1-19-02-20.tar.xz STM32MP15-Ecosystem-v1.0.0 Developer Package Sources] to the following directory:<br> '''$HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v1.0.0/Developer-Package'''
* Uncompress the tarball file to get the Linux® kernel tarball, the ST patches and the ST configuration fragments
 {{PC$}} cd $HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v1.0.0/Developer-Package
 {{PC$}} tar xvf en.SOURCES-kernel-stm32mp1-openstlinux-4.19-thud-mp1-19-02-20.tar.xz

==Prepare the Linux® kernel source code==
* Extract the Linux® kernel source
 {{PC$}} cd stm32mp1-openstlinux-4.19-thud-mp1-19-02-20/sources/arm-openstlinux_weston-linux-gnueabi/linux-stm32mp-4.19-r0
 {{PC$}} tar xvf linux-4.19.9.tar.xz
* Apply the ST patches
 {{PC$}} cd linux-4.19.9/
 {{PC$}} for p in `ls -1 ../*.patch`; do patch -p1 < $p; done
* Apply fragments
 {{PC$}} make multi_v7_defconfig fragment*.config
 {{PC$}} for f in `ls -1 ../fragment*.config`; do scripts/kconfig/merge_config.sh -m -r .config $f; done
 {{PC$}} yes <nowiki>''</nowiki> | make oldconfig

==Build the Linux® kernel source code for the first time==
{{Info|The first time the kernel is build it could take several minutes.}}
* Build kernel images (uImage and vmlinux) and device tree (dtbs)
 {{PC$}} make uImage vmlinux dtbs LOADADDR=0xC2000040
* Build kernel module
 {{PC$}} make modules
* Generate output build artifacts
 {{PC$}} mkdir -p $PWD/install_artifact/
 {{PC$}} make INSTALL_MOD_PATH="$PWD/install_artifact" modules_install

==Deploy the Linux® kernel on the board==
===Push the Linux® kernel into the board===
 {{PC$}} scp arch/arm/boot/uImage root@<board ip address>:/boot
===Push the devicetree into the board===
 {{PC$}} scp arch/arm/boot/dts/stm32mp157*.dtb root@<board ip address>:/boot
===Push the kernel modules into the board===
* Remove the link created inside the '''install_artifact/lib/modules/4.19.9''' directory
 {{PC$}} rm install_artifact/lib/modules/4.19.9/build install_artifact/lib/modules/4.19.9/source
* Optionally, strip kernel modules (to reduce the size of each kernel modules)
 {{PC$}} find install_artifact/ -name "*.ko" | xargs $STRIP --strip-debug --remove-section=.comment --remove-section=.note --preserve-dates
* Copy Kernel modules
 {{PC$}} scp -r install_artifact/lib/modules/* root@<ip of board>:/lib/modules
* Using the Linux console, re-generate the list of module dependencies (modules.dep) and the list of symbols provided by modules (modules.symbols)
 {{Board$}} /sbin/depmod -a
* Synchronize data on disk with memory
 {{Board$}} sync
===Reboot the board===
 {{Board$}} reboot

==Modifying a built-in Linux kernel device driver==
This simple example adds unconditional log information when the display driver is probed.<br><br>


* Using the Linux console, check that there is no log information when the display driver is probed
 {{Board$}} dmesg | grep -i stm_drm_platform_probe
 {{Board$}}

* Go to the Linux® kernel source directory
 {{PC$}} cd $HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v1.0.0/Developer-Package/stm32mp1-openstlinux-4.19-thud-mp1-19-02-20/sources/arm-openstlinux_weston-linux-gnueabi/linux-stm32mp-4.19-r0/linux-4.19.9
* Edit the ''./drivers/gpu/drm/stm/drv.c'' source file
* Add a log information in the ''stm_drm_platform_probe'' function as follow
 static int stm_drm_platform_probe(struct platform_device *pdev)
 {
 	struct device *dev = &pdev->dev;
 	struct drm_device *ddev;
 	int ret;
 	[...]

 	{{Highlight|DRM_INFO("Simple example - %s\n", __func__);}}

 	return 0;
 	[...]
 }
* Save the file
* Rebuitd the Linux® kernel
 {{PC$}} make uImage LOADADDR=0xC2000040
* Update the Linux kernel image into board
 {{PC$}} scp arch/arm/boot/uImage root@<board ip address>:/boot
* Reboot the board
 {{Board$}} reboot
* Check that there is now log information when the display driver is probed
 {{Board$}} dmesg | grep -i stm_drm_platform_probe
 [    2.764080] [drm] Simple example - stm_drm_platform_probe
Line 4: Line 4:
 
__NOTOC__
 
__NOTOC__
 
</noinclude>
 
</noinclude>
 
 
==Overview==
 
==Overview==
 
This stage explains how modify, rebuild and reload the Linux® kernel.<br>
 
This stage explains how modify, rebuild and reload the Linux® kernel.<br>

Attachments

Discussions