Difference between revisions of "Modify, rebuild and reload a firmware"

[quality revision] [unchecked revision]
m

Template:ArticleMainWriter


1 Overview[edit]

This stage explains how to modify, rebuild and reload a STM32MP1 Arm® Cortex®-M4 coprocessor firmware.

It proposes to customize the STM32MP1 Cube Package Application example OpenAMP_TTY_Echo using the MPU feature integrated in SW4STM32 IDE.

2 Open SW4STM32 IDE[edit]

  • Open System Workbench for STM32 IDE
File:SW4STM32 workspace.png
SW4STM32 workspace

3 Connect a console to the board[edit]

  • It's very convenient to use the serial console integrated in SW4STM32
File:SW4STM32 workspace serial disconnect 1.png
SW4STM32 Open the serial device by clicking this item
  • Connection is ok if you can see Linux log or prompt.
File:SW4STM32 workspace serial disconnect 2.png
SW4STM32 Serial Consol is ready
  • If for personal reason you prefer using another terminal ( ssh, minicom), it's then recommended to stop the Target Status Widget using the Serial port in SW4STM32 by right click on the bottom right corner then stop
  • It will avoid the following repetitive pattern in your Linux console
root@stm32mp1:~# ifconfig; echo __END__:$?
eth0      Link encap:Ethernet  HWaddr 00:80:E1:42:45:69  
          inet addr:10.48.1.143  Bcast:10.48.3.255  Mask:255.255.252.0
          inet6 addr: fe80::280:e1ff:fe42:4569/64 Scope:Link
          UP BROADCAST RUNNING MULTICAST  MTU:1500  Metric:1
          RX packets:37 errors:0 dropped:1 overruns:0 frame:0
          TX packets:26 errors:0 dropped:0 overruns:0 carrier:0
          collisions:0 txqueuelen:1000 
          RX bytes:5776 (5.6 KiB)  TX bytes:3146 (3.0 KiB)
          Interrupt:63 Base address:0xc000 

lo        Link encap:Local Loopback  
          inet addr:127.0.0.1  Mask:255.0.0.0
          inet6 addr: ::1/128 Scope:Host
          UP LOOPBACK RUNNING  MTU:65536  Metric:1
          RX packets:344 errors:0 dropped:0 overruns:0 frame:0
          TX packets:344 errors:0 dropped:0 overruns:0 carrier:0
          collisions:0 txqueuelen:1000 
          RX bytes:22880 (22.3 KiB)  TX bytes:22880 (22.3 KiB)

usb0      Link encap:Ethernet  HWaddr 4A:06:6C:16:19:EC  
          inet addr:192.168.7.2  Bcast:192.168.7.255  Mask:255.255.255.0
          inet6 addr: fe80::4806:6cff:fe16:19ec/64 Scope:Link
          UP BROADCAST RUNNING MULTICAST  MTU:1500  Metric:1
          RX packets:0 errors:0 dropped:0 overruns:0 frame:0
          TX packets:396 errors:0 dropped:0 overruns:0 carrier:0
          collisions:0 txqueuelen:1000 
          RX bytes:0 (0.0 B)  TX bytes:115397 (112.6 KiB)

__END__:0

4 Import an existing example in SW4STM32 IDE[edit]

  • Open the import screen File > Import... and select Existing Project into Workspace
File:SW4STM32 import.png
SW4STM32 import screen
  • Browse and select OpenAMP_TTY_echo application example
  • If you are using STM32MP157C-DK2 Discovery kit
$HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v1.0.0/Developer-Package/STM32Cube_FW_MP1_V1.0.0/Projects/STM32MP157C-DK2/Applications/OpenAMP/OpenAMP_TTY_echo
  • If you are using STM32MP157x-EV1 Evaluation board
$HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v1.0.0/Developer-Package/STM32Cube_FW_MP1_V1.0.0/Projects/STM32MP157C-EV1/Applications/OpenAMP/OpenAMP_TTY_echo
  • Click finish
  • The OpenAMP_TTY_echo project is open and you can browse inside using the left pan
File:SW4STM32 workspace project open.png
SW4STM32 workspace with project open

5 Build the firmware[edit]

  • Click the build button (the little hammer in the toolbar)
File:SW4STM32 workspace project build.png
SW4STM32 build the project
  • Build is finished with no error
File:SW4STM32 workspace project build finished.png
SW4STM32 build finished with no error

6 Upload the firmware through Linux console[edit]

  • If you are using STM32MP157C-DK2 Discovery kit
 cd $HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v1.0.0/Developer-Package/STM32Cube_FW_MP1_V1.0.0/Projects/STM32MP157C-DK2/Applications/OpenAMP/OpenAMP_TTY_echo/SW4STM32/OpenAMP_TTY_echo/
  • If you are using STM32MP157x-EV1 Evaluation board
 cd $HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v1.0.0/Developer-Package/STM32Cube_FW_MP1_V1.0.0/Projects/STM32MP157C-EV1/Applications/OpenAMP/OpenAMP_TTY_echo/SW4STM32/OpenAMP_TTY_echo/
  • Upload your firmware example into the board
 scp Debug/OpenAMP_TTY_echo.elf root@<board ip address>:/lib/firmware

7 Start the firmware through Linux console[edit]

  • Verify that no firmware is currently runnig
 cat /sys/class/remoteproc/remoteproc0/state
offline

If offline is displayed, that means that no firmware is currently running. If running is displayed, a firmware is currently running. You shoul then stop it using the following command

 echo stop > /sys/class/remoteproc/remoteproc0/state
  • Set the firmware name to be executed
 echo -n OpenAMP_TTY_echo.elf > /sys/class/remoteproc/remoteproc0/firmware
  • Start the firmware
 echo start > /sys/class/remoteproc/remoteproc0/state
  • Verify that the firmware is runnig
 cat /sys/class/remoteproc/remoteproc0/state
running

8 Upload and start the firmware with SW4STM32[edit]

Thanks to the STM32-CoPro-MPU which complete SW4STM32 from version 2.8.0, SW4STM32 can manage to load and start a STM32MP1 Arm® Cortex®-M4 coprocessor firmware.

For doing so open the Debug Configuration ot the OpenAMP_TTY_echo and select "Thru Linux core (Production mode)

The inet Address of the board should be already filled. Else try to update it thanks to the button on the right

File:SW4STM32 Production Mode.png
Select Production mode in Startup pane of Debug Configuration

When configuration is ok the "Debug" button on the bottom right turn to active and you can launch the debug session.

The Debug in Production Mode adds the cortex-M firmware transfer to the embedded Linux. This means also in case of network usage some specific pop-up appearing:

  • the SSH Password is to complete: the default one is root.
SSH password popup
  • the RSA key is to be approved.
RSA key popup

After download of the firmware SW4STM32 will start it and switch into Debug Perspective. You can then use all features of the debugger.

For further information and support on new MPU feature in SW4STM32, refer to Help menu of SW4STM32 "Micro Processor Unit (MPU) Family - MCU support "

9 Test the firmware[edit]

The OpenAMP_TTY_echo firmware do the following:

  • CPU2(CM4) initialize OPenAMP MW which initializes/configures IPCC peripheral through HAL and setup openamp-rpmsg framework infrastructure
  • CPU2(CM4) creates 2 rpmsg channels for 2 virtual UART instances UART0 and UART1
  • CPU2(CM4) is waiting for messages from CPU1(CA7) on these both channels
  • When CPU2(CM4) receives a message on 1 Virtual UART instance/rpmsg channel, it sends the message back to CPU1(CA7) on the same Virtual UART instance

If you have used SW4STM32 to load and start the firmware you should reopen the serial console.

  • Initialize the ttyRPMSG0 configuration
 stty -onlcr -echo -F /dev/ttyRPMSG0
  • Read constantly the ttyRPMSG0 channel in background
 cat /dev/ttyRPMSG0 &
  • Send a message on one ttyRPMSG0 channel and recieve the echo on the same ttyRPMSG0 channel
 echo "Hello Virtual UART0" > /dev/ttyRPMSG0
Hello Virtual UART0
  • You can perform the same steps with the ttyRPMSG1 channel


  • After playing a while you can stop the firmware
 echo stop > /sys/class/remoteproc/remoteproc0/state
  • If using SW4STM32 just terminate the debug session

10 Modify the firmware[edit]

The original firmware example receives a message for the host on one channel end sent back the same message to the host on the same channel.
As this is not so obvious on which channel the message is received, we propose to modify the firmware in order to add an indication to know what is the channel that is receiving the message.
Please modify main.c original code as follow:

File:SW4STM32 workspace project modification.png
SW4STM32 main.c file modification
  /* Infinite loop */
  /* USER CODE BEGIN WHILE */
  while (1)
  {

    OPENAMP_check_for_message();

    /* USER CODE END WHILE */
    if (VirtUart0RxMsg) {
      char msg_to_transmit[MAX_BUFFER_SIZE];
      int msg_size = 0;
      VirtUart0RxMsg = RESET;

      msg_size = snprintf(msg_to_transmit, MAX_BUFFER_SIZE, "Channel RPMSG0: ");
      msg_size += snprintf(msg_to_transmit + msg_size, MAX_BUFFER_SIZE, "%s\n", VirtUart0ChannelBuffRx);
      log_info("size of the message to transmit = %d bytes\n", msg_size);
      VIRT_UART_Transmit(&huart0, (uint8_t*)msg_to_transmit, msg_size);
    }

    if (VirtUart1RxMsg) {
      char msg_to_transmit[MAX_BUFFER_SIZE];
      uint16_t msg_size = 0;
      VirtUart1RxMsg = RESET;

      msg_size = snprintf(msg_to_transmit, MAX_BUFFER_SIZE, "Channel RPMSG1: ");
      msg_size += snprintf(msg_to_transmit + msg_size, MAX_BUFFER_SIZE, "%s\n", VirtUart1ChannelBuffRx);
      log_info("size of the message to transmit = %d bytes\n", msg_size);
      VIRT_UART_Transmit(&huart1, (uint8_t*)msg_to_transmit, msg_size);
    }
    /* USER CODE BEGIN 3 */
  }
  /* USER CODE END 3 */
  • Save your modifications

11 Rebuild, reload and test the modified firmware[edit]

11.1 Rebuild[edit]

  • Click the build button (the little hammer in the toolbar)
  • Wait the end of the build

11.2 Reload though Linux console[edit]

  • If you are using STM32MP157C-DK2 Discovery kit
 cd $HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v1.0.0/Developer-Package/STM32Cube_FW_MP1_V1.0.0/Projects/STM32MP157C-DK2/Applications/OpenAMP/OpenAMP_TTY_echo/SW4STM32/OpenAMP_TTY_echo/
  • If you are using STM32MP157x-EV1 Evaluation board
 cd $HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v1.0.0/Developer-Package/STM32Cube_FW_MP1_V1.0.0/Projects/STM32MP157C-EV1/Applications/OpenAMP/OpenAMP_TTY_echo/SW4STM32/OpenAMP_TTY_echo/
  • Upload your firmware example into the board
 scp Debug/OpenAMP_TTY_echo.elf root@<board ip address>:/lib/firmware

11.3 Start through Linux console[edit]

  • Verify that no firmware is currently running
 cat /sys/class/remoteproc/remoteproc0/state
offline

If "offline" is displayed, that means that no firmware is currently running. If "running" is displayed, a firmware is currently running. You should then stop it using the following command:

 echo stop > /sys/class/remoteproc/remoteproc0/state
  • Set the firmware name to be executed
 echo -n OpenAMP_TTY_echo.elf > /sys/class/remoteproc/remoteproc0/firmware
  • Start the firmware
 echo start > /sys/class/remoteproc/remoteproc0/state
  • Verify that the firmware is runnig
 cat /sys/class/remoteproc/remoteproc0/state
running

11.4 Reload and start with SW4STM32[edit]

Just relaunch the debug session but reply "No" to following popup in order to force load of the updated firmware.

File:Force Load of the updated binary.png
Force Load of the updated firmware

11.5 Test[edit]

  • Initialize the ttyRPMSG0 and ttyRPMSG1 configurations
 stty -onlcr -echo -F /dev/ttyRPMSG0
 stty -onlcr -echo -F /dev/ttyRPMSG1
  • Read constantly the ttyRPMSG0 and ttyRPMSG1 channels in background
 cat /dev/ttyRPMSG0 &
 cat /dev/ttyRPMSG1 &
  • Send a message on one ttyRPMSG0 channel and check the echo log
 echo "Hello Virtual UART0" > /dev/ttyRPMSG0
Channel RPMSG0: Hello Virtual UART0
  • Send a message on one ttyRPMSG1 channel and check the echo log
 echo "Hello Virtual UART1" > /dev/ttyRPMSG1
Channel RPMSG1: Hello Virtual UART1


Info white.png Information
When the firmware is running, you can output log from the firmware by using the following command:
cat /sys/kernel/debug/remoteproc/remoteproc0/trace0


  • After playing a while you can stop the firmware
 echo stop > /sys/class/remoteproc/remoteproc0/state
  • For SW4STM32, just terminate the debug session
<noinclude>

{{ArticleMainWriter | VincentA}}
[[Category:Sub-articles]]
__NOTOC__</noinclude>


==Overview==
This stage explains how to modify, rebuild and reload a STM32MP1 Arm® Cortex®-M4 coprocessor firmware.

It proposes to customize the STM32MP1 Cube Package Application example OpenAMP_TTY_Echo using the MPU feature integrated in SW4STM32 IDE.

==Open SW4STM32 IDE==
* Open System Workbench for STM32 IDE
[[File: SW4STM32_workspace.png|thumb|upright=2|center|link=|SW4STM32 workspace]]

==Connect a console to the board ==

* It's very convenient to use the serial console integrated in SW4STM32  
[[File: SW4STM32_workspace_serial_disconnect_1.png|thumb|upright=2|center|link=|SW4STM32 Open the serial device by clicking this item]]

* Connection is ok if you can see Linux log or prompt. 
[[File: SW4STM32_workspace_serial_disconnect_2.png|thumb|upright=2|center|link=|SW4STM32 Serial Consol is ready ]]

* If for personal reason you prefer using another terminal ( ssh, minicom), it's then recommended to stop the Target Status Widget using the Serial port in SW4STM32 by right click on the bottom right corner then stop 

[[File:Stop Serial widget zoom.png|thumb|upright=2|center|link=Stop the Target Status Widget]]

* It will avoid the following repetitive pattern in your Linux console<pre>

root@stm32mp1:~# ifconfig; echo __END__:$?
eth0      Link encap:Ethernet  HWaddr 00:80:E1:42:45:69  
          inet addr:10.48.1.143  Bcast:10.48.3.255  Mask:255.255.252.0
          inet6 addr: fe80::280:e1ff:fe42:4569/64 Scope:Link
          UP BROADCAST RUNNING MULTICAST  MTU:1500  Metric:1
          RX packets:37 errors:0 dropped:1 overruns:0 frame:0
          TX packets:26 errors:0 dropped:0 overruns:0 carrier:0
          collisions:0 txqueuelen:1000 
          RX bytes:5776 (5.6 KiB)  TX bytes:3146 (3.0 KiB)
          Interrupt:63 Base address:0xc000 

lo        Link encap:Local Loopback  
          inet addr:127.0.0.1  Mask:255.0.0.0
          inet6 addr: ::1/128 Scope:Host
          UP LOOPBACK RUNNING  MTU:65536  Metric:1
          RX packets:344 errors:0 dropped:0 overruns:0 frame:0
          TX packets:344 errors:0 dropped:0 overruns:0 carrier:0
          collisions:0 txqueuelen:1000 
          RX bytes:22880 (22.3 KiB)  TX bytes:22880 (22.3 KiB)

usb0      Link encap:Ethernet  HWaddr 4A:06:6C:16:19:EC  
          inet addr:192.168.7.2  Bcast:192.168.7.255  Mask:255.255.255.0
          inet6 addr: fe80::4806:6cff:fe16:19ec/64 Scope:Link
          UP BROADCAST RUNNING MULTICAST  MTU:1500  Metric:1
          RX packets:0 errors:0 dropped:0 overruns:0 frame:0
          TX packets:396 errors:0 dropped:0 overruns:0 carrier:0
          collisions:0 txqueuelen:1000 
          RX bytes:0 (0.0 B)  TX bytes:115397 (112.6 KiB)

__END__:0</pre>


==Import an existing example in SW4STM32 IDE==
* Open the import screen  '''File > Import...''' and select '''Existing Project into Workspace''' 
[[File: SW4STM32_import.png|thumb|upright=2|center|link=|SW4STM32 import screen]]
* Browse and select '''OpenAMP_TTY_echo''' application example
:* If you are using STM32MP157C-DK2 Discovery kit
::'''$HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v1.0.0/Developer-Package/STM32Cube_FW_MP1_V1.0.0/Projects/STM32MP157C-DK2/Applications/OpenAMP/OpenAMP_TTY_echo'''
:* If you are using STM32MP157x-EV1 Evaluation board
::'''$HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v1.0.0/Developer-Package/STM32Cube_FW_MP1_V1.0.0/Projects/STM32MP157C-EV1/Applications/OpenAMP/OpenAMP_TTY_echo'''
* Click finish
* The '''OpenAMP_TTY_echo''' project is open and you can browse inside using the left pan
[[File: SW4STM32_workspace_project_open.png|thumb|upright=2|center|link=|SW4STM32 workspace with project open]]

==Build the firmware==
* Click the build button (the little hammer in the toolbar)
[[File: SW4STM32_workspace_project_build.png|thumb|upright=2|center|link=|SW4STM32 build the project]]

* Build is finished with no error
[[File: SW4STM32_workspace_project_build_finished.png|thumb|upright=2|center|link=|SW4STM32 build finished with no error]]

==Upload the firmware through Linux console ==
* If you are using STM32MP157C-DK2 Discovery kit
 {{PC$}} cd $HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v1.0.0/Developer-Package/STM32Cube_FW_MP1_V1.0.0/Projects/STM32MP157C-DK2/Applications/OpenAMP/OpenAMP_TTY_echo/SW4STM32/OpenAMP_TTY_echo/
* If you are using STM32MP157x-EV1 Evaluation board
 {{PC$}} cd $HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v1.0.0/Developer-Package/STM32Cube_FW_MP1_V1.0.0/Projects/STM32MP157C-EV1/Applications/OpenAMP/OpenAMP_TTY_echo/SW4STM32/OpenAMP_TTY_echo/
* Upload your firmware example into the board
 {{PC$}} scp Debug/OpenAMP_TTY_echo.elf root@<board ip address>:/lib/firmware

==Start the firmware through Linux console ==
* Verify that no firmware is currently runnig
 {{Board$}} cat /sys/class/remoteproc/remoteproc0/state
 offline
If offline is displayed, that means that no firmware is currently running. If running is displayed, a firmware is currently running. You shoul then stop it using the following command
 {{Board$}} echo stop > /sys/class/remoteproc/remoteproc0/state
* Set the firmware name to be executed
 {{Board$}} echo -n OpenAMP_TTY_echo.elf > /sys/class/remoteproc/remoteproc0/firmware
* Start the firmware
 {{Board$}} echo start > /sys/class/remoteproc/remoteproc0/state
* Verify that the firmware is runnig
 {{Board$}} cat /sys/class/remoteproc/remoteproc0/state
 running

== Upload and start the firmware with SW4STM32 ==

Thanks to the STM32-CoPro-MPU which complete SW4STM32 from version 2.8.0, SW4STM32 can manage to load and start a STM32MP1 Arm® Cortex®-M4 coprocessor firmware. 

For doing so open the Debug Configuration ot the OpenAMP_TTY_echo and select "Thru Linux core (Production mode) 

The inet Address of the board should be already filled. Else try to update it thanks to the button on the right

[[File:SW4STM32 Production Mode.png|thumb|upright=42|center|link=|Select Production mode in Startup pane of Debug Configuration]]

When configuration is ok the "Debug" button on the bottom right turn to active and you can launch the debug session. 

The Debug in Production Mode adds the cortex-M firmware transfer to the embedded Linux. This means also in case of network usage some specific pop-up appearing: 

* the SSH Password is to complete: the default one is root.

[[File:DebugCfg-Launch-PM-EnterPwd.png|thumb|upright=2|center|link=|SSH password popup]]

* the RSA key is to be approved. 

[[File:DebugCfg-Launch-PM-RSA.png|thumb|upright=2|center|link=|RSA key popup]]

After download of the firmware SW4STM32 will start it and switch into Debug Perspective. You can then use all features of the debugger. 

For further information and support on new MPU feature in SW4STM32, refer to Help menu of SW4STM32 "Micro Processor Unit (MPU) Family - MCU support "

==Test the firmware==
The OpenAMP_TTY_echo firmware do the following:
*CPU2(CM4) initialize OPenAMP MW which initializes/configures IPCC peripheral through HAL and setup openamp-rpmsg framework infrastructure
*CPU2(CM4) creates 2 rpmsg channels for 2 virtual UART instances UART0 and UART1
*CPU2(CM4) is waiting for messages from CPU1(CA7) on these both channels
*When CPU2(CM4) receives a message on 1 Virtual UART instance/rpmsg channel, it sends the message back to CPU1(CA7) on the same Virtual UART instance

If you have used SW4STM32 to load and start the firmware you should reopen the serial console. 

* Initialize the ttyRPMSG0 configuration
 {{Board$}} stty -onlcr -echo -F /dev/ttyRPMSG0
* Read constantly the ttyRPMSG0 channel in background
 {{Board$}} cat /dev/ttyRPMSG0 &
* Send a message on one ttyRPMSG0 channel and recieve the echo on the same ttyRPMSG0 channel
 {{Board$}} echo "Hello Virtual UART0" > /dev/ttyRPMSG0
 Hello Virtual UART0
* You can perform the same steps with the ttyRPMSG1 channel

* After playing a while you can stop the firmware
 {{Board$}} echo stop > /sys/class/remoteproc/remoteproc0/state

* If using SW4STM32 just terminate the debug session

==Modify the firmware==
The original firmware example receives a message for the host on one channel end sent back the same message to the host on the same channel.<br>

As this is not so obvious on which channel the message is received, we propose to modify the firmware in order to add an indication to know what is the channel that is receiving the message.<br>

Please modify main.c original code as follow:
[[File: SW4STM32_workspace_project_modification.png|thumb|upright=2|center|link=|SW4STM32 main.c file modification]]

   /* Infinite loop */
   /* USER CODE BEGIN WHILE */
   while (1)
   {

     OPENAMP_check_for_message();

     /* USER CODE END WHILE */
     if (VirtUart0RxMsg) {
       {{highlight|char msg_to_transmit[MAX_BUFFER_SIZE];}}
       {{highlight|int msg_size &#61; 0;}}
       VirtUart0RxMsg = RESET;

       {{highlight|msg_size &#61; snprintf(msg_to_transmit, MAX_BUFFER_SIZE, "Channel RPMSG0: ");}}
       {{highlight|msg_size +&#61; snprintf(msg_to_transmit + msg_size, MAX_BUFFER_SIZE, "%s\n", VirtUart0ChannelBuffRx);}}
       {{highlight|log_info("size of the message to transmit &#61; %d bytes\n", msg_size);}}
       {{highlight|VIRT_UART_Transmit(&huart0, (uint8_t*)msg_to_transmit, msg_size);}}
     }

     if (VirtUart1RxMsg) {
       {{highlight|char msg_to_transmit[MAX_BUFFER_SIZE];}}
       {{highlight|uint16_t msg_size &#61; 0;}}
       VirtUart1RxMsg = RESET;

       {{highlight|msg_size &#61; snprintf(msg_to_transmit, MAX_BUFFER_SIZE, "Channel RPMSG1: ");}}
       {{highlight|msg_size +&#61; snprintf(msg_to_transmit + msg_size, MAX_BUFFER_SIZE, "%s\n", VirtUart1ChannelBuffRx);}}
       {{highlight|log_info("size of the message to transmit &#61; %d bytes\n", msg_size);}}
       {{highlight|VIRT_UART_Transmit(&huart1, (uint8_t*)msg_to_transmit, msg_size);}}
     }
     /* USER CODE BEGIN 3 */
   }
   /* USER CODE END 3 */

* Save your modifications

==Rebuild, reload and test the modified firmware==
===Rebuild===
* Click the build button (the little hammer in the toolbar)
* Wait the end of the build

===Reload though Linux console ===
* If you are using STM32MP157C-DK2 Discovery kit
 {{PC$}} cd $HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v1.0.0/Developer-Package/STM32Cube_FW_MP1_V1.0.0/Projects/STM32MP157C-DK2/Applications/OpenAMP/OpenAMP_TTY_echo/SW4STM32/OpenAMP_TTY_echo/
* If you are using STM32MP157x-EV1 Evaluation board
 {{PC$}} cd $HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v1.0.0/Developer-Package/STM32Cube_FW_MP1_V1.0.0/Projects/STM32MP157C-EV1/Applications/OpenAMP/OpenAMP_TTY_echo/SW4STM32/OpenAMP_TTY_echo/
* Upload your firmware example into the board
 {{PC$}} scp Debug/OpenAMP_TTY_echo.elf root@<board ip address>:/lib/firmware

===Start through Linux console ===
* Verify that no firmware is currently running
 {{Board$}} cat /sys/class/remoteproc/remoteproc0/state
 offline
If "offline" is displayed, that means that no firmware is currently running. If "running" is displayed, a firmware is currently running. You should then stop it using the following command:
 {{Board$}} echo stop > /sys/class/remoteproc/remoteproc0/state
* Set the firmware name to be executed
 {{Board$}} echo -n OpenAMP_TTY_echo.elf > /sys/class/remoteproc/remoteproc0/firmware
* Start the firmware
 {{Board$}} echo start > /sys/class/remoteproc/remoteproc0/state
* Verify that the firmware is runnig
 {{Board$}} cat /sys/class/remoteproc/remoteproc0/state
 running

===Reload and start with SW4STM32 ===

Just relaunch the debug session but reply "No" to following popup in order to force load of the updated firmware. 

[[File:Force Load of the updated binary.png|thumb|upright=2|center|link=|Force Load of the updated firmware]]

===Test===
* Initialize the ttyRPMSG0 and ttyRPMSG1 configurations
 {{Board$}} stty -onlcr -echo -F /dev/ttyRPMSG0
 {{Board$}} stty -onlcr -echo -F /dev/ttyRPMSG1
* Read constantly the ttyRPMSG0 and ttyRPMSG1 channels in background
 {{Board$}} cat /dev/ttyRPMSG0 &
 {{Board$}} cat /dev/ttyRPMSG1 &
* Send a message on one ttyRPMSG0 channel and check the echo log
 {{Board$}} echo "Hello Virtual UART0" > /dev/ttyRPMSG0
 Channel RPMSG0: Hello Virtual UART0
* Send a message on one ttyRPMSG1 channel and check the echo log
 {{Board$}} echo "Hello Virtual UART1" > /dev/ttyRPMSG1
 Channel RPMSG1: Hello Virtual UART1<br>

{{Info| When the firmware is running, you can output log from the firmware by using the following command:<br>
<pre>cat /sys/kernel/debug/remoteproc/remoteproc0/trace0</pre> }}<br>

* After playing a while you can stop the firmware
 {{Board$}} echo stop > /sys/class/remoteproc/remoteproc0/state

* For SW4STM32,  just terminate the debug session
Line 109: Line 109:
 
The inet Address of the board should be already filled. Else try to update it thanks to the button on the right
 
The inet Address of the board should be already filled. Else try to update it thanks to the button on the right
   
[[File:SW4STM32 Production Mode.png|thumb|upright=4|center|link=|Select Production mode in Startup pane of Debug Configuration]]
+
[[File:SW4STM32 Production Mode.png|thumb|upright=2|center|link=|Select Production mode in Startup pane of Debug Configuration]]
   
 
When configuration is ok the "Debug" button on the bottom right turn to active and you can launch the debug session.  
 
When configuration is ok the "Debug" button on the bottom right turn to active and you can launch the debug session.