Difference between revisions of "MMC overview"

[quality revision] [quality revision]
m
 

Template:ArticleMainWriter Template:ArticleApprovedVersion SUMMARY
The MMC (MultiMediaCard) / SD (secure digital) / SDIO (secure digital input/output) subsystem implements a standard Linux® host driver to interface with MMC / SD memory cards or SDIO cards.

1 Framework purpose[edit]

The purpose of this article is to introduce the MMC Linux® subsystem (MMC / SD) by:

  • providing general information
  • describing the main components/stakeholders

The SDIO is addressed in the WLAN overview.

2 System overview[edit]

MMC overview.png

2.1 Component description[edit]

  • User space applications handle file I/O management to view the card memory as a disk, whereas programs that perform raw I/O accesses see the memory as a block device[1].
  • VFS (Kernel space)

Virtual File System. Please refer to the VFS documentation [2].

  • MMC core/SD/MMC/SDIO (Kernel space)

The MMC core ensures compliance with MultiMediaCard (MMC)[3] / secure digital (SD)[4] / secure digital input/output (SDIO)[5].

  • SDMMC driver (Kernel space) / SDMMC (hardware)

The SDMMC driver handles:

  • the registers, the clock, the interrupt and the IDMA control.
  • the communications over the bus based on command/response and data transfers.

Please refer to the SDMMC internal peripheral.

2.2 API description[edit]

The MMC core handles the file system read/write calls.

3 Configuration[edit]

3.1 Kernel configuration[edit]

The MMC framework is activated by default in ST deliveries. If a specific configuration is needed, this section indicates how the MMC framework can be activated/inactivated in the kernel.

The MMC framework can be activated in the kernel configuration via Linux® Menuconfig tool: Menuconfig or how to configure kernel

[*] Device Drivers
    [*] MMC/SD/SDIO card support
        <*> HW reset support for eMMC
        <*> Simple HW reset support for MMC
        <*> MMC block device driver
            (16) Number of minors per block device
        ...
        <*> ARM AMBA Multimedia Card Interface support
        [*] STMicroelectronics STM32 SDMMC Controller

3.2 Device tree configuration[edit]

DT configuration can be done thanks to STM32CubeMX.

Please refer to the SDMMC device tree configuration.

4 How to use the framework[edit]

A file system, which handles read/write/erase operations, can be used with the MMC framework. Please refer to the EXT4 support through MMC.


5 How to trace and debug the framework[edit]

5.1 How to monitor[edit]

The sysfs interface provides detailed information on each mmc device:

root:~# cat /sys/kernel/debug/mmc0/ios
clock:          50000000 Hz
vdd:            21 (3.3 ~ 3.4 V)
bus mode:       2 (push-pull)
chip select:    0 (don't care)
power mode:     2 (on)
bus width:      2 (4 bits)
timing spec:    2 (sd high-speed)
signal voltage: 0 (3.30 V)
driver type:    0 (driver type B)

5.2 How to trace[edit]

For details on dynamic trace usage, refer to How to use the kernel dynamic debug.

root:~# echo "file drivers/mmc/* +p" > /sys/kernel/debug/dynamic_debug/control

6 Source code location[edit]

The MMC framework is available here .

7 References[edit]

Please refer to the following links for a full description of the MMC framework:

  1. https://en.wikipedia.org/wiki/Device_file#Block_devices
  2. VFS
  3. MultiMediaCard, embedded MultiMediaCard specification
  4. Secure Digital, secure digital specification
  5. Secure Digital Input Output, Secure Digital Input Output specification



<noinclude>

{{ArticleBasedOnModel | [[Framework overview article model]]}}
{{ArticleMainWriter | LudovicB}}
{{ArticleApprovedVersion | LudovicB | GeraldB, ChristopheK (Passed, 18Oct'18) | No previous approved version | AnneJ - 24Oct'18 - 9413 | 25Oct'18}}

[[Category:Mass storage]]</noinclude>


''''''SUMMARY '''<br>

The MMC (MultiMediaCard) / SD (secure digital) / SDIO (secure digital input/output) subsystem implements a standard Linux<sup>&reg;</sup> host driver to interface with MMC / SD memory cards or SDIO cards.

== Framework purpose ==
The purpose of this article is to introduce the MMC Linux<sup>&reg;</sup> subsystem (MMC / SD) by: 
* providing general information
* describing the main components/stakeholders

The SDIO is addressed in the [[WLAN_overview|WLAN overview]].

==System overview==

[[File:MMC_overview.png|center|link=]]

===Component description===
* User space applications handle '''file I/O''' management to view the card memory as a disk, whereas programs that perform '''raw I/O''' accesses see the memory as a block device<ref>https://en.wikipedia.org/wiki/Device_file#Block_devices</ref>.

* '''VFS''' (Kernel space)
Virtual File System. Please refer to the VFS documentation <ref>{{CodeSource | Linux kernel | Documentation/filesystems/vfs.txt | VFS}} </ref>.

* '''MMC core/SD/MMC/SDIO''' (Kernel space)
The '''MMC core''' ensures compliance with MultiMediaCard ('''MMC''')<ref>[https://www.jedec.org/standards-documents/technology-focus-areas/flash-memory-ssds-ufs-emmc/e-mmc MultiMediaCard], embedded MultiMediaCard specification</ref> / secure digital ('''SD''')<ref>[https://www.sdcard.org/ Secure Digital], secure digital specification</ref> / secure digital input/output ('''SDIO''')<ref>[https://www.sdcard.org/ Secure Digital Input Output], Secure Digital Input Output specification</ref>.

* '''SDMMC driver''' (Kernel space) / '''SDMMC''' (hardware) 
The '''SDMMC driver''' handles:
* the registers, the clock, the interrupt and the IDMA control.
* the communications over the bus based on command/response and data transfers.
Please refer to the [[SDMMC internal peripheral]].

===API description===
The MMC core handles the file system read/write calls.

==Configuration ==
===Kernel configuration===
The MMC framework is activated by default in ST deliveries. If a specific configuration is needed, this section indicates how the MMC framework can be activated/inactivated in the kernel.

The MMC framework can be activated in the kernel configuration via Linux<sup>&reg;</sup> Menuconfig tool: [[Menuconfig or how to configure kernel]]
<pre>

[*] Device Drivers
    [*] MMC/SD/SDIO card support<*> HW reset support for eMMC<*> Simple HW reset support for MMC<*> MMC block device driver
            (16) Number of minors per block device
        ...<*> ARM AMBA Multimedia Card Interface support
        [*] STMicroelectronics STM32 SDMMC Controller</pre>


===Device tree configuration===
DT configuration can be done thanks to [[STM32CubeMX]].

Please refer to the [[SDMMC_device_tree_configuration| SDMMC device tree configuration]].

==How to use the framework==
A file system, which handles read/write/erase operations, can be used with the MMC framework. Please refer to the [[How to support EXT4 through MMC|EXT4 support through MMC]].

==How to trace and debug the framework==

===How to monitor===
The sysfs interface provides detailed information on each mmc device:
<pre>

root:~# cat /sys/kernel/debug/mmc0/ios
clock:          50000000 Hz
vdd:            21 (3.3 ~ 3.4 V)
bus mode:       2 (push-pull)
chip select:    0 (don't care)
power mode:     2 (on)
bus width:      2 (4 bits)
timing spec:    2 (sd high-speed)
signal voltage: 0 (3.30 V)
driver type:    0 (driver type B)</pre>


===How to trace===
For details on dynamic trace usage, refer to [[How to use the kernel dynamic debug]].

root:~# echo "file drivers/mmc/* +p" > /sys/kernel/debug/dynamic_debug/control

==Source code location==
The MMC framework is available {{CodeSource | Linux kernel | drivers/mmc  | here}}.

==References==
Please refer to the following links for a full description of the MMC framework:
<references />

<noinclude>

{{ArticleBasedOnModel | Framework overview article model}}
[[Category:Mass storage]]</noinclude>
Line 1: Line 1:
<noinclude>
 
{{ArticleBasedOnModel | [[Framework overview article model]]}}
 
{{ArticleMainWriter | LudovicB}}
 
{{ArticleApprovedVersion | LudovicB | GeraldB, ChristopheK (Passed, 18Oct'18) | No previous approved version | AnneJ - 24Oct'18 - 9413 | 25Oct'18}}
 
 
[[Category:Mass storage]]
 
</noinclude>
 
 
 
'''SUMMARY '''<br>
 
'''SUMMARY '''<br>
 
The MMC (MultiMediaCard) / SD (secure digital) / SDIO (secure digital input/output) subsystem implements a standard Linux<sup>&reg;</sup> host driver to interface with MMC / SD memory cards or SDIO cards.
 
The MMC (MultiMediaCard) / SD (secure digital) / SDIO (secure digital input/output) subsystem implements a standard Linux<sup>&reg;</sup> host driver to interface with MMC / SD memory cards or SDIO cards.
Line 96: Line 88:
   
 
<references />
 
<references />
  +
  +
<noinclude>
  +
{{ArticleBasedOnModel | Framework overview article model}}
  +
[[Category:Mass storage]]
  +
</noinclude>