Difference between revisions of "MDMA device tree configuration"
[quality revision] | [quality revision] |
m
|
m (→DT bindings documentation)
|
Contents
1 Article purpose[edit]
This article explains how to configure the MDMA internal peripheral when it is assigned to the Linux® OS. In that case, it is controlled by the Dmaengine overview.
The configuration is performed using the Device tree mechanism that provides a hardware description of the MDMA internal peripheral, used by the STM32 MDMA Linux driver and by the DMA framework.
Hardware description is a combination of:
- STM32 MDMA peripheral
- and STM32 MDMA client
2 DT bindings documentation[edit]
Complete device tree bindings can be found at this location: [1].
3 DT configuration[edit]
This hardware description is a combination of the STM32 microprocessor device tree files (.dtsi extension) and board device tree files (.dts extension). See the Device tree for an explanation of the device tree file split.
STM32CubeMX can be used to generate the board device tree. Refer to How to configure the DT using STM32CubeMX for more details.
3.1 DT configuration (STM32 level)[edit]
At device level, MDMA declared is declared as follows:
mdma1: dma@58000000 {
compatible = "st,stm32h7-mdma";
reg = <0x58000000 0x1000>;
interrupts = <GIC_SPI 122 IRQ_TYPE_LEVEL_HIGH>;
clocks = <&rcc MDMA>;
resets = <&scmi0_reset RST_SCMI0_MDMA>;
#dma-cells = <6>;
dma-channels = <32>;
dma-requests = <48>;
};
The DTS file is located Under under arch/arm/boot/dts/stm32mp157cstm32mp151.dtsi .
![]() |
This device tree part is related to STM32 microprocessors. It must be kept as is, without being modified by the end-user. |
3.2 DT configuration (board level)[edit]
No board device tree configuration is required.
The whole configuration remains at STM32 level.
4 How to configure the DT using STM32CubeMX[edit]
The STM32CubeMX tool can be used to configure the STM32MPU device and get the corresponding platform configuration device tree files.
The STM32CubeMX may not support all the properties described in the above DT bindings documentation paragraph. If so, the tool inserts user sections in the generated device tree. These sections can then be edited to add some properties and they are preserved from one generation to another. Refer to STM32CubeMX user manual for further information.
5 References[edit]
Please refer to the following links for additional information:
== Article purpose == This article explains how to configure the [[MDMA internal peripheral]] when it is assigned to the Linux<sup>®</sup> OS. In that case, it is controlled by the [[Dmaengine overview]]. The configuration is performed using the [[Device tree]] mechanism that provides a hardware description of the [[MDMA internal peripheral]], used by the STM32 MDMA Linux driver and by the [[Dmaengine overview|DMA framework]]. Hardware description is a combination of: * STM32 MDMA peripheral * and STM32 MDMA client == DT bindings documentation == Complete device tree bindings can be found at this location: <ref>{{CodeSource | Linux kernel | Documentation/devicetree/bindings/dma/st,stm32-mdma.txtyaml}}</ref>. == DT configuration == This hardware description is a combination of the '''STM32 microprocessor''' device tree files (''.dtsi'' extension) and '''board''' device tree files (''.dts'' extension). See the [[Device tree]] for an explanation of the device tree file split. '''STM32CubeMX''' can be used to generate the board device tree. Refer to [[#How_to_configure_the_DT_using_STM32CubeMX|How to configure the DT using STM32CubeMX]] for more details. ===DT configuration (STM32 level) === At device level, MDMA declared is declared as follows: <pre> mdma1: dma@58000000 { compatible = "st,stm32h7-mdma"; reg = <0x58000000 0x1000>; interrupts = <GIC_SPI 122 IRQ_TYPE_LEVEL_HIGH>; clocks = <&rcc MDMA>;resets = <&scmi0_reset RST_SCMI0_MDMA>;#dma-cells = <6>; dma-channels = <32>; dma-requests = <48>; };</pre> The DTS file is located Underunder {{CodeSource | Linux kernel | arch/arm/boot/dts/stm32mp157cstm32mp151.dtsi}}. {{Warning|This device tree part is related to STM32 microprocessors. It must be kept as is, without being modified by the end-user.}} === DT configuration (board level) === No board device tree configuration is required.<br> The whole configuration remains at STM32 level. ==How to configure the DT using STM32CubeMX== The [[STM32CubeMX]] tool can be used to configure the STM32MPU device and get the corresponding [[Device_tree#STM32|platform configuration device tree]] files.<br /> The STM32CubeMX may not support all the properties described in the above [[#DT bindings documentation|DT bindings documentation]] paragraph. If so, the tool inserts '''user sections''' in the generated device tree. These sections can then be edited to add some properties and they are preserved from one generation to another. Refer to [[STM32CubeMX]] user manual for further information. ==References== Please refer to the following links for additional information: <references /> <noinclude> [[Category:Device tree configuration]] [[Category:DMA]] {{ArticleBasedOnModel | Peripheral or framework device tree configuration model}} {{PublicationRequestId | 9468 | 2018-10-31 | AnneJ}}</noinclude>
(3 intermediate revisions by the same user not shown) | |||
Line 9: | Line 9: | ||
== DT bindings documentation == |
== DT bindings documentation == |
||
− | Complete device tree bindings can be found at this location: <ref>{{CodeSource | Linux kernel | Documentation/devicetree/bindings/dma/stm32-mdma. |
+ | Complete device tree bindings can be found at this location: <ref>{{CodeSource | Linux kernel | Documentation/devicetree/bindings/dma/st,stm32-mdma.yaml}}</ref>. |
== DT configuration == |
== DT configuration == |
||
Line 17: | Line 17: | ||
===DT configuration (STM32 level) === |
===DT configuration (STM32 level) === |
||
− | At device level, MDMA |
+ | At device level, MDMA is declared as follows: |
<pre> |
<pre> |
||
Line 25: | Line 25: | ||
interrupts = <GIC_SPI 122 IRQ_TYPE_LEVEL_HIGH>; |
interrupts = <GIC_SPI 122 IRQ_TYPE_LEVEL_HIGH>; |
||
clocks = <&rcc MDMA>; |
clocks = <&rcc MDMA>; |
||
+ | resets = <&scmi0_reset RST_SCMI0_MDMA>; |
||
#dma-cells = <6>; |
#dma-cells = <6>; |
||
dma-channels = <32>; |
dma-channels = <32>; |
||
Line 31: | Line 32: | ||
</pre> |
</pre> |
||
− | The DTS file is located |
+ | The DTS file is located under {{CodeSource | Linux kernel | arch/arm/boot/dts/stm32mp151.dtsi}}. |
{{Warning|This device tree part is related to STM32 microprocessors. It must be kept as is, without being modified by the end-user.}} |
{{Warning|This device tree part is related to STM32 microprocessors. It must be kept as is, without being modified by the end-user.}} |