Difference between revisions of "MB1272"

[quality revision] [quality revision]
m
m ([PFU]added internal information on backup battery usable for Discovery)

Template:ArticleApprovedVersion


1 Board overview[edit]

MB1272 motherboard STM32MP157x 12x12 with PMIC and DDR3, revision C-0.1: part of the STM32MP157x-DKx Discovery kit

Note that:

  • MB1272 for STM32MP157A-DK1 Discovery kit doesn't include the "WLAN + Bluetooth" component (muRata LBEE5KL1DX)
  • MB1272 for STM32MP157C-DK2 Discovery kit includes the "WLAN + Bluetooth" component (Murata LBEE5KL1DX)


GPIO expansion WLAN + Bluetooth (muRata LBEE5KL1DX): only for STM32MP157C-DK2 Discovery kit Backup battery connector DSI LCD connector PMIC (STPMIC1A) DDR3L 16 bits USB type A LED (red LD1) 4 x USB type A (host) USB type C (power 5V-3A) Power LED (green LD2) STM32MP157x 12x12 HDMI USB type C (DRP) Ethernet Ethernet LED (green LD3) Wakeup button Audio codec headset Audio codec (Cirrus CS42L51) Reset button User LED (green LD5) User button (USER1) User LED (red LD6) User button (USER2) User LED (orange LD7) User LED (blue LD8) USB micro-B (ST-LINK/V2-1) ST-LINK/V2-1 LED (bicolor LD4) ST-LINK/V2-1 DFU HDMI connector
MB1272 front side (picture not contractual)

Details of some LEDs:

  • LD1: red if USB type A connection established
  • LD2: green if power connection established
  • LD3: green flashing the Ethernet connection established
  • LD4: red flashing if ST-LINK/V2-1 connection not established, else green
  • LD5, LD6, LD7, LD8: some user LEDs are used to reflect the system activity, whereas the others are left free and can be directly used by the application, as explained in the LEDs and buttons on STM32 MPU boards article


Arduino Uno connector (part 1) Arduino LED (green LD9) MicroSD 3.0 card Boot mode selection Arduino Uno connector (part 2)
MB1272 back side (picture is not contractual)

2 Links[edit]

MB1272 schematics

<noinclude>

{{ArticleApprovedVersion | Jean-ChristopheT | BernardP  | No previous approved version | PhilipS - 12Sep'18 - 8421| 17Sep'18}} 
[[Category:STM32MP15 Discovery kits]]
[[Category:STM32MP15]]
[[Category:ST boards]]</noinclude>


== Board overview ==
'''MB1272 motherboard STM32MP157x 12x12 with PMIC and DDR3''', revision C-0.1: part of the STM32MP157x-DKx Discovery kit

Note that:
* MB1272 for STM32MP157A-'''DK1''' Discovery kit doesn't include the  "WLAN + Bluetooth" component (muRata LBEE5KL1DX)
* MB1272 for STM32MP157C-'''DK2''' Discovery kit includes the  "WLAN + Bluetooth" component (Murata LBEE5KL1DX)

{{
ImageMap|Image:MB1272_front_side.png {{!}} thumb{{!}} 800px {{!}} center{{!}} MB1272 front side (picture not contractual)
rect 322 48 814 130 [[#GPIO | GPIO expansion]]
rect 80 243 151 310 [[#WLAN BT | WLAN + Bluetooth (muRata LBEE5KL1DX): only for STM32MP157C-DK2 Discovery kit]]
rect 238 130 322 193 [[#Battery | Backup battery connector]]
rect 238 193 322 454 [[#DSI | DSI LCD connector]]
rect 343 158 425 237 [[#PMIC | PMIC (STPMIC1A)]]
rect 511 177 592 330 [[#DDR3L | DDR3L 16 bits]]
rect 639 274 678 318 [[#LD1 | USB type A LED (red LD1)]]
poly 1081 24 814 24 814 130 678 130 678 338 831 338 831 381 1081 381 [[#USB type A | 4 x USB type A (host)]]
rect 46 380 172 479 [[#USB power | USB type C (power 5V-3A)]]
rect 132 342 204 380 [[#LD2 | Power LED (green LD2)]]
rect 496 350 607 485 [[#STM32MP157 | STM32MP157x 12x12]]
rect 704 390 814 517 [[#HDMI | HDMI]]
poly 1081 381 831 381 831 338 764 338 764 390 812 391 814 517 1081 517 [[#USB type C | USB type C (DRP)]]
poly 383 479 12 479 12 690 250 690 250 557 383 557 [[#Ethernet | Ethernet]]
rect 172 434 216 488 [[#LD3 | Ethernet LED (green LD3)]]
rect 250 642 322 758 [[#Wakeup button | Wakeup button]]
rect 338 557 447 758 [[#Headset | Audio codec headset]]
rect 467 557 523 626 [[#udio codec | Audio codec (Cirrus CS42L51)]]
rect 473 642 512 758 [[#Reset button | Reset button]]
rect 512 626 547 699 [[#User LEDs | User LED (green LD5)]]
rect 547 642 587 758 [[#User button B3 | User button (USER1)]]
rect 587 626 624 699 [[#User LEDs | User LED (red LD6)]]
rect 624 642 662 758 [[#User button B4 | User button (USER2)]]
rect 662 626 699 699 [[#User LEDs | User LED (orange LD7)]]
rect 699 662 735 734 [[#User LEDs | User LED (blue LD8)]]
poly 839 535 699 535 699 631 753 631 753 733 839 735 [[#ST-LINK USB | USB micro-B (ST-LINK/V2-1)]]
rect 839 576 890 662 [[#LD4 | ST-LINK/V2-1 LED (bicolor LD4)]]
rect 839 673 951 720 [[#ST-LINK DFU | ST-LINK/V2-1 DFU]]
rect 951 533 1081 700 [[#HDMI connector | HDMI connector]]
}}{{InternalInfo|CN3 could be used to connect a CR2032 lithium battery, wired on a Molex Picoblade 2 circuits pitch 1.25mm type 51021-0200  (1-VBAT, 2-GND).<br/>Like Thinkpad 02K6541, 02K6572, 02K7075, 02K7087, 08K8050, 92P0986, 92P0991 models. }}

Details of some LEDs:
* <span id="LD1">LD1</span>: red if USB type A connection established
* <span id="LD2">LD2</span>: green if power connection established
* <span id="LD3">LD3</span>: green flashing the Ethernet connection established
* <span id="LD4">LD4</span>: red flashing if ST-LINK/V2-1 connection not established, else green
* <span id="User LEDs">LD5, LD6, LD7, LD8</span>: some user LEDs are used to reflect the system activity, whereas the others are left free and can be directly used by the application, as explained in the [[LEDs and buttons on STM32 MPU boards]] article

{{
ImageMap|Image:MB1272_back_side.png {{!}} thumb{{!}} 800px {{!}} center{{!}} MB1272 back side (picture is not contractual)
rect 310 100 866 173 [[#Arduino1 | Arduino Uno connector (part 1)]]
rect 344 173 381 236 [[#LD9 | Arduino LED (green LD9)]]
rect 850 190 1091 386 [[#MicroSD | MicroSD 3.0 card]]
rect 46 531 124 720 [[#Boot | Boot mode selection]]
rect 420 548 836 674 [[#Arduino2 | Arduino Uno connector (part 2)]]
}}

== Links ==
[[STM32MP15 resources#MB1272 schematics|MB1272 schematics]]
Line 45: Line 45:
 
rect 951 533 1081 700 [[#HDMI connector | HDMI connector]]
 
rect 951 533 1081 700 [[#HDMI connector | HDMI connector]]
 
}}
 
}}
  +
{{InternalInfo|CN3 could be used to connect a CR2032 lithium battery, wired on a Molex Picoblade 2 circuits pitch 1.25mm type 51021-0200  (1-VBAT, 2-GND).<br/>Like Thinkpad 02K6541, 02K6572, 02K7075, 02K7087, 08K8050, 92P0986, 92P0991 models. }}
   
 
Details of some LEDs:
 
Details of some LEDs: