Difference between revisions of "LPTIM Linux driver"
[quality revision] | [quality revision] |
m
|
m
|
Contents
1 Article purpose[edit]
This article introduces the LPTIM Linux® driver for the LPTIM internal peripheral[1]:
- Which LPTIM features are supported by the driver
- How to configure, use and debug the driver
- What is the driver structure, and where the source code can be found.
2 Short description[edit]
The LPTIM[1] Linux driver (kernel space) is based on the PWM, IIO and IIO counter frameworks. It provides several functionalities:
MFD driver:
- handles common resources (registers, clock)
PWM driver:
- handles the PWM output channel (single channel)
IIO hardware trigger driver:
- handles hardware trigger sources (synchronously with PWM) for other internal peripherals such as ADC[2], DAC[3], DFSDM[4]
IIO counter Counter driver:
- handles the quadrature encoder interface[5] as well as the external event counter.
3 Configuration[edit]
3.1 Kernel configuration[edit]
Activate the LPTIM[1] Linux driver in the kernel configuration using the Linux Menuconfig tool: Menuconfig or how to configure kernel.
Enable the following configurations (as well as their dependencies):
- CONFIG_MFD_STM32_LPTIMER
- CONFIG_PWM_STM32_LP
- CONFIG_IIO_STM32_LPTIMER_TRIGGER
- CONFIG_STM32_LPTIMER_CNT
Device Drivers ---> -> Multifunction device drivers ---> <*> Support for STM32 lowLow-powerPower timerTimer -> Pulse-width modulation (PWM) support ---> <*> STMicroelectronics STM32 PWM LP -> Industrial I/O support ---> -> Triggers - standalone ---> <*> STM32 lowLow-powerPower timerTimer triggerTrigger -> CountersCounter support ---> <*> STM32 low-powerLP timerTimer encoder counter driver
3.2 Device tree[edit]
Refer to the LPTIM device tree configuration article when configuring the LPTIM Linux kernel driver.
4 How to use[edit]
How to use PWM with sysfs interface
How to set up a TIM or LPTIM trigger using the sysfs interface
How to use the quadrature encoder with the sysfs interface
5 How to trace and debug[edit]
The LPTIM Linux driver can access LPTIM registers through REGMAP.
It comes with debugfs[6] entries, which allow dumping registers:
$ cd /sys/kernel/debug/regmap $ ls 40004000.timer 40009000.timer $ cd 40009000.timer $ cat registers 000: 00000003 004: 00000000 008: 00000000 ...
It also comes with tracepoints[7]:
$ cd /sys/kernel/debug/tracing $ cat available_events | grep regmap ... regmap:regmap_reg_read regmap:regmap_reg_write
6 Source code location[edit]
The LPTIM Linux driver is composed of:
- stm32-lptimer.c driver to handle common resources, such as registers and clock.
- pwm-stm32-lp.c driver to handle PWM channel
- stm32-lptimer-trigger.c driver to handle trigger sources for other internal peripherals
- stm32-lptimer-cnt.c driver to handle quadrature encoder and external event counter
- include/linux/mfd/stm32-lptimer.h and include/linux/iio/timer/stm32-lptim-trigger.h header files
7 References[edit]
{{EcosystemFlow/Warning| flow=Current}} ==== Article purpose == This article introduces the LPTIM Linux<sup>®</sup> driver for the LPTIM internal peripheral<ref name="LPTIM internal peripheral">[[LPTIM internal peripheral]]</ref>: * Which LPTIM features are supported by the driver * How to configure, use and debug the driver * What is the driver structure, and where the source code can be found. {{ReviewsComments|-- [[User:Nathalie Sangouard|Nathalie Sangouard]] ([[User talk:Nathalie Sangouard|talk]]) 16:48, 13 November 2020 (CET)NathalieS , Fabrice G<br />Article to be updated to be compliant with ecosystem v2.1.0 (BZ 95795), some example on ''clock event'' must be added}} == Short description == The ''LPTIM''<ref name="LPTIM internal peripheral"/> Linux driver (kernel space) is based on the [[PWM overview|PWM]] and , [[IIO overview|IIO]] and <span style="color: {{STLightBlue}};">counter</span> frameworks. It provides several functionalities: '''MFD driver''': * handles common resources (registers, clock) '''PWM driver''': * handles the '''PWM output''' channel (single channel) '''IIO hardware trigger driver''': * handles hardware '''trigger sources''' (synchronously with PWM) for other internal peripherals such as ADC<ref name="adc_internal">[[ADC internal peripheral]]</ref>, DAC<ref name="dac_internal">[[DAC internal peripheral]]</ref>, DFSDM<ref name="dfsdm_internal">[[DFSDM internal peripheral]]</ref> '''IIO counter Counter driver''': * handles the '''quadrature encoder''' interface<ref name="quadrature_encoder">[https://en.wikipedia.org/wiki/Rotary_encoder#Incremental_encoder Incremental encoder overview]</ref> as well as the external event counter. == Configuration == === Kernel configuration === Activate the LPTIM<ref name="LPTIM internal peripheral"/> Linux driver in the kernel configuration using the Linux Menuconfig tool: [[Menuconfig or how to configure kernel]]. Enable the following configurations (as well as their dependencies): * CONFIG_MFD_STM32_LPTIMER * CONFIG_PWM_STM32_LP * CONFIG_IIO_STM32_LPTIMER_TRIGGER * CONFIG_STM32_LPTIMER_CNT<pre> Device Drivers ---> -> Multifunction device drivers ---><*> Support for STM32 low-power timerLow-Power Timer -> Pulse-width modulation (PWM) support ---><*> STMicroelectronics STM32 PWM LP -> Industrial I/O support ---> -> Triggers - standalone ---><*> STM32 low-power timer trigger -> Counters ---><*> STM32 low-power timerLow-Power Timer Trigger -> Counter support ---><*> STM32 LP Timer encoder counter driver</pre> === Device tree === Refer to the [[LPTIM device tree configuration]] article when configuring the LPTIM Linux kernel driver. == How to use == [[PWM_overview#How_to_use_PWM_with_sysfs_interface|How to use PWM with sysfs interface]] [[How to use the IIO user space interface#How to set up a TIM or LPTIM trigger using the sysfs interface|How to set up a TIM or LPTIM trigger using the sysfs interface]] [[How to use the IIO user space interface#How to use the quadrature encoder with the sysfs interface|How to use the quadrature encoder with the sysfs interface]] ==How to trace and debug== The LPTIM Linux driver can access LPTIM registers through REGMAP. It comes with debugfs<ref name="debugfs">[[Debugfs]]</ref> entries, which allow dumping registers: $ cd /sys/kernel/debug/regmap $ ls 40004000.timer 40009000.timer $ cd 40009000.timer $ cat registers 000: 00000003 004: 00000000 008: 00000000 ... It also comes with tracepoints<ref name="ftrace">[[Ftrace]]</ref>: $ cd /sys/kernel/debug/tracing $ cat available_events | grep regmap ... regmap:regmap_reg_read regmap:regmap_reg_write == Source code location == The LPTIM Linux driver is composed of: * {{CodeSource | Linux kernel | drivers/mfd/stm32-lptimer.c | stm32-lptimer.c driver}} to handle common resources, such as registers and clock. * {{CodeSource | Linux kernel | drivers/pwm/pwm-stm32-lp.c | pwm-stm32-lp.c driver}} to handle PWM channel * {{CodeSource | Linux kernel | drivers/iio/trigger/stm32-lptimer-trigger.c | stm32-lptimer-trigger.c driver}} to handle trigger sources for other internal peripherals * {{CodeSource | Linux kernel | drivers/iio/counter/stm32-lptimer-cnt.c | stm32-lptimer-cnt.c driver}} to handle quadrature encoder and external event counter * {{CodeSource | Linux kernel | include/linux/mfd/stm32-lptimer.h}} and {{CodeSource | Linux kernel | include/linux/iio/timer/stm32-lptim-trigger.h}} header files ==References==<references /> <noinclude> [[Category:Timers|1]] [[Category:IIO]] {{PublicationRequestId | 9230 | 2018-10-16 | AnneJ}} {{ArticleBasedOnModel | Linux driver article model}}</noinclude>
(2 intermediate revisions by 2 users not shown) | |||
Line 1: | Line 1: | ||
− | |||
== Article purpose == |
== Article purpose == |
||
This article introduces the LPTIM Linux<sup>®</sup> driver for the LPTIM internal peripheral<ref name="LPTIM internal peripheral">[[LPTIM internal peripheral]]</ref>: |
This article introduces the LPTIM Linux<sup>®</sup> driver for the LPTIM internal peripheral<ref name="LPTIM internal peripheral">[[LPTIM internal peripheral]]</ref>: |
||
Line 6: | Line 5: | ||
* What is the driver structure, and where the source code can be found. |
* What is the driver structure, and where the source code can be found. |
||
− | {{ReviewsComments|-- |
+ | {{ReviewsComments|-- NathalieS , Fabrice G<br />Article to be updated to be compliant with ecosystem v2.1.0 (BZ 95795), some example on ''clock event'' must be added}} |
== Short description == |
== Short description == |
||
− | The ''LPTIM''<ref name="LPTIM internal peripheral"/> Linux driver (kernel space) is based on the [[PWM overview|PWM]] |
+ | The ''LPTIM''<ref name="LPTIM internal peripheral"/> Linux driver (kernel space) is based on the [[PWM overview|PWM]], [[IIO overview|IIO]] and <span style="color: {{STLightBlue}};">counter</span> frameworks. It provides several functionalities: |
'''MFD driver''': |
'''MFD driver''': |
||
Line 17: | Line 16: | ||
'''IIO hardware trigger driver''': |
'''IIO hardware trigger driver''': |
||
* handles hardware '''trigger sources''' (synchronously with PWM) for other internal peripherals such as ADC<ref name="adc_internal">[[ADC internal peripheral]]</ref>, DAC<ref name="dac_internal">[[DAC internal peripheral]]</ref>, DFSDM<ref name="dfsdm_internal">[[DFSDM internal peripheral]]</ref> |
* handles hardware '''trigger sources''' (synchronously with PWM) for other internal peripherals such as ADC<ref name="adc_internal">[[ADC internal peripheral]]</ref>, DAC<ref name="dac_internal">[[DAC internal peripheral]]</ref>, DFSDM<ref name="dfsdm_internal">[[DFSDM internal peripheral]]</ref> |
||
− | ''' |
+ | '''Counter driver''': |
* handles the '''quadrature encoder''' interface<ref name="quadrature_encoder">[https://en.wikipedia.org/wiki/Rotary_encoder#Incremental_encoder Incremental encoder overview]</ref> as well as the external event counter. |
* handles the '''quadrature encoder''' interface<ref name="quadrature_encoder">[https://en.wikipedia.org/wiki/Rotary_encoder#Incremental_encoder Incremental encoder overview]</ref> as well as the external event counter. |
||
Line 32: | Line 31: | ||
Device Drivers ---> |
Device Drivers ---> |
||
-> Multifunction device drivers ---> |
-> Multifunction device drivers ---> |
||
− | <*> Support for STM32 |
+ | <*> Support for STM32 Low-Power Timer
|
-> Pulse-width modulation (PWM) support ---> |
-> Pulse-width modulation (PWM) support ---> |
||
<*> STMicroelectronics STM32 PWM LP |
<*> STMicroelectronics STM32 PWM LP |
||
-> Industrial I/O support ---> |
-> Industrial I/O support ---> |
||
-> Triggers - standalone ---> |
-> Triggers - standalone ---> |
||
− | <*> STM32 |
+ | <*> STM32 Low-Power Timer Trigger
|
− | + |
-> Counter support ---> |
|
− | + |
<*> STM32 LP Timer encoder counter driver |
|
</pre> |
</pre> |
||
Line 79: | Line 78: | ||
* {{CodeSource | Linux kernel | drivers/pwm/pwm-stm32-lp.c | pwm-stm32-lp.c driver}} to handle PWM channel |
* {{CodeSource | Linux kernel | drivers/pwm/pwm-stm32-lp.c | pwm-stm32-lp.c driver}} to handle PWM channel |
||
* {{CodeSource | Linux kernel | drivers/iio/trigger/stm32-lptimer-trigger.c | stm32-lptimer-trigger.c driver}} to handle trigger sources for other internal peripherals |
* {{CodeSource | Linux kernel | drivers/iio/trigger/stm32-lptimer-trigger.c | stm32-lptimer-trigger.c driver}} to handle trigger sources for other internal peripherals |
||
− | * {{CodeSource | Linux kernel | drivers |
+ | * {{CodeSource | Linux kernel | drivers/counter/stm32-lptimer-cnt.c | stm32-lptimer-cnt.c driver}} to handle quadrature encoder and external event counter |
* {{CodeSource | Linux kernel | include/linux/mfd/stm32-lptimer.h}} and {{CodeSource | Linux kernel | include/linux/iio/timer/stm32-lptim-trigger.h}} header files |
* {{CodeSource | Linux kernel | include/linux/mfd/stm32-lptimer.h}} and {{CodeSource | Linux kernel | include/linux/iio/timer/stm32-lptim-trigger.h}} header files |
||