Difference between revisions of "Kmemleak"

[quality revision] [quality revision]
m
 

1 Article purpose[edit]

This article provides the basic information needed to start using the Linux kernel tool: kmemleak[1].

2 Introduction[edit]

The following table provides a brief description of the tool, as well as its availability depending on the software packages:

Yes: this tool is either present (ready to use or to be activated), or can be integrated and activated on the software package.

No: this tool is not present and cannot be integrated, or it is present but cannot be activated on the software package.

Tool STM32MPU Embedded Software distribution STM32MPU Embedded Software distribution for Android™
Name Category Purpose Starter Package Developer Package Distribution Package Starter Package Developer Package Distribution Package
kmemleak Monitoring tools kmemleak[1] provides a means to detect possible kernel memory leaks in a similar way to a tracing garbage collector, with the difference that the orphan objects are not freed, but only reported via /sys/kernel/debug/kmemleak. No Yes Yes No No Yes

3 Installing the trace and debug tool on your target board[edit]

In order to use kmemleak, the Linux kernel configuration must activate CONFIG_DEBUG_KMEMLEAK:

Symbol: DEBUG_KMEMLEAK
Location:
  Kernel Hacking --->
    Memory Debugging -->
      [*] Kernel memory leak detector

For ecosystem release ≥ v2.0.0 :

In this ecosystem release, this is possible to enable/disable automatic kmemleak scan at boot up.
This configuration is activated by default when DEBUG_KMEMLEAK configuration is set.

Symbol: DEBUG_KMEMLEAK_AUTO_SCAN
Location:
  Kernel Hacking --->
    Memory Debugging -->
      [*] Kernel memory leak detector
        Enable kmemleak auto scan thread on boot up

For ecosystem release ≤ v1.1.0 :

Since memory may be allocated or freed before kmemleak is initialised, an early log buffer is used to store these actions.
In this ecosystem release, the default buffer size is limited, and this is recommended to increase it.

Warning.png If kmemleak reports "early log buffer exceeded" and debugfs entry is not present, you can increase the log buffer size by changing the configuration value, for example to 5000
Symbol: DEBUG_KMEMLEAK_EARLY_LOG_SIZE [=400]
Location:
Range: [200 40000]
  Kernel Hacking --->
    Memory Debugging -->
      [*] Kernel memory leak detector
        (400) Maximum kmemleak early log entries

3.1 Using STM32MPU Embedded Software Distribution[edit]

3.1.1 Developer Package[edit]

To enable CONFIG_DEBUG_KMEMLEAK in the Linux kernel configuration, please refer to the Menuconfig or how to configure kernel article to find instructions for modification of the configuration and recompiling Linux kernel image in Developer Package context.

3.1.2 Distribution Package[edit]

To enable CONFIG_DEBUG_KMEMLEAK in the Linux kernel configuration, please refer to the Menuconfig or how to configure kernel article to find instructions for modifying the configuration and recompiling the Linux kernel image in the Distribution Package context.

3.2 Using STM32MPU Embedded Software Distribution for Android™[edit]

3.2.1 Distribution Package[edit]

To enable CONFIG_DEBUG_KMEMLEAK in the Linux kernel configuration, please refer to the How to customize kernel for Android article to find instructions for modification of the configuration and recompiling Linux kernel image in Distribution Package context.

4 Getting started[edit]

Android logo.png Below information is related to the Android™ distribution
Need to enable root access rights
  • Using ADB shell is ADB link available:
PC $> adb root
PC $> adb shell
Board $> ...
  • Using uart console shell:
Board $> su
Board $> ...

4.1 Reading kmemleak report[edit]

A kernel thread scans the memory every 10 minutes (by default) and prints the number of new unreferenced objects found. To display the details of all the possible memory leaks:

Board $> cat /sys/kernel/debug/kmemleak

Note: debugfs is mounted by default, otherwise you can mount it using the following command. Please refer to the Debugfs article.

Kmemleak result example: contains an extract of the memory content, and backtrace of function calls, to help you when debugging.

unreferenced object 0xed638800 (size 64):
  comm "swapper/0", pid 1, jiffies 4294937542 (age 197.490s)
  hex dump (first 32 bytes):
    01 00 00 00 77 f9 ff 7a cf 37 dd e3 01 00 00 00  ....w..z.7......
    00 92 63 ed 40 00 00 00 00 00 00 00 01 00 00 00  ..c.@...........
  backtrace:
    [<c048d130>] pinconf_generic_parse_dt_config+0x10c/0x13c
    [<c0490f88>] stm32_pctrl_dt_node_to_map+0x90/0x3f4
    [<c048ca58>] pinctrl_dt_to_map+0x130/0x35c
    [<c04895a0>] create_pinctrl+0x60/0x3b0
    [<c0489a08>] devm_pinctrl_get+0x38/0x68
    [<c0582a24>] pinctrl_bind_pins+0x48/0x280
    [<c055f7f8>] driver_probe_device+0xc0/0x470
    [<c055fca8>] __driver_attach+0x100/0x11c
    [<c055db08>] bus_for_each_dev+0x4c/0x9c
    [<c055ecc4>] bus_add_driver+0x1c0/0x264
    [<c0560910>] driver_register+0x78/0xf4
    [<c0101c48>] do_one_initcall+0x44/0x168
    [<c0f00e74>] kernel_init_freeable+0x1c0/0x24c
    [<c0a65ac4>] kernel_init+0x8/0x110
    [<c0108b50>] ret_from_fork+0x14/0x24
    [<ffffffff>] 0xffffffff

4.2 Trigerring an intermediate memory scan[edit]

Board $> echo scan > /sys/kernel/debug/kmemleak

4.3 Clearing the list of all current possible memory leaks[edit]

Board $> echo clear > /sys/kernel/debug/kmemleak

4.4 All kmemleak commands[edit]

Memory scanning parameters can be modified at run-time by writing to the /sys/kernel/debug/kmemleak file. The following parameters are supported:

off         - disable kmemleak (irreversible)
stack=on    - enable the task stacks scanning (default)
stack=off   - disable the tasks stacks scanning
scan=on     - start the automatic memory scanning thread (default)
scan=off    - stop the automatic memory scanning thread
scan=<secs> - set the automatic memory scanning period in seconds (default 600, 0 to stop the automatic scanning)
scan        - trigger a memory scan
clear       - clear list of current memory leak suspects, done by marking all current reported unreferenced objects in grey, or freeing all kmemleak objects if kmemleak is disabled.
dump=<addr> - dump information about the object found at <addr>

5 To go further[edit]

If enabled in the Linux kernel configuration, Kmemleak can also be disabled at boot time by passing kmemleak=off on the kernel command line.


Conversely, if CONFIG_DEBUG_KMEMLEAK_DEFAULT_OFF is enabled in the Linux kernel configuration, kmemleak is disabled by default.

Symbol: DEBUG_KMEMLEAK_DEFAULT_OFF
Location:
  Kernel Hacking --->
    Memory Debugging -->
      [*] Kernel memory leak detector
        [*] Default kmemleak to off

Passing kmemleak=on on the kernel command line enables the function.

6 References[edit]


  • Useful external links
Document link Document Type Description
Kernel Memory Leak Detector Standard Documentation from kernel.org


== Article purpose ==
This article provides the basic information needed to start using the Linux kernel tool: '''kmemleak'''<ref name=procodedotorg/>.

== Introduction ==
{{:Trace_and_debug_tools_assignment_table_template}}<onlyinclude>

 | [[Kmemleak|kmemleak]]
 | [[:Category:Monitoring tools|Monitoring tools]]
 | style="text-align:left;" | '''kmemleak'''<ref name=procodedotorg>http://www.procode.org/kmemleak/</ref> provides a means to detect possible kernel memory leaks in a similar way to a tracing garbage collector, with the difference that the orphan objects are not freed, but only reported via /sys/kernel/debug/kmemleak.
 | {{N}} || {{Y}} || {{Y}}
 | {{N}} || {{N}} || {{Y}}
 |-</onlyinclude>

 |}

== Installing the trace and debug tool on your target board =={{ReviewsComments|JPR w20.02: for next ecosystem release v2.x (K5.4), new config DEBUG_KMEMLEAK_AUTO_SCAN to be added}}
In order to use '''kmemleak''', the Linux kernel configuration must activate CONFIG_DEBUG_KMEMLEAK:
 Symbol: '''DEBUG_KMEMLEAKIn order to use '''kmemleak''', the Linux kernel configuration must activate CONFIG_DEBUG_KMEMLEAK:
 Symbol: '''DEBUG_KMEMLEAK'''
 Location:
   Kernel Hacking --->
     Memory Debugging -->
       {{highlight|[*] Kernel memory leak detector}}

'''For {{EcosystemRelease | revision=2.0.0 | range=and after}}''':

In this ecosystem release, this is possible to enable/disable automatic kmemleak scan at boot up.<br>

This configuration is activated by default when DEBUG_KMEMLEAK configuration is set.
 Symbol: '''DEBUG_KMEMLEAK_AUTO_SCAN'''
 Location:
   Kernel Hacking --->
     Memory Debugging -->{{highlight|[*] Kernel memory leak detector

         {{highlight|Enable kmemleak auto scan thread on boot up}}
<div class="mw-collapsible mw-collapsed">

'''For {{EcosystemRelease | revision=1.1.0 | range=and before}}''':<div class="mw-collapsible-content">


Since memory may be allocated or freed before kmemleak is initialised, an early log buffer is used to store these actions.<br>

In this ecosystem release, the default buffer size is limited, and this is recommended to increase it.
{{Warning|If kmemleak reports "''early log buffer exceeded''" and debugfs entry is not present, you can increase the log buffer size by changing the configuration value, for example to 5000
 Symbol: '''DEBUG_KMEMLEAK_EARLY_LOG_SIZE''' [&#61;400]
 Location:
 {{Green|Range: [200 40000]}}
   Kernel Hacking --->
     Memory Debugging -->
       [*] Kernel memory leak detector
         {{highlight|(400) Maximum kmemleak early log entries}}
}}</div></div>


=== Using STM32MPU Embedded Software Distribution ===
==== Developer Package ====
To enable '''CONFIG_DEBUG_KMEMLEAK''' in the Linux kernel configuration, please refer to the [[Menuconfig or how to configure kernel]] article to find instructions for modification of the configuration and recompiling Linux kernel image in Developer Package context.

==== Distribution Package ====
To enable '''CONFIG_DEBUG_KMEMLEAK''' in the Linux kernel configuration, please refer to the [[Menuconfig or how to configure kernel]] article to find instructions for modifying the configuration and recompiling the Linux kernel image in the Distribution Package context.

=== Using STM32MPU Embedded Software Distribution for Android&trade; ===
==== Distribution Package ====
To enable '''CONFIG_DEBUG_KMEMLEAK''' in the Linux kernel configuration, please refer to the [[How to customize kernel for Android]] article to find instructions for modification of the configuration and recompiling Linux kernel image in Distribution Package context.

== Getting started ==
{{Android | Need to enable root access rights
*Using ADB shell is ADB link available:
 {{PC$}} adb root
 {{PC$}} adb shell
 {{Board$}} ...
*Using uart console shell:
 {{Board$}} su
 {{Board$}} ...
}}
=== Reading kmemleak report ===
A kernel thread scans the memory every 10 minutes (by default) and prints the number of new unreferenced objects found. To display the details of all the possible memory leaks:
 {{Board$}} cat /sys/kernel/debug/kmemleak

''Note'': debugfs is mounted by default, otherwise you can mount it using the following command. Please refer to the [[Debugfs]] article.

Kmemleak result example: contains an extract of the memory content, and backtrace of function calls, to help you when debugging.
 unreferenced object 0xed638800 (size 64):
   comm "swapper/0", pid 1, jiffies 4294937542 (age 197.490s)
   hex dump (first 32 bytes):
     01 00 00 00 77 f9 ff 7a cf 37 dd e3 01 00 00 00  ....w..z.7......
     00 92 63 ed 40 00 00 00 00 00 00 00 01 00 00 00  ..c.@...........
   backtrace:
     [<c048d130>] pinconf_generic_parse_dt_config+0x10c/0x13c
     [<c0490f88>] stm32_pctrl_dt_node_to_map+0x90/0x3f4
     [<c048ca58>] pinctrl_dt_to_map+0x130/0x35c
     [<c04895a0>] create_pinctrl+0x60/0x3b0
     [<c0489a08>] devm_pinctrl_get+0x38/0x68
     [<c0582a24>] pinctrl_bind_pins+0x48/0x280
     [<c055f7f8>] driver_probe_device+0xc0/0x470
     [<c055fca8>] __driver_attach+0x100/0x11c
     [<c055db08>] bus_for_each_dev+0x4c/0x9c
     [<c055ecc4>] bus_add_driver+0x1c0/0x264
     [<c0560910>] driver_register+0x78/0xf4
     [<c0101c48>] do_one_initcall+0x44/0x168
     [<c0f00e74>] kernel_init_freeable+0x1c0/0x24c
     [<c0a65ac4>] kernel_init+0x8/0x110
     [<c0108b50>] ret_from_fork+0x14/0x24
     [<ffffffff>] 0xffffffff

=== Trigerring an intermediate memory scan ===
 {{Board$}} echo scan > /sys/kernel/debug/kmemleak

=== Clearing the list of all current possible memory leaks ===
 {{Board$}} echo clear > /sys/kernel/debug/kmemleak

=== All kmemleak commands ===
Memory scanning parameters can be modified at run-time by writing to the <code>/sys/kernel/debug/kmemleak</code> file. The following parameters are supported:
 '''off'''         - disable kmemleak (irreversible)
 '''stack=on'''    - enable the task stacks scanning (default)
 '''stack=off'''   - disable the tasks stacks scanning
 '''scan=on'''     - start the automatic memory scanning thread (default)
 '''scan=off'''    - stop the automatic memory scanning thread
 '''scan=<secs>''' - set the automatic memory scanning period in seconds (default 600, 0 to stop the automatic scanning)
 '''scan'''        - trigger a memory scan
 '''clear'''       - clear list of current memory leak suspects, done by marking all current reported unreferenced objects in grey, or freeing all kmemleak objects if kmemleak is disabled.
 '''dump=<addr>''' - dump information about the object found at <addr>


== To go further ==
If enabled in the Linux kernel configuration, Kmemleak can also be disabled at boot time by passing {{highlight|kmemleak{{=}}off}} on the kernel command line.

Conversely, if '''CONFIG_DEBUG_KMEMLEAK_DEFAULT_OFF''' is enabled in the Linux kernel configuration, kmemleak is disabled by default.
 Symbol: '''DEBUG_KMEMLEAK_DEFAULT_OFF'''
 Location:
   Kernel Hacking --->
     Memory Debugging -->
       [*] Kernel memory leak detector
         {{highlight|[*] Default kmemleak to off}}
Passing {{highlight|kmemleak{{=}}on}} on the kernel command line enables the function.

== References ==<references />


* Useful external links
{|
! scope=col | Document link
! scope=col | Document Type
! scope=col | Description
|-
| [https://www.kernel.org/doc/html/latest/{{DocSource | domain=Linux kernel | path=dev-tools/kmemleak.html | text=Kernel Memory Leak Detector]}}

| Standard
| Documentation from kernel.org
|}

{{ArticleBasedOnModel | Trace and debug tools article model }}
{{PublicationRequestId | 9880 | 07Dec'18 }}

[[Category:Linux monitoring tools]]
(One intermediate revision by one other user not shown)
Line 15: Line 15:
   
 
== Installing the trace and debug tool on your target board ==
 
== Installing the trace and debug tool on your target board ==
{{ReviewsComments|JPR w20.02: for next ecosystem release v2.x (K5.4), new config DEBUG_KMEMLEAK_AUTO_SCAN to be added}}
 
 
In order to use '''kmemleak''', the Linux kernel configuration must activate CONFIG_DEBUG_KMEMLEAK:
 
In order to use '''kmemleak''', the Linux kernel configuration must activate CONFIG_DEBUG_KMEMLEAK:
 
  Symbol: '''DEBUG_KMEMLEAK'''
 
  Symbol: '''DEBUG_KMEMLEAK'''
Line 22: Line 21:
 
     Memory Debugging -->
 
     Memory Debugging -->
 
       {{highlight|[*] Kernel memory leak detector}}
 
       {{highlight|[*] Kernel memory leak detector}}
  +
  +
'''For {{EcosystemRelease | revision=2.0.0 | range=and after}}''':
  +
  +
In this ecosystem release, this is possible to enable/disable automatic kmemleak scan at boot up.<br>
  +
This configuration is activated by default when DEBUG_KMEMLEAK configuration is set.
  +
Symbol: '''DEBUG_KMEMLEAK_AUTO_SCAN'''
  +
Location:
  +
  Kernel Hacking --->
  +
    Memory Debugging -->
  +
      [*] Kernel memory leak detector
  +
        {{highlight|Enable kmemleak auto scan thread on boot up}}
   
 
<div class="mw-collapsible mw-collapsed">
 
<div class="mw-collapsible mw-collapsed">
Line 132: Line 142:
 
! scope=col | Description
 
! scope=col | Description
 
|-
 
|-
| [https://www.kernel.org/doc/html/latest/dev-tools/kmemleak.html Kernel Memory Leak Detector]
+
| {{DocSource | domain=Linux kernel | path=dev-tools/kmemleak.html | text=Kernel Memory Leak Detector}}
 
| Standard
 
| Standard
 
| Documentation from kernel.org
 
| Documentation from kernel.org