Difference between revisions of "KeyGen release note"

[quality revision] [quality revision]
m
m (Remove comments)

Template:ArticleMainWriter Template:ReviewersList Template:ArticleApprovedVersion


The STM32MP Key Generator tool (KeyGen) generates three "key" files:

  • a public Key file.
  • a private Key file.
  • a Hash public key file.

More information can be found in the detailed release notes referenced later in this article.

KeyGen - Version 1.0.0[edit]

KeyGen for Linux® and Windows® host PC
Download

Version 1.0.0

Template:STdotcomInfo

Installing the KeyGen tool
  • To use STM32MP KeyGen Tool, the installation of STM32CubeProgrammer is needed.
  • The installation is then complete. To use this tool, follow the instruction given in KeyGen tool.
Detailed release note
  • Full details about the content of this tool release are available here.
  • For former releases, please go through the archives of the ecosystem release note.
<noinclude>

{{ArticleMainWriter|AymenA}}
{{ReviewersList|To be completed by LionelD}}
{{ArticleApprovedVersion | NathalieS | Jean-ChristopheT | No previous approved version | AnneJ - 28Jun'18 - 7993 | 29Jun'18}}

[[Category:Release notes]]
[[Category:KeyGen tool]]
{{UpdateNeededForNewRelease|
* Copy the current release (first chapter) in the "Archives" chapter
* Change the version of the tool
* Change the name of the archive file
* Change the download URLs
}}</noinclude>


The STM32MP Key Generator tool (KeyGen) generates three "key" files:
* a public Key file.
* a private Key file.
* a Hash public key file.
More information can be found in the detailed release notes referenced later in this article. 

==KeyGen - Version 1.0.0 ==

{| class="st_table"
|-
!colspan="3" | KeyGen for Linux<sup>&reg;</sup> and Windows<sup>&reg;</sup> host PC
|-
| '''Download''' 
|colspan="2" |
'''Version 1.0.0'''
{{InternalInfo|[https://codex.cro.st.com/file/download.php/5092/99293/SetupSTM32CubeProgrammer.zip SetupSTM32CubeProgrammer.zip]}}
{{STdotcomInfo|
* KeyGen is integrated in [[STM32CubeProgrammer]] package available [https://www.st.com/en/development-tools/stm32cubeprog.html here]}}
|-
| '''Installing the KeyGen tool''' 
|colspan="2" |
* To use STM32MP KeyGen Tool, the installation of [[STM32CubeProgrammer]] is needed.
* '''The installation is then complete'''. To use this tool, follow the instruction given in [[KeyGen tool]].
|-
| '''Detailed release note''' 
| colspan="2" | 
* Full details about the content of this tool release are available [https://www.st.com/en/development-tools/stm32cubeprog.html here].
* For former releases, please go through the [[STM32MP15 ecosystem release note#Archives| archives]] of the ecosystem release note.|}{{ReviewsComments| DHU W906.4: I can't see this file in the Windows installation of the STM32Cubeprogrammer, which is supposed to host the complete keygen resources <br> LDE W907.3: Maybe better to give Installation directory for CubeProgrammer as it is included in the same tool now and no pdf present in the package yet (Used 2.0.0-rc4)}}
|}
Line 43: Line 43:
 
* Full details about the content of this tool release are available [https://www.st.com/en/development-tools/stm32cubeprog.html here].
 
* Full details about the content of this tool release are available [https://www.st.com/en/development-tools/stm32cubeprog.html here].
 
* For former releases, please go through the [[STM32MP15 ecosystem release note#Archives| archives]] of the ecosystem release note.
 
* For former releases, please go through the [[STM32MP15 ecosystem release note#Archives| archives]] of the ecosystem release note.
{{ReviewsComments| DHU W906.4: I can't see this file in the Windows installation of the STM32Cubeprogrammer, which is supposed to host the complete keygen resources <br> LDE W907.3: Maybe better to give Installation directory for CubeProgrammer as it is included in the same tool now and no pdf present in the package yet (Used 2.0.0-rc4)}}
 
 
|}
 
|}

Attachments

Discussions