- Last edited one week ago ago
Install the SDK
1 Overview[edit]
This stage explains how to install the SDK.
The SDK for OpenSTLinux distribution provides a standalone cross-development toolchain and libraries tailored to the contents of the specific image flashed onto the board.
2 Host computer configuration[edit]
2.1 Install extra packages[edit]
Additional Ubuntu packages must be installed to perform basic development tasks, basic cross-compilation (via Developer Package) or more complex cross-compilation such as OpenEmbedded does (via Distribution Package):
- Packages required by OpenEmbedded/Yocto (details here):
sudo apt-get update sudo apt-get install gawk wget git diffstat unzip texinfo gcc build-essential chrpath socat cpio python3 python3-pip python3-pexpect xz-utils debianutils iputils-ping python3-git python3-jinja2 libegl1-mesa libsdl1.2-dev pylint3 xterm python3-subunit mesa-common-dev zstd liblz4-tool sudo apt-get install make xsltproc docbook-utils fop dblatex xmlto sudo apt-get install libmpc-dev libgmp-dev
- Packages needed for some "Developer Package" use cases:
sudo apt-get install build-essential libssl-dev
- Package for repo (used to download the "Distribution Package" source code):
Please follow the installation instructions described in repo.
For Ubuntu 20.04, first set python3 as default: sudo apt install python-is-python3
- Useful tools:
sudo apt-get install coreutils bsdmainutils sed curl bc lrzsz corkscrew cvs subversion mercurial nfs-common nfs-kernel-server libarchive-zip-perl dos2unix texi2html diffstat libxml2-utils
2.2 Additional configurations[edit]
Additional configurations have to be installed to support up to 16 partitions per MMC. By default, on Linux® systems, a maximum of 8 partitions are allowed on MMC. All Packages (Starter Package, ...) need more than 10 partitions for the storage device. In order to extend the number of partitions per device to 16, the following options must be added to modprobe:
echo 'options mmc_block perdev_minors=16' > /tmp/mmc_block.conf sudo mv /tmp/mmc_block.conf /etc/modprobe.d/mmc_block.conf
3 Download the SDK[edit]
The software package is provided AS IS, and by downloading it, you agree to be bound to the terms of the software license agreement (SLA). The detailed content licenses can be found here.
- Download the Developer Package SDK into the following directory: $HOME/STM32MPU_workspace/tmp
- Uncompress the tarball file to get the SDK installation script
cd $HOME/STM32MPU_workspace/tmp
tar xvf SDK-x86_64-stm32mp1-openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15.tar.xz
4 Run the SDK installation script[edit]
- Create your STM32MP1 Developer Package SDK directory on your host computer
mkdir -p $HOME/STM32MPU_workspace/STM32MP1-Ecosystem-v4.0.0/Developer-Package/SDK
- Change the permissions of the SDK installation script so that it is executable
chmod +x stm32mp1-openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/sdk/st-image-weston-openstlinux-weston-stm32mp1-x86_64-toolchain-4.0.1-openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15.sh
- Execute the SDK installation script
./stm32mp1-openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/sdk/st-image-weston-openstlinux-weston-stm32mp1-x86_64-toolchain-4.0.1-openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15.sh -d <working directory absolute path>/Developer-Package/SDK
- The following log is output when the installation is successful:
ST OpenSTLinux - Weston - (A Yocto Project Based Distro) SDK installer version 4.0.1-openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15 =================================================================================================================================== You are about to install the SDK to "/home/osboxes/STM32MPU_workspace/STM32MP1-Ecosystem-v4.0.0/Developer-Package/SDK". Proceed [Y/n]? Y Extracting SDK............................................................................................................................................................................................................................done Setting it up...done SDK has been successfully set up and is ready to be used. Each time you wish to use the SDK in a new shell session, you need to source the environment setup script e.g. $ . /home/osboxes/STM32MPU_workspace/STM32MP1-Ecosystem-v4.0.0/Developer-Package/SDK/environment-setup-cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi
5 Start the SDK up[edit]
cd $HOME/STM32MPU_workspace/STM32MP1-Ecosystem-v4.0.0/Developer-Package
source SDK/environment-setup-cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi
The following checks ensure that the environment is correctly set up:
- Check the target architecture
echo $ARCH arm
- Check the toolchain binary prefix for the target tools
echo $CROSS_COMPILE arm-ostl-linux-gnueabi-
- Check the C compiler version
$CC --version arm-ostl-linux-gnueabi-gcc (GCC) 11.2.0 Copyright (C) 2021 Free Software Foundation, Inc. This is free software; see the source for copying conditions. There is NO warranty; not even for MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.
- Check that the SDK version is the expected one (e.g.)
echo $OECORE_SDK_VERSION
4.0.1-openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15
If any of these commands fails or does not return the expected result, try to reinstall the SDK.