This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.1 Overview[edit source]
This stage explains how to install the System Workbench for STM32 IDE to develop on the Arm® Cortex®-M4 coprocessor of the STM32MP1.
2 Install System Workbench for STM32 IDE[edit source]
In order to support the STM32 MPU Family, ST provides STM32-CoPro-MPU plugin which completes System Workbench for STM32 from Ac6.
This plugin is delivered in SW4STM32 from version 2.8.0.
The easiest way to install System Workbench for STM32 IDE is to follow instructions on the System Workbench for STM32 web page.
Useful links:
- Installing System Workbench for STM32 with installer
- Downloading the System Workbench for STM32 installer