Approved version. Approved on: 08:59, 7 October 2019
You are viewing an old version of this page. Return to the latest version.
- Last edited 8 months ago ago
Install STM32CubeMP1 package
Revision as of 10:15, 20 February 2019 by Registered User
Template/file changes in this version are pending review.
The stable version was approved on 29 June 2023.
1 Overview[edit]
This stage explains how to install the STM32Cube MP1 Package.
2 Install STM32Cube MP1 package[edit]
- Download STM32CubeMP1 Package v1.0.0 to the following directory:
$HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v1.0.0/Developer-Package - Uncompress the archive file to get the STM32CubeMP1 Package
unzip en.stm32cubemp1_v1-0-0.zip
3 STM32Cube MP1 package structure[edit]
The STM32Cube MP1 Package is located in your $HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v1.0.0/Developer-Package directory and is named STM32Cube_FW_MP1_V1.0.0:
STM32Cube_FW_MP1_V1.0.0 ├── Drivers │ ├── BSP BSP drivers for the supported STM32MP1 boards │ │ └── [...] │ ├── CMSIS │ │ └── [...] │ └── STM32MP1xx_HAL_Driver HAL drivers for the supported STM32MP1 devices │ └── [...] ├── _htmresc │ └── [...] ├── License.md ├── Middlewares │ └── [...] ├── package.xml ├── Projects │ ├── STM32CubeProjectsList.html List of examples and applications for STM32CubeMP1 Package │ ├── STM32MP157C-DK2 Set of examples and applications → STM32MP15 Discovery kits │ │ └── [...] │ └── STM32MP157C-EV1 Set of examples and applications → STM32MP15 Evaluation boards │ └── [...] ├── Readme.md ├── Release_Notes.html Release note for STM32CubeMP1 Package └── Utilities └── [...]