Difference between revisions of "IP Linux command line"

[quality revision] [quality revision]
Template:ArticleMainWriter

Template:ArticleApprovedVersion

1 Article purpose[edit]

This article provides the basic information needed to start using the Linux kernel tool: ip [1].

2 Introduction[edit]

The following table provides a brief description of the tool, as well as its availability depending on the software packages:

Yes: this tool is either present (ready to use or to be activated), or can be integrated and activated on the software package.

No: this tool is not present and cannot be integrated, or it is present but cannot be activated on the software package.

Under construction.png Coming soon
Tool STM32MPU Embedded Software distribution STM32MPU Embedded Software distribution for Android™
Only supported for STM32MP15x lines More info.png
Warning white.png Warning
The STM32MPU distribution for Android™ is not available in the v4 ecosystem releases: refer to the IP Linux command line page for the v2 ecosystem releases (in archived wiki).
Name Category Purpose Starter Package Developer Package Distribution Package Starter Package Developer Package Distribution Package
ip Monitoring tools ip[1] shows / manipulates routing, devices, policy routing and tunnels of network interfaces.

ip replaces the deprecated command ifconfig

Yes Yes Yes Yes Yes Yes

3 Installing the trace and debug tool on your target board[edit]

3.1 Using the STM32MPU Embedded Software distribution[edit]

ip is installed by default (/sbin/ip) and is ready to be used with all STM32MPU software packages.

 which ip
/sbin/ip

It is integrated into the Weston image distribution by using the following meta-st package recipie to enable the iproute2 module: meta-st/meta-st-openstlinux/recipes-st/packagegroups/packagegroup-framework-tools.bb.

RDEPENDS_packagegroup-framework-tools-network-base = "\
   ethtool         \
   iproute2        \
   "

3.2 Using the STM32MPU Embedded Software distribution for Android™[edit]

Under construction.png Coming soon

ip is installed by default (/system/bin/ip) and is ready to be used with all STM32MPU software packages for Android™.

 which ip
/system/bin/ip

It is integrated in Android image distribution through Android base makefile: build/make/target/product/core_minimal.mk:

# Base modules (will move elsewhere, previously user tagged)
PRODUCT_PACKAGES += \
    BackupRestoreConfirmation \
    CompanionDeviceManager \
   ...
   ims-common \
   ip \
   ip-up-vpn \
   ...

4 Getting started[edit]

Android logo.png Below information is related to the Android™ distribution
Need to enable root access rights for any changes
  • Using ADB shell is ADB link available:
 adb root
 adb shell
 ...

  • Using uart console shell:
 su
 ...

  • To check network interfaces
 ip addr show
1: lo: <LOOPBACK,UP,LOWER_UP> mtu 65536 qdisc noqueue state UNKNOWN group default qlen 1000
    link/loopback 00:00:00:00:00:00 brd 00:00:00:00:00:00
    inet 127.0.0.1/8 scope host lo
       valid_lft forever preferred_lft forever
    inet6 ::1/128 scope host 
       valid_lft forever preferred_lft forever
2: can0: <NOARP,ECHO> mtu 16 qdisc noop state DOWN group default qlen 10
    link/can 
3: eth0: <BROADCAST,MULTICAST,UP,LOWER_UP> mtu 1500 qdisc mq state UP group default qlen 1000
    link/ether 00:80:e1:42:43:65 brd ff:ff:ff:ff:ff:ff
    inet 192.168.1.237/22 brd 192.168.3.255 scope global dynamic eth0
       valid_lft 172057sec preferred_lft 172057sec
    inet 192.168.0.4/32 scope global eth0
       valid_lft forever preferred_lft forever
    inet6 fe80::280:e1ff:fe42:4365/64 scope link 
       valid_lft forever preferred_lft forever
4: sit0@NONE: <NOARP> mtu 1480 qdisc noop state DOWN group default qlen 1000
    link/sit 0.0.0.0 brd 0.0.0.0
  • To assign an IP address to an interface
 ip addr add 192.168.1.53 dev eth0
  • To remove an IP adress
 ip addr del 192.168.1.53 dev eth0
  • To enable an interface
 ip link set eth0 up
  • To disable an interface
 ip link set eth0 down
  • To check a route table
 ip route show
default via 192.168.3.254 dev eth0 proto dhcp src 192.168.1.237 metric 1024 
192.168.0.0/22 dev eth0 proto kernel scope link src 192.168.1.237 
192.168.3.254 dev eth0 proto dhcp scope link src 192.168.1.237 metric 1024 
  • To add a static route
 ip route add 192.168.2.0/16 via 192.168.1.1 dev eth0
  • To remove a static route
 ip route del 192.168.2.0/16
  • To set the default gateway
 ip route add default via 192.168.1.1

5 To go further[edit]

Some usage examples are available for reference[2].

6 References[edit]


  • Useful external links
Document link Document Type Description
IP Command example Standard Documentation from tecmint
ifconfig vs ip Standard Documentation


<noinclude>

{{ArticleBasedOnModel | [[Trace and debug tools article model]]}}
{{ArticleMainWriter | Jean-PhilippeR}}

{{ ArticleApprovedVersion | Jean-PhilippeR | Jean-ChristopheT, AlexandreT | No previous approved version  | PhilipS - 22Nov'18 - 9716 | 23Nov'18 }}

[[Category:Linux monitoring tools]]</noinclude>

== Article purpose ==
This article provides the basic information needed to start using the Linux kernel tool: '''ip''' <ref name=ipmanpage/>.

== Introduction ==
{{:Trace_and_debug_tools_assignment_table_template}}<onlyinclude>

 | [[IP Linux command line|ip]]
 | [[:Category:Monitoring tools|Monitoring tools]]
 | style="text-align:left;" | '''ip'''<ref name=ipmanpage>https://linux.die.net/man/8/ip</ref> shows / manipulates routing, devices, policy routing and tunnels of network interfaces.<br>

{{highlight|'''ip''' replaces the deprecated command [[Ifconfig|ifconfig]]}}
 || {{Y}} || {{Y}} || {{Y}}
 | colspan="3" | {{UnderConstruction}}| {{Y}} || {{Y}} || {{Y}}|-</onlyinclude>

 |}

== Installing the trace and debug tool on your target board ==
=== Using the STM32MPU Embedded Software distribution ===
'''ip''' is installed by default (/sbin/ip) and is ready to be used with all STM32MPU software packages.
 {{Board$}} which ip
 /sbin/ip

It is integrated into the Weston image distribution by using the following meta-st package recipie to enable the iproute2 module: <code>''meta-st/meta-st-openstlinux/recipes-st/packagegroups/packagegroup-framework-tools.bb''</code>.
 RDEPENDS_packagegroup-framework-tools-network-base = "\
    ethtool         \
    {{green|'''iproute2'''}}        \
    "

=== Using the STM32MPU Embedded Software distribution for Android&trade; ==={{UnderConstruction}}

== Getting started ==
* '''ip''' is installed by default (/system/bin/ip) and is ready to be used with all STM32MPU software packages for Android&trade;.
 {{Board$}} which ip
 /system/bin/ip

It is integrated in Android image distribution through Android base makefile: <code>''build/make/target/product/core_minimal.mk''</code>:
 # Base modules (will move elsewhere, previously user tagged)
 PRODUCT_PACKAGES += \
     BackupRestoreConfirmation \
     CompanionDeviceManager \
    ...
    ims-common \
    {{green|'''ip \'''}}
    ip-up-vpn \
    ...

== Getting started ==
{{Android | Need to enable root access rights for any changes
*Using ADB shell is ADB link available:
 {{PC$}} adb root
 {{PC$}} adb shell
 {{Board$}} ...
*Using uart console shell:
 {{Board$}} su
 {{Board$}} ...
}}

* To check network interfaces
 {{Board$}} ip addr show
 1: lo: <LOOPBACK,UP,LOWER_UP> mtu 65536 qdisc noqueue state UNKNOWN group default qlen 1000
     link/loopback 00:00:00:00:00:00 brd 00:00:00:00:00:00
     inet 127.0.0.1/8 scope host lo
        valid_lft forever preferred_lft forever
     inet6 ::1/128 scope host 
        valid_lft forever preferred_lft forever
 2: can0: <NOARP,ECHO> mtu 16 qdisc noop state DOWN group default qlen 10
     link/can 
 3: eth0: <BROADCAST,MULTICAST,UP,LOWER_UP> mtu 1500 qdisc mq state UP group default qlen 1000
     link/ether 00:80:e1:42:43:65 brd ff:ff:ff:ff:ff:ff
     inet 192.168.1.237/22 brd 192.168.3.255 scope global dynamic eth0
        valid_lft 172057sec preferred_lft 172057sec
     inet 192.168.0.4/32 scope global eth0
        valid_lft forever preferred_lft forever
     inet6 fe80::280:e1ff:fe42:4365/64 scope link 
        valid_lft forever preferred_lft forever
 4: sit0@NONE: <NOARP> mtu 1480 qdisc noop state DOWN group default qlen 1000
     link/sit 0.0.0.0 brd 0.0.0.0

* To assign an IP address to an interface
 {{Board$}} ip addr add 192.168.1.53 dev eth0

* To remove an IP adress
 {{Board$}} ip addr del 192.168.1.53 dev eth0

* To enable an interface
 {{Board$}} ip link set eth0 up

* To disable an interface
 {{Board$}} ip link set eth0 down

* To check a route table
 {{Board$}} ip route show
 default via 192.168.3.254 dev eth0 proto dhcp src 192.168.1.237 metric 1024 
 192.168.0.0/22 dev eth0 proto kernel scope link src 192.168.1.237 
 192.168.3.254 dev eth0 proto dhcp scope link src 192.168.1.237 metric 1024 

* To add a static route
 {{Board$}} ip route add 192.168.2.0/16 via 192.168.1.1 dev eth0

* To remove a static route
 {{Board$}} ip route del 192.168.2.0/16

* To set the default gateway
 {{Board$}} ip route add default via 192.168.1.1

== To go further ==
Some usage examples are available for reference<ref>https://www.linuxtechi.com/ip-command-examples-for-linux-users/</ref>.

== References ==<references />


* Useful external links
{|
! scope=col | Document link
! scope=col | Document Type
! scope=col | Description
|-
| [http://www.tecmint.com/ip-command-examples IP Command example]
| Standard
| Documentation from tecmint
|-
| [https://tty1.net/blog/2010/ifconfig-ip-comparison_en.html '''ifconfig''' vs '''ip''']
| Standard
| Documentation
|}


{{ ArticleBasedOnModel | Trace and debug tools article model }}
{{ PublicationRequestId | 9716 | 22Nov'18 }}

[[Category:Linux monitoring tools]]
(One intermediate revision by the same user not shown)
Line 1: Line 1:
<noinclude>
 
{{ArticleBasedOnModel | [[Trace and debug tools article model]]}}
 
{{ArticleMainWriter | Jean-PhilippeR}}
 
 
{{ ArticleApprovedVersion | Jean-PhilippeR | Jean-ChristopheT, AlexandreT | No previous approved version  | PhilipS - 22Nov'18 - 9716 | 23Nov'18 }}
 
 
[[Category:Linux monitoring tools]]
 
</noinclude>
 
 
 
== Article purpose ==
 
== Article purpose ==
 
This article provides the basic information needed to start using the Linux kernel tool: '''ip''' <ref name=ipmanpage/>.
 
This article provides the basic information needed to start using the Linux kernel tool: '''ip''' <ref name=ipmanpage/>.
Line 19: Line 10:
 
{{highlight|'''ip''' replaces the deprecated command [[Ifconfig|ifconfig]]}}
 
{{highlight|'''ip''' replaces the deprecated command [[Ifconfig|ifconfig]]}}
 
  || {{Y}} || {{Y}} || {{Y}}
 
  || {{Y}} || {{Y}} || {{Y}}
  | colspan="3" | {{UnderConstruction}}
+
  || {{Y}} || {{Y}} || {{Y}}
 
  |-
 
  |-
 
</onlyinclude>
 
</onlyinclude>
Line 30: Line 21:
 
  /sbin/ip
 
  /sbin/ip
   
It is integrated into the Weston image distribution by using the following meta-st package recipie to enable the iproute2 module: ''meta-st/meta-st-openstlinux/recipes-st/packagegroups/packagegroup-framework-tools.bb''.
+
It is integrated into the Weston image distribution by using the following meta-st package recipie to enable the iproute2 module: <code>''meta-st/meta-st-openstlinux/recipes-st/packagegroups/packagegroup-framework-tools.bb''</code>.
 
  RDEPENDS_packagegroup-framework-tools-network-base = "\
 
  RDEPENDS_packagegroup-framework-tools-network-base = "\
 
     ethtool        \
 
     ethtool        \
Line 37: Line 28:
   
 
=== Using the STM32MPU Embedded Software distribution for Android&trade; ===
 
=== Using the STM32MPU Embedded Software distribution for Android&trade; ===
{{UnderConstruction}}
+
'''ip''' is installed by default (/system/bin/ip) and is ready to be used with all STM32MPU software packages for Android&trade;.
  +
{{Board$}} which ip
  +
/system/bin/ip
  +
 
  +
It is integrated in Android image distribution through Android base makefile: <code>''build/make/target/product/core_minimal.mk''</code>:
  +
# Base modules (will move elsewhere, previously user tagged)
  +
PRODUCT_PACKAGES += \
  +
    BackupRestoreConfirmation \
  +
    CompanionDeviceManager \
  +
    ...
  +
    ims-common \
  +
    {{green|'''ip \'''}}
  +
    ip-up-vpn \
  +
    ...
   
 
== Getting started ==
 
== Getting started ==
  +
{{Android | Need to enable root access rights for any changes
  +
*Using ADB shell is ADB link available:
  +
{{PC$}} adb root
  +
{{PC$}} adb shell
  +
{{Board$}} ...
  +
*Using uart console shell:
  +
{{Board$}} su
  +
{{Board$}} ...
  +
}}
  +
 
* To check network interfaces
 
* To check network interfaces
 
  {{Board$}} ip addr show
 
  {{Board$}} ip addr show
Line 109: Line 123:
 
| Documentation
 
| Documentation
 
|}
 
|}
  +
  +
{{ ArticleBasedOnModel | Trace and debug tools article model }}
  +
{{ PublicationRequestId | 9716 | 22Nov'18 }}
  +
  +
[[Category:Linux monitoring tools]]