Approved version. Approved on: 08:50, 11 October 2018
- Last edited 2 years ago ago
IIO libiio
Template:ArticleMainWriter Template:ReviewersList Template:ArticleApprovedVersion
Summary
Libiio is a complete library which offers tools and an interface to develop an application using IIO subsystem.
Contents
1 Article purpose[edit]
The purpose of this article is to:
- briefly introduce the libiio main features and API
- provide few examples, using libiio tools
2 Introduction[edit]
- Libiio is a user space library that provides an interface for user space applications. It is basically a wrapper that resides above the following interfaces:
- /sys/bus/iio/devices sysfs interface (for configuration/setting)
- /dev/iio/deviceX device interface (for data)
- Libiio also provides tools that can be used for testing
- Libiio design goals:
- Interface with the kernel, to access IIO[1] devices
- Provide proper data structures and functions to the user application
- Support for local and remote backends allowing applications to access the devices when running on a local or a remote machine
The full description of the IIO library is provided by the author of the library, see below references:
3 API description[edit]
The API description can be found here: https://analogdevicesinc.github.io/libiio
4 Tools[edit]
Libiio offers tools such as:
- iiod server daemon
- iio_info to dump attributes
root@stm32mp1:~# iio_info Library version: 0.8 (git tag: v0.8) IIO context created with local backend. Backend version: 0.8 (git tag: v0.8) Backend description string: Linux stm32mp1 4.14.0-00004-gafe4a31 #778 SMP PREEMPT Tue Aug 28 14:02:25 CEST 2018 armv7l IIO context has 3 devices: trigger1: tim6_trgo 0 channels found: 3 device-specific attributes found: attr 0: sampling_frequency value: 100 attr 1: master_mode value: reset attr 2: master_mode_available value: reset enable update compare_pulse OC1REF OC2REF OC3REF OC4REF iio:device0: 48003000.adc:adc@0 (buffer capable) 2 channels found: voltage0: (input, index: 0, format: le:U16/16>>0) 3 channel-specific attributes found: attr 0: raw value: 72 attr 1: offset value: 0 attr 2: scale value: 0.044250488 voltage1: (input, index: 1, format: le:U16/16>>0) 3 channel-specific attributes found: attr 0: raw value: 1746 attr 1: offset value: 0 attr 2: scale value: 0.044250488 ...
- iio_readdev[4] (to read or scan from a device)
STM32AP [rc=0]# iio_readdev -t trigger1 -s 8 -b 8 iio:device0 voltage0 voltage1 | hexdump 0000000 0068 055a 0058 0520 00b4 03df 0070 055f 0000010 0096 03d6 0089 038f 0077 05c8 0096 03b3
See also: How to use the IIO user space interface
5 Source code[edit]
Libiio can be downloaded on a public github[5]. It can be cloned using git command:
git clone https://github.com/analogdevicesinc/libiio.git
Tools source code can be found under libiio "tests" directory.
6 Installation on your target[edit]
Libiio and the tools it provides are embedded by default in OpenSTLinux distribution.
7 References[edit]
- ↑ IIO overview, IIO subsystem overview
- ↑ https://wiki.analog.com/resources/tools-software/linux-software/libiio, What is libiio
- ↑ https://wiki.analog.com/resources/tools-software/linux-software/libiio_internals, About libiio
- ↑ https://wiki.analog.com/resources/tools-software/linux-software/libiio/iio_readdev, iio_readdev
- ↑ https://github.com/analogdevicesinc/libiio, libiio download link