Approved version. Approved on: 08:50, 11 October 2018
You are viewing an old version of this page. Return to the latest version.
Version of 08:50, 11 October 2018 by Fgasni00
Difference between revisions of "IIO libiio"
[quality revision] | [quality revision] |
|
m
|
Template:ArticleMainWriter Template:ReviewersList Template:ArticleApprovedVersion
SummaryApplicable for | STM32MP13x lines, STM32MP15x lines |
Libiio is a complete library which offers tools and an interface to develop an application using IIO subsystem.
Contents
1 Article purpose[edit]
The purpose of this article is to:
- briefly introduce the libiio main features and API
- provide few examples, using libiio tools
2 Introduction[edit]
- Libiio is a user space library that provides an interface for user space applications. It is basically a wrapper that resides above the following interfaces:
- /sys/bus/iio/devices sysfs interface (for configuration/setting)
- /dev/iio/deviceX device interface (for data)
- Libiio also provides tools that can be used for testing
- Libiio design goals:
- Interface with the kernel, to access IIO[1] devices
- Provide proper data structures and functions to the user application
- Support for local and remote backends allowing applications to access the devices when running on a local or a remote machine
The full description of the IIO library is provided by the author of the library, see below references:
3 API description[edit]
The API description can be found here: https://analogdevicesinc.github.io/libiio
4 Tools[edit]
Libiio offers tools such as:
- iiod server daemon
- iio_info to dump attributes
root@stm32mp1:~# iio_info Library version: 0.8 (git tag: v0.8) IIO context created with local backend. Backend version: 0.8 (git tag: v0.8) Backend description string: Linux stm32mp1 4.14.0-00004-gafe4a31 #778 SMP PREEMPT Tue Aug 28 14:02:25 CEST 2018 armv7l IIO context has 3 devices: trigger1: tim6_trgo 0 channels found: 3 device-specific attributes found: attr 0: sampling_frequency value: 100 attr 1: master_mode value: reset attr 2: master_mode_available value: reset enable update compare_pulse OC1REF OC2REF OC3REF OC4REF iio:device0: 48003000.adc:adc@0 (buffer capable) 2 channels found: voltage0: (input, index: 0, format: le:U16/16>>0) 3 channel-specific attributes found: attr 0: raw value: 72 attr 1: offset value: 0 attr 2: scale value: 0.044250488 voltage1: (input, index: 1, format: le:U16/16>>0) 3 channel-specific attributes found: attr 0: raw value: 1746 attr 1: offset value: 0 attr 2: scale value: 0.044250488 ...
- iio_readdev[4] (to read or scan from a device)
STM32AP [rc=0]# iio_readdev -t trigger1 -s 8 -b 8 iio:device0 voltage0 voltage1 | hexdump 0000000 0068 055a 0058 0520 00b4 03df 0070 055f 0000010 0096 03d6 0089 038f 0077 05c8 0096 03b3
See also: How to use the IIO user space interface
5 Source code[edit]
Libiio can be downloaded on a public github[5]. It can be cloned using git command:
git clone https://github.com/analogdevicesinc/libiio.git
Tools source code can be found under libiio "tests" directory.
6 Installation on your target[edit]
Libiio and the tools it provides are embedded by default in OpenSTLinux distribution.
7 References[edit]
- ↑ IIO overview, IIO subsystem overview
- ↑ https://wiki.analog.com/resources/tools-software/linux-software/libiio, What is libiio
- ↑ https://wiki.analog.com/resources/tools-software/linux-software/libiio_internals, About libiio
- ↑ https://wiki.analog.com/resources/tools-software/linux-software/libiio/iio_readdev, iio_readdev
- ↑ https://github.com/analogdevicesinc/libiio, libiio download link
<noinclude> {{ArticleMainWriter|FabriceG}} {{ReviewersList|OlivierM, ArnaudP, ErwanLR}} {{ArticleApprovedVersion | FabriceG| ErwanLR | No previous approved version| BrunoB - 11Oct'18 - 9165 | 11Oct'18}} [[Category:IIO|1]]</noinclude> '''Summary''' <br> ''{{ApplicableFor |MPUs list=STM32MP13x, STM32MP15x |MPUs checklist=STM32MP13x,STM32MP15x }}</noinclude> ''Libiio'' is a complete library which offers tools and an interface to develop an application using [[IIO overview|IIO subsystem]]. == Article purpose == The purpose of this article is to: * briefly introduce the ''libiio'' main features and API * provide few examples, using ''libiio'' tools == Introduction == * ''Libiio'' is a [[IIO_overview#User_space_interface|user space]] library that provides an '''interface''' for user space applications. It is basically a wrapper that resides above the following interfaces: # '''/sys/bus/iio/devices''' sysfs interface (for configuration/setting) # '''/dev/iio/deviceX''' device interface (for data) * ''Libiio'' also provides '''tools''' that can be used for testing * ''Libiio'' design goals: # Interface with the kernel, to access IIO<ref name="IIO overview">[[IIO overview]], IIO subsystem overview</ref> devices # Provide proper data structures and functions to the user application # Support for local and remote backends allowing applications to access the devices when running on a local or a remote machine The full description of the IIO library is provided by the author of the library, see below references: * What is libiio<ref>[https://wiki.analog.com/resources/tools-software/linux-software/libiio https://wiki.analog.com/resources/tools-software/linux-software/libiio], What is libiio</ref>. * About libiio<ref>[https://wiki.analog.com/resources/tools-software/linux-software/libiio_internals https://wiki.analog.com/resources/tools-software/linux-software/libiio_internals], About libiio</ref>. == API description == The API description can be found here: https://analogdevicesinc.github.io/libiio == Tools == ''Libiio'' offers tools such as: * ''iiod'' server daemon * ''iio_info'' to dump attributes root@stm32mp1:~# iio_info Library version: 0.8 (git tag: v0.8) IIO context created with local backend. Backend version: 0.8 (git tag: v0.8) Backend description string: Linux stm32mp1 4.14.0-00004-gafe4a31 #778 SMP PREEMPT Tue Aug 28 14:02:25 CEST 2018 armv7l IIO context has 3 devices: {{highlight|trigger1}}: tim6_trgo 0 channels found: 3 device-specific attributes found: attr 0: sampling_frequency value: 100 attr 1: master_mode value: reset attr 2: master_mode_available value: reset enable update compare_pulse OC1REF OC2REF OC3REF OC4REF {{highlight|iio:device0}}: 48003000.adc:adc@0 (buffer capable) 2 channels found: {{highlight|voltage0}}: (input, index: 0, format: le:U16/16>>0) 3 channel-specific attributes found: attr 0: raw value: 72 attr 1: offset value: 0 attr 2: scale value: 0.044250488 {{highlight|voltage1}}: (input, index: 1, format: le:U16/16>>0) 3 channel-specific attributes found: attr 0: raw value: 1746 attr 1: offset value: 0 attr 2: scale value: 0.044250488 ... * ''iio_readdev''<ref>[https://wiki.analog.com/resources/tools-software/linux-software/libiio/iio_readdev https://wiki.analog.com/resources/tools-software/linux-software/libiio/iio_readdev], iio_readdev</ref> (to read or scan from a device) STM32AP [rc=0]# iio_readdev -t {{highlight|trigger1}} -s 8 -b 8 {{highlight|iio:device0}} {{highlight|voltage0 voltage1}} | hexdump 0000000 0068 055a 0058 0520 00b4 03df 0070 055f 0000010 0096 03d6 0089 038f 0077 05c8 0096 03b3 See also: [[How to use the IIO user space interface]] == Source code == ''Libiio'' can be downloaded on a public github<ref>[https://github.com/analogdevicesinc/libiio https://github.com/analogdevicesinc/libiio], libiio download link </ref>. It can be cloned using git command:<pre>git clone https://github.com/analogdevicesinc/libiio.git</pre> Tools source code can be found under libiio "[https://github.com/analogdevicesinc/libiio/tree/master/tests tests]" directory. == Installation on your target == ''Libiio'' and the tools it provides are embedded by default in [[OpenSTLinux distribution]]. ==References==<references /> <noinclude> [[Category:IIO|1]] {{PublicationRequestId | 9165 | 2018-10-18 | BrunoB}}</noinclude>
(2 intermediate revisions by 2 users not shown) | |||
Line 1: | Line 1: | ||
− | <noinclude> |
+ | <noinclude>{{ApplicableFor
|
− | {{ |
+ | |MPUs list=STM32MP13x, STM32MP15x
|
− | + | |MPUs checklist=STM32MP13x,STM32MP15x
|
|
− | + | }}</noinclude> |
|
− | |||
− | </noinclude |
||
− | |||
− | |||
''Libiio'' is a complete library which offers tools and an interface to develop an application using [[IIO overview|IIO subsystem]]. |
''Libiio'' is a complete library which offers tools and an interface to develop an application using [[IIO overview|IIO subsystem]]. |
||
Line 76: | Line 72: | ||
==References== |
==References== |
||
<references /> |
<references /> |
||
+ | |||
+ | <noinclude> |
||
+ | [[Category:IIO|1]] |
||
+ | {{PublicationRequestId | 9165 | 2018-10-18 | BrunoB}} |
||
+ | </noinclude> |
Retrieved from "https://wiki.st.com/stm32mpu/index.php?title=IIO_libiio&oldid=79496"