IIO Linux kernel tools

Applicable for STM32MP13x lines, STM32MP15x lines

Linux® kernel provides some user space tools that can be used for testing the IIO subsystem.

1 Article purpose[edit]

The purpose of this article is to:

  • briefly introduce the IIO user space tools that comes with the Linux® kernel
  • provide a few examples using these tools

2 Introduction[edit]

These tools use IIO sysfs and character device directly without libiio (See IIO user space interface for further details).

3 Tools[edit]

The Linux® kernel provides the following IIO user space tools:

  • lsiio: example application that provides a list of IIO devices and triggers.
root@stm32mp1:~# lsiio
Device 001: 48003000.adc:adc@100
Device 000: 48003000.adc:adc@0
Trigger 018: tim3_ch4
Trigger 007: tim1_ch3
...
root@stm32mp1:~# iio_event_monitor /dev/iio:device0 &
Event: time: 1529352199639112110, type: voltage, channel: 0, evtype: thresh, direction: either
Event: time: ...
  • iio_generic_buffer: example application that reads data from buffer.
  • iio_utils: set of routines built-in above IIO tools, typically used to access sysfs files.

4 Source code[edit]

The Linux® kernel IIO tools source code can be found under tools/iio[1] directory:

5 Installation on your target[edit]

The Linux® kernel IIO tools aren't embedded by default in OpenSTLinux distribution. They can be compiled independently and then installed on the target. See How to build Linux kernel user space tools.

6 References[edit]

  1. tools/iio , Linux® IIO tools source code