Difference between revisions of "I2C internal peripheral"

[quality revision] [quality revision]
m (Peripheral assignment)
m
Applicable for STM32MP13x lines, STM32MP15x lines

1 Article purpose[edit]

The purpose of this article is to:

  • briefly introduce the I2C peripheral and its main features
  • indicate the level of security supported by this hardware block
  • explain how each instance can be allocated to the runtime contexts and linked to the corresponding software components
  • explain, when necessary, how to configure the I2C peripheral.

2 Peripheral overview[edit]

The I2C bus interface serves as an interface between the microcontroller and the serial I2C bus.
It provides multi-master capability, and controls all I2C bus-specific sequencing, protocol, arbitration and timing.
The I2C controller allows to be a slave as well if need be.
It is also SMBus 2.0 compatible.
For more information about I2C please refer to this link: I2C wikipedia[1] or i2c-bus.org[2]
For more information about SMBus please refer to this link: SMBus wikipedia[3] or i2c-bus.org[4]

2.1 Features[edit]

Here are the main features:

  • Multi-master
  • Standard (100 KHz) and fast speed modes (400 KHz and Plus 1 MHz)
  • I2C 10-bit address
  • I2C slave capabilities (programmable I2C address)
  • DMA capabilities
  • SMBus 2.0 compatible
    • Standard bus protocol (quick command; byte, word, block read/write)
    • Host notification
    • Alert

Refer to the STM32MP13 reference manuals or STM32MP15 reference manuals for the complete list of features, and to the software components, introduced below, to see which features are implemented.

2.2 Security support[edit]

2.2.1 On STM32MP13x lines Warning.png[edit]

There are five I2C instances:

  • I2C instances 1 and 2 are non-secure.
  • I2C instances 3, 4 and 5 can be secure (under ETZPC control).

2.2.2 On STM32MP15x lines More info.png[edit]

There are six I2C instances:

  • I2C instances 1, 2, 3 and 5 are non-secure.
  • I2C instances 4 and 6 can be secure (under ETZPC control).

3 Peripheral usage and associated software[edit]

3.1 Boot time[edit]

The I2C peripheral is usually not used at boot time. But it may be used by the SSBL and/or FSBL (see Boot chain overview), for example, to configure a PMIC (see PMIC hardware components), or to access data stored in an external EEPROM.

3.2 Runtime[edit]

3.2.1 Overview[edit]

Secure instances can be allocated to:

  • the Arm® Cortex®-A7 secure core to be controlled in OP-TEE by the OP-TEE I2C driver

All I2C instances can be allocated to:

  • the Arm® Cortex®-A7 non-secure core to be controlled in U-Boot or Linux® by the I2C framework

On STM32MP15x lines More info.png, all but I2C4&6 instances can be allocated to:

Chapter Peripheral assignment describes which peripheral instance can be assigned to which context.

3.2.2 Software frameworks[edit]

3.2.2.1 On STM32MP13x lines Warning.png[edit]
Domain Peripheral Software components Comment
OP-TEE Linux
Low speed interface I2C OP-TEE I2C driver I2C Engine framework
3.2.2.2 On STM32MP15x lines More info.png[edit]

Internal peripherals software table template

| Low speed interface
| I2C
| OP-TEE I2C driver
|  I2C Engine framework
| STM32Cube I2C driver
|
|-
|}

3.2.3 Peripheral configuration[edit]

The configuration is applied by the firmware running in the context to which the peripheral is assigned. The configuration can be done alone via the STM32CubeMX tool for all internal peripherals, and then manually completed (particularly for external peripherals), according to the information given in the corresponding software framework article.

For Linux® kernel configuration, please refer to I2C configuration.

Please refer to I2C device tree configuration for detailed information on how to configure I2C peripherals.

3.2.4 Peripheral assignment[edit]

3.2.4.1 On STM32MP13x lines Warning.png[edit]

Click on the right to expand the legend...

STM32MP13IPsOverview.png

Check boxes illustrate the possible peripheral allocations supported by STM32 MPU Embedded Software:

  • means that the peripheral can be assigned () to the given runtime context.
  • means that the peripheral can be assigned to the given runtime context, but this configuration is not supported in STM32 MPU Embedded Software distribution.
  • is used for system peripherals that cannot be unchecked because they are statically connected in the device.

Refer to How to assign an internal peripheral to a runtime context for more information on how to assign peripherals manually or via STM32CubeMX.
The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possiblities might be described in STM32MP13 reference manuals.

Domain Peripheral Runtime allocation Comment
Instance Cortex-A7
secure
(OP-TEE)
Cortex-A7
non-secure
(Linux)
Low speed interface I2C I2C1
I2C2
I2C3 Assignment (single choice)
I2C4 Assignment (single choice)
I2C5 Assignment (single choice)
3.2.4.2 On STM32MP15x lines More info.png[edit]

Internal peripherals assignment table template

| rowspan="6" | Low speed interface
| rowspan="6" | I2C
| I2C1
| 
| 
| 
| Assignment (single choice)
|-
| I2C2
| 
| 
| 
| Assignment (single choice)
|-
| I2C3
| 
| 
| 
| Assignment (single choice)
|-
| I2C4
|  
| 
|
| Assignment (single choice). 
Used for PMIC control on ST boards. |- | I2C5 | | | | Assignment (single choice) |- | I2C6 | | | | Assignment (single choice) |-

|}

4 References[edit]


== <noinclude>{{ApplicableFor
|MPUs list=STM32MP13x, STM32MP15x
|MPUs checklist=STM32MP13x,STM32MP15x
}}</noinclude>

== Article purpose ==
The purpose of this article is to:
* briefly introduce the I2C peripheral and its main features
* indicate the level of security supported by this hardware block
* explain how each instance can be allocated to the runtime contexts and linked to the corresponding software components
* explain, when necessary, how to configure the I2C peripheral.

==Peripheral overview==
The I2C bus interface serves as an interface between the microcontroller and the serial I2C bus.<br>

It provides multi-master capability, and controls all I2C bus-specific sequencing, protocol, arbitration and timing.<br>

The I2C controller allows to be a slave as well if need be.<br>

It is also SMBus 2.0 compatible.<br />

For more information about I2C please refer to this link: '''I2C wikipedia'''<ref name="I2C">http://en.wikipedia.org/wiki/I2C</ref> or '''i2c-bus.org'''<ref name="I2C specification">https://www.i2c-bus.org/specification/</ref><br>

For more information about SMBus please refer to this link: '''SMBus wikipedia'''<ref name="Wiki SMBus">https://en.wikipedia.org/wiki/System_Management_Bus</ref> or '''i2c-bus.org'''<ref name="SMBus">https://www.i2c-bus.org/smbus/</ref>


===Features===
Here are the main features:
* Multi-master
* Standard (100 KHz) and fast speed modes (400 KHz and Plus 1 MHz)
* I2C 10-bit address
* I2C slave capabilities (programmable I2C address)
* DMA capabilities
* SMBus 2.0 compatible
** Standard bus protocol (quick command; byte, word, block read/write)
** Host notification
** Alert

Refer to the [[STM32MP13 resources#Reference manuals|STM32MP13 reference manuals]] or [[STM32MP15 resources#Reference manuals|STM32MP15 reference manuals]] for the complete list of features, and to the software components, introduced below, to see which features are implemented.

===Security support===
==== On {{MicroprocessorDevice | device=13}} ====
There are five I2C instances:
*I2C instances 1 and 2 are '''non-secure'''.
*I2C instances 3, 4 and 5 can be '''secure''' (under [[ETZPC_internal_peripheral|ETZPC]] control).
==== On {{MicroprocessorDevice | device=15}} ====
There are six I2C instances:
*I2C instances 1, 2, 3 and 5 are '''non-secure'''.
*I2C instances 4 and 6 can be '''secure''' (under [[ETZPC_internal_peripheral|ETZPC]] control).

==Peripheral usage and associated software==
===Boot time===
The I2C peripheral is usually not used at boot time. But it may be used by the SSBL and/or FSBL (see [[Boot chain overview]]), for example, to configure a PMIC (see [[PMIC hardware components]]), or to access data stored in an external EEPROM.

===Runtime===
====Overview====
Secure instances can be allocated to:
* the Arm<sup>&reg;</sup> Cortex<sup>&reg;</sup>-A7 secure core to be controlled in OP-TEE by the [[OP-TEE_overview|OP-TEE I2C driver]]
All I2C instances can be allocated to:
* the Arm<sup>&reg;</sup> Cortex<sup>&reg;</sup>-A7 non-secure core to be controlled in U-Boot or Linux<sup>&reg;</sup> by the [[I2C overview|I2C framework]]
On {{MicroprocessorDevice | device=15}}, all but I2C4&6 instances can be allocated to:
* the Arm<sup>&reg;</sup> Cortex<sup>&reg;</sup>-M4 to be controlled in STM32Cube MPU Package by [[STM32CubeMP1 architecture|STM32Cube I2C driver]]

Chapter [[#Peripheral assignment|Peripheral assignment]] describes which peripheral instance can be assigned to which context.

====Software frameworks====
===== On {{MicroprocessorDevice | device=13}} =====
{{:STM32MP13 internal peripherals software table template}}
 | Low speed interface
 | [[I2C internal peripheral|I2C]]
 | [[OP-TEE_overview|OP-TEE I2C driver]]
 | [[I2C overview| I2C Engine framework]]
 |
 |-
 |}
===== On {{MicroprocessorDevice | device=15}} =====
{{:Internal_peripherals_software_table_template}}
 | Low speed interface
 | [[I2C internal peripheral|I2C]]
 | [[OP-TEE_overview|OP-TEE I2C driver]]
 | [[I2C overview| I2C Engine framework]]
 | [[STM32CubeMP1 architecture|STM32Cube I2C driver]]
 |
 |-
 |}

====Peripheral configuration====
The configuration is applied by the firmware running in the context to which the peripheral is assigned. The configuration can be done alone via the [[STM32CubeMX]] tool for all internal peripherals, and then manually completed (particularly for external peripherals), according to the information given in the corresponding software framework article.

For Linux<sup>&reg;</sup> kernel configuration, please refer to [[I2C overview#Configuration|I2C configuration]].

Please refer to [[I2C device tree configuration]] for detailed information on how to configure I2C peripherals.

====Peripheral assignment====
===== On {{MicroprocessorDevice | device=13}} =====
{{:STM32MP13_internal_peripherals_assignment_table_template}}<section begin=stm32mp13 />

 | rowspan="5" | Low speed interface
 | rowspan="5" | [[I2C internal peripheral|I2C]]
 | I2C1
 | 
 | <span title="assignable peripheral" style="font-size:21px"></span>

 |
 |-
 | I2C2
 | 
 | <span title="assignable peripheral" style="font-size:21px"></span>

 | 
 |-
 | I2C3
 | <span title="assignable peripheral" style="font-size:21px"></span>

 | <span title="assignable peripheral" style="font-size:21px"></span>

 | Assignment (single choice)
 |-
 | I2C4
 | <span title="assignable peripheral" style="font-size:21px"></span>

 | <span title="assignable peripheral" style="font-size:21px"></span>

 | Assignment (single choice)
 |-
 | I2C5
 | <span title="assignable peripheral" style="font-size:21px"></span>

 | <span title="assignable peripheral" style="font-size:21px"></span>

 | Assignment (single choice)
 |-<section end=stm32mp13 />

 |}
===== On {{MicroprocessorDevice | device=15}} =====
{{:Internal_peripherals_assignment_table_template}}<section begin=stm32mp15 />

 | rowspan="6" | Low speed interface
 | rowspan="6" | [[I2C internal peripheral|I2C]]
 | I2C1
 | 
 | <span title="assignable peripheral" style="font-size:21px"></span>

 | <span title="assignable peripheral" style="font-size:21px"></span>

 | Assignment (single choice)
 |-
 | I2C2
 | 
 | <span title="assignable peripheral" style="font-size:21px"></span>

 | <span title="assignable peripheral" style="font-size:21px"></span>

 | Assignment (single choice)
 |-
 | I2C3
 | 
 | <span title="assignable peripheral" style="font-size:21px"></span>

 | <span title="assignable peripheral" style="font-size:21px"></span>

 | Assignment (single choice)
 |-
 | I2C4
 | <span title="assignable peripheral" style="font-size:21px"></span> 

 | <span title="assignable peripheral" style="font-size:21px"></span>

 |
 | Assignment (single choice). <br />Used for PMIC control on [[:Category:Getting_started_with_STM32MP1_boards|ST boards]].
 |-
 | I2C5
 | 
 | <span title="assignable peripheral" style="font-size:21px"></span>

 | <span title="assignable peripheral" style="font-size:21px"></span>

 | Assignment (single choice)
 |-
 | I2C6
 | <span title="assignable peripheral" style="font-size:21px"></span> 

 | <span title="assignable peripheral" style="font-size:21px"></span>

 |
 | Assignment (single choice)
 |-<section end=stm32mp15 />

 |}

==References==<references/>

<noinclude>

[[Category:Low speed interface peripherals]]
{{PublicationRequestId | 9111 | 2018-10-12 | AlainF}}
{{ArticleBasedOnModel | Internal peripheral article model}}</noinclude>
Line 1: Line 1:
  +
<noinclude>{{ApplicableFor
  +
|MPUs list=STM32MP13x, STM32MP15x
  +
|MPUs checklist=STM32MP13x,STM32MP15x
  +
}}</noinclude>
 
== Article purpose ==
 
== Article purpose ==
 
The purpose of this article is to:
 
The purpose of this article is to: